Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages

Structures and functions required by UDC.

Functions

void udi_hid_kbd_disable (void)
 
bool udi_hid_kbd_enable (void)
 
uint8_t udi_hid_kbd_getsetting (void)
 
bool udi_hid_kbd_setup (void)
 

Variables

UDC_DESC_STORAGE udi_api_t udi_api_hid_kbd
 Global structure which contains standard UDI API for UDC. More...
 
UDC_DESC_STORAGE udi_api_t udi_api_hid_kbd
 Global structure which contains standard UDI interface for UDC. More...
 

void udi_hid_kbd_disable ( void  )
uint8_t udi_hid_kbd_getsetting ( void  )

UDC_DESC_STORAGE udi_api_t udi_api_hid_kbd

Global structure which contains standard UDI API for UDC.

Global structure which contains standard UDI API for UDC.

UDC_DESC_STORAGE udi_api_t udi_api_hid_kbd
Initial value:
= {
.enable = (bool(*)(void))udi_hid_kbd_enable,
.disable = (void (*)(void))udi_hid_kbd_disable,
.setup = (bool(*)(void))udi_hid_kbd_setup,
.getsetting = (uint8_t(*)(void))udi_hid_kbd_getsetting,
.sof_notify = NULL,
}
uint8_t udi_hid_kbd_getsetting(void)
Definition: udi_hid_kbd.c:216
bool udi_hid_kbd_setup(void)
Definition: udi_hid_kbd.c:207
void udi_hid_kbd_disable(void)
Definition: udi_hid_kbd.c:201
bool udi_hid_kbd_enable(void)
Definition: udi_hid_kbd.c:189
unsigned char bool
Boolean.
Definition: compiler.h:160

Global structure which contains standard UDI interface for UDC.

Global structure which contains standard UDI API for UDC.