Microchip® Advanced Software Framework

ui.c File Reference

User Interface.

Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include "ui.h"

Macros

#define MOUSE_MOVE_RANGE   (3*4)
 

Functions

 ISR (ui_wakeup_isr, AVR32_GPIO_IRQ_GROUP, 0)
 
void ui_init (void)
 Initializes the user interface. More...
 
void ui_powerdown (void)
 Enters the user interface in power down mode. More...
 
void ui_process (uint16_t framenumber)
 This process is called each 1ms It is called only if the USB interface is enabled. More...
 
void ui_wakeup (void)
 Exits the user interface of power down mode. More...
 
void ui_wakeup_disable (void)
 Disables the asynchronous interrupts of the user interface. More...
 
void ui_wakeup_enable (void)
 Enables the asynchronous interrupts of the user interface. More...
 

Variables

static eic_options_t eic_options
 Structure holding the configuration parameters of the EIC low level driver. More...
 

#define MOUSE_MOVE_RANGE   (3*4)

Referenced by ui_process().

ISR ( ui_wakeup_isr  ,
AVR32_GPIO_IRQ_GROUP  ,
 
)
void ui_init ( void  )
void ui_powerdown ( void  )

Enters the user interface in power down mode.

References LED0, LED1, and LED_Off().

Referenced by main(), and main_suspend_action().

void ui_wakeup ( void  )

Exits the user interface of power down mode.

References LED0, and LED_On().

Referenced by main_resume_action().

void ui_wakeup_disable ( void  )

Disables the asynchronous interrupts of the user interface.

References eic_disable_line(), EXT_INT6, EXT_INT7, gpio_disable_pin_interrupt(), GPIO_PUSH_BUTTON_0, and GPIO_PUSH_BUTTON_1.

Referenced by main_remotewakeup_disable().

void ui_wakeup_enable ( void  )

eic_options_t eic_options
static
Initial value:
= {
.eic_edge = 0,
.eic_level = EIC_LEVEL_LOW_LEVEL,
.eic_filter = EIC_FILTER_ENABLED,
.eic_async = EIC_ASYNCH_MODE
}
#define EIC_ASYNCH_MODE
Definition: eic.h:115
#define EIC_FILTER_ENABLED
Definition: eic.h:107
#define EIC_LEVEL_LOW_LEVEL
Definition: eic.h:100
#define EIC_MODE_LEVEL_TRIGGERED
Definition: eic.h:87

Structure holding the configuration parameters of the EIC low level driver.