Common User Interface for HID Mouse application.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
void ui_init | ( | void | ) |
Initializes the user interface.
References acc_init(), cpu_irq_restore(), cpu_irq_save(), GPIO_PUSH_BUTTON_0, irq_register_handler, LED0, LED1, LED_Off(), LED_On(), SYSCLK_ADC, and sysclk_enable_pba_module().
Referenced by main().
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
References LED0, LED1, and LED_Off().
Referenced by main(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References acc_update(), gpio_get_pin_value(), GPIO_PUSH_BUTTON_0, GPIO_PUSH_BUTTON_1, HID_MOUSE_BTN_DOWN, HID_MOUSE_BTN_UP, is_acc_abs_angle_x(), is_acc_abs_angle_y(), is_joystick_down(), is_joystick_pressed(), is_joystick_up(), LED1, LED_Off(), LED_On(), MOUSE_MOVE_RANGE, udi_hid_mouse_btnleft(), udi_hid_mouse_btnmiddle(), udi_hid_mouse_btnright(), udi_hid_mouse_moveScroll(), udi_hid_mouse_moveX(), and udi_hid_mouse_moveY().
Referenced by main(), and main_sof_action().
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
References LED0, and LED_On().
Referenced by main_resume_action().
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
References eic_disable_line(), EXT_INT6, EXT_INT7, gpio_disable_pin_interrupt(), GPIO_PUSH_BUTTON_0, and GPIO_PUSH_BUTTON_1.
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
References eic_enable_line(), eic_init(), eic_options_t::eic_line, EXT_INT6, EXT_INT7, gpio_enable_module_pin(), gpio_enable_pin_interrupt(), gpio_enable_pin_pull_up(), GPIO_PIN_CHANGE, GPIO_PUSH_BUTTON_0, and GPIO_PUSH_BUTTON_1.
Referenced by main_remotewakeup_enable().