USBC host driver Compliance with common driver UHD.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <string.h>
#include <stdlib.h>
#include "conf_usb_host.h"
#include "sysclk.h"
#include "uhd.h"
#include "usbc_otg.h"
#include "usbc_host.h"
#include "sleepmgr.h"
Data Structures | |
struct | uhd_ctrl_request_t |
Structure to store the high level setup request. More... | |
struct | uhd_pipe_job_t |
Structure definition to store registered jobs on a pipe. More... | |
Macros | |
#define | dbg_print(...) |
#define | dbgp_ctrl(...) |
#define | dbgp_ep(...) |
#define | UHD_BULK_INTERVAL_MIN 1 |
#define | UHD_USB_INT_FUN USBC_Handler |
#define | UHD_USB_INT_LEVEL 5 |
Functions | |
ISR (UHD_USB_INT_FUN) | |
Function called by USBC interrupt handler to manage USB interrupts. More... | |
void | otg_dual_disable (void) |
Uninitialize the dual role This function is implemented in usbc_host.c file. More... | |
bool | otg_dual_enable (void) |
Initialize the dual role This function is implemented in usbc_host.c file. More... | |
void | udc_start (void) |
Start the USB Device stack. More... | |
void | udc_stop (void) |
Stop the USB Device stack. More... | |
void | udd_interrupt (void) |
static void | uhd_ctrl_interrupt (void) |
Manages the events related to control endpoint. More... | |
static void | uhd_ctrl_phase_data_in (void) |
Manages the DATA IN phase on control endpoint. More... | |
static void | uhd_ctrl_phase_data_in_start (void) |
Starts the DATA IN phase on control endpoint. More... | |
static void | uhd_ctrl_phase_data_out (void) |
Manages the DATA OUT phase on control endpoint. More... | |
static void | uhd_ctrl_phase_setup (void) |
Sends a USB setup packet to start a control request sequence. More... | |
static void | uhd_ctrl_phase_zlp_in (void) |
Starts the ZLP IN phase on control endpoint. More... | |
static void | uhd_ctrl_phase_zlp_out (void) |
Starts the ZLP OUT phase on control endpoint. More... | |
static void | uhd_ctrl_request_end (uhd_trans_status_t status) |
Call the callback linked to control request and start the next request from the queue. More... | |
void | uhd_disable (bool b_id_stop) |
Disables the USB host mode. More... | |
void | uhd_enable (void) |
Enables the USB host mode Start the ID pin management if the ID pin is available. More... | |
bool | uhd_ep0_alloc (usb_add_t add, uint8_t ep_size) |
Configures and enables a control endpoint 0. More... | |
void | uhd_ep_abort (usb_add_t add, usb_ep_t endp) |
Aborts an on-going transfer on an endpoint. More... | |
static void | uhd_ep_abort_pipe (uint8_t pipe, uhd_trans_status_t status) |
Aborts the on-going transfer on a pipe. More... | |
bool | uhd_ep_alloc (usb_add_t add, usb_ep_desc_t *ep_desc, uhd_speed_t speed) |
Configures and enables an endpoint. More... | |
void | uhd_ep_free (usb_add_t add, usb_ep_t endp) |
Disables an endpoint or all endpoint of a device. More... | |
bool | uhd_ep_run (usb_add_t add, usb_ep_t endp, bool b_shortpacket, uint8_t *buf, iram_size_t buf_size, uint16_t timeout, uhd_callback_trans_t callback) |
Allows to receive or send data on an endpoint. More... | |
uint16_t | uhd_get_frame_number (void) |
Returns the current Start Of Frame (SOF) number. More... | |
uint16_t | uhd_get_microframe_number (void) |
Returns the current micro start of frame number. More... | |
static uint8_t | uhd_get_pipe (usb_add_t add, usb_ep_t endp) |
Returns the pipe number matching a USB endpoint. More... | |
uhd_speed_t | uhd_get_speed (void) |
Returns the speed of connected device. More... | |
static void | uhd_interrupt (void) |
Function called by USBC interrupt to manage USB host interrupts. More... | |
bool | uhd_is_suspend (void) |
Test if the suspend state is enabled on the USB line. More... | |
static void | uhd_pipe_finish_job (uint8_t pipe, uhd_trans_status_t status) |
Call the callback linked to the end of pipe transfer. More... | |
static uhd_trans_status_t | uhd_pipe_get_error (uint8_t pipe) |
Translates the USBC pipe error to UHD error. More... | |
static void | uhd_pipe_interrupt (uint8_t pipe) |
Manages the following pipe interrupts: More... | |
static void | uhd_pipe_trans_complet (uint8_t pipe) |
Computes and starts the next transfer on a pipe. More... | |
void | uhd_resume (void) |
Enables the IDLE state on the USB line. More... | |
void | uhd_send_reset (uhd_callback_reset_t callback) |
Enables the Reset state on the USB line. More... | |
bool | uhd_setup_request (usb_add_t add, usb_setup_req_t *req, uint8_t *payload, uint16_t payload_size, uhd_callback_setup_run_t callback_run, uhd_callback_setup_end_t callback_end) |
Add a setup request in the control endpoint setup queue. More... | |
static void | uhd_sof_interrupt (void) |
Manages timeouts and actions based on SOF events. More... | |
void | uhd_suspend (void) |
Enables the suspend state on the USB line. More... | |
USB IO PADs handlers | |
static void | otg_id_handler (void) |
USB ID pin change handler. More... | |
static void | uhd_vbus_handler (void) |
USB VBus pin change handler. More... | |
static void | uhd_vberr_handler (void) |
USB VBus error pin change handler. More... | |
Variables | |
static volatile uhd_desc_table_t | uhd_g_pipe_table [UHD_PEP_NB] |
USB SRAM data containing pipe descriptor table The content of the USB SRAM can be : More... | |
static bool | otg_initialized = false |
State of USBC OTG initialization. More... | |
static uhd_callback_reset_t | uhd_reset_callback = NULL |
Store the callback to be call at the end of reset signal. More... | |
Management of bulk/interrupt/isochronous endpoints | |
The UHD manages the data transfer on endpoints:
| |
static uhd_pipe_job_t | uhd_pipe_job [UHD_PEP_NB-1] |
Array to register a job on bulk/interrupt/isochronous endpoint. More... | |
static uint8_t | uhd_suspend_start |
Variables to manage the suspend/resume sequence. More... | |
static uint8_t | uhd_resume_start |
static uint8_t | uhd_pipes_unfreeze |
static uint8_t | uhd_pipes_error |
Variable to manage error on pipes. More... | |
Power management | |
enum | uhd_usbc_state_enum { UHD_STATE_OFF = 0, UHD_STATE_WAIT_ID_HOST = 1, UHD_STATE_NO_VBUS = 2, UHD_STATE_DISCONNECT = 3, UHD_STATE_SUSPEND = 4, UHD_STATE_IDLE = 5 } |
States of USBC interface. More... | |
static void | uhd_sleep_mode (enum uhd_usbc_state_enum new_state) |
Manages the sleep mode following the USBC state. More... | |
Control endpoint low level management routine. | |
This function performs control endpoint management. It handles the SETUP/DATA/HANDSHAKE phases of a control transaction. | |
enum | uhd_ctrl_request_phase_t { UHD_CTRL_REQ_PHASE_SETUP = 0, UHD_CTRL_REQ_PHASE_DATA_OUT = 1, UHD_CTRL_REQ_PHASE_DATA_IN = 2, UHD_CTRL_REQ_PHASE_ZLP_IN = 3, UHD_CTRL_REQ_PHASE_ZLP_OUT = 4 } |
Bit definitions to store setup request state machine. More... | |
uint32_t | uhd_ctrl_buffer [64/4] |
Buffer to store the sent/received data on control endpoint. More... | |
static bool | uhd_b_zlp_out_delayed = false |
Flag to delay a ZLP OUT on control endpoint. More... | |
struct uhd_ctrl_request_t * | uhd_ctrl_request_first |
Entry points of setup request list. More... | |
struct uhd_ctrl_request_t * | uhd_ctrl_request_last |
volatile uint16_t | uhd_ctrl_request_timeout |
Remaining time for on-going setup request (No request on-going if equal 0) More... | |
uint16_t | uhd_ctrl_nb_trans |
Number of transfered byte on DATA phase of current setup request. More... | |
static bool | uhd_b_suspend_requested |
Flag to delay a suspend request after all on-going setup request. More... | |
uhd_ctrl_request_phase_t | uhd_ctrl_request_phase |
#define dbg_print | ( | ... | ) |
Referenced by uhd_interrupt(), and uhd_sof_interrupt().
#define dbgp_ctrl | ( | ... | ) |
Referenced by uhd_ctrl_interrupt(), uhd_ctrl_request_end(), and uhd_sof_interrupt().
#define dbgp_ep | ( | ... | ) |
Referenced by uhd_pipe_finish_job(), uhd_pipe_interrupt(), and uhd_sof_interrupt().
#define UHD_BULK_INTERVAL_MIN 1 |
Referenced by uhd_ep_alloc().
#define UHD_USB_INT_FUN USBC_Handler |
#define UHD_USB_INT_LEVEL 5 |
Referenced by otg_dual_enable(), and uhd_enable().
void udd_interrupt | ( | void | ) |
Referenced by ISR().