Human interface on EVK1100 :
- PWR led is on when power present
- Led 0 is on when USB OTG cable is plugged
- Led 1 is on when Vbus is present
- Led 2 is on when a device is connected
- Led 3 blinks when the device is enumerated and USB in idle mode
- Led 4 is on when the mouse left button is down
- Led 5 is on when the mouse right button is down
- Led 6 is on when the mouse move
- Led 7 is on when a bad Vbus level has been detected
- Switch PB0 allows to enter the device in suspend mode
- Switch PB1 allows to enter the device in suspend mode with remote wakeup feature authorized
- Only Push joystick button can be used to wakeup USB device in suspend mode
Note: On board the LED labels are incremented of one. E.g. Led0 in software corresponding at Led1 label on board.