#include "queue.h"
Macros | |
#define | semBINARY_SEMAPHORE_QUEUE_LENGTH ( ( uint8_t ) 1U ) |
#define | semGIVE_BLOCK_TIME ( ( TickType_t ) 0U ) |
#define | semSEMAPHORE_QUEUE_ITEM_LENGTH ( ( uint8_t ) 0U ) |
#define | uxSemaphoreGetCount(xSemaphore) uxQueueMessagesWaiting( ( QueueHandle_t ) ( xSemaphore ) ) |
semphr.h More... | |
#define | vSemaphoreDelete(xSemaphore) vQueueDelete( ( QueueHandle_t ) ( xSemaphore ) ) |
#define | xSemaphoreGetMutexHolder(xSemaphore) xQueueGetMutexHolder( ( xSemaphore ) ) |
semphr.h More... | |
#define | xSemaphoreGetMutexHolderFromISR(xSemaphore) xQueueGetMutexHolderFromISR( ( xSemaphore ) ) |
semphr.h More... | |
#define | xSemaphoreGive(xSemaphore) xQueueGenericSend( ( QueueHandle_t ) ( xSemaphore ), NULL, semGIVE_BLOCK_TIME, queueSEND_TO_BACK ) |
#define | xSemaphoreGiveFromISR(xSemaphore, pxHigherPriorityTaskWoken) xQueueGiveFromISR( ( QueueHandle_t ) ( xSemaphore ), ( pxHigherPriorityTaskWoken ) ) |
#define | xSemaphoreTake(xSemaphore, xBlockTime) xQueueSemaphoreTake( ( xSemaphore ), ( xBlockTime ) ) |
#define | xSemaphoreTakeFromISR(xSemaphore, pxHigherPriorityTaskWoken) xQueueReceiveFromISR( ( QueueHandle_t ) ( xSemaphore ), NULL, ( pxHigherPriorityTaskWoken ) ) |
semphr. More... | |
Typedefs | |
typedef QueueHandle_t | SemaphoreHandle_t |
#define semBINARY_SEMAPHORE_QUEUE_LENGTH ( ( uint8_t ) 1U ) |
#define semGIVE_BLOCK_TIME ( ( TickType_t ) 0U ) |
#define semSEMAPHORE_QUEUE_ITEM_LENGTH ( ( uint8_t ) 0U ) |
#define uxSemaphoreGetCount | ( | xSemaphore | ) | uxQueueMessagesWaiting( ( QueueHandle_t ) ( xSemaphore ) ) |
UBaseType_t uxSemaphoreGetCount( SemaphoreHandle_t xSemaphore );
If the semaphore is a counting semaphore then uxSemaphoreGetCount() returns its current count value. If the semaphore is a binary semaphore then uxSemaphoreGetCount() returns 1 if the semaphore is available, and 0 if the semaphore is not available.
#define vSemaphoreDelete | ( | xSemaphore | ) | vQueueDelete( ( QueueHandle_t ) ( xSemaphore ) ) |
#define xSemaphoreGetMutexHolder | ( | xSemaphore | ) | xQueueGetMutexHolder( ( xSemaphore ) ) |
TaskHandle_t xSemaphoreGetMutexHolder( SemaphoreHandle_t xMutex );
If xMutex is indeed a mutex type semaphore, return the current mutex holder. If xMutex is not a mutex type semaphore, or the mutex is available (not held by a task), return NULL.
Note: This is a good way of determining if the calling task is the mutex holder, but not a good way of determining the identity of the mutex holder as the holder may change between the function exiting and the returned value being tested.
#define xSemaphoreGetMutexHolderFromISR | ( | xSemaphore | ) | xQueueGetMutexHolderFromISR( ( xSemaphore ) ) |
TaskHandle_t xSemaphoreGetMutexHolderFromISR( SemaphoreHandle_t xMutex );
If xMutex is indeed a mutex type semaphore, return the current mutex holder. If xMutex is not a mutex type semaphore, or the mutex is available (not held by a task), return NULL.
#define xSemaphoreGive | ( | xSemaphore | ) | xQueueGenericSend( ( QueueHandle_t ) ( xSemaphore ), NULL, semGIVE_BLOCK_TIME, queueSEND_TO_BACK ) |
#define xSemaphoreGiveFromISR | ( | xSemaphore, | |
pxHigherPriorityTaskWoken | |||
) | xQueueGiveFromISR( ( QueueHandle_t ) ( xSemaphore ), ( pxHigherPriorityTaskWoken ) ) |
Referenced by main_msc_notify_trans().
#define xSemaphoreTake | ( | xSemaphore, | |
xBlockTime | |||
) | xQueueSemaphoreTake( ( xSemaphore ), ( xBlockTime ) ) |
Referenced by ctrl_access_lock(), and main_memories_trans_task().
#define xSemaphoreTakeFromISR | ( | xSemaphore, | |
pxHigherPriorityTaskWoken | |||
) | xQueueReceiveFromISR( ( QueueHandle_t ) ( xSemaphore ), NULL, ( pxHigherPriorityTaskWoken ) ) |
semphr.
h
xSemaphoreTakeFromISR( SemaphoreHandle_t xSemaphore, BaseType_t *pxHigherPriorityTaskWoken )
Macro to take a semaphore from an ISR. The semaphore must have previously been created with a call to xSemaphoreCreateBinary() or xSemaphoreCreateCounting().
Mutex type semaphores (those created using a call to xSemaphoreCreateMutex()) must not be used with this macro.
This macro can be used from an ISR, however taking a semaphore from an ISR is not a common operation. It is likely to only be useful when taking a counting semaphore when an interrupt is obtaining an object from a resource pool (when the semaphore count indicates the number of resources available).
xSemaphore | A handle to the semaphore being taken. This is the handle returned when the semaphore was created. |
pxHigherPriorityTaskWoken | xSemaphoreTakeFromISR() will set *pxHigherPriorityTaskWoken to pdTRUE if taking the semaphore caused a task to unblock, and the unblocked task has a priority higher than the currently running task. If xSemaphoreTakeFromISR() sets this value to pdTRUE then a context switch should be requested before the interrupt is exited. |
typedef QueueHandle_t SemaphoreHandle_t |