User Interface.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_loop_back_state (bool b_started) |
Notify the state of loopback It is called when a the loopback is started and stopped. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
Variables | |
static volatile bool | ui_b_loopback = true |
void ui_init | ( | void | ) |
void ui_loop_back_state | ( | bool | b_started | ) |
Notify the state of loopback It is called when a the loopback is started and stopped.
b_started | loopback started if true, else stopped |
References ui_b_loopback.
Referenced by main_setup_in_received(), main_setup_out_received(), main_vendor_bulk_in_received(), main_vendor_bulk_out_received(), main_vendor_int_in_received(), and main_vendor_int_out_received().
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
References LED_0_PIN, and LED_Off.
Referenced by main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References LED_0_PIN, LED_Off, LED_On, and ui_b_loopback.
Referenced by main_sof_action().
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
References LED_0_PIN, and LED_On.
Referenced by main_resume_action().
Referenced by ui_loop_back_state(), and ui_process().