License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Quick Start Guide for the System Clock Management | Service (SAMV71) |
Advanced use case - Peripheral Bus Clock | Management (SAMV71) |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick start guide for USB host vendor module (UHI vendor) | This is the quick start guide for the USB host vendor module (UHI vendor) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
conf_clock.h examples with USB support | Content of conf_clock.h for AT32UC3A0, AT32UC3A1, AT32UC3B devices (USBB): |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
"SAMV71-XLTRA - Operating frequencies" | This page lists several definition related to the board operating frequency |
"SAMV71-XLTRA - Board informations" | This page lists several definition related to the board description |
"SAMV71-XPRO - CAN" | This page lists definitions related to CAN0 and CAN1 |
Todo List | |