Functions | |
struct win_window * | wtk_check_box_as_child (struct wtk_check_box *check_box) |
This function returns a reference to the window that should be used when managing the widget, such as move, resize, destroy and reparenting. More... | |
struct wtk_check_box * | wtk_check_box_create (struct win_window *parent, struct win_area const *area, char const *caption, bool selected, win_command_t command_data) |
This function creates a new check box widget. More... | |
win_command_t | wtk_check_box_get_command (struct wtk_check_box *check_box) |
This function returns the window command of the specified check box, as set when the widget was created. More... | |
bool | wtk_check_box_is_selected (struct wtk_check_box const *check_box) |
This function returns true if the check box is selected. More... | |
void | wtk_check_box_set (struct wtk_check_box *check_box, bool selected) |
This function sets the value of the check box according to the "selected" parameter. More... | |
void | wtk_check_box_size_hint (struct win_point *size, const char *caption) |
Get minimum widget size. More... | |
void | wtk_check_box_toggle (struct wtk_check_box *check_box) |
This function toggles the value of a check box. More... | |
enum | wtk_check_box_state { WTK_CHECKBOX_NORMAL, WTK_CHECKBOX_PRESSED } |
Valid states for check box, relevant to pointer and keyboard operations. More... | |
static bool | wtk_check_box_handler (struct win_window *win, enum win_event_type type, void const *data) |
This function is the window event handler for check box widgets. More... | |
#define | WTK_CHECKBOX_BOX_SIZE 12 |
Size of checkbox square. More... | |
#define | WTK_CHECKBOX_BOX_X 0 |
Checkbox square X offset. More... | |
#define | WTK_CHECKBOX_BOX_Y 0 |
Checkbox square Y offset. More... | |
#define | WTK_CHECKBOX_CAPTION_X (WTK_CHECKBOX_BOX_SIZE + 4) |
Checkbox caption text X offset. More... | |
#define | WTK_CHECKBOX_CAPTION_Y 0 |
Checkbox caption text Y offset. More... | |
#define | WTK_CHECKBOX_BOX_COLOR GFX_COLOR_BLACK |
Checkbox square frame color. More... | |
#define | WTK_CHECKBOX_BACKGROUND_COLOR GFX_COLOR_WHITE |
Checkbox square background color. More... | |
#define | WTK_CHECKBOX_SELECT_COLOR GFX_COLOR_DK_RED |
Checkbox square select mark color. More... | |
#define | WTK_CHECKBOX_CAPTION_COLOR GFX_COLOR_BLACK |
Checkbox caption text color. More... | |
#define WTK_CHECKBOX_BACKGROUND_COLOR GFX_COLOR_WHITE |
Checkbox square background color.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_BOX_COLOR GFX_COLOR_BLACK |
Checkbox square frame color.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_BOX_SIZE 12 |
Size of checkbox square.
Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().
#define WTK_CHECKBOX_BOX_X 0 |
Checkbox square X offset.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_BOX_Y 0 |
Checkbox square Y offset.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_CAPTION_COLOR GFX_COLOR_BLACK |
Checkbox caption text color.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_CAPTION_X (WTK_CHECKBOX_BOX_SIZE + 4) |
Checkbox caption text X offset.
Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().
#define WTK_CHECKBOX_CAPTION_Y 0 |
Checkbox caption text Y offset.
Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().
#define WTK_CHECKBOX_SELECT_COLOR GFX_COLOR_DK_RED |
Checkbox square select mark color.
Referenced by wtk_check_box_handler().
enum wtk_check_box_state |
struct win_window* wtk_check_box_as_child | ( | struct wtk_check_box * | check_box | ) |
This function returns a reference to the window that should be used when managing the widget, such as move, resize, destroy and reparenting.
check_box | Check box widget to manage. |
References Assert, and wtk_check_box::container.
Referenced by app_widget_launch().
struct wtk_check_box* wtk_check_box_create | ( | struct win_window * | parent, |
struct win_area const * | area, | ||
char const * | caption, | ||
bool | selected, | ||
win_command_t | command | ||
) |
This function creates a new check box widget.
It allocates required memory and intializes necessary windows to create the widget. If there is not enough memory, the function returns NULL.
To destroy the widget and all its contents, and free its memory, call win_destroy() on the check box' child reference, given by wtk_check_box_as_child(), like this: "win_destroy(wtk_check_box_as_child(my_check_box_ptr));". Usually it will be destroyed automatically when it's parent is destroyed.
parent | Parent window, possibly wtk_frame_as_parent(my_frame_ptr). |
area | Area of the internal contents. |
caption | Pointer to caption string. Will be copied into widget. |
selected | Initial state of check box, true if checked/selected. |
command | Command to send to parent window. Must be non-zero to be enabled. |
References win_attributes::area, Assert, win_attributes::background, win_attributes::behavior, wtk_check_box::caption, wtk_check_box::command, wtk_check_box::container, win_attributes::custom, win_attributes::event_handler, membag_alloc(), membag_free(), wtk_check_box::selected, wtk_check_box::state, WIN_BEHAVIOR_REDRAW_PARENT, win_create(), wtk_check_box_handler(), WTK_CHECKBOX_NORMAL, and wtk_copy_string().
Referenced by app_widget_launch().
win_command_t wtk_check_box_get_command | ( | struct wtk_check_box * | check_box | ) |
This function returns the window command of the specified check box, as set when the widget was created.
check_box | Check box widget to manage. |
References Assert, and wtk_check_box::command.
|
static |
This function is the window event handler for check box widgets.
It handles all events sent to the windows composing the widget.
win | Window receiving the event. |
type | The event type. |
data | Custom data, depending on event type. |
References Assert, wtk_check_box::caption, wtk_check_box::command, wtk_check_box::container, win_command_event::data, GFX_COLOR_TRANSPARENT, gfx_draw_filled_rect, gfx_draw_rect, gfx_draw_string(), membag_free(), win_clip_region::origin, win_command_event::recipient, wtk_check_box::selected, win_command_event::sender, wtk_check_box::state, sysfont, WIN_EVENT_DESTROY, WIN_EVENT_DRAW, WIN_EVENT_POINTER, win_get_custom_data(), win_grab_pointer(), win_is_inside_window(), WIN_POINTER_PRESS, WIN_POINTER_RELEASE, win_queue_command_event(), win_redraw(), wtk_check_box_toggle(), WTK_CHECKBOX_BACKGROUND_COLOR, WTK_CHECKBOX_BOX_COLOR, WTK_CHECKBOX_BOX_SIZE, WTK_CHECKBOX_BOX_X, WTK_CHECKBOX_BOX_Y, WTK_CHECKBOX_CAPTION_COLOR, WTK_CHECKBOX_CAPTION_X, WTK_CHECKBOX_CAPTION_Y, WTK_CHECKBOX_NORMAL, WTK_CHECKBOX_PRESSED, WTK_CHECKBOX_SELECT_COLOR, win_point::x, and win_point::y.
Referenced by wtk_check_box_create().
bool wtk_check_box_is_selected | ( | struct wtk_check_box const * | check_box | ) |
This function returns true if the check box is selected.
References Assert, and wtk_check_box::selected.
void wtk_check_box_set | ( | struct wtk_check_box * | check_box, |
bool | selected | ||
) |
This function sets the value of the check box according to the "selected" parameter.
The graphics will be updated if the box is visible.
check_box | Check box to update. |
selected | Value to set for checkbox. True if check box is selected, false otherwise |
References Assert, wtk_check_box::container, wtk_check_box::selected, and win_redraw().
void wtk_check_box_size_hint | ( | struct win_point * | size, |
const char * | caption | ||
) |
Get minimum widget size.
This function returns the minimum size that is required for showing the full widget and the caption.
size | Suggested size for the widget |
caption | Pointer to caption string to use for widget. |
References Assert, gfx_get_string_bounding_box(), sysfont, WTK_CHECKBOX_BOX_SIZE, WTK_CHECKBOX_CAPTION_X, WTK_CHECKBOX_CAPTION_Y, win_point::x, and win_point::y.
Referenced by app_widget_launch().
void wtk_check_box_toggle | ( | struct wtk_check_box * | check_box | ) |
This function toggles the value of a check box.
If it is not selected, it will be set to a selected/checked state, and vice versa. The graphics will be updated if the box is visible.
check_box | Check box to toggle. |
References Assert, wtk_check_box::container, wtk_check_box::selected, and win_redraw().
Referenced by wtk_check_box_handler().