This example will create a simple touch-enabled GUI on the board display, using the Widget Toolkit library.
For boards using the mXT143E Xplained only:
For the UC3C-EK only:
The widget library API can be found here, while the graphics service API can be found here.
This example has been tested with the following kits:
On startup the example application will create a simple GUI on the display of the board, showing a slider, progress bar, check boxes, radio buttons and a standard button. Touching the display will manipulate each of these widgets.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.