Graphic Widget Toolkit library example 2 application.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | MAXTOUCH_TWI_ADDRESS 0x4a |
Address of the mXT143E on TWI bus. More... | |
Functions | |
int | main (void) |
main example code More... | |
static void | mxt_init (struct mxt_device *device) |
Set maXTouch configuration. More... | |
static bool | read_touch_event (struct mxt_device *device, struct win_pointer_event *win_touch_event) |
Convert touch events from the touchscreen into window pointer events. More... | |
static void | setup_gui_root_window (void) |
Configure the root GUI window. More... | |
static void | show_out_of_memory_error (void) |
Show an out of memory error on the display. More... | |
#define MAXTOUCH_TWI_ADDRESS 0x4a |
Address of the mXT143E on TWI bus.
Referenced by mxt_init().
int main | ( | void | ) |
main example code
The main function will draw all the graphic primitives from the graphic library on a line from left to right (incrementing x) and repeat this from bottom to top with varying colors (incrementing y). Below the figures it draws the Atmel logo centered on the screen.
References app_widget_launch(), board_init(), gfx_init, membag_init(), mxt_init(), read_touch_event(), setup_gui_root_window(), show_out_of_memory_error(), sysclk_init(), win_init(), win_process_events(), and win_queue_pointer_event().
|
static |
Set maXTouch configuration.
This function writes a set of predefined, optimal maXTouch configuration data to the mXT143E Xplained.
device | Pointer to mxt_device struct |
References Assert, delay_ms, MAXTOUCH_TWI_ADDRESS, MXT143E_XPLAINED_CHG, MXT_GEN_ACQUISITIONCONFIG_T8, MXT_GEN_COMMANDPROCESSOR_CALIBRATE, MXT_GEN_COMMANDPROCESSOR_RESET, MXT_GEN_COMMANDPROCESSOR_T6, MXT_GEN_POWERCONFIG_T7, mxt_get_object_address(), mxt_init_device(), MXT_PROCG_TOUCHSUPPRESSION_T48, MXT_RESET_TIME, MXT_TOUCH_MULTITOUCHSCREEN_T9, MXT_TWI_SPEED, mxt_write_config_object(), mxt_write_config_reg(), twi_options_t::speed, status, STATUS_OK, TWI_INTERFACE, twi_master_setup(), and UNUSED.
Referenced by main().
|
static |
Convert touch events from the touchscreen into window pointer events.
Reads touch events in from the touchscreen and converts them into a Window Manager pointer event, for enqueuing into the window event queue.
References win_pointer_event::buttons, gfx_get_height(), gfx_get_width(), win_pointer_event::is_relative, mxt_is_message_pending(), MXT_MOVE_EVENT, MXT_PRESS_EVENT, mxt_read_touch_event(), MXT_RELEASE_EVENT, win_pointer_event::pos, mxt_touch_event::status, STATUS_OK, win_pointer_event::type, WIN_POINTER_MOVE, WIN_POINTER_PRESS, WIN_POINTER_RELEASE, WIN_TOUCH_BUTTON, mxt_touch_event::x, win_point::x, mxt_touch_event::y, and win_point::y.
Referenced by main().
|
static |
Configure the root GUI window.
Configures the root window background to be a tiled version of the Atmel company logo, and sets it as being visible.
References atmel_logo_small, win_attributes::background, WIN_ATTR_BACKGROUND, win_get_attributes(), win_get_root(), win_root, win_set_attributes(), and win_show().
Referenced by main().
|
static |
Show an out of memory error on the display.
Shows a full screen error when called, signaling that the system ran out of memory when initializing a WTK application.
References GFX_COLOR_BLACK, GFX_COLOR_RED, GFX_COLOR_TRANSPARENT, gfx_draw_filled_rect, gfx_draw_string_aligned(), gfx_get_height(), gfx_get_width(), gfx_set_clipping(), sysfont, TEXT_ALIGN_CENTER, and TEXT_POS_CENTER.
Referenced by main().