Widget ToolKit training widget.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
Color scheme | |
#define | APP_BACKGROUND_COLOR GFX_COLOR(50, 50, 50) |
Background color for application. More... | |
Widget sizes and positions | |
#define | LABEL_POS_X 10 |
Label position on top of display. More... | |
#define | LABEL_POS_Y 10 |
Label position on top of display. More... | |
#define | SLIDER_POS_X 10 |
Slider position. More... | |
#define | SLIDER_POS_Y 60 |
Slider position. More... | |
#define | SLIDER_SIZE_X 80 |
Slider size on display. More... | |
#define | SLIDER_SIZE_Y 40 |
Slider size on display. More... | |
#define | SLIDER_PB_SPACING_X 10 |
Spacing from slider to progress bar. More... | |
#define | PB_SIZE_X SLIDER_SIZE_X |
Slider progress bar on display. More... | |
#define | PB_SIZE_Y SLIDER_SIZE_Y |
Slider progress bar on display. More... | |
Widget configurations | |
#define | SLIDER_MAX_VALUE 100 |
Max value for slider. More... | |
Enumerations | |
enum | app_widget_ids { SLIDER_ID = 1, BUTTON_ID } |
Event command ID for the application widgets. More... | |
Functions | |
void | app_widget_launch () |
Setup widget demo. More... | |
static void | sub_frame_draw_handler (struct win_window *win, struct win_clip_region const *clip) |
Frame draw event handler. More... | |
static bool | widget_frame_command_handler (struct wtk_basic_frame *frame, win_command_t command_data) |
Frame command events handler. More... | |
Variables | |
Static text strings | |
static const char * | demo_string = "Demonstrating widgets" |
Description for label. More... | |
Static variables | |
static struct wtk_basic_frame * | main_frame |
Pointer to frame for application. More... | |
static struct wtk_slider * | slider |
Pointer to slider. More... | |
static struct wtk_progress_bar * | progress_bar |
Pointer to progress bar. More... | |
static struct gfx_bitmap | frame_background |
Frame background bitmap. More... | |
static uint8_t | counter |
Counter for button. More... | |
static struct wtk_basic_frame * | sub_frame |
Pointer to the sub-frame. More... | |
static struct gfx_bitmap | sub_frame_background |
Sub-frame background bitmap. More... | |
#define APP_BACKGROUND_COLOR GFX_COLOR(50, 50, 50) |
Background color for application.
Referenced by app_widget_launch().
#define LABEL_POS_X 10 |
Label position on top of display.
Referenced by app_widget_launch().
#define LABEL_POS_Y 10 |
Label position on top of display.
Referenced by app_widget_launch().
#define PB_SIZE_X SLIDER_SIZE_X |
Slider progress bar on display.
Referenced by app_widget_launch().
#define PB_SIZE_Y SLIDER_SIZE_Y |
Slider progress bar on display.
Referenced by app_widget_launch().
#define SLIDER_MAX_VALUE 100 |
Max value for slider.
Referenced by app_widget_launch().
#define SLIDER_PB_SPACING_X 10 |
Spacing from slider to progress bar.
Referenced by app_widget_launch().
#define SLIDER_POS_X 10 |
Slider position.
Referenced by app_widget_launch().
#define SLIDER_POS_Y 60 |
Slider position.
Referenced by app_widget_launch().
#define SLIDER_SIZE_X 80 |
Slider size on display.
Referenced by app_widget_launch().
#define SLIDER_SIZE_Y 40 |
Slider size on display.
Referenced by app_widget_launch().
enum app_widget_ids |
void app_widget_launch | ( | void | ) |
Setup widget demo.
This function launches the widget demo.
References APP_BACKGROUND_COLOR, gfx_bitmap::color, gfx_bitmap::data, demo_string, frame_background, GFX_BITMAP_SOLID, GFX_COLOR, gfx_get_height(), gfx_get_width(), LABEL_POS_X, LABEL_POS_Y, win_window::parent, PB_SIZE_X, PB_SIZE_Y, win_area::pos, win_area::size, SLIDER_ID, SLIDER_MAX_VALUE, SLIDER_PB_SPACING_X, SLIDER_POS_X, SLIDER_POS_Y, SLIDER_SIZE_X, SLIDER_SIZE_Y, gfx_bitmap::type, widget_frame_command_handler(), win_destroy(), win_get_root(), win_root, win_show(), wtk_basic_frame_as_child(), wtk_basic_frame_create(), wtk_label_as_child(), wtk_label_create(), wtk_label_size_hint(), wtk_progress_bar_as_child(), wtk_progress_bar_create(), WTK_PROGRESS_BAR_HORIZONTAL, wtk_slider_as_child(), WTK_SLIDER_CMD_RELEASE, wtk_slider_create(), WTK_SLIDER_HORIZONTAL, win_point::x, and win_point::y.
Referenced by main().
|
static |
Frame draw event handler.
This function will draw the contents of the sub-frame.
References counter.
|
static |
Frame command events handler.
This function handles the command events generated by the widgets.
References BUTTON_ID, SLIDER_ID, wtk_progress_bar_set_value(), and wtk_slider_get_value().
Referenced by app_widget_launch().
|
static |
Counter for button.
Referenced by sub_frame_draw_handler().
|
static |
Description for label.
Referenced by app_widget_launch().
|
static |
Frame background bitmap.
Referenced by app_widget_launch().
|
static |
Pointer to frame for application.
|
static |
Pointer to progress bar.
|
static |
Pointer to slider.
Referenced by wtk_slider_create(), and wtk_slider_handler().
|
static |
Pointer to the sub-frame.
|
static |
Sub-frame background bitmap.