This is the skeleton application to be used with the application note AVR1614: Widget Toolkit - Getting Started.
The main files of interest to the user are:
This training has been tested with the mXT143E Xplained on the following boards:
Please ensure that the SPI mode switch on the mXT143E Xplained is in the correct position for your evaluation board:
This application is made as a training to introduce users to some of the available widgets in the Widget toolkit.
Initially this application will draw a basic frame filling the entire screen and add a slider and a progress bar on the upper half of the screen.
The user's task is then to add a sub-frame and a button. The button should increment a counter presented in the sub-frame each time the button is pressed.
The most relevant module dependencies for this training are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.