See Quick start guide for the maXTouch component.
This component provides low-level read/write access to the configuration and data registers on a maXTouch device. It has only been tested on mxt143E parts, but it should be easy to add support for other maXTouch devices. This is a common API for all supported architectures in ASF.
The component is not interrupt driven and the maXTouch device has to be polled to see if there are any pending messages, and the mxt_read_message function reads out the messages pending. For reading out only touch events, the mxt_read_touch_event function can be used. As mentioned the component is not interrupt driven, but by configuring a pin change interrupt on the CHG pin, the application can receive interrupts when there are messages pending.
Data Structures | |
struct | mxt_conf_messageprocessor_t5 |
Object message. More... | |
struct | mxt_device |
maXTouch device information data container struct More... | |
struct | mxt_gen_commandprocessor_t6 |
Commandprocessor T6 object. More... | |
struct | mxt_info_object |
Identification header. More... | |
struct | mxt_object |
Object table entry. More... | |
struct | mxt_report_id_map |
Map of the report ID vs object type and instance. More... | |
struct | mxt_touch_event |
Touch event struct. More... | |
Typedefs | |
typedef void(* | mxt_message_handler_t )(struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message) |
Message handler prototype. More... | |
Enumerations | |
enum | mxt_object_type { MXT_GEN_MESSAGEPROCESSOR_T5 = 5, MXT_GEN_COMMANDPROCESSOR_T6 = 6, MXT_GEN_POWERCONFIG_T7 = 7, MXT_GEN_ACQUISITIONCONFIG_T8 = 8, MXT_TOUCH_MULTITOUCHSCREEN_T9 = 9, MXT_SPT_COMMSCONFIG_T18 = 18, MXT_SPT_MESSAGECOUNT_T44 = 44, MXT_PROCG_TOUCHSUPPRESSION_T48 = 48 } |
Object types. More... | |
Functions | |
status_code_t | mxt_close_device (struct mxt_device *device) |
Closes the twi connection and frees memory. More... | |
int8_t | mxt_get_message_count (struct mxt_device *device) |
Get pending message count. More... | |
uint16_t | mxt_get_object_address (struct mxt_device *device, uint8_t object_id, uint8_t instance) |
Get memory address to object. More... | |
enum mxt_object_type | mxt_get_object_type (struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message) |
Get object type from message. More... | |
status_code_t | mxt_init_device (struct mxt_device *device, twi_master_t interface, uint8_t chip_adr, uint32_t chgpin) |
Initialize maXTouch device connected to TWIx module. More... | |
bool | mxt_is_message_pending (struct mxt_device *device) |
Report if there is any pending messages in the queue. More... | |
status_code_t | mxt_load_configuration (struct mxt_device *device, void *configuration_data) |
status_code_t | mxt_probe_device (twi_master_t interface, uint8_t chip_adr) |
Probe for a maXTouch connected to a specific TWI line. More... | |
status_code_t | mxt_process_messages (struct mxt_device *device) |
Process message queue on maXTouch device. More... | |
status_code_t | mxt_read_config_object (struct mxt_device *device, mxt_memory_adr memory_adr, void *obj_data) |
Read object configuration. More... | |
status_code_t | mxt_read_config_reg (struct mxt_device *device, mxt_memory_adr memory_adr, uint8_t *value) |
Read object register. More... | |
status_code_t | mxt_read_message (struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message) |
Get next message in queue. More... | |
status_code_t | mxt_read_touch_event (struct mxt_device *device, struct mxt_touch_event *touch_event) |
Read next touch event in queue, skip other events (other events are lost) More... | |
void | mxt_set_message_handler (struct mxt_device *device, mxt_message_handler_t handler) |
Set message handler. More... | |
status_code_t | mxt_write_config_object (struct mxt_device *device, mxt_memory_adr memory_adr, void *obj_data) |
Write object configuration. More... | |
status_code_t | mxt_write_config_reg (struct mxt_device *device, mxt_memory_adr memory_adr, uint8_t value) |
Write object register. More... | |
COMMSCONFIG T18 object control register bit positions | |
#define | MXT_COMMSCONFIG_T18_CHG_MODE_bp 2 |
#define | MXT_COMMSCONFIG_T18_DISMNTR_bp 7 |
COMMANDPROCESSOR T6 object register offset | |
#define | MXT_GEN_COMMANDPROCESSOR_RESET 0 |
#define | MXT_GEN_COMMANDPROCESSOR_BACKUPNV 1 |
#define | MXT_GEN_COMMANDPROCESSOR_CALIBRATE 2 |
#define | MXT_GEN_COMMANDPROCESSOR_REPORTALL 3 |
#define | MXT_GEN_COMMANDPROCESSOR_DIAGNOSTIC 5 |
Touch event types | |
#define | MXT_UNGRIP_EVENT 1 |
#define | MXT_SUPPRESS_EVENT 2 |
#define | MXT_AMP_EVENT 4 |
#define | MXT_VECTOR_EVENT 8 |
#define | MXT_MOVE_EVENT 16 |
#define | MXT_RELEASE_EVENT 32 |
#define | MXT_PRESS_EVENT 64 |
#define | MXT_DETECT_EVENT 128 |
#define MXT_AMP_EVENT 4 |
#define MXT_COMMSCONFIG_T18_CHG_MODE_bp 2 |
#define MXT_COMMSCONFIG_T18_DISMNTR_bp 7 |
#define MXT_DETECT_EVENT 128 |
#define MXT_GEN_COMMANDPROCESSOR_BACKUPNV 1 |
#define MXT_GEN_COMMANDPROCESSOR_CALIBRATE 2 |
Referenced by mxt_init().
#define MXT_GEN_COMMANDPROCESSOR_DIAGNOSTIC 5 |
#define MXT_GEN_COMMANDPROCESSOR_REPORTALL 3 |
#define MXT_GEN_COMMANDPROCESSOR_RESET 0 |
Referenced by mxt_init().
#define MXT_MOVE_EVENT 16 |
Referenced by main().
#define MXT_PRESS_EVENT 64 |
Referenced by main().
#define MXT_RELEASE_EVENT 32 |
Referenced by main().
#define MXT_SUPPRESS_EVENT 2 |
#define MXT_UNGRIP_EVENT 1 |
#define MXT_VECTOR_EVENT 8 |
typedef void(* mxt_message_handler_t)(struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message) |
Message handler prototype.
*device | Pointer to mxt_device struct |
*message | Pointer to mxt_message struct |
enum mxt_object_type |
status_code_t mxt_close_device | ( | struct mxt_device * | device | ) |
Closes the twi connection and frees memory.
*device | Pointer to mxt_device instance |
References mxt_device::info_object, mxt_device::object_list, mxt_device::report_id_map, and STATUS_OK.
int8_t mxt_get_message_count | ( | struct mxt_device * | device | ) |
Get pending message count.
*device | Pointer to mxt_device instance |
References twi_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, mxt_get_object_address(), MXT_SPT_MESSAGECOUNT_T44, STATUS_OK, and twi_master_read().
uint16_t mxt_get_object_address | ( | struct mxt_device * | device, |
uint8_t | object_id, | ||
uint8_t | instance | ||
) |
Get memory address to object.
*device | Pointer to mxt_device instance |
object_id | Object ID |
instance | Object instance |
References mxt_device::info_object, mxt_info_object::obj_count, mxt_device::object_list, mxt_object::start_address, and mxt_object::type.
Referenced by mxt_get_message_count(), mxt_init(), and mxt_read_message().
enum mxt_object_type mxt_get_object_type | ( | struct mxt_device * | device, |
struct mxt_conf_messageprocessor_t5 * | message | ||
) |
Get object type from message.
*device | Pointer to mxt_device instance |
*message | Message buffer |
References mxt_report_id_map::object_type, mxt_device::report_id_map, and mxt_conf_messageprocessor_t5::reportid.
Referenced by mxt_read_touch_event().
status_code_t mxt_init_device | ( | struct mxt_device * | device, |
twi_master_t | interface, | ||
uint8_t | chip_adr, | ||
uint32_t | chgpin | ||
) |
Initialize maXTouch device connected to TWIx module.
*interface | Pointer to TWI register set |
*device | Pointer to mxt_device instance |
chip_adr | I2C address to maXTouch device |
chgpin | IOPORT pin instance attached to the maXTouch device's /CHG pin |
References mxt_device::chgpin, ERR_BAD_DATA, mxt_device::handler, mxt_device::interface, mxt_device::multitouch_report_offset, mxt_device::mxt_chip_adr, mxt_create_report_id_map(), mxt_get_report_id_offset(), mxt_info_le_to_cpu(), mxt_read_info_block(), MXT_TOUCH_MULTITOUCHSCREEN_T9, mxt_validate_info_block(), and STATUS_OK.
Referenced by mxt_init().
bool mxt_is_message_pending | ( | struct mxt_device * | device | ) |
Report if there is any pending messages in the queue.
*device | Pointer to mxt_device instance |
References mxt_device::chgpin, and ioport_get_pin_level().
Referenced by main(), mxt_process_messages(), and mxt_read_touch_event().
status_code_t mxt_load_configuration | ( | struct mxt_device * | device, |
void * | configuration_data | ||
) |
status_code_t mxt_probe_device | ( | twi_master_t | interface, |
uint8_t | chip_adr | ||
) |
Probe for a maXTouch connected to a specific TWI line.
interface | Pointer to TWI register set |
*chip_adr | I2C address to maXTouch device |
References twi_packet::addr, ERR_BAD_ADDRESS, mxt_info_object::family_ID, MXT_FAMILY_143E, MXT_MEM_ADDR, MXT_VARIANT_143E, STATUS_OK, twi_master_read(), TWI_SUCCESS, and mxt_info_object::variant_ID.
status_code_t mxt_process_messages | ( | struct mxt_device * | device | ) |
Process message queue on maXTouch device.
*device | Pointer to mxt_device instance |
References ERR_BAD_ADDRESS, mxt_device::handler, mxt_is_message_pending(), mxt_read_message(), and STATUS_OK.
status_code_t mxt_read_config_object | ( | struct mxt_device * | device, |
mxt_memory_adr | memory_adr, | ||
void * | obj_data | ||
) |
Read object configuration.
*device | Pointer to mxt_device instance |
memory_adr | Memory address to the object |
*obj_data | Pointer to a large enough memory buffer |
References twi_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, mxt_get_object_size(), STATUS_OK, and twi_master_read().
status_code_t mxt_read_config_reg | ( | struct mxt_device * | device, |
mxt_memory_adr | memory_adr, | ||
uint8_t * | value | ||
) |
Read object register.
*device | Pointer to mxt_device instance |
memory_adr | Memory address to the register |
*value | Pointer to a 1 byte buffer to store the data in |
References twi_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, STATUS_OK, and twi_master_read().
status_code_t mxt_read_message | ( | struct mxt_device * | device, |
struct mxt_conf_messageprocessor_t5 * | message | ||
) |
Get next message in queue.
*device | Pointer to mxt_device instance |
*message | Pointer to mxt_message instance |
References twi_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, MXT_GEN_MESSAGEPROCESSOR_T5, mxt_get_object_address(), MXT_TWI_MSG_SIZE_T5, mxt_validate_message(), STATUS_OK, and twi_master_read().
Referenced by mxt_process_messages(), and mxt_read_touch_event().
status_code_t mxt_read_touch_event | ( | struct mxt_device * | device, |
struct mxt_touch_event * | touch_event | ||
) |
Read next touch event in queue, skip other events (other events are lost)
*device | Pointer to mxt_device instance |
*touch_event | Pointer to mxt_touch_event instance |
References ERR_BAD_DATA, mxt_touch_event::id, mxt_conf_messageprocessor_t5::message, mxt_device::multitouch_report_offset, mxt_get_object_type(), mxt_is_message_pending(), mxt_read_message(), MXT_TOUCH_MULTITOUCHSCREEN_T9, mxt_conf_messageprocessor_t5::reportid, mxt_touch_event::size, mxt_touch_event::status, STATUS_OK, mxt_touch_event::x, and mxt_touch_event::y.
Referenced by main().
void mxt_set_message_handler | ( | struct mxt_device * | device, |
mxt_message_handler_t | handler | ||
) |
Set message handler.
*device | Pointer to mxt_device instance |
handler | Message handler function |
References mxt_device::handler.
status_code_t mxt_write_config_object | ( | struct mxt_device * | device, |
mxt_memory_adr | memory_adr, | ||
void * | obj_data | ||
) |
Write object configuration.
*device | Pointer to mxt_device instance |
memory_adr | Memory address to the object |
*obj_data | Pointer to memory buffer containing object data |
References twi_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, mxt_get_object_size(), STATUS_OK, and twi_master_write().
Referenced by mxt_init().
status_code_t mxt_write_config_reg | ( | struct mxt_device * | device, |
mxt_memory_adr | memory_adr, | ||
uint8_t | value | ||
) |
Write object register.
*device | Pointer to mxt_device instance |
memory_adr | Memory address to register |
value | Value to be written to register |
References twi_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, STATUS_OK, and twi_master_write().
Referenced by mxt_init().