This is the unit test application for the MAC Symbol Counter Driver(MACSC). It will test overflow,compare and backoff slot counter functionality of the MACSC.
All AVR MEGARF devices with MACSC can be used
See the documentation for the individual unit test functions here for detailed descriptions of the tests.
This example depends directly on the following modules:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/