Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups
Timer/Counter (TC) Timeout Driver

This timeout functionality driver uses the asynchronous Timer/Counter (TC) as time source in order to have a system tick.

Since this is the asynchronous TC module, it's convenient to use a 32KHz crystal as timeout source for real time timing. Typical tick rate is in the range 1 - 1000Hz.

The timeout functionality is a configurable number of independent timeouts that are specified in number of ticks. They can be both singleshot and periodic.

As this driver provides a software layer on top of the TC module it will have some performance penalty, so for high performance it would be recommended to implement a more specific use by implementing your own interrupt handler based on this as a reference.

Configuration

Configuration is done in the configuration file : conf_tc_timeout.h

Configuration defines:

If both CONFIG_TC_TIMEOUT_CLOCK_SOURCE_TOSC and CONFIG_TC_TIMEOUT_CLOCK_SOURCE_EXCLK are undefined the IO clock is used as clock source.

Interface

First, the timeout internal setup needs to be configured and this is done by the function tc_timeout_init().

There are different functions for starting a timer:

Polling for timer status can be done with tc_timeout_test_and_clear_expired(), and this will also clear the expired flag in case of periodic timer.

A running timer can be stopped with tc_timeout_stop().

Common to all the function arguments are a timeout identifier, this is a number starting from 0 to identify the timeout. Maximum of this parameter is controlled by the configuration CONFIG_TC_TIMEOUT_COUNT.

The start timeout function uses timeout values represented in number of ticks.

Usage

First of all, the include file is needed:

#include "tc_timeout.h"

Then the timeout internals need to be set up by calling:

For simple usage starting a singleshot timeout for timeout id 0 and a timeout value of 100 ticks:

// do whats needed after timeout has expired

Accuracy

Since this is a timeout layer on top of a system tick; the trigger time of a timeout is fully depending on this system tick. This means that you might not know when the next tick will count down your timeout, and this inaccuracy can be from 0 to 1 system tick.

E.g.: If you want a timeout of 1 system tick and use 1 as your timeout value, this might trigger immediately. So, if you have a requirement to wait at least 1 system tick, it would be recommended to use the requested value

However, if you know the system tick has passed or are using periodic timeout you can be confident in the timing.

Modules

 Timer/Counter (TC) Timeout Driver internals
 

Macros

#define CONFIG_TC_TIMEOUT_CLOCK_SOURCE_HZ   32768
 Clock source speed in Hz. More...
 
#define CONFIG_TC_TIMEOUT_CLOCK_SOURCE_TOSC
 If defined, use crystal on TOSC as clock source. More...
 
#define CONFIG_TC_TIMEOUT_COUNT   2
 Maximum number of TC based timers to allow. More...
 
#define CONFIG_TC_TIMEOUT_TICK_HZ   1024
 Ticks per second used as time base for timers. More...
 
#define TC_TIMEOUT_CLK_PER_TICK   (CONFIG_TC_TIMEOUT_CLOCK_SOURCE_HZ / CONFIG_TC_TIMEOUT_TICK_HZ)
 Number of clocks per tick. More...
 
#define TC_TIMEOUT_COMP   (TC_TIMEOUT_CLK_PER_TICK / TC_TIMEOUT_PRESCALER - 1)
 Comparator value. More...
 
#define TC_TIMEOUT_PRESCALER   1
 Prescaler value. More...
 
#define TC_TIMEOUT_PRESCALER_MASK   (1 << CS20)
 Prescaler mask bits. More...
 
#define TC_TIMEOUT_TICK_HZ
 Actual TC timeout tick rate. More...
 

Typedefs

typedef uint8_t tc_timeout_id_t
 Timeout identifier. More...
 

Functions

void tc_timeout_init (void)
 Initialize TC timeout. More...
 
void tc_timeout_start_offset (tc_timeout_id_t id, uint16_t period, uint16_t start_offset)
 Start periodic timeout with a specific start timeout. More...
 
void tc_timeout_start_periodic (tc_timeout_id_t id, uint16_t period)
 Start periodic timeout. More...
 
void tc_timeout_start_singleshot (tc_timeout_id_t id, uint16_t timeout)
 Start singleshot timeout. More...
 
void tc_timeout_stop (tc_timeout_id_t id)
 Stop running timeout. More...
 
bool tc_timeout_test_and_clear_expired (tc_timeout_id_t id)
 Test and clear expired flag for running timeout. More...
 

#define CONFIG_TC_TIMEOUT_CLOCK_SOURCE_HZ   32768

Clock source speed in Hz.

This is typically either the IO clock (F_CPU) or clock crystal (32768Hz).

#define CONFIG_TC_TIMEOUT_CLOCK_SOURCE_TOSC

If defined, use crystal on TOSC as clock source.

If this or CONFIG_TC_TIMEOUT_CLOCK_SOURCE_EXCLK is undefined, the IO clock will be used.

#define CONFIG_TC_TIMEOUT_COUNT   2

Maximum number of TC based timers to allow.

This is limited by to 8 due to internal driver limits.

Referenced by ISR().

#define CONFIG_TC_TIMEOUT_TICK_HZ   1024

Ticks per second used as time base for timers.

#define TC_TIMEOUT_CLK_PER_TICK   (CONFIG_TC_TIMEOUT_CLOCK_SOURCE_HZ / CONFIG_TC_TIMEOUT_TICK_HZ)

Number of clocks per tick.

#define TC_TIMEOUT_COMP   (TC_TIMEOUT_CLK_PER_TICK / TC_TIMEOUT_PRESCALER - 1)

Comparator value.

Referenced by tc_timeout_init().

#define TC_TIMEOUT_PRESCALER   1

Prescaler value.

#define TC_TIMEOUT_PRESCALER_MASK   (1 << CS20)

Prescaler mask bits.

Referenced by tc_timeout_init().

#define TC_TIMEOUT_TICK_HZ
Value:
#define TC_TIMEOUT_COMP
Comparator value.
Definition: tc_timeout.h:233
#define TC_TIMEOUT_PRESCALER
Prescaler value.
Definition: tc_timeout.h:226
#define CONFIG_TC_TIMEOUT_CLOCK_SOURCE_HZ
Clock source speed in Hz.

Actual TC timeout tick rate.

Referenced by main().

typedef uint8_t tc_timeout_id_t

Timeout identifier.

Index for timeout to use. Limited by max value configured with CONFIG_TC_TIMEOUT_COUNT.

void tc_timeout_init ( void  )

Initialize TC timeout.

Initializes Timer/Counter for desired tick rate and starts it.

References TC_TIMEOUT_ASSR_MASK, TC_TIMEOUT_COMP, TC_TIMEOUT_OCIE, TC_TIMEOUT_OCR, TC_TIMEOUT_PRESCALER_MASK, TC_TIMEOUT_TCCRA, and TC_TIMEOUT_TIMSK.

Referenced by main().

void tc_timeout_start_offset ( tc_timeout_id_t  id,
uint16_t  period,
uint16_t  start_offset 
)

Start periodic timeout with a specific start timeout.

Parameters
idtc_timeout_id_t
periodTime period in number of ticks
start_offsetTime to first timeout in number of ticks

References tc_timeout_struct::count, cpu_irq_restore(), cpu_irq_save(), tc_timeout_struct::period, tc_timeout_active, tc_timeout_array, and tc_timeout_expired.

Referenced by tc_timeout_start_periodic(), and tc_timeout_start_singleshot().

void tc_timeout_start_periodic ( tc_timeout_id_t  id,
uint16_t  period 
)

Start periodic timeout.

Parameters
idtc_timeout_id_t
periodTime period in number of ticks

References tc_timeout_start_offset().

Referenced by main().

void tc_timeout_start_singleshot ( tc_timeout_id_t  id,
uint16_t  timeout 
)

Start singleshot timeout.

Parameters
idtc_timeout_id_t
timeoutTimeout in number of ticks

References tc_timeout_start_offset().

void tc_timeout_stop ( tc_timeout_id_t  id)

Stop running timeout.

Parameters
idtc_timeout_id_t

References cpu_irq_restore(), cpu_irq_save(), and tc_timeout_active.

bool tc_timeout_test_and_clear_expired ( tc_timeout_id_t  id)

Test and clear expired flag for running timeout.

Parameters
idtc_timeout_id_t
Return values
trueTimer have expired; clearing expired flag
falseTimer still running

References cpu_irq_restore(), cpu_irq_save(), and tc_timeout_expired.

Referenced by main().