This is the unit test for the MEGARF USART driver. It communicates with itself by looping back using a jumper on the external USART RX/TX pins.
This example has been tested with the following setup(s):
See the documentation for the individual unit test functions here for detailed descriptions of the tests.
This example depends directly on the following modules:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.