AVR477 Target Application is used for demonstration of the capabilities of the AVR477 Touch Remote Control.
1.RZ600 USB board along with the AT86RF231 radio board
2.RCB128RFA1 mounted on the Sensor Terminal Board(STB) connected over TWI to the QT600 kit
The Target Application receives QTouch Data over air as RF4CE packets and transfers them to QTouch Studio for analysis of touch data.
When RZ600 is used,the USB HID interfacde is used for communication to QTouch Studio.
When the STB-RCB128RFA1 is used,the touch data is received by the RCB128RFA1 over air and transferred over TWI to the QT600 kit. QT600,then,transfers this data over USB to QTStudio.