License | Copyright (c) 2017-2018 Microchip Technology Inc |
License | Copyright (c) 2014-2018 Microchip Technology Inc |
Quick Start Guide for the MEGA Sleep Driver | This is the quick start guide for the Sleep Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
Quick Start Guide for the MEGARF MACSC Driver | This is the quick start guide for the macscc_group , with step-by-step instructions on how to configure and use the driver for a specific use case |
Overview | This application demonstrates a simple example to turn on and off the board LED |
MEGA LED Example | Overview: |
Quick Start Guide for the SPI Master Driver | This is the quick start guide for the SPI Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Basic setup for SPI master on XMEGA devices | |
Quick Start Guide for the MEGARF ext int Driver | This is the quick start guide for the Global interrupt management , with step-by-step instructions on how to configure and use the driver for a specific use case |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
 Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Quickstart guide for Common service TWI | This is the quickstart guide for the Common service TWI, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
AVR477 Target | |
AVR477 Remote | |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quick Start Guide | This is the quick start guide for the EPD Xplained Pro extension board with Pervasive Displays Inc |
Quick start guide for MEGARF TWI driver | This is the quick start guide for the TWI Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Quick start guide for WDT driver | This is the quick start guide for the Watchdog Timer (WDT), with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 Reset WDT in interrupt mode | In this use case, the WDT is configured for: |
Quick start guide for Calendar service | This is the quick start guide for the Calendar service, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 Calculate time between dates | The use case will let the user calculate the time between two dates, by first calculating the dates from two timestamps |
Todo List | |
Deprecated List | |