This is a low-level driver implementation for the MEGA RF sleep controller.
Modules | |
Quick Start Guide(s) | |
In this section you can find a list of all Quick Start guides related to the Sleep controller driver. | |
Functions | |
static void | sleep_disable (void) |
Disable sleep. More... | |
static void | sleep_enable (void) |
Enable sleep. More... | |
static void | sleep_set_mode (enum SLEEP_SMODE_enum mode) |
Set new sleep mode. More... | |
|
inlinestatic |
Disable sleep.
Referenced by example_cmp2_int_cb(), and sleepmgr_sleep().
|
inlinestatic |
Enable sleep.
Referenced by main(), sleepmgr_sleep(), and sm_sleep().
|
inlinestatic |
Set new sleep mode.
mode | Sleep mode, from the device IO header file. |
Referenced by main(), sleepmgr_sleep(), and sm_init().