|
#define | aBaseSlotDuration (60) |
| The number of symbols forming a superframe slot when the superframe order is equal to 0. More...
|
|
#define | aBaseSuperframeDuration |
| The number of symbols forming a superframe when the superframe order is equal to 0. More...
|
|
#define | ACK_PAYLOAD_LEN (0x03) |
| Length (in octets) of ACK payload. More...
|
|
#define | aGTSDescPersistenceTime (4) |
| The number of superframes in which a GTS descriptor exists in the beacon frame of a PAN coordinator. More...
|
|
#define | aMaxBeaconOverhead (75) |
| The maximum number of octets added by the MAC sublayer to the payload of its beacon frame. More...
|
|
#define | aMaxBeaconPayloadLength (aMaxPHYPacketSize - aMaxBeaconOverhead) |
| The maximum size, in octets, of a beacon payload. More...
|
|
#define | aMaxLostBeacons (4) |
| The number of consecutive lost beacons that will cause the MAC sublayer of a receiving device to declare a loss of synchronization. More...
|
|
#define | aMaxMACPayloadSize (aMaxPHYPacketSize - aMinMPDUOverhead) |
| The maximum number of octets that can be transmitted in the MAC Payload field. More...
|
|
#define | aMaxMACSafePayloadSize |
| The maximum number of octets that can be transmitted in the MAC Payload field of an unsecured MAC frame that will be guaranteed not to exceed aMaxPHYPacketSize. More...
|
|
#define | aMaxMPDUUnsecuredOverhead (25) |
| The maximum number of octets added by the MAC sublayer to the PSDU without security. More...
|
|
#define | aMaxPHYPacketSize (127) |
| Maximum size of PHY packet. More...
|
|
#define | aMaxSIFSFrameSize (18) |
| The maximum size of an MPDU, in octets, that can be followed by a SIFS period. More...
|
|
#define | aMinCAPLength (440) |
| The minimum number of symbols forming the CAP. More...
|
|
#define | aMinMPDUOverhead (9) |
| The minimum number of octets added by the MAC sublayer to the PSDU. More...
|
|
#define | aNumSuperframeSlots (16) |
| The number of slots contained in any superframe. More...
|
|
#define | ASSOC_PERMIT_BIT_POS (15) |
| Association permit bit position. More...
|
|
#define | ASSOCIATION_RESERVED (3) |
| Association status code value (see wpan_mlme_associate_resp()). More...
|
|
#define | ASSOCIATION_SUCCESSFUL (0) |
| Association status code value (see wpan_mlme_associate_resp()). More...
|
|
#define | aTurnaroundTime (12) |
| Maximum turnaround Time of the radio to switch from Rx to Tx or Tx to Rx in symbols. More...
|
|
#define | aUnitBackoffPeriod (20) |
| The number of symbols forming the basic time period used by the CSMA-CA algorithm. More...
|
|
#define | BATT_LIFE_EXT_BIT_POS (12) |
| Battery life extention bit position. More...
|
|
#define | BROADCAST (0xFFFF) |
| Generic 16 bit broadcast address. More...
|
|
#define | CLEAR_ADDR_64 (0ULL) |
| Unused EUI-64 address. More...
|
|
#define | CONV_DBM_TO_phyTransmitPower(dbm_value) |
| Converts a dBm value to a phyTransmitPower value. More...
|
|
#define | CONV_phyTransmitPower_TO_DBM(phyTransmitPower_value) |
| Converts a phyTransmitPower value to a dBm value. More...
|
|
#define | ED_VAL_LEN (1) |
| Length of the ED value parameter number field. More...
|
|
#define | EXT_ADDR_LEN (8) |
| Length (in octets) of extended address. More...
|
|
#define | FCF1_FV_2003 (0) |
| The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield fcf1. More...
|
|
#define | FCF1_FV_2006 (1) |
| The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield fcf1. More...
|
|
#define | FCF1_FV_2012 (2) |
| The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield fcf1. More...
|
|
#define | FCF1_FV_MASK (3 << FCF1_FV_SHIFT) |
| The mask for the frame version subfield fcf1. More...
|
|
#define | FCF1_FV_SHIFT (4) |
| Shift value for the frame version subfield fcf1. More...
|
|
#define | FCF_2_DEST_ADDR_OFFSET (2) |
| Offset of Destination Addressing Mode of octet two of MHR. More...
|
|
#define | FCF_2_SOURCE_ADDR_OFFSET (6) |
| Offset of Source Addressing Mode of octet two of MHR. More...
|
|
#define | FCF_ACK_REQUEST (1 << 5) |
| The mask for the ACK request bit of the FCF. More...
|
|
#define | FCF_DEST_ADDR_OFFSET (10) |
| Defines the offset of the destination address. More...
|
|
#define | FCF_FRAME_PENDING (1 << 4) |
| The mask for the frame pending bit of the FCF. More...
|
|
#define | FCF_FRAME_VERSION_2003 (0 << 12) |
| The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield. More...
|
|
#define | FCF_FRAME_VERSION_2006 (1 << 12) |
| The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield. More...
|
|
#define | FCF_FRAME_VERSION_2012 (2 << 12) |
| The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield. More...
|
|
#define | FCF_FRAMETYPE_ACK (0x02) |
| Define the ACK frame type. More...
|
|
#define | FCF_FRAMETYPE_BEACON (0x00) |
| Defines the beacon frame type. More...
|
|
#define | FCF_FRAMETYPE_DATA (0x01) |
| Define the data frame type. More...
|
|
#define | FCF_FRAMETYPE_LLDN (0x04) |
| Define the LLDN frame type. More...
|
|
#define | FCF_FRAMETYPE_MAC_CMD (0x03) |
| Define the command frame type. More...
|
|
#define | FCF_FRAMETYPE_MASK (0x07) |
| Defines a mask for the frame type. More...
|
|
#define | FCF_FRAMETYPE_MP (0x05) |
| Define the multipurpose frame type. More...
|
|
#define | FCF_GET_FRAMETYPE(x) ((x) & FCF_FRAMETYPE_MASK) |
| Macro to get the frame type. More...
|
|
#define | FCF_LEN (2) |
| Length (in octets) of FCF. More...
|
|
#define | FCF_LONG_ADDR (0x03) |
| Address Mode: LONG. More...
|
|
#define | FCF_NO_ADDR (0x00) |
| Address Mode: NO ADDRESS. More...
|
|
#define | FCF_PAN_ID_COMPRESSION (1 << 6) |
| The mask for the PAN ID compression bit of the FCF. More...
|
|
#define | FCF_RESERVED_ADDR (0x01) |
| Address Mode: RESERVED. More...
|
|
#define | FCF_SECURITY_ENABLED (1 << 3) |
| The mask for the security enable bit of the FCF. More...
|
|
#define | FCF_SET_DEST_ADDR_MODE(x) |
| Macro to set the destination address mode. More...
|
|
#define | FCF_SET_FRAMETYPE(x) (x) |
| A macro to set the frame type. More...
|
|
#define | FCF_SET_SOURCE_ADDR_MODE(x) |
| Macro to set the source address mode. More...
|
|
#define | FCF_SHORT_ADDR (0x02) |
| Address Mode: SHORT. More...
|
|
#define | FCF_SOURCE_ADDR_OFFSET (14) |
| Defines the offset of the source address. More...
|
|
#define | FCS_LEN (2) |
| Length (in octets) of FCS. More...
|
|
#define | GTS_ALLOCATE (1) |
|
#define | GTS_DEALLOCATE (0) |
|
#define | GTS_RX_SLOT (1) |
|
#define | GTS_SLOT_LENGTH_1 (0x01) |
|
#define | GTS_SLOT_LENGTH_10 (0x0A) |
|
#define | GTS_SLOT_LENGTH_11 (0x0B) |
|
#define | GTS_SLOT_LENGTH_12 (0x0C) |
|
#define | GTS_SLOT_LENGTH_13 (0x0D) |
|
#define | GTS_SLOT_LENGTH_14 (0x0E) |
|
#define | GTS_SLOT_LENGTH_15 (0x0F) |
|
#define | GTS_SLOT_LENGTH_2 (0x02) |
|
#define | GTS_SLOT_LENGTH_3 (0x03) |
|
#define | GTS_SLOT_LENGTH_4 (0x04) |
|
#define | GTS_SLOT_LENGTH_5 (0x05) |
|
#define | GTS_SLOT_LENGTH_6 (0x06) |
|
#define | GTS_SLOT_LENGTH_7 (0x07) |
|
#define | GTS_SLOT_LENGTH_8 (0x08) |
|
#define | GTS_SLOT_LENGTH_9 (0x09) |
|
#define | GTS_TX_SLOT (0) |
|
#define | INVALID_SHORT_ADDRESS (0xFFFF) |
| Invalid short address. More...
|
|
#define | INVERSE_CHANNEL_MASK (~VALID_CHANNEL_MASK) |
| Inverse channel masks for scanning. More...
|
|
#define | LENGTH_FIELD_LEN (1) |
| Size of the length parameter. More...
|
|
#define | LQI_LEN (1) |
| Length of the LQI number field. More...
|
|
#define | MAC_NO_SHORT_ADDR_VALUE (0xFFFE) |
| MAC is using long address (by now). More...
|
|
#define | macAckWaitDuration (0x40) |
| The maximum number of symbols to wait for an acknowledgment frame to arrive following a transmitted data frame. More...
|
|
#define | macAssociatedPANCoord (0x56) |
| Indication of whether the device is associated to the PAN through the PAN coordinator. More...
|
|
#define | macAssociatedPANCoord_def (false) |
| Default value for PIB macAssociatedPANCoord. More...
|
|
#define | macAssociationPermit (0x41) |
| Indication of whether a coordinator is currently allowing association. More...
|
|
#define | macAssociationPermit_def (false) |
| Default value for PIB macAssociationPermit. More...
|
|
#define | macAutoRequest (0x42) |
| Indication of whether a device automatically sends a data request command if its address is listed in the beacon frame. More...
|
|
#define | macAutoRequest_def (true) |
| Default value for PIB macAutoRequest. More...
|
|
#define | macBattLifeExt (0x43) |
| Indication of whether battery life extension, by reduction of coordinator receiver operation time during the CAP, is enabled. More...
|
|
#define | macBattLifeExt_def (false) |
| Default value for PIB macBattLifeExt. More...
|
|
#define | macBattLifeExtPeriods (0x44) |
| The number of backoff periods during which the receiver is enabled following a beacon in battery life extension mode. More...
|
|
#define | macBattLifeExtPeriods_def (6) |
| Default value for PIB macBattLifeExtPeriods. More...
|
|
#define | macBeaconOrder (0x47) |
| Specification of how often the coordinator transmits a beacon. More...
|
|
#define | macBeaconOrder_def (15) |
| Default value for PIB macBeaconOrder. More...
|
|
#define | macBeaconPayload (0x45) |
| The contents of the beacon payload. More...
|
|
#define | macBeaconPayloadLength (0x46) |
| The length, in octets, of the beacon payload. More...
|
|
#define | macBeaconPayloadLength_def (0) |
| Default value for PIB macBeaconPayloadLength. More...
|
|
#define | macBeaconTxTime (0x48) |
| The time that the device transmitted its last beacon frame, in symbol periods. More...
|
|
#define | macBeaconTxTime_def (0x000000) |
| Default value for PIB macBeaconTxTime. More...
|
|
#define | macBSN (0x49) |
| The sequence number added to the transmitted beacon frame. More...
|
|
#define | macCoordExtendedAddress (0x4A) |
| The 64 bit address of the coordinator with which the device is associated. More...
|
|
#define | macCoordShortAddress (0x4B) |
| The 16 bit short address assigned to the coordinator with which the device is associated. More...
|
|
#define | macCoordShortAddress_def (0xFFFF) |
| Default value for PIB macCoordShortAddress. More...
|
|
#define | macDSN (0x4C) |
| The sequence number added to the transmitted data or MAC command frame. More...
|
|
#define | macGTSPermit (0x4D) |
| macGTSPermit is true if the PAN coordinator is to accept GTS requests, false otherwise. More...
|
|
#define | macGTSPermit_def (true) |
| Default value for PIB macGTSPermit. More...
|
|
#define | macIeeeAddress (0xF0) |
| Private MAC PIB attribute to allow setting the MAC address in test mode. More...
|
|
#define | macMaxBE (0x57) |
| The maximum value of the backoff exponent, BE, in the CSMA-CA algorithm. More...
|
|
#define | macMaxCSMABackoffs (0x4E) |
| The maximum number of backoffs the CSMA-CA algorithm will attempt before declaring a channel access failure. More...
|
|
#define | macMaxCSMABackoffs_def (4) |
| Default value for PIB macMaxCSMABackoffs. More...
|
|
#define | macMaxFrameRetries (0x59) |
| The maximum number of retries allowed after a transmission failure. More...
|
|
#define | macMaxFrameTotalWaitTime (0x58) |
| The maximum number of CAP symbols in a beaconenabled PAN, or symbols in a nonbeacon-enabled PAN, to wait either for a frame intended as a response to a data request frame or for a broadcast frame following a beacon with the Frame Pending subfield set to one. More...
|
|
#define | macMaxNumRxFramesDuringBackoff (0x7F) |
| Private MAC PIB attribute to control the CSMA algorithm. More...
|
|
#define | macMinBE (0x4F) |
| The minimum value of the backoff exponent in the CSMA-CA algorithm. More...
|
|
#define | macMinLIFSPeriod (0x5E) |
| The minimum number of symbols forming a LIFS period. More...
|
|
#define | macMinLIFSPeriod_def (40) |
| Default value for PIB macMinLIFSPeriod. More...
|
|
#define | macMinSIFSPeriod (0x5F) |
| The minimum number of symbols forming a SIFS period. More...
|
|
#define | macMinSIFSPeriod_def (12) |
| Default value for PIB macMinSIFSPeriod. More...
|
|
#define | macPANCoordExtendedAddress (0x7D) |
| The 64-bit address of the PAN coordinator. More...
|
|
#define | macPANCoordShortAddress (0x7E) |
| The 16-bit short address assinged to the PAN coordinator. More...
|
|
#define | macPANId (0x50) |
| The 16 bit identifier of the PAN on which the device is operating. More...
|
|
#define | macPANId_def (0xFFFF) |
| Default value for PIB macPANId. More...
|
|
#define | macPromiscuousMode (0x51) |
| This indicates whether the MAC sublayer is in a promiscuous (receive all) mode. More...
|
|
#define | macResponseWaitTime (0x5A) |
| The maximum time, in multiples of aBaseSuperframeDuration, a device shall wait for a response command frame to be available following a request command frame. More...
|
|
#define | macResponseWaitTime_def (32 * aBaseSuperframeDuration) |
| Default value for PIB macResponseWaitTime. More...
|
|
#define | macRxOnWhenIdle (0x52) |
| This indicates whether the MAC sublayer is to enable its receiver during idle periods. More...
|
|
#define | macRxOnWhenIdle_def (false) |
| Default value for PIB macRxOnWhenIdle. More...
|
|
#define | macSecurityEnabled (0x5D) |
| Indication of whether the MAC sublayer has security enabled. More...
|
|
#define | macSecurityEnabled_def (false) |
| Default value for PIB macSecurityEnabled. More...
|
|
#define | macShortAddress (0x53) |
| The 16 bit address that the device uses to communicate in the PAN. More...
|
|
#define | macShortAddress_def (0xFFFF) |
| Default value for PIB macShortAddress. More...
|
|
#define | macSuperframeOrder (0x54) |
| This specifies the length of the active portion of the superframe, including the beacon frame. More...
|
|
#define | macSuperframeOrder_def (15) |
| Default value for PIB macSuperframeOrder. More...
|
|
#define | macSyncSymbolOffset (0x5B) |
| The offset, measured in symbols, between the symbol boundary at which the MLME captures the timestamp of each transmitted or received frame, and the onset of the first symbol past the SFD, namely, the first symbol of the Length field. More...
|
|
#define | macTimestampSupported (0x5C) |
| Indication of whether the MAC sublayer supports the optional timestamping feature for incoming and outgoing data frames. More...
|
|
#define | macTransactionPersistenceTime (0x55) |
| The maximum time (in superframe periods) that a transaction is stored by a coordinator and indicated in its beacon. More...
|
|
#define | macTransactionPersistenceTime_def (0x01F4) |
| Default value for PIB macTransactionPersistenceTime. More...
|
|
#define | MAX_KEY_ID_FIELD_LEN (9) |
| Maximum length of the key id field. More...
|
|
#define | MAX_MGMT_FRAME_LENGTH (30) |
| Maximum size of the management frame(Association Response frame) More...
|
|
#define | MIN_FRAME_LENGTH (8) |
| Minimum size of a valid frame other than an Ack frame. More...
|
|
#define | MLME_SCAN_TYPE_ACTIVE (0x01) |
| Active scan (see wpan_mlme_scan_req()) More...
|
|
#define | MLME_SCAN_TYPE_ED (0x00) |
| Energy scan (see wpan_mlme_scan_req()) More...
|
|
#define | MLME_SCAN_TYPE_ORPHAN (0x03) |
| Orphan scan (see wpan_mlme_scan_req()) More...
|
|
#define | MLME_SCAN_TYPE_PASSIVE (0x02) |
| Passive scan (see wpan_mlme_scan_req()) More...
|
|
#define | NO_PIB_INDEX (0) |
|
#define | NON_BEACON_NWK (0x0F) |
| BO value for nonbeacon-enabled network. More...
|
|
#define | NUM_LONG_PEND_ADDR(x) (((x) & 0x70) >> 4) |
| Mask for the number of long addresses pending. More...
|
|
#define | NUM_SHORT_PEND_ADDR(x) ((x) & 0x07) |
| Mask for the number of short addresses pending. More...
|
|
#define | PAN_ACCESS_DENIED (2) |
| Association status code value (see wpan_mlme_associate_resp()). More...
|
|
#define | PAN_AT_CAPACITY (1) |
| Association status code value (see wpan_mlme_associate_resp()). More...
|
|
#define | PAN_COORD_BIT_POS (14) |
| PAN coordinator bit position. More...
|
|
#define | PAN_ID_LEN (2) |
| Length (in octets) of PAN ID. More...
|
|
#define | PL_POS_DST_ADDR_START (6) |
| Octet start position of Destination Address field within payload array of frame_info_t. More...
|
|
#define | PL_POS_DST_PAN_ID_START (4) |
| Octet start position of Destination PAN-Id field within payload array of frame_info_t. More...
|
|
#define | PL_POS_FCF_1 (1) |
| Octet position of FCF octet one within payload array of frame_info_t. More...
|
|
#define | PL_POS_FCF_2 (2) |
| Octet position of FCF octet two within payload array of frame_info_t. More...
|
|
#define | PL_POS_SEQ_NUM (3) |
| Octet position of Sequence Number octet within payload array of frame_info_t. More...
|
|
#define | SEQ_NUM_LEN (1) |
| Length of the sequence number field. More...
|
|
#define | SHORT_ADDR_LEN (2) |
| Length (in octets) of short address. More...
|
|
#define | WPAN_TXOPT_ACK (0x01) |
| Value for TxOptions parameter in wpan_mcps_data_req(). More...
|
|
#define | WPAN_TXOPT_GTS (0x02) |
| Value for TxOptions parameter in wpan_mcps_data_req(). More...
|
|
#define | WPAN_TXOPT_GTS_ACK (0x03) |
| Value for TxOptions parameter in wpan_mcps_data_req(). More...
|
|
#define | WPAN_TXOPT_INDIRECT (0x04) |
| Value for TxOptions parameter in wpan_mcps_data_req(). More...
|
|
#define | WPAN_TXOPT_INDIRECT_ACK (0x05) |
| Value for TxOptions parameter in wpan_mcps_data_req(). More...
|
|
#define | WPAN_TXOPT_OFF (0x00) |
| Value for TxOptions parameter in wpan_mcps_data_req(). More...
|
|
|
#define | phyCurrentChannel (0x00) |
| The RF channel to use for all following transmissions and receptions. More...
|
|
#define | phyChannelsSupported (0x01) |
| The 5 most significant bits (MSBs) (b27, ..., b31) of phyChannelsSupported shall be reserved and set to 0, and the 27 LSBs (b0, b1, ..., b26) shall indicate the status (1 = available, 0 = unavailable) for each of the 27 valid channels (bk shall indicate the status of channel k). More...
|
|
#define | phyTransmitPower (0x02) |
| The 2 MSBs represent the tolerance on the transmit power: 00 = 1 dB 01 = 3 dB 10 = 6 dB The 6 LSBs represent a signed integer in twos-complement format, corresponding to the nominal transmit power of the device in decibels relative to 1 mW. More...
|
|
#define | phyCCAMode (0x03) |
| The CCA mode. More...
|
|
#define | phyCurrentPage (0x04) |
| This is the current PHY channel page. More...
|
|
#define | phyMaxFrameDuration (0x05) |
| The maximum number of symbols in a frame: = phySHRDuration + ceiling([aMaxPHYPacketSize + 1] x phySymbolsPerOctet) More...
|
|
#define | phySHRDuration (0x06) |
| The duration of the synchronization header (SHR) in symbols for the current PHY. More...
|
|
#define | phySymbolsPerOctet (0x07) |
| The number of symbols per octet for the current PHY. More...
|
|
#define | PHY_OVERHEAD (5) |
| Number of octets added by the PHY: 4 sync octets + SFD octet. More...
|
|