Microchip® Advanced Software Framework

nand_flash_common.h File Reference

Common definition of NAND Flash.

This file contains some common definition for NAND Flash module.

Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "conf_nf.h"
#include "board.h"

Macros

#define NAND_COMMAND_COPYBACK_PROGRAM_1   0x85
 
#define NAND_COMMAND_COPYBACK_PROGRAM_2   0x10
 
#define NAND_COMMAND_COPYBACK_READ_1   0x00
 
#define NAND_COMMAND_COPYBACK_READ_2   0x35
 
#define NAND_COMMAND_ERASE_1   0x60
 
#define NAND_COMMAND_ERASE_2   0xD0
 
#define NAND_COMMAND_RANDOM_IN   0x85
 
#define NAND_COMMAND_RANDOM_OUT   0x05
 
#define NAND_COMMAND_RANDOM_OUT_2   0xE0
 
#define NAND_COMMAND_READ_1   0x00
 
#define NAND_COMMAND_READ_2   0x30
 
#define NAND_COMMAND_READ_A   0x00
 
#define NAND_COMMAND_READ_C   0x50
 
#define NAND_COMMAND_READID   0x90
 
#define NAND_COMMAND_RESET   0xFF
 
#define NAND_COMMAND_STATUS   0x70
 
#define NAND_COMMAND_WRITE_1   0x80
 
#define NAND_COMMAND_WRITE_2   0x10
 
#define NAND_COMMON_ERROR_BADBLOCK   12
 
#define NAND_COMMON_ERROR_BLOCKNOTMAPPED   2
 
#define NAND_COMMON_ERROR_CANNOTCOPY   14
 
#define NAND_COMMON_ERROR_CANNOTERASE   13
 
#define NAND_COMMON_ERROR_CANNOTREAD   6
 
#define NAND_COMMON_ERROR_CANNOTWRITE   7
 
#define NAND_COMMON_ERROR_CORRUPTEDDATA   9
 
#define NAND_COMMON_ERROR_ECC_NOT_COMPATIBLE   15
 
#define NAND_COMMON_ERROR_MAPPINGNOTFOUND   5
 
#define NAND_COMMON_ERROR_NOBLOCKFOUND   4
 
#define NAND_COMMON_ERROR_NOMAPPING   11
 
#define NAND_COMMON_ERROR_NOMOREBLOCKS   1
 NAND Flash maximum supported values Since no memory allocation is available, limits have been set on various characteristics of a NAND Flash chip: More...
 
#define NAND_COMMON_ERROR_OUTOFBOUNDS   3
 
#define NAND_COMMON_ERROR_UNKNOWNMODEL   8
 
#define NAND_COMMON_ERROR_WRONGSTATUS   10
 
#define NAND_STATUS_ERROR   (1 << 0)
 
#define NAND_STATUS_READY   (1 << 6)
 

#define NAND_COMMAND_COPYBACK_PROGRAM_1   0x85

Referenced by copy_page().

#define NAND_COMMAND_COPYBACK_PROGRAM_2   0x10

Referenced by copy_page().

#define NAND_COMMAND_COPYBACK_READ_1   0x00

Referenced by copy_page().

#define NAND_COMMAND_COPYBACK_READ_2   0x35

Referenced by copy_page().

#define NAND_COMMAND_ERASE_1   0x60

Referenced by erase_block().

#define NAND_COMMAND_ERASE_2   0xD0

Referenced by erase_block().

#define NAND_COMMAND_RANDOM_IN   0x85
#define NAND_COMMAND_RANDOM_OUT   0x05
#define NAND_COMMAND_RANDOM_OUT_2   0xE0
#define NAND_COMMAND_READ_1   0x00
#define NAND_COMMAND_READ_2   0x30
#define NAND_COMMAND_READ_A   0x00
#define NAND_COMMAND_READ_C   0x50
#define NAND_COMMAND_READID   0x90

Referenced by nand_flash_raw_read_id().

#define NAND_COMMAND_RESET   0xFF

Referenced by nand_flash_raw_reset().

#define NAND_COMMAND_STATUS   0x70

Referenced by check_status().

#define NAND_COMMAND_WRITE_1   0x80

Referenced by write_page().

#define NAND_COMMAND_WRITE_2   0x10

Referenced by write_page().

#define NAND_COMMON_ERROR_BLOCKNOTMAPPED   2
#define NAND_COMMON_ERROR_CANNOTCOPY   14

Referenced by copy_page().

#define NAND_COMMON_ERROR_CANNOTERASE   13

Referenced by erase_block().

#define NAND_COMMON_ERROR_CANNOTREAD   6
#define NAND_COMMON_ERROR_CANNOTWRITE   7

Referenced by copy_page(), and write_page().

#define NAND_COMMON_ERROR_CORRUPTEDDATA   9
#define NAND_COMMON_ERROR_ECC_NOT_COMPATIBLE   15
#define NAND_COMMON_ERROR_MAPPINGNOTFOUND   5
#define NAND_COMMON_ERROR_NOBLOCKFOUND   4
#define NAND_COMMON_ERROR_NOMAPPING   11
#define NAND_COMMON_ERROR_NOMOREBLOCKS   1

NAND Flash maximum supported values Since no memory allocation is available, limits have been set on various characteristics of a NAND Flash chip:

Maximums

  • NAND_COMMON_MAX_BLOCK_NUMBER
  • NAND_COMMON_MAX_PAGES_PER_BLOCK
  • NAND_COMMON_MAX_PAGE_SIZE
  • NAND_COMMON_MAX_PAGE_SPARE_SIZE
  • NAND_COMMON_MAX_SPARE_ECC_BYTES
  • NAND_COMMON_MAX_SPARE_EXTRA_BYTES NAND Flash error codes NAND Flash API methods return either 0 (indicating that there was no error), or one of the following error codes:
  • NAND_COMMON_ERROR_NOMOREBLOCKS
  • NAND_COMMON_ERROR_BLOCKNOTMAPPED
  • NAND_COMMON_ERROR_OUTOFBOUNDS
  • NAND_COMMON_ERROR_NOBLOCKFOUND
  • NAND_COMMON_ERROR_MAPPINGNOTFOUND
  • NAND_COMMON_ERROR_CANNOTREAD
  • NAND_COMMON_ERROR_CANNOTWRITE
  • NAND_COMMON_ERROR_UNKNOWNMODEL
  • NAND_COMMON_ERROR_CORRUPTEDDATA
  • NAND_COMMON_ERROR_WRONGSTATUS
  • NAND_COMMON_ERROR_NOMAPPING
  • NAND_COMMON_ERROR_BADBLOCK
  • NAND_COMMON_ERROR_CANNOTERASE
  • NAND_COMMON_ERROR_CANNOTCOPY
  • NAND_COMMON_ERROR_ECC_NOT_COMPATIBLE
#define NAND_COMMON_ERROR_OUTOFBOUNDS   3
#define NAND_COMMON_ERROR_UNKNOWNMODEL   8
#define NAND_COMMON_ERROR_WRONGSTATUS   10
#define NAND_STATUS_ERROR   (1 << 0)

Referenced by check_status().

#define NAND_STATUS_READY   (1 << 6)

Referenced by check_status().