Resistive Touch Service.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | DEBOUNCE_TIME 6 /* 10 * 6 = 60 ms */ |
Delay for pushbutton debouncing (the time-base is 10 ms). More... | |
#define | MULTI_FACTOR 1024 |
The multiplicator value used by the calibration algorithm to avoid working on float values. More... | |
#define | POINTS_MAX_ERROR 5 |
Maximum difference in pixels between the test point and the measured point. More... | |
Typedefs | |
typedef enum rtouch_pen_state_enum | rtouch_pen_state_t |
Pen state definitions. More... | |
Enumerations | |
enum | rtouch_pen_state_enum { STATE_PEN_RELEASED = 0, STATE_PEN_PRESSED = 1, STATE_PEN_DEBOUNCE = 2 } |
Pen state definitions. More... | |
Functions | |
uint32_t | rtouch_compute_calibration (rtouch_calibration_point_t *points) |
Perform the calibration process using the provided points. More... | |
void | rtouch_disable (void) |
Disable the resistive touch service. More... | |
static void | rtouch_disable_pen_interrupt (void) |
Disable PEN interrupts. More... | |
void | rtouch_enable (void) |
Enable the resistive touch service for touch detection and sampling. More... | |
static void | rtouch_enable_pen_interrupt (void) |
Enable PEN interrupts. More... | |
static void | rtouch_get_calibrated_point (const rtouch_point_t *p_raw, rtouch_point_t *p_point) |
Interpolate the provided raw measurements using the previously calculated slope. More... | |
rtouch_event_handler_t | rtouch_get_event_handler (void) |
Get the touch event handler. More... | |
uint32_t | rtouch_init (const uint32_t ul_width, const uint32_t ul_height) |
Initialize the resistive touch service. More... | |
static uint8_t | rtouch_is_calibrated (void) |
Indicates if the calibration of the touch screen is Ok. More... | |
static void | rtouch_pen_handler (void) |
Handler for PEN interrupts. More... | |
void | rtouch_process (void) |
Core function for resistive touch service. More... | |
void | rtouch_set_calibration_parameter (int32_t xslope, int32_t yslope, int32_t rawx, int32_t rawy) |
Set calibration parameters when manual calibration procedure is not performed. More... | |
void | rtouch_set_event_handler (rtouch_event_handler_t handler) |
Set the touch event handler. More... | |
void | rtouch_wait_pressed (void) |
Wait touch pressed. More... | |
void | rtouch_wait_released (void) |
Wait touch released. More... | |
Variables | |
static rtouch_calibration_point_t | calibration_point_0 |
First calibration point (required for processing point). More... | |
static rtouch_event_t | event |
Current touch screen event. More... | |
static rtouch_event_handler_t | event_handler |
User event handler function pointer. More... | |
static int32_t | g_l_xslope |
Slope for interpoling touchscreen measurements along the X-axis. More... | |
static int32_t | g_l_yslope |
Slope for interpoling touchscreen measurements along the Y-axis. More... | |
static uint32_t | g_ul_height |
static volatile uint32_t | g_ul_is_calibrated = 0 |
indicates if the touch screen has been calibrated. More... | |
static volatile uint32_t | g_ul_is_rtouch_enabled = 0 |
Touch screen enable flag. More... | |
static volatile uint32_t | g_ul_timepress = 0 |
last time when the pen is pressed on the touchscreen. More... | |
static volatile uint32_t | g_ul_timerelease = 0 |
last time when the pen is released. More... | |
static volatile uint32_t | g_ul_timestamp = 0 |
Global g_ul_timestamp in milliseconds since start of application. More... | |
static uint32_t | g_ul_width |
Panel size. More... | |
static volatile rtouch_pen_state_t | pen_state = STATE_PEN_RELEASED |
Pen current state. More... | |
#define DEBOUNCE_TIME 6 /* 10 * 6 = 60 ms */ |
Delay for pushbutton debouncing (the time-base is 10 ms).
Referenced by rtouch_process().
#define MULTI_FACTOR 1024 |
The multiplicator value used by the calibration algorithm to avoid working on float values.
Referenced by rtouch_compute_calibration(), and rtouch_get_calibrated_point().
#define POINTS_MAX_ERROR 5 |
Maximum difference in pixels between the test point and the measured point.
Referenced by rtouch_compute_calibration(), and rtouch_process().
typedef enum rtouch_pen_state_enum rtouch_pen_state_t |
Pen state definitions.
|
static |
Disable PEN interrupts.
Disable the interrupt
References rtouch_disable_interrupt.
Referenced by rtouch_disable().
|
static |
Enable PEN interrupts.
Initialize interrupts
Enable the interrupt
References rtouch_enable_interrupt, rtouch_pen_handler(), and rtouch_set_handler.
Referenced by rtouch_enable().
|
static |
Interpolate the provided raw measurements using the previously calculated slope.
The resulting x and y coordinates are stored in an array.
p_data | Raw measurement data. |
p_point | Array in which x and y will be stored. |
References g_l_xslope, g_l_yslope, g_ul_height, g_ul_width, MULTI_FACTOR, rtouch_calibration_point_struct::panel, rtouch_calibration_point_struct::raw, rtouch_point_struct::x, and rtouch_point_struct::y.
Referenced by rtouch_compute_calibration(), and rtouch_process().
|
static |
Indicates if the calibration of the touch screen is Ok.
References g_ul_is_calibrated.
Referenced by rtouch_process().
|
static |
Handler for PEN interrupts.
Check if the touch screen has been pressed
References g_ul_timestamp, rtouch_is_pressed, STATE_PEN_DEBOUNCE, STATE_PEN_PRESSED, and STATE_PEN_RELEASED.
Referenced by rtouch_enable_pen_interrupt().
|
static |
First calibration point (required for processing point).
|
static |
Current touch screen event.
Referenced by win_process_events(), win_queue_command_event(), win_queue_keyboard_event(), win_queue_pointer_event(), wtk_button_handler(), wtk_check_box_handler(), wtk_frame_handler(), wtk_icon_button_handler(), wtk_radio_button_handler(), and wtk_slider_handler().
|
static |
User event handler function pointer.
Referenced by rtouch_get_event_handler(), and rtouch_process().
|
static |
Slope for interpoling touchscreen measurements along the X-axis.
Referenced by rtouch_get_calibrated_point().
|
static |
Slope for interpoling touchscreen measurements along the Y-axis.
Referenced by rtouch_get_calibrated_point().
|
static |
Referenced by rtouch_get_calibrated_point().
|
static |
indicates if the touch screen has been calibrated.
If not, Callback functions are not called.
Referenced by rtouch_is_calibrated().
|
static |
Touch screen enable flag.
|
static |
last time when the pen is pressed on the touchscreen.
Referenced by rtouch_process().
|
static |
last time when the pen is released.
Referenced by rtouch_process().
|
static |
Global g_ul_timestamp in milliseconds since start of application.
Referenced by rtouch_pen_handler(), and rtouch_process().
|
static |
Panel size.
Referenced by rtouch_get_calibrated_point().
|
static |
Pen current state.