Microchip® Advanced Software Framework

udp_device.h File Reference

USB Device Driver for UDP.

Compliant with common UDD driver.

Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "preprocessor.h"
#include "conf_board.h"
#include "board.h"
#include "ioport.h"
#include "pio.h"
#include "pio_handler.h"

Macros

#define Is_udd_endpoint_status_enabled(status)   (Tst_bits(status, UDP_CSR_EPEDS))
 
#define Is_udd_endpoint_status_error(status)   (Tst_bits(status, UDP_CSR_ISOERROR))
 
#define Is_udd_endpoint_status_in(status)   (Tst_bits(status, UDP_CSR_DIR))
 
#define Is_udd_endpoint_status_rx_all(status)   ((status & (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1)) == (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1))
 
#define Is_udd_endpoint_status_rx_any_bank(status)   (Tst_bits(status, UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK0))
 
#define Is_udd_endpoint_status_rx_bank0(status)   (Tst_bits(status, UDP_CSR_RX_DATA_BK0))
 
#define Is_udd_endpoint_status_rx_bank1(status)   (Tst_bits(status, UDP_CSR_RX_DATA_BK1))
 
#define Is_udd_endpoint_status_rx_setup(status)   (Tst_bits(status, UDP_CSR_RXSETUP))
 
#define Is_udd_endpoint_status_stall_pending(status)   (Tst_bits(status, UDP_CSR_STALLSENT|UDP_CSR_FORCESTALL))
 
#define Is_udd_endpoint_status_stall_sent(status)   (Tst_bits(status, UDP_CSR_STALLSENT))
 
#define Is_udd_endpoint_status_stalled(status)   (Tst_bits(status, UDP_CSR_FORCESTALL))
 
#define Is_udd_endpoint_status_tx_complete(status)   (Tst_bits(status, UDP_CSR_TXCOMP))
 
#define Is_udd_endpoint_status_tx_ready(status)   (Tst_bits(status, UDP_CSR_TXPKTRDY))
 
#define udd_get_endpoint_status(ep)   (UDP->UDP_CSR[ep])
 
#define udd_get_endpoint_status_byte_count(status)   (Rd_bitfield(status, UDP_CSR_RXBYTECNT_Msk))
 
#define udd_get_endpoint_status_toggle(status)   (Rd_bits(status, UDP_CSR_DTGLE))
 
#define udd_get_endpoint_status_type(status)   (Rd_bits(status, UDP_CSR_EPTYPE_Msk))
 
UDP Device properties

These macros give IP properties (from datasheets)

#define udd_get_endpoint_max_nbr()   (7)
 Get maximal number of endpoints (3S 4S 4E, 0~7) More...
 
#define UDD_MAX_PEP_NB   (udd_get_endpoint_max_nbr()+1)
 
#define udd_get_endpoint_bank_max_nbr(ep)   (((ep)==0||(ep)==3)?1:2)
 Get maximal number of banks of endpoint (3S, 1~2) More...
 
#define udd_get_endpoint_size_max(ep)   (((ep)==4||(ep)==5)?512:64)
 Get maximal size of endpoint (3S, 512/64) More...
 
#define udd_is_endpoint_support_iso(ep)   (((ep)==0||(ep)==3)?false:true)
 Get isochronous support (3S, endpoints 0 and 3 not support) More...
 
#define Is_udd_endpoint_dma_supported(ep)   (false)
 Get DMA support of endpoints (3S, always false) More...
 
#define Is_udd_endpoint_high_bw_supported(ep)   (false)
 Get High Band Width support of endpoints (3S, always false) More...
 
UDP Device vbus pin management

UDP peripheral does not support vbus management and it's monitored by a PIO pin.

This feature is optional, and it is enabled if USB_VBUS_PIN is defined in board.h and CONF_BOARD_USB_VBUS_DETECT defined in conf_board.h.

Note
ioport_init() must be invoked before using vbus pin functions since they use IOPORT API,
See Also
Common IOPORT API.
#define UDD_VBUS_DETECT
 
#define UDD_VBUS_IO   (defined(USB_VBUS_PIN) && UDD_VBUS_DETECT)
 
#define USB_VBUS_WKUP   0
 
#define udd_vbus_init(handler)
 
#define Is_udd_vbus_high()   ioport_get_pin_level(USB_VBUS_PIN)
 
#define Is_udd_vbus_low()   (!Is_udd_vbus_high())
 
#define udd_enable_vbus_interrupt()   pio_enable_pin_interrupt(USB_VBUS_PIN)
 
#define udd_disable_vbus_interrupt()   pio_disable_pin_interrupt(USB_VBUS_PIN)
 
#define udd_ack_vbus_interrupt(high)
 
UDP peripheral enable/disable
Warning
The UDP peripheral clock in the Power Management Controller (PMC) must be enabled before any read/write operations to the UDP registers including the UDP_TXVC register.
#define udd_enable_periph_ck()   pmc_enable_periph_clk(ID_UDP)
 
#define udd_disable_periph_ck()   pmc_disable_periph_clk(ID_UDP)
 
#define Is_udd_periph_ck_enabled()   pmc_is_periph_clk_enabled(ID_UDP)
 
UDP device attach control (by Pull-up)

These macros manage the UDP Device attach.

#define udd_detach_device()   ( Clr_bits(UDP->UDP_TXVC, UDP_TXVC_PUON))
 detaches from USB bus More...
 
#define udd_attach_device()   ( Set_bits(UDP->UDP_TXVC, UDP_TXVC_PUON))
 attaches to USB bus More...
 
#define Is_udd_detached()   (!Tst_bits(UDP->UDP_TXVC, UDP_TXVC_PUON))
 test if the device is detached More...
 
USBB UDP transceiver management

These macros allows to enable/disable pad and USBB hardware

#define udd_enable_transceiver()   ( Clr_bits(UDP->UDP_TXVC, UDP_TXVC_TXVDIS))
 
#define udd_disable_transceiver()   ( Set_bits(UDP->UDP_TXVC, UDP_TXVC_TXVDIS))
 
#define Is_udd_transceiver_enabled()   (!Tst_bits(UDP->UDP_TXVC, UDP_TXVC_TXVDIS))
 
UDP device bus events control

These macros manage the UDP Device bus events.

#define udd_disable_all_events()   (UDP->IDR = 0xFFFF)
 Manage misc events. More...
 
#define udd_disable_endpoint_events()   (UDP->IDR = 0xFF)
 
#define udd_enable_wakeups()   (UDP->UDP_IER = (UDP_IER_RXRSM|UDP_IER_EXTRSM|UDP_IER_WAKEUP))
 
#define udd_disable_wakeups()   (UDP->UDP_IDR = (UDP_IDR_RXRSM|UDP_IDR_EXTRSM|UDP_IDR_WAKEUP))
 
#define udd_ack_wakeups()   (UDP->UDP_ICR = (UDP_ICR_RXRSM|UDP_ICR_EXTRSM|UDP_ICR_WAKEUP))
 
#define Is_udd_any_wakeup()   (Tst_bits(UDP->UDP_ISR, (UDP_ICR_RXRSM|UDP_ICR_EXTRSM|UDP_ICR_WAKEUP)))
 
#define Is_udd_expected_wakeup()   ((UDP->UDP_ISR & (UDP_ICR_RXRSM|UDP_ICR_EXTRSM|UDP_ICR_WAKEUP)) & UDP->UDP_IMR)
 
#define udd_enable_remote_wake_up()   ( Set_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_RMWUPE))
 Manage remote wake-up event. More...
 
#define udd_disable_remote_wake_up()   ( Clr_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_RMWUPE))
 
#define Is_udd_remote_wake_up_enabled()   ( Tst_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_RMWUPE))
 
#define udd_initiate_remote_wake_up()
 
#define Is_udd_pending_remote_wake_up()   ( Tst_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_RSMINPR))
 
#define udd_enable_ext_resume_interrupt()   (UDP->UDP_IER = UDP_IER_EXTRSM)
 Manage end of resume event (ext/rx resume) The USB controller detects a valid "End of Resume" signal initiated by the host or detects a external "Resume" signal. More...
 
#define udd_disable_ext_resume_interrupt()   (UDP->UDP_IDR = UDP_IER_EXTRSM)
 
#define Is_udd_ext_resume_interrupt_enabled()   (Tst_bits(UDP->UDP_IMR, UDP_IMR_EXTRSM))
 
#define udd_ack_ext_resume()   (UDP->UDP_ICR = UDP_IER_EXTRSM)
 
#define Is_udd_ext_resume()   (Tst_bits(UDP->UDP_ISR, UDP_IER_EXTRSM))
 
#define udd_enable_resume_interrupt()   (UDP->UDP_IER = UDP_IER_RXRSM)
 
#define udd_disable_resume_interrupt()   (UDP->UDP_IDR = UDP_IDR_RXRSM)
 
#define Is_udd_resume_interrupt_enabled()   (Tst_bits(UDP->UDP_IMR, UDP_IMR_RXRSM))
 
#define udd_ack_resume()   (UDP->UDP_ICR = UDP_ICR_RXRSM)
 
#define Is_udd_resume()   (Tst_bits(UDP->UDP_ISR, UDP_ISR_RXRSM))
 
#define udd_enable_wake_up_interrupt()   (UDP->UDP_IER = UDP_IER_WAKEUP)
 Manage wake-up event (=usb line activity) The USB controller is reactivated by a filtered non-idle signal from the lines. More...
 
#define udd_disable_wake_up_interrupt()   (UDP->UDP_IDR = UDP_IDR_WAKEUP)
 
#define Is_udd_wake_up_interrupt_enabled()   (Tst_bits(UDP->UDP_IMR, UDP_IMR_WAKEUP))
 
#define udd_ack_wake_up()   (UDP->UDP_ICR = UDP_ICR_WAKEUP)
 
#define Is_udd_wake_up()   (Tst_bits(UDP->UDP_ISR, UDP_ISR_WAKEUP))
 
#define udd_ack_reset()   (UDP->UDP_ICR = UDP_ISR_ENDBUSRES)
 Manage reset event Set when a USB "End of Reset" has been detected. More...
 
#define Is_udd_reset()   (Tst_bits(UDP->UDP_ISR, UDP_ISR_ENDBUSRES))
 
#define udd_enable_sof_interrupt()   (UDP->UDP_IER = UDP_ISR_SOFINT)
 Manage start of frame event. More...
 
#define udd_disable_sof_interrupt()   (UDP->UDP_IDR = UDP_ISR_SOFINT)
 
#define Is_udd_sof_interrupt_enabled()   (Tst_bits(UDP->UDP_IMR, UDP_ISR_SOFINT))
 
#define udd_ack_sof()   (UDP->UDP_ICR = UDP_ISR_SOFINT)
 
#define Is_udd_sof()   (Tst_bits(UDP->UDP_ISR, UDP_ISR_SOFINT))
 
#define udd_frame_number()   (Rd_bitfield(UDP->UDP_FRM_NUM, UDP_FRM_NUM_FRM_NUM_Msk))
 
#define Is_udd_frame_number_crc_error()   (Tst_bits(UDP->UDP_FRM_NUM, UDP_FRM_NUM_FRM_ERR))
 
#define udd_enable_suspend_interrupt()   (UDP->UDP_IER = UDP_ISR_RXSUSP)
 Manage suspend event. More...
 
#define udd_disable_suspend_interrupt()   (UDP->UDP_IDR = UDP_ISR_RXSUSP)
 
#define Is_udd_suspend_interrupt_enabled()   (Tst_bits(UDP->UDP_IMR, UDP_ISR_RXSUSP))
 
#define udd_ack_suspend()   (UDP->UDP_ICR = UDP_ISR_RXSUSP)
 
#define udd_raise_suspend()   (UDP->UDP_ISR = UDP_ISR_RXSUSP)
 
#define Is_udd_suspend()   (Tst_bits(UDP->UDP_ISR, UDP_ISR_RXSUSP))
 
UDP device address control

These macros manage the UDP Device address.

#define udd_enable_address()   (Set_bits(UDP->UDP_FADDR, UDP_FADDR_FEN))
 enables USB device address More...
 
#define udd_disable_address()   (Clr_bits(UDP->UDP_FADDR, UDP_FADDR_FEN))
 disables USB device address More...
 
#define Is_udd_address_enabled()   (Tst_bits(UDP->UDP_FADDR, UDP_FADDR_FEN))
 
#define udd_configure_address(addr)   (Wr_bitfield(UDP->UDP_FADDR, UDP_FADDR_FADD_Msk, addr))
 configures the USB device address More...
 
#define udd_get_configured_address()   (Rd_bitfield(UDP->UDP_FADDR, UDP_FADDR_FADD_Msk))
 gets the currently configured USB device address More...
 
#define udd_enable_address_state()   (Set_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_FADDEN))
 sets the device in address state More...
 
#define udd_disable_address_state()   (Clr_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_FADDEN))
 bring back device to the default state More...
 
#define Is_udd_address_state_enabled()   (Tst_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_FADDEN))
 Check if the device is in address state. More...
 
UDP device configured control

These macros manage the UDP Device configure state.

#define udd_enable_configured_state()   (Set_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_CONFG))
 sets USB device in configured state More...
 
#define udd_disable_configured_state()   (Clr_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_CONFG))
 
#define Is_udd_configured_state_enabled()   (Tst_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_CONFG))
 
UDP Device endpoint drivers

These macros manage the common features of the endpoints.

#define UDP_REG_NO_EFFECT_1_ALL
 Generic macro for CSR register access. More...
 
#define udp_set_csr(ep, bits)
 
#define udp_clear_csr(ep, bits)
 
#define udp_write_csr(ep, mask, bits)
 
UDP Device endpoint configuration
#define udd_enable_endpoint(ep)   udp_set_csr(ep, UDP_CSR_EPEDS)
 enables the selected endpoint More...
 
#define udd_disable_endpoint(ep)   udp_clear_csr(ep, UDP_CSR_EPEDS)
 disables the selected endpoint More...
 
#define Is_udd_endpoint_enabled(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_EPEDS))
 tests if the selected endpoint is enabled More...
 
#define udd_reset_endpoint(ep)
 resets the selected endpoint More...
 
#define Is_udd_resetting_endpoint(ep)   (Tst_bits(UDP->UDP_RST_EP, UDP_RST_EP_EP0 << (ep)))
 tests if the selected endpoint is being reset More...
 
#define udd_configure_endpoint_type(ep, type)   udp_write_csr(ep, UDP_CSR_EPTYPE_Msk, type)
 configures the selected endpoint type (shifted) More...
 
#define udd_get_endpoint_type(ep)   (Rd_bits(UDP->UDP_CSR[ep], UDP_CSR_EPTYPE_Msk))
 gets the configured selected endpoint type (shifted) More...
 
#define Is_udd_endpoint_type_in(ep)   (Tst_bits(UDP->UDP_CSR[ep], 0x4 << UDP_CSR_EPTYPE_Pos))
 
#define udd_configure_endpoint_direction(ep, dir)   udp_write_csr(ep, UDP_CSR_DIR, (dir << 7) & UDP_CSR_DIR)
 configures the selected endpoint direction (shifted) More...
 
#define udd_set_endpoint_direction_in(ep)   udp_set_csr(ep, UDP_CSR_DIR)
 configures the selected endpoint direction as IN (shifted) More...
 
#define udd_get_endpoint_direction(ep)   (Rd_bits(UDP->UDP_CSR[ep], UDP_CSR_DIR))
 gets the configured selected endpoint direction (shifted) More...
 
#define Is_udd_endpoint_in(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_DIR))
 
#define udd_configure_endpoint(ep, type, dir)
 configures selected endpoint in one step (type and dir are not shifted definitions) More...
 
#define Is_udd_endpoint_configured(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_EPEDS))
 tests if current endpoint is configured (=enabled) More...
 
#define udd_control_direction()   (Rd_bits(UDP->UDP_CSR[0], UDP_CSR_DIR))
 returns the control direction More...
 
#define udd_data_toggle(ep)   (Rd_bits(UDP->UDP_CSR[ep], UDP_CSR_DTGLE))
 returns data toggle More...
 
UDP Device control endpoint interrupts

These macros control the endpoints interrupts.

#define udd_enable_endpoint_interrupt(ep)   (UDP->UDP_IER = UDP_IER_EP0INT << (ep))
 enables the selected endpoint interrupt More...
 
#define udd_disable_endpoint_interrupt(ep)   (UDP->UDP_IDR = UDP_IDR_EP0INT << (ep))
 disables the selected endpoint interrupt More...
 
#define Is_udd_endpoint_interrupt_enabled(ep)   (Tst_bits(UDP->UDP_IMR, UDP_IMR_EP0INT << (ep)))
 tests if the selected endpoint interrupt is enabled More...
 
#define Is_udd_endpoint_interrupt(ep)   (Tst_bits(UDP->UDP_ISR, UDP_ISR_EP0INT << (ep)))
 tests if an interrupt is triggered by the selected endpoint More...
 
#define udd_get_interrupt_endpoint_number()   (ctz(((UDP->UDP_ISR) & (UDP->UDP_IMR)) | (1 << UDD_MAX_PEP_NB)))
 returns the lowest endpoint number generating an endpoint interrupt or UDD_MAX_PEP_NB if none More...
 
UDP Device control endpoint errors

These macros control the endpoint errors.

#define Is_udd_endpoint_stall_pending(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_FORCESTALL|UDP_CSR_STALLSENT))
 
#define udd_enable_stall_handshake(ep)   udp_set_csr(ep, UDP_CSR_FORCESTALL)
 enables the STALL handshake More...
 
#define udd_disable_stall_handshake(ep)   udp_clear_csr(ep, UDP_CSR_FORCESTALL)
 disables the STALL handshake More...
 
#define Is_udd_endpoint_stall_requested(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_FORCESTALL))
 tests if STALL handshake request is running More...
 
#define Is_udd_stall(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_STALLSENT))
 tests if STALL sent More...
 
#define udd_ack_stall(ep)   udp_clear_csr(ep, UDP_CSR_STALLSENT)
 acks STALL sent More...
 
#define Is_udd_crc_error(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_ISOERROR))
 tests if CRC ERROR ISO detected More...
 
#define udd_ack_crc_error(ep)   udp_clear_csr(ep, UDP_CSR_ISOERROR)
 acks CRC ERROR ISO detected More...
 
UDP Device control endpoint transfer

These macros control the endpoint transfer.

#define udd_byte_count(ep)   (Rd_bitfield(UDP->UDP_CSR[ep], UDP_CSR_RXBYTECNT_Msk))
 returns the byte count More...
 
#define Is_udd_all_banks_received(ep)   ((UDP->UDP_CSR[ep] & (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1)) == (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1))
 test if both banks received More...
 
#define Is_udd_any_bank_received(ep)   (Tst_bits(UDP->UDP_CSR[ep], (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1)))
 test if Any of the Bank received More...
 
#define Is_udd_bank0_received(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_RX_DATA_BK0))
 test if Bank 0 received More...
 
#define udd_ack_bank0_received(ep)   udp_clear_csr(ep, UDP_CSR_RX_DATA_BK0)
 acks Bank 0 received More...
 
#define Is_udd_bank1_received(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_RX_DATA_BK1))
 test if Bank 1 received More...
 
#define udd_ack_bank1_received(ep)   udp_clear_csr(ep, UDP_CSR_RX_DATA_BK1)
 acks Bank 1 received More...
 
#define udd_nb_banks_received(ep)
 returns the number of received banks More...
 
#define Is_udd_setup_received(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_RXSETUP))
 tests if SETUP received More...
 
#define udd_ack_setup_received(ep)   udp_clear_csr(ep, UDP_CSR_RXSETUP)
 acks SETUP received More...
 
#define Is_udd_in_pending(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_TXPKTRDY|UDP_CSR_TXCOMP))
 tests if IN pending (TX ready or IN sending) More...
 
#define Is_udd_in_sent(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_TXCOMP))
 tests if IN sending More...
 
#define udd_ack_in_sent(ep)   udp_clear_csr(ep, UDP_CSR_TXCOMP)
 acks IN sending More...
 
#define Is_udd_transmit_ready(ep)   (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_TXPKTRDY))
 tests if transmit packet is ready More...
 
#define udd_set_transmit_ready(ep)   udp_set_csr(ep, UDP_CSR_TXPKTRDY)
 set transmit packet ready More...
 
#define udd_kill_data_in_fifo(ep, dual_bank)
 cancel transmission data held in banks (if TXPKTRDY is set) More...
 
#define udd_endpoint_fifo_read(ep)   (UDP->UDP_FDR[ep])
 read one byte from endpoint fifo More...
 
#define udd_endpoint_fifo_write(ep, byte)
 write one byte to endpoint fifo More...
 

Functions

static __always_inline void io_pin_init (uint32_t pin, uint32_t flags, IRQn_Type port_irqn, uint8_t irq_level, void(*handler)(uint32_t, uint32_t), uint32_t wkup)
 

#define Is_udd_address_enabled ( )    (Tst_bits(UDP->UDP_FADDR, UDP_FADDR_FEN))
#define Is_udd_address_state_enabled ( )    (Tst_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_FADDEN))

Check if the device is in address state.

Referenced by udd_getaddress().

#define Is_udd_all_banks_received (   ep)    ((UDP->UDP_CSR[ep] & (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1)) == (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1))

test if both banks received

#define Is_udd_any_bank_received (   ep)    (Tst_bits(UDP->UDP_CSR[ep], (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1)))

test if Any of the Bank received

Referenced by udd_ep_abort(), and udd_ep_interrupt().

#define Is_udd_bank0_received (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_RX_DATA_BK0))

test if Bank 0 received

Referenced by udd_ctrl_in_sent(), udd_ctrl_interrupt(), and udd_ep_ack_out_received().

#define Is_udd_bank1_received (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_RX_DATA_BK1))

test if Bank 1 received

Referenced by udd_ep_ack_out_received().

#define Is_udd_configured_state_enabled ( )    (Tst_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_CONFG))
#define Is_udd_crc_error (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_ISOERROR))

tests if CRC ERROR ISO detected

#define Is_udd_endpoint_configured (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_EPEDS))

tests if current endpoint is configured (=enabled)

#define Is_udd_endpoint_enabled (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_EPEDS))

tests if the selected endpoint is enabled

Referenced by udd_ep_alloc(), udd_ep_run(), and udd_ep_wait_stall_clear().

#define Is_udd_endpoint_in (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_DIR))
#define Is_udd_endpoint_interrupt (   ep)    (Tst_bits(UDP->UDP_ISR, UDP_ISR_EP0INT << (ep)))

tests if an interrupt is triggered by the selected endpoint

Referenced by udd_ctrl_interrupt().

#define Is_udd_endpoint_interrupt_enabled (   ep)    (Tst_bits(UDP->UDP_IMR, UDP_IMR_EP0INT << (ep)))

tests if the selected endpoint interrupt is enabled

Referenced by udd_ep_interrupt().

#define Is_udd_endpoint_stall_pending (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_FORCESTALL|UDP_CSR_STALLSENT))

Referenced by udd_ep_is_halted().

#define Is_udd_endpoint_stall_requested (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_FORCESTALL))

tests if STALL handshake request is running

Referenced by udd_ep_clear_halt(), udd_ep_out_received(), udd_ep_run(), and udd_ep_wait_stall_clear().

#define Is_udd_endpoint_status_enabled (   status)    (Tst_bits(status, UDP_CSR_EPEDS))
#define Is_udd_endpoint_status_error (   status)    (Tst_bits(status, UDP_CSR_ISOERROR))
#define Is_udd_endpoint_status_in (   status)    (Tst_bits(status, UDP_CSR_DIR))
#define Is_udd_endpoint_status_rx_all (   status)    ((status & (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1)) == (UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK1))
#define Is_udd_endpoint_status_rx_any_bank (   status)    (Tst_bits(status, UDP_CSR_RX_DATA_BK0|UDP_CSR_RX_DATA_BK0))
#define Is_udd_endpoint_status_rx_bank0 (   status)    (Tst_bits(status, UDP_CSR_RX_DATA_BK0))
#define Is_udd_endpoint_status_rx_bank1 (   status)    (Tst_bits(status, UDP_CSR_RX_DATA_BK1))
#define Is_udd_endpoint_status_rx_setup (   status)    (Tst_bits(status, UDP_CSR_RXSETUP))
#define Is_udd_endpoint_status_stall_pending (   status)    (Tst_bits(status, UDP_CSR_STALLSENT|UDP_CSR_FORCESTALL))
#define Is_udd_endpoint_status_stall_sent (   status)    (Tst_bits(status, UDP_CSR_STALLSENT))
#define Is_udd_endpoint_status_stalled (   status)    (Tst_bits(status, UDP_CSR_FORCESTALL))
#define Is_udd_endpoint_status_tx_complete (   status)    (Tst_bits(status, UDP_CSR_TXCOMP))
#define Is_udd_endpoint_status_tx_ready (   status)    (Tst_bits(status, UDP_CSR_TXPKTRDY))
#define Is_udd_endpoint_type_in (   ep)    (Tst_bits(UDP->UDP_CSR[ep], 0x4 << UDP_CSR_EPTYPE_Pos))

Referenced by udd_ep_finish_job().

#define Is_udd_in_pending (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_TXPKTRDY|UDP_CSR_TXCOMP))

tests if IN pending (TX ready or IN sending)

Referenced by udd_ep_run().

#define Is_udd_in_sent (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_TXCOMP))

tests if IN sending

Referenced by udd_ctrl_interrupt(), and udd_ep_interrupt().

#define Is_udd_resetting_endpoint (   ep)    (Tst_bits(UDP->UDP_RST_EP, UDP_RST_EP_EP0 << (ep)))

tests if the selected endpoint is being reset

#define Is_udd_setup_received (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_RXSETUP))

tests if SETUP received

Referenced by udd_ctrl_interrupt().

#define Is_udd_stall (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_STALLSENT))

tests if STALL sent

Referenced by udd_ctrl_interrupt(), and udd_ep_interrupt().

#define Is_udd_transmit_ready (   ep)    (Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_TXPKTRDY))

tests if transmit packet is ready

Referenced by udd_ep_abort(), and udd_ep_set_halt().

#define udd_ack_bank0_received (   ep)    udp_clear_csr(ep, UDP_CSR_RX_DATA_BK0)

acks Bank 0 received

Referenced by udd_ctrl_out_received(), and udd_ep_ack_out_received().

#define udd_ack_bank1_received (   ep)    udp_clear_csr(ep, UDP_CSR_RX_DATA_BK1)

acks Bank 1 received

Referenced by udd_ep_ack_out_received().

#define udd_ack_crc_error (   ep)    udp_clear_csr(ep, UDP_CSR_ISOERROR)

acks CRC ERROR ISO detected

#define udd_ack_in_sent (   ep)    udp_clear_csr(ep, UDP_CSR_TXCOMP)

acks IN sending

Referenced by udd_ctrl_in_sent(), udd_ep_abort(), and udd_ep_interrupt().

#define udd_ack_setup_received (   ep)    udp_clear_csr(ep, UDP_CSR_RXSETUP)

acks SETUP received

Referenced by udd_ctrl_setup_received().

#define udd_ack_stall (   ep)    udp_clear_csr(ep, UDP_CSR_STALLSENT)

acks STALL sent

Referenced by udd_ctrl_interrupt(), udd_ep_clear_halt(), and udd_ep_interrupt().

#define udd_byte_count (   ep)    (Rd_bitfield(UDP->UDP_CSR[ep], UDP_CSR_RXBYTECNT_Msk))

returns the byte count

Referenced by udd_ctrl_out_received(), udd_ctrl_setup_received(), and udd_ep_out_received().

#define udd_configure_address (   addr)    (Wr_bitfield(UDP->UDP_FADDR, UDP_FADDR_FADD_Msk, addr))

configures the USB device address

Referenced by udd_reset_ep_ctrl(), and udd_set_address().

#define udd_configure_endpoint (   ep,
  type,
  dir 
)
Value:
do { \
(UDP_CSR_EPTYPE_Msk \
|UDP_CSR_DIR|UDP_CSR_EPEDS), \
((((type) << UDP_CSR_EPTYPE_Pos)\
& UDP_CSR_EPTYPE_Msk)\
|(((dir) << 7) & UDP_CSR_DIR) \
|(UDP_CSR_EPEDS))); \
} while(0)
#define udp_write_csr(ep, mask, bits)
Definition: udp_device.h:318

configures selected endpoint in one step (type and dir are not shifted definitions)

Referenced by udd_ep_alloc(), and udd_reset_ep_ctrl().

#define udd_configure_endpoint_direction (   ep,
  dir 
)    udp_write_csr(ep, UDP_CSR_DIR, (dir << 7) & UDP_CSR_DIR)

configures the selected endpoint direction (shifted)

#define udd_configure_endpoint_type (   ep,
  type 
)    udp_write_csr(ep, UDP_CSR_EPTYPE_Msk, type)

configures the selected endpoint type (shifted)

#define udd_control_direction ( )    (Rd_bits(UDP->UDP_CSR[0], UDP_CSR_DIR))

returns the control direction

#define udd_data_toggle (   ep)    (Rd_bits(UDP->UDP_CSR[ep], UDP_CSR_DTGLE))

returns data toggle

#define udd_disable_address ( )    (Clr_bits(UDP->UDP_FADDR, UDP_FADDR_FEN))

disables USB device address

Referenced by udd_set_address().

#define udd_disable_address_state ( )    (Clr_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_FADDEN))

bring back device to the default state

Referenced by ISR(), and udd_set_address().

#define udd_disable_configured_state ( )    (Clr_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_CONFG))

Referenced by ISR().

#define udd_disable_endpoint (   ep)    udp_clear_csr(ep, UDP_CSR_EPEDS)

disables the selected endpoint

Referenced by udd_ep_free().

#define udd_disable_endpoint_interrupt (   ep)    (UDP->UDP_IDR = UDP_IDR_EP0INT << (ep))

disables the selected endpoint interrupt

Referenced by udd_ep_abort(), udd_ep_interrupt(), and udd_ep_out_received().

#define udd_disable_stall_handshake (   ep)    udp_clear_csr(ep, UDP_CSR_FORCESTALL)

disables the STALL handshake

Referenced by udd_ep_clear_halt().

#define udd_enable_address ( )    (Set_bits(UDP->UDP_FADDR, UDP_FADDR_FEN))

enables USB device address

Referenced by udd_reset_ep_ctrl(), and udd_set_address().

#define udd_enable_address_state ( )    (Set_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_FADDEN))

sets the device in address state

Referenced by udd_set_address().

#define udd_enable_configured_state ( )    (Set_bits(UDP->UDP_GLB_STAT, UDP_GLB_STAT_CONFG))

sets USB device in configured state

#define udd_enable_endpoint (   ep)    udp_set_csr(ep, UDP_CSR_EPEDS)

enables the selected endpoint

Referenced by udd_reset_ep_ctrl().

#define udd_enable_endpoint_interrupt (   ep)    (UDP->UDP_IER = UDP_IER_EP0INT << (ep))

enables the selected endpoint interrupt

Referenced by udd_ep_run(), udd_ep_set_halt(), and udd_reset_ep_ctrl().

#define udd_enable_stall_handshake (   ep)    udp_set_csr(ep, UDP_CSR_FORCESTALL)

enables the STALL handshake

Referenced by udd_ctrl_stall_data(), udd_ep_interrupt(), and udd_ep_set_halt().

#define udd_endpoint_fifo_read (   ep)    (UDP->UDP_FDR[ep])

read one byte from endpoint fifo

Referenced by udd_ctrl_out_received(), udd_ctrl_setup_received(), and udd_ep_out_received().

#define udd_endpoint_fifo_write (   ep,
  byte 
)
Value:
do { \
UDP->UDP_FDR[ep] = byte; \
} while (0)

write one byte to endpoint fifo

Referenced by udd_ctrl_in_sent(), and udd_ep_write_fifo().

#define udd_get_configured_address ( )    (Rd_bitfield(UDP->UDP_FADDR, UDP_FADDR_FADD_Msk))

gets the currently configured USB device address

Referenced by udd_getaddress().

#define udd_get_endpoint_direction (   ep)    (Rd_bits(UDP->UDP_CSR[ep], UDP_CSR_DIR))

gets the configured selected endpoint direction (shifted)

#define udd_get_endpoint_status (   ep)    (UDP->UDP_CSR[ep])
#define udd_get_endpoint_status_byte_count (   status)    (Rd_bitfield(status, UDP_CSR_RXBYTECNT_Msk))
#define udd_get_endpoint_status_toggle (   status)    (Rd_bits(status, UDP_CSR_DTGLE))
#define udd_get_endpoint_status_type (   status)    (Rd_bits(status, UDP_CSR_EPTYPE_Msk))
#define udd_get_endpoint_type (   ep)    (Rd_bits(UDP->UDP_CSR[ep], UDP_CSR_EPTYPE_Msk))

gets the configured selected endpoint type (shifted)

Referenced by udd_ep_interrupt().

#define udd_get_interrupt_endpoint_number ( )    (ctz(((UDP->UDP_ISR) & (UDP->UDP_IMR)) | (1 << UDD_MAX_PEP_NB)))

returns the lowest endpoint number generating an endpoint interrupt or UDD_MAX_PEP_NB if none

#define udd_kill_data_in_fifo (   ep,
  dual_bank 
)
Value:
do { \
if ((dual_bank)) { \
udp_clear_csr(ep, UDP_CSR_TXPKTRDY); \
while ( Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_TXPKTRDY));\
udp_set_csr(ep, UDP_CSR_TXPKTRDY); \
while (!Tst_bits(UDP->UDP_CSR[ep], UDP_CSR_TXPKTRDY));\
} \
udp_clear_csr(ep, UDP_CSR_TXPKTRDY); \
} while (0)
#define udp_clear_csr(ep, bits)
Definition: udp_device.h:305
#define Tst_bits(value, mask)
Tests the bits of a value specified by a given bit-mask.
Definition: compiler.h:503
#define udp_set_csr(ep, bits)
Definition: udp_device.h:292

cancel transmission data held in banks (if TXPKTRDY is set)

Referenced by udd_ep_abort().

#define udd_nb_banks_received (   ep)
Value:
(Rd_bitfield(UDP->UDP_CSR[ep], UDP_CSR_RX_DATA_BK0) + \
Rd_bitfield(UDP->UDP_CSR[ep], UDP_CSR_RX_DATA_BK1))
#define Rd_bitfield(value, mask)
Reads the bit-field of a value specified by a given bit-mask.
Definition: compiler.h:539

returns the number of received banks

#define udd_reset_endpoint (   ep)
Value:
do { \
Set_bits(UDP->UDP_RST_EP, UDP_RST_EP_EP0 << (ep));\
while (!(UDP->UDP_RST_EP & (UDP_RST_EP_EP0 << (ep))));\
Clr_bits(UDP->UDP_RST_EP, UDP_RST_EP_EP0 << (ep));\
} while(0)
#define Clr_bits(lvalue, mask)
Clears the bits of a C lvalue specified by a given bit-mask.
Definition: compiler.h:512
#define Set_bits(lvalue, mask)
Sets the bits of a C lvalue specified by a given bit-mask.
Definition: compiler.h:521

resets the selected endpoint

Referenced by udd_ep_abort(), udd_ep_alloc(), and udd_ep_clear_halt().

#define udd_set_endpoint_direction_in (   ep)    udp_set_csr(ep, UDP_CSR_DIR)

configures the selected endpoint direction as IN (shifted)

Referenced by udd_ctrl_setup_received().

#define udd_set_transmit_ready (   ep)    udp_set_csr(ep, UDP_CSR_TXPKTRDY)

set transmit packet ready

Referenced by udd_ctrl_in_sent(), udd_ctrl_send_zlp_in(), udd_ep_in_sent(), and udd_ep_interrupt().

#define udp_clear_csr (   ep,
  bits 
)
Value:
do { \
volatile uint32_t reg; \
reg = UDP->UDP_CSR[ep]; \
reg &= ~(bits); \
UDP->UDP_CSR[ep] = reg; \
while (UDP->UDP_CSR[ep] & bits); \
} while (0)
#define UDP_REG_NO_EFFECT_1_ALL
Generic macro for CSR register access.
Definition: udp_device.h:283

Clears specified bit(s) in the UDP_CSR.

Parameters
epEndpoint number.
bitsBitmap to set to 0.
#define UDP_REG_NO_EFFECT_1_ALL
Value:
(UDP_CSR_RX_DATA_BK0 |\
UDP_CSR_RX_DATA_BK1 |\
UDP_CSR_STALLSENT |\
UDP_CSR_RXSETUP |\
UDP_CSR_TXCOMP)

Generic macro for CSR register access.

Note
Due to synchronization between MCK and UDPCK, the software application must wait for the end of the write operation before executing another write by polling the bits which must be set/cleared.
In a preemptive environment, set or clear the flag and wait for a time of 1 UDPCK clock cycle and 1 peripheral clock cycle. However, RX_DATA_BK0, TXPKTRDY, RX_DATA_BK1 require wait times of 3 UDPCK clock cycles and 5 peripheral clock cycles before accessing DPR.Bitmap for all status bits in CSR that are not effected by a value 1.
#define udp_set_csr (   ep,
  bits 
)
Value:
do { \
volatile uint32_t reg; \
reg = UDP->UDP_CSR[ep]; \
reg |= (bits); \
UDP->UDP_CSR[ep] = reg; \
while ((UDP->UDP_CSR[ep] & bits) != bits); \
} while (0)
#define UDP_REG_NO_EFFECT_1_ALL
Generic macro for CSR register access.
Definition: udp_device.h:283

Sets specified bit(s) in the UDP_CSR.

Parameters
epEndpoint number.
bitsBitmap to set to 1.
#define udp_write_csr (   ep,
  mask,
  bits 
)
Value:
do { \
volatile uint32_t reg; \
reg = UDP->UDP_CSR[ep]; \
reg &= ~(mask); \
reg |= bits & mask; \
UDP->UDP_CSR[ep] = reg; \
while ((UDP->UDP_CSR[ep] & bits) != bits); \
} while (0);
#define UDP_REG_NO_EFFECT_1_ALL
Generic macro for CSR register access.
Definition: udp_device.h:283

Write specified bit(s) in the UDP_CSR.

Parameters
epEndpoint number.
bitsBitmap to write.

static __always_inline void io_pin_init ( uint32_t  pin,
uint32_t  flags,
IRQn_Type  port_irqn,
uint8_t  irq_level,
void(*)(uint32_t, uint32_t)  handler,
uint32_t  wkup 
)
static