The Widget toolkit implements many common widgets for use on a graphical display using the functionality of Window system and Graphics library.
The following widgets are implemented:
This component driver depends on the following modules:
Modules | |
Basic frame widget | |
Basic frame widget provides a frame with only a background color. | |
Button widget | |
Check box widget | |
Frame widget | |
Frame widget provides a frame with border and a title bar. | |
Icon button widget | |
Label widget | |
Plot widget | |
Progress bar widget | |
Radio button widget | |
Slider widget | |
Typedefs | |
typedef uint16_t | wtk_string_size_t |
Datatype holding the length of strings. More... | |
Functions | |
void | wtk_copy_string (char *dest, char const *source) |
This function copies the string contents, including the zero terminator, from source to destination. More... | |
uint8_t | wtk_rescale_value (uint8_t value, uint8_t from_scale, uint8_t to_scale) |
Rescale 8-bit value. More... | |
#define | WTK_FRAME_RIGHTBORDER 2 |
Right frame border size. More... | |
#define | WTK_FRAME_TOPBORDER 2 |
Top frame border size. More... | |
#define | WTK_FRAME_BOTTOMBORDER 4 |
Bottom frame border size. More... | |
#define | WTK_FRAME_RESIZE_RADIUS 7 |
Radius of resize handle (second quadrant of circle). More... | |
#define | WTK_FRAME_RESIZE_WIDTH (WTK_FRAME_RESIZE_RADIUS + 1) |
Width of resize handle. More... | |
#define | WTK_FRAME_RESIZE_HEIGHT (WTK_FRAME_RESIZE_RADIUS + 1) |
Height of resize handle. More... | |
#define | WTK_FRAME_MIN_WIDTH (WTK_FRAME_RESIZE_WIDTH - WTK_FRAME_RIGHTBORDER) |
Minimum width of contents window of a frame. More... | |
#define | WTK_FRAME_MIN_HEIGHT (WTK_FRAME_RESIZE_HEIGHT - WTK_FRAME_BOTTOMBORDER) |
Minimum height of contents window of a frame. More... | |
#define | WTK_FRAME_TITLEBAR_HEIGHT 9 |
Height of titlebar area. More... | |
#define | WTK_FRAME_CAPTION_X 3 |
Caption text X offset inside title bar. More... | |
#define | WTK_FRAME_CAPTION_Y 1 |
Caption text Y offset inside title bar. More... | |
#define | WTK_FRAME_BACKGROUND_COLOR GFX_COLOR(192, 192, 128) |
Background color of frame contents window. More... | |
#define | WTK_FRAME_BORDER_COLOR GFX_COLOR(240, 240, 240) |
Frame border color. More... | |
#define | WTK_FRAME_TITLEBAR_COLOR GFX_COLOR(128, 128, 255) |
Background color of frame title bar. More... | |
#define | WTK_FRAME_CAPTION_COLOR GFX_COLOR(255, 255, 255) |
Caption text foreground color. More... | |
#define | WTK_FRAME_RESIZE_COLOR GFX_COLOR(64, 192, 192) |
Resize handle color. More... | |
#define | WTK_DRAG_THRESHOLD 4 |
Distance from origin before dragging operation kicks in. More... | |
#define | WTK_DRAG_HANDLE_RADIUS 4 |
Radius of drag origin and target handles. More... | |
#define | WTK_DRAG_PIXMAP_SIZE (WTK_DRAG_HANDLE_RADIUS * 2 + 1) |
Pixmap pixel count for storing drag handle background graphics. More... | |
#define | WTK_DRAG_ORIGIN_COLOR GFX_COLOR(255, 0, 0) |
Drag origin handle color. More... | |
#define | WTK_DRAG_TARGET_COLOR GFX_COLOR(0, 255, 0) |
Drag target handle color. More... | |
#define | WTK_BUTTON_BACKGROUND_COLOR GFX_COLOR(128, 128, 128) |
Color of button background (text color when highlighted). More... | |
#define | WTK_BUTTON_CAPTION_COLOR GFX_COLOR(255, 255, 255) |
Color of button text (background color when highlighted). More... | |
#define | WTK_CHECKBOX_BOX_X 0 |
Checkbox square X offset. More... | |
#define | WTK_CHECKBOX_BOX_Y 0 |
Checkbox square Y offset. More... | |
#define | WTK_CHECKBOX_CAPTION_X (WTK_CHECKBOX_BOX_SIZE + 4) |
Checkbox caption text X offset. More... | |
#define | WTK_CHECKBOX_CAPTION_Y 0 |
Checkbox caption text Y offset. More... | |
#define | WTK_CHECKBOX_BOX_COLOR GFX_COLOR(0, 0, 0) |
Checkbox square frame color. More... | |
#define | WTK_CHECKBOX_BACKGROUND_COLOR GFX_COLOR_WHITE |
Checkbox square background color. More... | |
#define | WTK_CHECKBOX_SELECT_COLOR GFX_COLOR(128, 0, 0) |
Checkbox square select mark color. More... | |
#define | WTK_CHECKBOX_CAPTION_COLOR GFX_COLOR(255, 255, 255) |
Checkbox caption text color. More... | |
typedef uint8_t | wtk_radio_group_size_t |
Datatype holding reference count for radio button groups. More... | |
#define | WTK_RADIOBUTTON_RADIUS 4 |
Radius of radio button circle. More... | |
#define | WTK_RADIOBUTTON_BUTTON_X (WTK_RADIOBUTTON_RADIUS) |
Radio button circle center X offset. More... | |
#define | WTK_RADIOBUTTON_BUTTON_Y (WTK_RADIOBUTTON_RADIUS) |
Radio button circle center Y offset. More... | |
#define | WTK_RADIOBUTTON_CAPTION_X ((WTK_RADIOBUTTON_RADIUS * 2) + 4) |
Radio button caption text X offset. More... | |
#define | WTK_RADIOBUTTON_CAPTION_Y 0 |
Radio button caption text Y offset. More... | |
#define | WTK_RADIOBUTTON_BUTTON_COLOR GFX_COLOR(0, 0, 0) |
Radio button circle color. More... | |
#define | WTK_RADIOBUTTON_BACKGROUND_COLOR GFX_COLOR_WHITE |
Radio button circle background color. More... | |
#define | WTK_RADIOBUTTON_SELECT_COLOR GFX_COLOR(128, 0, 0) |
Radio button select mark color. More... | |
#define | WTK_RADIOBUTTON_CAPTION_COLOR GFX_COLOR(255, 255, 255) |
Radio button caption text color. More... | |
#define | WTK_SLIDER_KNOB_WIDTH 10 |
Width of the slider knob, including borders, in pixels. More... | |
#define | WTK_SLIDER_BORDER_COLOR GFX_COLOR(0, 0, 0) |
Color of all the slider's borders. More... | |
#define | WTK_SLIDER_BACKGROUND_COLOR GFX_COLOR(128, 128, 128) |
Color of the slider's background. More... | |
#define | WTK_SLIDER_KNOB_COLOR_NORMAL GFX_COLOR(255, 128, 0) |
Color of the slider knob when normal. More... | |
#define | WTK_SLIDER_KNOB_COLOR_MOVING GFX_COLOR(255, 255, 255) |
Color of the slider knob when moving. More... | |
typedef uint8_t | wtk_icon_group_size_t |
Datatype holding reference count for icon button groups. More... | |
#define | WTK_ICONBUTTON_SELECT_COLOR GFX_COLOR(0, 0, 255) |
Icon button select mark color. More... | |
#define | WTK_PLOT_BORDER_COLOR GFX_COLOR(0, 0, 0) |
Color of the plot's frame border. More... | |
#define | WTK_PLOT_SCALE_FACTOR 128 |
Scale factor for fixed-point calculation. More... | |
#define | WTK_PLOT_TICK_MARKER_LENGTH 5 |
The length of the tick marker. More... | |
#define WTK_BUTTON_BACKGROUND_COLOR GFX_COLOR(128, 128, 128) |
Color of button background (text color when highlighted).
Referenced by wtk_button_handler().
#define WTK_BUTTON_CAPTION_COLOR GFX_COLOR(255, 255, 255) |
Color of button text (background color when highlighted).
Referenced by wtk_button_handler().
#define WTK_CHECKBOX_BACKGROUND_COLOR GFX_COLOR_WHITE |
Checkbox square background color.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_BOX_COLOR GFX_COLOR(0, 0, 0) |
Checkbox square frame color.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_BOX_X 0 |
Checkbox square X offset.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_BOX_Y 0 |
Checkbox square Y offset.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_CAPTION_COLOR GFX_COLOR(255, 255, 255) |
Checkbox caption text color.
Referenced by wtk_check_box_handler().
#define WTK_CHECKBOX_CAPTION_X (WTK_CHECKBOX_BOX_SIZE + 4) |
Checkbox caption text X offset.
Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().
#define WTK_CHECKBOX_CAPTION_Y 0 |
Checkbox caption text Y offset.
Referenced by wtk_check_box_handler(), and wtk_check_box_size_hint().
#define WTK_CHECKBOX_SELECT_COLOR GFX_COLOR(128, 0, 0) |
Checkbox square select mark color.
Referenced by wtk_check_box_handler().
#define WTK_DRAG_HANDLE_RADIUS 4 |
Radius of drag origin and target handles.
Referenced by wtk_continue_drag(), wtk_start_drag(), and wtk_stop_drag().
#define WTK_DRAG_ORIGIN_COLOR GFX_COLOR(255, 0, 0) |
Drag origin handle color.
Referenced by wtk_start_drag().
#define WTK_DRAG_PIXMAP_SIZE (WTK_DRAG_HANDLE_RADIUS * 2 + 1) |
Pixmap pixel count for storing drag handle background graphics.
Referenced by wtk_continue_drag(), wtk_start_drag(), and wtk_stop_drag().
#define WTK_DRAG_TARGET_COLOR GFX_COLOR(0, 255, 0) |
Drag target handle color.
Referenced by wtk_continue_drag(), and wtk_start_drag().
#define WTK_DRAG_THRESHOLD 4 |
Distance from origin before dragging operation kicks in.
Referenced by wtk_is_drag_threshold_exceeded().
#define WTK_FRAME_BACKGROUND_COLOR GFX_COLOR(192, 192, 128) |
Background color of frame contents window.
#define WTK_FRAME_BORDER_COLOR GFX_COLOR(240, 240, 240) |
Frame border color.
Referenced by wtk_frame_handler().
#define WTK_FRAME_BOTTOMBORDER 4 |
Bottom frame border size.
Referenced by wtk_frame_handler(), and wtk_resize_frame().
#define WTK_FRAME_CAPTION_COLOR GFX_COLOR(255, 255, 255) |
Caption text foreground color.
Referenced by wtk_frame_handler().
#define WTK_FRAME_CAPTION_X 3 |
Caption text X offset inside title bar.
Referenced by wtk_frame_handler().
#define WTK_FRAME_CAPTION_Y 1 |
Caption text Y offset inside title bar.
Referenced by wtk_frame_handler().
#define WTK_FRAME_MIN_HEIGHT (WTK_FRAME_RESIZE_HEIGHT - WTK_FRAME_BOTTOMBORDER) |
Minimum height of contents window of a frame.
Referenced by wtk_resize_frame().
#define WTK_FRAME_MIN_WIDTH (WTK_FRAME_RESIZE_WIDTH - WTK_FRAME_RIGHTBORDER) |
Minimum width of contents window of a frame.
Referenced by wtk_resize_frame().
#define WTK_FRAME_RESIZE_COLOR GFX_COLOR(64, 192, 192) |
Resize handle color.
Referenced by wtk_frame_handler().
#define WTK_FRAME_RESIZE_HEIGHT (WTK_FRAME_RESIZE_RADIUS + 1) |
Height of resize handle.
Referenced by wtk_frame_create(), and wtk_resize_frame().
#define WTK_FRAME_RESIZE_RADIUS 7 |
Radius of resize handle (second quadrant of circle).
Referenced by wtk_frame_handler().
#define WTK_FRAME_RESIZE_WIDTH (WTK_FRAME_RESIZE_RADIUS + 1) |
Width of resize handle.
Referenced by wtk_frame_create(), and wtk_resize_frame().
#define WTK_FRAME_RIGHTBORDER 2 |
Right frame border size.
Referenced by wtk_frame_handler(), and wtk_resize_frame().
#define WTK_FRAME_TITLEBAR_COLOR GFX_COLOR(128, 128, 255) |
Background color of frame title bar.
Referenced by wtk_frame_handler().
#define WTK_FRAME_TITLEBAR_HEIGHT 9 |
Height of titlebar area.
Referenced by wtk_frame_create(), wtk_frame_handler(), and wtk_resize_frame().
#define WTK_FRAME_TOPBORDER 2 |
Top frame border size.
Referenced by wtk_frame_create(), wtk_frame_handler(), and wtk_resize_frame().
#define WTK_ICONBUTTON_SELECT_COLOR GFX_COLOR(0, 0, 255) |
Icon button select mark color.
Referenced by wtk_icon_button_handler().
#define WTK_PLOT_BORDER_COLOR GFX_COLOR(0, 0, 0) |
Color of the plot's frame border.
Referenced by wtk_plot_handler().
#define WTK_PLOT_SCALE_FACTOR 128 |
Scale factor for fixed-point calculation.
Referenced by wtk_plot_create(), and wtk_plot_draw().
#define WTK_PLOT_TICK_MARKER_LENGTH 5 |
The length of the tick marker.
Referenced by wtk_plot_grid_draw().
#define WTK_RADIOBUTTON_BACKGROUND_COLOR GFX_COLOR_WHITE |
Radio button circle background color.
Referenced by wtk_radio_button_handler().
#define WTK_RADIOBUTTON_BUTTON_COLOR GFX_COLOR(0, 0, 0) |
Radio button circle color.
Referenced by wtk_radio_button_handler().
#define WTK_RADIOBUTTON_BUTTON_X (WTK_RADIOBUTTON_RADIUS) |
Radio button circle center X offset.
Referenced by wtk_radio_button_handler().
#define WTK_RADIOBUTTON_BUTTON_Y (WTK_RADIOBUTTON_RADIUS) |
Radio button circle center Y offset.
Referenced by wtk_radio_button_handler(), and wtk_radio_button_size_hint().
#define WTK_RADIOBUTTON_CAPTION_COLOR GFX_COLOR(255, 255, 255) |
Radio button caption text color.
Referenced by wtk_radio_button_handler().
#define WTK_RADIOBUTTON_CAPTION_X ((WTK_RADIOBUTTON_RADIUS * 2) + 4) |
Radio button caption text X offset.
Referenced by wtk_radio_button_handler(), and wtk_radio_button_size_hint().
#define WTK_RADIOBUTTON_CAPTION_Y 0 |
Radio button caption text Y offset.
Referenced by wtk_radio_button_handler(), and wtk_radio_button_size_hint().
#define WTK_RADIOBUTTON_RADIUS 4 |
Radius of radio button circle.
Referenced by wtk_radio_button_handler(), and wtk_radio_button_size_hint().
#define WTK_RADIOBUTTON_SELECT_COLOR GFX_COLOR(128, 0, 0) |
Radio button select mark color.
Referenced by wtk_radio_button_handler().
#define WTK_SLIDER_BACKGROUND_COLOR GFX_COLOR(128, 128, 128) |
Color of the slider's background.
Referenced by wtk_slider_handler().
#define WTK_SLIDER_BORDER_COLOR GFX_COLOR(0, 0, 0) |
Color of all the slider's borders.
Referenced by wtk_slider_handler().
#define WTK_SLIDER_KNOB_COLOR_MOVING GFX_COLOR(255, 255, 255) |
Color of the slider knob when moving.
Referenced by wtk_slider_handler().
#define WTK_SLIDER_KNOB_COLOR_NORMAL GFX_COLOR(255, 128, 0) |
Color of the slider knob when normal.
Referenced by wtk_slider_handler().
#define WTK_SLIDER_KNOB_WIDTH 10 |
Width of the slider knob, including borders, in pixels.
Referenced by wtk_slider_create(), wtk_slider_handler(), and wtk_slider_set_value().
typedef uint8_t wtk_icon_group_size_t |
Datatype holding reference count for icon button groups.
typedef uint8_t wtk_radio_group_size_t |
Datatype holding reference count for radio button groups.
typedef uint16_t wtk_string_size_t |
Datatype holding the length of strings.
void wtk_copy_string | ( | char * | dest, |
char const * | source | ||
) |
This function copies the string contents, including the zero terminator, from source to destination.
The caller is responsible for providing memory for the destination string, either on the stack, static, or dynamically allocated.
dest | Destination string. |
source | Source string, zero terminated. |
References Assert.
Referenced by wtk_button_create(), wtk_check_box_create(), wtk_frame_create(), wtk_label_change(), wtk_label_create(), and wtk_radio_button_create().
uint8_t wtk_rescale_value | ( | uint8_t | value, |
uint8_t | from_scale, | ||
uint8_t | to_scale | ||
) |
Rescale 8-bit value.
This function is used by, e.g., the slider widget for computing the slider knob position from a given value and vice versa. It returns a value with the same data width as the input, meaning value cannot exceed from_scale, or overflows will occur.
The formula is:
value | Value to rescale. |
from_scale | Maximum of old scale for value. |
to_scale | Maximum of scale for new value. |
References Assert.
Referenced by wtk_plot_add_value(), wtk_plot_set_grid(), wtk_progress_bar_create(), wtk_progress_bar_set_value(), wtk_slider_create(), wtk_slider_handler(), and wtk_slider_set_value().