Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
SAM4L Asynchronous Timer (AST) Driver

This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Asynchronous Timer functionality.

The Asynchronous Timer can generate periodic interrupts and peripheral events from output from the prescaler, as well as alarm interrupts and peripheral events, which can trigger at any counter value.

Devices from the following series can use this module:

The outline of this documentation is as follows:

Prerequisites

There are no prerequisites for this module.

Module Overview

The AST module in the SAM4L devices is a 32-bit counter, with a 32-bit programmable prescaler. Typically, the AST clock is run continuously, including in the device's low-power sleep modes, to track the current time and date information. The AST can also wake-up the system from backup mode using either the alarm wakeup, periodic wakeup, or overflow wake-up mechanisms.

The AST has been designed to meet the system tick and Real-Time Clock requirements of most embedded operating systems.

In this driver, the AST is operated in Calendar Mode. This allows for an easy integration of a Real-Time Clock and calendar into a user application to track the passing of time and/or perform scheduled tasks.

Whilst operating in Calendar Mode, the AST features:

Alarm Interrupt

The AST has a device dependent number of independent hardware alarms that can be configured by the user application. These alarms will be triggered on a match with the current clock value, and can be set up to trigger an interrupt, event, or both. The AST can also be configured to clear the clock value on alarm match which will generate an overflow interrupt.

Note
Refer to module configuration at the end of the AST section of the device datasheet for the number of alarms supported.

Whilst in Calendar Mode and using a nominal 1Hz input clock frequency, a register overflow will occur after 64 years.

Periodic Events

The AST can generate events at periodic intervals, allowing for direct peripheral actions without CPU intervention. The periodic events can be generated on an AST prescaler match, and will be generated on the rising edge transition of the specified bit. The resulting periodic frequency can be calculated by the following formula:

\[ f_{PERIODIC}=\frac{f_{ASY}}{2^{n+1}} \]

Where \(f_{ASY}\) refers to the asynchronous clock set up in the AST module configuration.

Note
The connection of events between modules requires the use of the SAM4L Peripheral Event Controller (PEVC) to route an output event of one module to the the input event of another. For more information on event routing, refer to the event driver documentation.

Digital Tuner

The AST module contains Digital Tuner logic to compensate for inaccurate source clock frequencies, which would otherwise result in skewed time measurements.

Special Considerations

Crystal Selection

The external crystal selection used by the AST module in the final system design must take into account:

Year Limit

The AST module has a year range of 63 years from the starting year configured when the module is initialized. Dates outside the start to end year range described below will need software adjustment:

\[ [YEAR_{START}, YEAR_{START}+64] \]

Extra Information

For extra information, see Extra Information for Asynchronous Timer Driver. This includes:

Examples

For a list of examples related to this driver, see Examples for Asynchronous Timer Driver.

API Overview

Data Structures

struct  ast_calendar
 
struct  ast_calv
 Description for Calendar Field. More...
 
struct  ast_config
 AST configuration. More...
 

Macros

#define AST_POLL_TIMEOUT   10000
 Timeout to prevent code hang in clock initialization. More...
 

Typedefs

typedef void(* ast_callback_t )(void)
 AST interrupt callback. More...
 
typedef enum ast_event_source ast_event_source_t
 AST event source. More...
 
typedef enum ast_interrupt_source ast_interrupt_source_t
 AST interrupt source. More...
 
typedef enum ast_mode ast_mode_t
 AST Calendar Mode. More...
 
typedef enum ast_oscillator_type ast_oscillator_type_t
 AST Oscillator type. More...
 
typedef enum ast_wakeup_source ast_wakeup_source_t
 AST wake-up source. More...
 

Enumerations

enum  ast_event_source {
  AST_EVENT_ALARM = 0,
  AST_EVENT_PER,
  AST_EVENT_OVF
}
 AST event source. More...
 
enum  ast_interrupt_source {
  AST_INTERRUPT_ALARM = 0,
  AST_INTERRUPT_PER,
  AST_INTERRUPT_OVF,
  AST_INTERRUPT_READY,
  AST_INTERRUPT_CLKREADY
}
 AST interrupt source. More...
 
enum  ast_mode {
  AST_COUNTER_MODE = 0,
  AST_CALENDAR_MODE = 1
}
 AST Calendar Mode. More...
 
enum  ast_oscillator_type {
  AST_OSC_RC = 0,
  AST_OSC_32KHZ = 1,
  AST_OSC_PB = 2,
  AST_OSC_GCLK = 3,
  AST_OSC_1KHZ = 4
}
 AST Oscillator type. More...
 
enum  ast_wakeup_source {
  AST_WAKEUP_ALARM = 0,
  AST_WAKEUP_PER,
  AST_WAKEUP_OVF
}
 AST wake-up source. More...
 

Functions

void ast_clear_interrupt_flag (Ast *ast, ast_interrupt_source_t source)
 Clear an AST interrupt status flag. More...
 
void ast_clear_prescalar (Ast *ast)
 Clear the AST periodic prescaler counter to zero. More...
 
uint32_t ast_configure_digital_tuner (Ast *ast, uint32_t input_freq, uint32_t tuned_freq)
 Tune the AST prescaler frequency to the desired frequency. More...
 
void ast_disable (Ast *ast)
 Disable the AST counter and module. More...
 
void ast_disable_digital_tuner (Ast *ast)
 Disable the AST digital tuner. More...
 
void ast_disable_event (Ast *ast, ast_event_source_t source)
 Disable an AST event. More...
 
void ast_disable_interrupt (Ast *ast, ast_interrupt_source_t source)
 Disable an AST interrupt. More...
 
void ast_disable_wakeup (Ast *ast, ast_wakeup_source_t source)
 Disable an AST asynchronous wake-up source. More...
 
void ast_enable (Ast *ast)
 Enable the AST module. More...
 
void ast_enable_counter_clear_on_alarm (Ast *ast, uint8_t alarm_channel)
 Enable the option to clear the counter on an AST alarm. More...
 
void ast_enable_event (Ast *ast, ast_event_source_t source)
 Enable an AST event. More...
 
void ast_enable_interrupt (Ast *ast, ast_interrupt_source_t source)
 Enable an AST interrupt. More...
 
void ast_enable_wakeup (Ast *ast, ast_wakeup_source_t source)
 Enable an AST asynchronous wake-up source. More...
 
void ast_init_digital_tuner (Ast *ast, bool add, uint8_t value, uint8_t exp)
 Initialize the AST digital tuner. More...
 
static bool ast_is_busy (Ast *ast)
 Check the busy status of AST. More...
 
static bool ast_is_clkbusy (Ast *ast)
 Check the busy status of the AST clock. More...
 
bool ast_is_enabled (Ast *ast)
 Check the status of the AST module. More...
 
struct ast_calendar ast_read_calendar_value (Ast *ast)
 Get the AST current calendar value. More...
 
static uint32_t ast_read_counter_value (Ast *ast)
 Get the AST current counter value. More...
 
static uint32_t ast_read_interrupt_mask (Ast *ast)
 Get the AST interrupt mask value. More...
 
static uint32_t ast_read_status (Ast *ast)
 Get the status of AST. More...
 
void ast_set_callback (Ast *ast, ast_interrupt_source_t source, ast_callback_t callback, uint8_t irq_line, uint8_t irq_level)
 Set callback for AST interrupts. More...
 
uint32_t ast_set_config (Ast *ast, struct ast_config *ast_conf)
 Initialize and enable the AST module in Calendar Mode or Counter Mode. More...
 
static void ast_start (Ast *ast)
 Start the AST counter. More...
 
static void ast_stop (Ast *ast)
 Stop the AST counter. More...
 
void ast_write_alarm0_value (Ast *ast, uint32_t alarm_value)
 Set the AST alarm0 value. More...
 
void ast_write_calendar_value (Ast *ast, struct ast_calendar calendar)
 Set the AST current calendar value. More...
 
void ast_write_counter_value (Ast *ast, uint32_t ast_counter)
 Set the AST current counter value. More...
 
void ast_write_periodic0_value (Ast *ast, uint32_t pir)
 Set the AST periodic0 value. More...
 

Predefined PSEL Values

#define AST_PSEL_32KHZ_1HZ   14
 The PSEL value to set the AST source clock (after the prescaler) to 1Hz, when using an external 32-kHz crystal. More...
 
#define AST_PSEL_RC_1_76HZ   15
 The PSEL value to set the AST source clock (after the prescaler) to 1.76Hz when using the internal RC oscillator (~ 115kHz) More...
 

#define AST_POLL_TIMEOUT   10000

Timeout to prevent code hang in clock initialization.

Referenced by ast_set_config().

#define AST_PSEL_32KHZ_1HZ   14

The PSEL value to set the AST source clock (after the prescaler) to 1Hz, when using an external 32-kHz crystal.

Referenced by config_ast().

#define AST_PSEL_RC_1_76HZ   15

The PSEL value to set the AST source clock (after the prescaler) to 1.76Hz when using the internal RC oscillator (~ 115kHz)

typedef void(* ast_callback_t)(void)

AST interrupt callback.

AST event source.

Enumerator
AST_EVENT_ALARM 

Alarm event generation.

AST_EVENT_PER 

Peripheral event generation.

AST_EVENT_OVF 

Counter overflow event generation.

AST interrupt source.

Enumerator
AST_INTERRUPT_ALARM 

Alarm interrupt.

AST_INTERRUPT_PER 

Periodic interrupt.

AST_INTERRUPT_OVF 

Overflow interrupt.

AST_INTERRUPT_READY 

Synchronization complete interrupt.

AST_INTERRUPT_CLKREADY 

Clock synchronization complete interrupt.

enum ast_mode

AST Calendar Mode.

Enumerator
AST_COUNTER_MODE 

Counter Mode.

AST_CALENDAR_MODE 

Calendar Mode.

AST Oscillator type.

Enumerator
AST_OSC_RC 

System RC oscillator (RCSYS)

AST_OSC_32KHZ 

32kHz oscillator (OSC32 or RC32)

AST_OSC_PB 

APB clock.

AST_OSC_GCLK 

Generic clock (GCLK)

AST_OSC_1KHZ 

1kHz clock from the 32kHz oscillator or 32kHz RC oscillator (CLK_1K)

AST wake-up source.

Enumerator
AST_WAKEUP_ALARM 

Alarm wake-up source.

AST_WAKEUP_PER 

Peripheral interrupt wake-up source.

AST_WAKEUP_OVF 

Counter overflow wake-up source.

void ast_clear_interrupt_flag ( Ast *  ast,
ast_interrupt_source_t  source 
)

Clear an AST interrupt status flag.

Parameters
[in,out]astModule hardware register base address pointer
[in]sourceAST interrupt source for which the status is to be cleared

References AST_INTERRUPT_ALARM, AST_INTERRUPT_CLKREADY, AST_INTERRUPT_OVF, AST_INTERRUPT_PER, AST_INTERRUPT_READY, and ast_is_busy().

Referenced by ast_per_callback(), and config_ast().

void ast_clear_prescalar ( Ast *  ast)

Clear the AST periodic prescaler counter to zero.

Parameters
[in,out]astModule hardware register base address pointer

References ast_is_busy().

uint32_t ast_configure_digital_tuner ( Ast *  ast,
uint32_t  input_freq,
uint32_t  tuned_freq 
)

Tune the AST prescaler frequency to the desired frequency.

Note
Refer to the section entitled "digital tuner" in the ast chapter of the device-specific datasheet for more information.
Parameters
[in,out]astModule hardware register base address pointer
[in]input_freqPrescaled AST Clock Frequency
[in]tuned_freqDesired AST frequency

References ast_init_digital_tuner(), and div_ceil.

void ast_disable ( Ast *  ast)

Disable the AST counter and module.

Parameters
[in,out]astModule hardware register base address pointer

References ast_is_busy(), SLEEPMGR_BACKUP, sleepmgr_unlock_mode(), and sysclk_disable_peripheral_clock().

void ast_disable_digital_tuner ( Ast *  ast)

Disable the AST digital tuner.

Parameters
[in,out]astModule hardware register base address pointer

References ast_is_busy().

void ast_disable_event ( Ast *  ast,
ast_event_source_t  source 
)

Disable an AST event.

Parameters
[in,out]astModule hardware register base address pointer
[in]sourceAST event source to be disabled

References AST_EVENT_ALARM, AST_EVENT_OVF, AST_EVENT_PER, and ast_is_busy().

void ast_disable_interrupt ( Ast *  ast,
ast_interrupt_source_t  source 
)

Disable an AST interrupt.

Parameters
[in,out]astModule hardware register base address pointer
[in]sourceAST interrupt source to be disabled

References AST_INTERRUPT_ALARM, AST_INTERRUPT_CLKREADY, AST_INTERRUPT_OVF, AST_INTERRUPT_PER, AST_INTERRUPT_READY, and ast_is_busy().

void ast_disable_wakeup ( Ast *  ast,
ast_wakeup_source_t  source 
)

Disable an AST asynchronous wake-up source.

Parameters
[in,out]astModule hardware register base address pointer
[in]sourceAST wake-up source to be disabled

References ast_is_busy(), AST_WAKEUP_ALARM, AST_WAKEUP_OVF, and AST_WAKEUP_PER.

void ast_enable ( Ast *  ast)

Enable the AST module.

Parameters
[in]astModule hardware register base address pointer

References SLEEPMGR_BACKUP, sleepmgr_lock_mode(), and sysclk_enable_peripheral_clock().

Referenced by config_ast().

void ast_enable_counter_clear_on_alarm ( Ast *  ast,
uint8_t  alarm_channel 
)

Enable the option to clear the counter on an AST alarm.

Parameters
[in,out]astModule hardware register base address pointer
[in]alarm_channelAST Alarm Channel

References ast_is_busy().

void ast_enable_event ( Ast *  ast,
ast_event_source_t  source 
)

Enable an AST event.

Parameters
[in,out]astModule hardware register base address pointer
[in]sourceAST event source to be enabled

References AST_EVENT_ALARM, AST_EVENT_OVF, AST_EVENT_PER, and ast_is_busy().

void ast_enable_interrupt ( Ast *  ast,
ast_interrupt_source_t  source 
)

Enable an AST interrupt.

Parameters
[in,out]astModule hardware register base address pointer
[in]sourceAST interrupt source to be enabled

References AST_INTERRUPT_ALARM, AST_INTERRUPT_CLKREADY, AST_INTERRUPT_OVF, AST_INTERRUPT_PER, AST_INTERRUPT_READY, and ast_is_busy().

Referenced by ast_set_callback().

void ast_enable_wakeup ( Ast *  ast,
ast_wakeup_source_t  source 
)

Enable an AST asynchronous wake-up source.

Parameters
[in,out]astModule hardware register base address pointer
[in]sourceAST wake-up source to be enabled

References ast_is_busy(), AST_WAKEUP_ALARM, AST_WAKEUP_OVF, and AST_WAKEUP_PER.

Referenced by config_ast().

void ast_init_digital_tuner ( Ast *  ast,
bool  add,
uint8_t  value,
uint8_t  exp 
)

Initialize the AST digital tuner.

Parameters
[in,out]astModule hardware register base address pointer
[in]addSet to true if the frequency needs to be increased, false if it has to be decreased.
[in]valueParameter used in the formula
[in]expParameter used in the formula

References ast_is_busy().

Referenced by ast_configure_digital_tuner().

static bool ast_is_clkbusy ( Ast *  ast)
inlinestatic

Check the busy status of the AST clock.

Parameters
[in]astModule hardware register base address pointer
Returns
AST clock busy status.
Return values
falseAST clock is not busy
trueAST clock is busy

Referenced by ast_set_config().

bool ast_is_enabled ( Ast *  ast)

Check the status of the AST module.

Parameters
[in,out]astModule hardware register base address pointer
Return values
falseAST is not enabled
trueAST is enabled

References ast_is_busy().

struct ast_calendar ast_read_calendar_value ( Ast *  ast)

Get the AST current calendar value.

Note
There maybe a compiler warning about returning a structure type value, however it is safe because ast_calendar is actually uint32_t type.
Parameters
[in]astModule hardware register base address pointer
Returns
The AST current calendar value.

References ast_calendar::field.

static uint32_t ast_read_counter_value ( Ast *  ast)
inlinestatic

Get the AST current counter value.

Parameters
[in]astModule hardware register base address pointer
Returns
AST current counter value.
static uint32_t ast_read_interrupt_mask ( Ast *  ast)
inlinestatic

Get the AST interrupt mask value.

Parameters
[in]astModule hardware register base address pointer
Returns
AST Interrupt mask value.
static uint32_t ast_read_status ( Ast *  ast)
inlinestatic

Get the status of AST.

Parameters
[in]astModule hardware register base address pointer
Returns
AST status.
void ast_set_callback ( Ast *  ast,
ast_interrupt_source_t  source,
ast_callback_t  callback,
uint8_t  irq_line,
uint8_t  irq_level 
)

Set callback for AST interrupts.

Parameters
[in,out]astModule hardware register base address pointer
[in]sourceAST interrupt source
[in]callbackCallback function pointer
[in]irq_lineInterrupt line
[in]irq_levelInterrupt level

References ast_callback_pointer, and ast_enable_interrupt().

Referenced by config_ast().

uint32_t ast_set_config ( Ast *  ast,
struct ast_config ast_conf 
)

Initialize and enable the AST module in Calendar Mode or Counter Mode.

Note
If you use the 32kHz oscillator it will be enabled by this function.
Parameters
[in,out]astModule hardware register base address pointer
[in]ast_confAST configuration structure pointer
Returns
Initialization result.
Return values
0Initialization failed due to a software timeout
1Initialization succeeded

References AST_CALENDAR_MODE, AST_COUNTER_MODE, ast_is_busy(), ast_is_clkbusy(), AST_POLL_TIMEOUT, ast_write_calendar_value(), ast_write_counter_value(), ast_config::calendar, ast_config::counter, ast_config::mode, ast_config::osc_type, and ast_config::psel.

Referenced by config_ast().

static void ast_start ( Ast *  ast)
inlinestatic

Start the AST counter.

Parameters
[in,out]astModule hardware register base address pointer

References ast_is_busy().

Referenced by test_backup_mode(), test_retention_mode(), and test_wait_mode().

static void ast_stop ( Ast *  ast)
inlinestatic

Stop the AST counter.

Parameters
[in,out]astModule hardware register base address pointer

References ast_is_busy().

Referenced by ast_per_callback(), button_handler(), and config_ast().

void ast_write_alarm0_value ( Ast *  ast,
uint32_t  alarm_value 
)

Set the AST alarm0 value.

Parameters
[in,out]astModule hardware register base address pointer
[in]alarm_valueAST alarm0 value

References ast_is_busy().

void ast_write_calendar_value ( Ast *  ast,
struct ast_calendar  calendar 
)

Set the AST current calendar value.

Parameters
[in,out]astModule hardware register base address pointer
[in]calendarStartup date structure

References ast_is_busy(), and ast_calendar::field.

Referenced by ast_set_config().

void ast_write_counter_value ( Ast *  ast,
uint32_t  ast_counter 
)

Set the AST current counter value.

Parameters
[in,out]astModule hardware register base address pointer
[in]ast_counterStartup counter value

References ast_is_busy().

Referenced by ast_set_config(), and button_handler().

void ast_write_periodic0_value ( Ast *  ast,
uint32_t  pir 
)

Set the AST periodic0 value.

Parameters
[in,out]astModule hardware register base address pointer
[in]pirAST periodic0

References ast_is_busy().

Referenced by config_ast().