Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
FLASHCALW - FLASH Controller Double-Word

See Quickstart guide for SAM FLASHCALW driver.

FLASHCALW interfaces a flash block with the 32-bit internal HSB bus.

Flash Properties

uint32_t flashcalw_get_flash_size (void)
 Gets the size of the whole flash array. More...
 
uint32_t flashcalw_get_page_count (void)
 Gets the total number of pages in the flash array. More...
 
uint32_t flashcalw_get_page_count_per_region (void)
 Gets the number of pages in each flash region. More...
 
uint32_t flashcalw_get_page_region (int32_t page_number)
 Gets the region number of a page. More...
 
uint32_t flashcalw_get_region_first_page_number (uint32_t region)
 Gets the number of the first page of a region. More...
 

FLASHC Control

uint32_t flashcalw_get_wait_state (void)
 Gets the number of wait states of flash read accesses. More...
 
void flashcalw_set_wait_state (uint32_t wait_state)
 Sets the number of wait states of flash read accesses. More...
 
void flashcalw_set_flash_waitstate_and_readmode (uint32_t cpu_f_hz, uint32_t ps_value, bool is_fwu_enabled)
 Depending on the CPU frequency, on the Power Scaling mode and on the Fast Wakeup mode, set the wait states of flash read accesses and enable or disable the High speed read mode. More...
 
bool flashcalw_is_ready_int_enabled (void)
 Tells whether the Flash Ready interrupt is enabled. More...
 
void flashcalw_enable_ready_int (bool enable)
 Enables or disables the Flash Ready interrupt. More...
 
bool flashcalw_is_lock_error_int_enabled (void)
 Tells whether the Lock Error interrupt is enabled. More...
 
void flashcalw_enable_lock_error_int (bool enable)
 Enables or disables the Lock Error interrupt. More...
 
bool flashcalw_is_prog_error_int_enabled (void)
 Tells whether the Programming Error interrupt is enabled. More...
 
void flashcalw_enable_prog_error_int (bool enable)
 Enables or disables the Programming Error interrupt. More...
 
#define FLASH_FWS_0_MAX_FREQ   CHIP_FREQ_FWS_0
 
#define FLASH_FWS_1_MAX_FREQ   CHIP_FREQ_FWS_1
 
#define FLASH_HSEN_FWS_0_MAX_FREQ   CHIP_FREQ_FLASH_HSEN_FWS_0
 
#define FLASH_HSEN_FWS_1_MAX_FREQ   CHIP_FREQ_FLASH_HSEN_FWS_1
 

FLASHCALW Status

void(*volatile flashcalw_wait_until_ready )(void) = flashcalw_default_wait_until_ready
 Pointer to the function used by the driver when it needs to wait until the FLASHCALW is ready to run a new command. More...
 
static uint32_t flashcalw_error_status = 0
 Sticky error status of the FLASHCALW. More...
 
bool flashcalw_is_ready (void)
 Tells whether the FLASHCALW is ready to run a new command. More...
 
void flashcalw_default_wait_until_ready (void)
 Waits actively until the FLASHCALW is ready to run a new command. More...
 
static uint32_t flashcalw_get_error_status (void)
 Gets the error status of the FLASHCALW. More...
 
bool flashcalw_is_lock_error (void)
 Tells whether a Lock Error has occurred during the last function called that issued one or more FLASHCALW commands. More...
 
bool flashcalw_is_programming_error (void)
 Tells whether a Programming Error has occurred during the last function called that issued one or more FLASHCALW commands. More...
 

FLASHCALW Command Control

uint32_t flashcalw_get_command (void)
 Gets the last issued FLASHCALW command. More...
 
uint32_t flashcalw_get_page_number (void)
 Gets the current FLASHCALW page number. More...
 
void flashcalw_issue_command (uint32_t command, int page_number)
 Issues a FLASHCALW command. More...
 

FLASHCALW Global Commands

void flashcalw_no_operation (void)
 Issues a No Operation command to the FLASHCALW. More...
 
void flashcalw_erase_all (void)
 Issues an Erase All command to the FLASHCALW. More...
 

FLASHCALW Protection Mechanisms

bool flashcalw_is_security_bit_active (void)
 Tells whether the Security bit is active. More...
 
void flashcalw_set_security_bit (void)
 Activates the Security bit. More...
 
bool flashcalw_is_page_region_locked (uint32_t page_number)
 Tells whether the region of a page is locked. More...
 
bool flashcalw_is_region_locked (uint32_t region)
 Tells whether a region is locked. More...
 
void flashcalw_lock_page_region (int page_number, bool lock)
 Locks or unlocks the region of a page. More...
 
void flashcalw_lock_region (uint32_t region, bool lock)
 Locks or unlocks a region. More...
 
void flashcalw_lock_all_regions (bool lock)
 Locks or unlocks all regions. More...
 

Access to General-Purpose Fuses

bool flashcalw_read_gp_fuse_bit (uint32_t gp_fuse_bit)
 Reads a general-purpose fuse bit. More...
 
uint64_t flashcalw_read_gp_fuse_bitfield (uint32_t pos, uint32_t width)
 Reads a general-purpose fuse bit-field. More...
 
uint8_t flashcalw_read_gp_fuse_byte (uint32_t gp_fuse_byte)
 Reads a general-purpose fuse byte. More...
 
uint64_t flashcalw_read_all_gp_fuses (void)
 Reads all general-purpose fuses. More...
 
bool flashcalw_erase_gp_fuse_bit (uint32_t gp_fuse_bit, bool check)
 Erases a general-purpose fuse bit. More...
 
bool flashcalw_erase_gp_fuse_bitfield (uint32_t pos, uint32_t width, bool check)
 Erases a general-purpose fuse bit-field. More...
 
bool flashcalw_erase_gp_fuse_byte (uint32_t gp_fuse_byte, bool check)
 Erases a general-purpose fuse byte. More...
 
bool flashcalw_erase_all_gp_fuses (bool check)
 Erases all general-purpose fuses. More...
 
void flashcalw_write_gp_fuse_bit (uint32_t gp_fuse_bit, bool value)
 Writes a general-purpose fuse bit. More...
 
void flashcalw_write_gp_fuse_bitfield (uint32_t pos, uint32_t width, uint64_t value)
 Writes a general-purpose fuse bit-field. More...
 
void flashcalw_write_gp_fuse_byte (uint32_t gp_fuse_byte, uint8_t value)
 Writes a general-purpose fuse byte. More...
 
void flashcalw_write_all_gp_fuses (uint64_t value)
 Writes all general-purpose fuses. More...
 
void flashcalw_set_gp_fuse_bit (uint32_t gp_fuse_bit, bool value)
 Sets a general-purpose fuse bit with the appropriate erase and write operations. More...
 
void flashcalw_set_gp_fuse_bitfield (uint32_t pos, uint32_t width, uint64_t value)
 Sets a general-purpose fuse bit-field with the appropriate erase and write operations. More...
 
void flashcalw_set_gp_fuse_byte (uint32_t gp_fuse_byte, uint8_t value)
 Sets a general-purpose fuse byte with the appropriate erase and write operations. More...
 
void flashcalw_set_all_gp_fuses (uint64_t value)
 Sets all general-purpose fuses with the appropriate erase and write operations. More...
 

Access to Flash Pages

void flashcalw_clear_page_buffer (void)
 Clears the page buffer. More...
 
bool flashcalw_is_page_erased (void)
 Tells whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased. More...
 
bool flashcalw_quick_page_read (int page_number)
 Applies the Quick Page Read command to a page. More...
 
bool flashcalw_erase_page (int page_number, bool check)
 Erases a page. More...
 
bool flashcalw_erase_all_pages (bool check)
 Erases all pages within the flash array. More...
 
void flashcalw_write_page (int page_number)
 Writes a page from the page buffer. More...
 
bool flashcalw_quick_user_page_read (void)
 Issues a Quick Page Read User Page command to the FLASHCALW. More...
 
bool flashcalw_erase_user_page (bool check)
 Erases the User page. More...
 
void flashcalw_write_user_page (void)
 Writes the User page from the page buffer. More...
 
volatile void * flashcalw_memset8 (volatile void *dst, uint8_t src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the repeated src source byte. More...
 
volatile void * flashcalw_memset16 (volatile void *dst, uint16_t src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source half-word. More...
 
volatile void * flashcalw_memset32 (volatile void *dst, uint32_t src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source word. More...
 
volatile void * flashcalw_memset64 (volatile void *dst, uint64_t src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source double-word. More...
 
volatile void * flashcalw_memcpy (volatile void *dst, const void *src, size_t nbytes, bool erase)
 Copies nbytes bytes to the flash destination pointed to by dst from the source pointed to by src. More...
 

PicoCache interfaces

void flashcalw_picocache_enable (void)
 Enable PicoCache. More...
 
void flashcalw_picocache_disable (void)
 Disable PicoCache. More...
 
uint32_t flashcalw_picocache_get_status (void)
 Get PicoCache status. More...
 
void flashcalw_picocache_invalid_all (void)
 Invalid all PicoCache lines. More...
 
void flashcalw_picocache_invalid_line (uint32_t index)
 Invalid specific cache line. More...
 
void flashcalw_picocache_set_monitor_mode (uint32_t mode)
 Set PicoCache monitor mode. More...
 
void flashcalw_picocache_enable_monitor (void)
 Enable PicoCache monitor. More...
 
void flashcalw_picocache_disable_monitor (void)
 Disable PicoCache monitor. More...
 
void flashcalw_picocache_reset_monitor (void)
 Reset PicoCache monitor. More...
 
uint32_t flashcalw_picocache_get_monitor_cnt (void)
 Get PicoCache monitor count number. More...
 
uint32_t flashcalw_picocache_get_version (void)
 Get PicoCache version. More...
 

#define FLASH_FWS_0_MAX_FREQ   CHIP_FREQ_FWS_0
#define FLASH_FWS_1_MAX_FREQ   CHIP_FREQ_FWS_1
#define FLASH_HSEN_FWS_0_MAX_FREQ   CHIP_FREQ_FLASH_HSEN_FWS_0
#define FLASH_HSEN_FWS_1_MAX_FREQ   CHIP_FREQ_FLASH_HSEN_FWS_1

void flashcalw_clear_page_buffer ( void  )

Clears the page buffer.

This command resets all bits in the page buffer to one. Write accesses to the page buffer can only change page buffer bits from one to zero.

Warning
The page buffer is not automatically reset after a page write.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_issue_command().

Referenced by flashcalw_memcpy(), and flashcalw_memset64().

void flashcalw_default_wait_until_ready ( void  )

Waits actively until the FLASHCALW is ready to run a new command.

This is the default function assigned to flashcalw_wait_until_ready.

References flashcalw_is_ready().

void flashcalw_enable_lock_error_int ( bool  enable)

Enables or disables the Lock Error interrupt.

Parameters
enableWhether to enable the Lock Error interrupt: true or false.
void flashcalw_enable_prog_error_int ( bool  enable)

Enables or disables the Programming Error interrupt.

Parameters
enableWhether to enable the Programming Error interrupt: true or false.
void flashcalw_enable_ready_int ( bool  enable)

Enables or disables the Flash Ready interrupt.

Parameters
enableWhether to enable the Flash Ready interrupt: true or false.
void flashcalw_erase_all ( void  )

Issues an Erase All command to the FLASHCALW.

This command erases all bits in the flash array, the general-purpose fuse bits and the Security bit. The User page is not erased.

This command also ensures that all volatile memories, such as register file and RAMs, are erased before the Security bit is erased, i.e. deactivated.

Warning
A Lock Error is issued if at least one region is locked or the bootloader protection is active.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
An erase operation can only set bits.

References flashcalw_issue_command().

bool flashcalw_erase_all_gp_fuses ( bool  check)

Erases all general-purpose fuses.

Parameters
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
An erase operation can only set bits.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

use (uint64_t)-1 instead of 0xFFFFFFFFFFFFFFFFULL to avoid compilation warning

References flashcalw_issue_command(), and flashcalw_read_all_gp_fuses().

Referenced by flashcalw_erase_gp_fuse_byte(), and flashcalw_set_all_gp_fuses().

bool flashcalw_erase_all_pages ( bool  check)

Erases all pages within the flash array.

Parameters
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if at least one region is locked or the bootloader protection is active.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
An erase operation can only set bits.

References flashcalw_erase_page(), flashcalw_error_status, and flashcalw_get_page_count().

bool flashcalw_erase_gp_fuse_bit ( uint32_t  gp_fuse_bit,
bool  check 
)

Erases a general-purpose fuse bit.

Parameters
gp_fuse_bitThe general-purpose fuse bit: 0 to 63.
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
An erase operation can only set bits.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_issue_command(), and flashcalw_read_gp_fuse_bit().

Referenced by flashcalw_erase_gp_fuse_bitfield(), flashcalw_set_gp_fuse_bit(), and main().

bool flashcalw_erase_gp_fuse_bitfield ( uint32_t  pos,
uint32_t  width,
bool  check 
)

Erases a general-purpose fuse bit-field.

Parameters
posThe bit-position of the general-purpose fuse bit-field: 0 to 63.
widthThe bit-width of the general-purpose fuse bit-field: 0 to 64.
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
An erase operation can only set bits.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_erase_gp_fuse_bit(), flashcalw_error_status, flashcalw_read_gp_fuse_bitfield(), and Min.

bool flashcalw_erase_gp_fuse_byte ( uint32_t  gp_fuse_byte,
bool  check 
)

Erases a general-purpose fuse byte.

Parameters
gp_fuse_byteThe general-purpose fuse byte: 0 to 7.
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
An erase operation can only set bits.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_erase_all_gp_fuses(), flashcalw_error_status, flashcalw_read_all_gp_fuses(), flashcalw_read_gp_fuse_byte(), and flashcalw_write_gp_fuse_byte().

Referenced by flashcalw_set_gp_fuse_byte().

bool flashcalw_erase_page ( int  page_number,
bool  check 
)

Erases a page.

Parameters
page_numberThe page number:
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Warning
A Lock Error is issued if the command is applied to a page belonging to a locked region or to the bootloader protected area.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
An erase operation can only set bits.

References flashcalw_error_status, flashcalw_issue_command(), and flashcalw_quick_page_read().

Referenced by flashcalw_erase_all_pages(), flashcalw_memcpy(), flashcalw_memset64(), and program_memory().

bool flashcalw_erase_user_page ( bool  check)

Erases the User page.

Parameters
checkWhether to check erase: true or false.
Returns
Whether the erase succeeded or always true if erase check was not requested.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
An erase operation can only set bits.

References flashcalw_issue_command(), and flashcalw_quick_user_page_read().

Referenced by flashcalw_memcpy(), and flashcalw_memset64().

uint32_t flashcalw_get_command ( void  )

Gets the last issued FLASHCALW command.

Returns
The last issued FLASHCALW command.
static uint32_t flashcalw_get_error_status ( void  )
static

Gets the error status of the FLASHCALW.

Returns
The error status of the FLASHCALW built up from FLASHCALW_FSR_LOCKE and FLASHCALW_FSR_PROGE.
Warning
This hardware error status is cleared by all functions reading the Flash Status Register (FSR). This function is therefore not part of the driver's API which instead presents flashcalw_is_lock_error and flashcalw_is_programming_error.

Referenced by flashcalw_issue_command().

uint32_t flashcalw_get_flash_size ( void  )

Gets the size of the whole flash array.

Returns
The size of the whole flash array in Bytes.

Referenced by flashcalw_get_page_count(), flashcalw_memcpy(), and flashcalw_memset64().

uint32_t flashcalw_get_page_count ( void  )

Gets the total number of pages in the flash array.

Returns
The total number of pages in the flash array.

References FLASH_PAGE_SIZE, and flashcalw_get_flash_size().

Referenced by flashcalw_erase_all_pages(), and flashcalw_get_page_count_per_region().

uint32_t flashcalw_get_page_count_per_region ( void  )

Gets the number of pages in each flash region.

Returns
The number of pages in each flash region.

References FLASH_NB_OF_REGIONS, and flashcalw_get_page_count().

Referenced by flashcalw_get_page_region(), and flashcalw_get_region_first_page_number().

uint32_t flashcalw_get_page_number ( void  )

Gets the current FLASHCALW page number.

Returns
The current FLASHCALW page number.

Referenced by flashcalw_get_page_region().

uint32_t flashcalw_get_page_region ( int32_t  page_number)

Gets the region number of a page.

Parameters
page_numberThe page number:
Returns
The region number of the specified page.

References flashcalw_get_page_count_per_region(), and flashcalw_get_page_number().

Referenced by flashcalw_is_page_region_locked().

uint32_t flashcalw_get_region_first_page_number ( uint32_t  region)

Gets the number of the first page of a region.

Parameters
regionThe region number: 0 to (FLASHCALW_REGIONS - 1).
Returns
The number of the first page of the specified region.

References flashcalw_get_page_count_per_region().

Referenced by flashcalw_lock_region().

uint32_t flashcalw_get_wait_state ( void  )

Gets the number of wait states of flash read accesses.

Returns
The number of wait states of flash read accesses.
bool flashcalw_is_lock_error ( void  )

Tells whether a Lock Error has occurred during the last function called that issued one or more FLASHCALW commands.

Returns
Whether a Lock Error has occurred during the last function called that issued one or more FLASHCALW commands.

Referenced by program_memory().

bool flashcalw_is_lock_error_int_enabled ( void  )

Tells whether the Lock Error interrupt is enabled.

Returns
Whether the Lock Error interrupt is enabled.
bool flashcalw_is_page_erased ( void  )

Tells whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased.

Returns
Whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased.

Referenced by flashcalw_quick_page_read(), and flashcalw_quick_user_page_read().

bool flashcalw_is_page_region_locked ( uint32_t  page_number)

Tells whether the region of a page is locked.

Parameters
page_numberThe page number:
Returns
Whether the region of the specified page is locked.

References flashcalw_get_page_region(), and flashcalw_is_region_locked().

bool flashcalw_is_prog_error_int_enabled ( void  )

Tells whether the Programming Error interrupt is enabled.

Returns
Whether the Programming Error interrupt is enabled.
bool flashcalw_is_programming_error ( void  )

Tells whether a Programming Error has occurred during the last function called that issued one or more FLASHCALW commands.

Returns
Whether a Programming Error has occurred during the last function called that issued one or more FLASHCALW commands.

Referenced by program_memory().

bool flashcalw_is_ready ( void  )

Tells whether the FLASHCALW is ready to run a new command.

Returns
Whether the FLASHCALW is ready to run a new command.

Referenced by flashcalw_default_wait_until_ready().

bool flashcalw_is_ready_int_enabled ( void  )

Tells whether the Flash Ready interrupt is enabled.

Returns
Whether the Flash Ready interrupt is enabled.
bool flashcalw_is_region_locked ( uint32_t  region)

Tells whether a region is locked.

Parameters
regionThe region number: 0 to (FLASHCALW_REGIONS - 1).
Returns
Whether the specified region is locked.

References FLASHCALW_REGIONS.

Referenced by flashcalw_is_page_region_locked().

bool flashcalw_is_security_bit_active ( void  )

Tells whether the Security bit is active.

Returns
Whether the Security bit is active.

Referenced by main().

void flashcalw_issue_command ( uint32_t  command,
int  page_number 
)

Issues a FLASHCALW command.

Parameters
commandThe command: FLASHCALW_FCMD_CMD_x.
page_numberThe page number to apply the command to:
  • 0 to (flashcalw_get_page_count() - 1): a page number within the flash array;
  • < 0: use this to apply the command to the current page number or if the command does not apply to any page number;
  • this argument may have other meanings according to the command. See the FLASHCALW chapter of the MCU datasheet.
Warning
A Lock Error is issued if the command violates the protection mechanism.
A Programming Error is issued if the command is invalid.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_get_error_status(), and flashcalw_wait_until_ready.

Referenced by flashcalw_clear_page_buffer(), flashcalw_erase_all(), flashcalw_erase_all_gp_fuses(), flashcalw_erase_gp_fuse_bit(), flashcalw_erase_page(), flashcalw_erase_user_page(), flashcalw_lock_page_region(), flashcalw_no_operation(), flashcalw_quick_page_read(), flashcalw_quick_user_page_read(), flashcalw_set_flash_waitstate_and_readmode(), flashcalw_set_security_bit(), flashcalw_write_gp_fuse_bit(), flashcalw_write_gp_fuse_byte(), flashcalw_write_page(), and flashcalw_write_user_page().

void flashcalw_lock_all_regions ( bool  lock)

Locks or unlocks all regions.

Parameters
lockWhether to lock the regions: true or false.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_error_status, flashcalw_lock_region(), and FLASHCALW_REGIONS.

void flashcalw_lock_page_region ( int  page_number,
bool  lock 
)

Locks or unlocks the region of a page.

Parameters
page_numberThe page number:
lockWhether to lock the region of the specified page: true or false.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_issue_command().

Referenced by flashcalw_lock_region().

void flashcalw_lock_region ( uint32_t  region,
bool  lock 
)

Locks or unlocks a region.

Parameters
regionThe region number: 0 to (FLASHCALW_REGIONS - 1).
lockWhether to lock the specified region: true or false.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_get_region_first_page_number(), and flashcalw_lock_page_region().

Referenced by flashcalw_lock_all_regions().

volatile void* flashcalw_memcpy ( volatile void *  dst,
const void *  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the source pointed to by src.

The destination areas that are not within the flash array or the User page are caught by an Assert() operation.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcPointer to source data.
nbytesNumber of bytes to copy.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
If copying takes place between areas that overlap, the behavior is undefined.
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References Assert, FLASH_PAGE_SIZE, flashcalw_clear_page_buffer(), flashcalw_erase_page(), flashcalw_erase_user_page(), flashcalw_error_status, flashcalw_get_flash_size(), flashcalw_write_page(), flashcalw_write_user_page(), Union64::u64, and Union64::u8.

Referenced by program_memory().

volatile void* flashcalw_memset16 ( volatile void *  dst,
uint16_t  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source half-word.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcSource half-word.
nbytesNumber of bytes to set.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_memset32().

Referenced by flashcalw_memset8().

volatile void* flashcalw_memset32 ( volatile void *  dst,
uint32_t  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source word.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcSource word.
nbytesNumber of bytes to set.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_memset64().

Referenced by flashcalw_memset16().

volatile void* flashcalw_memset64 ( volatile void *  dst,
uint64_t  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source double-word.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcSource double-word.
nbytesNumber of bytes to set.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References Align_down, FLASH_PAGE_SIZE, flashcalw_clear_page_buffer(), flashcalw_erase_page(), flashcalw_erase_user_page(), flashcalw_error_status, flashcalw_get_flash_size(), flashcalw_write_page(), flashcalw_write_user_page(), Get_align, Min, Test_align, StructCVPtr::u16ptr, UnionVPtr::u32ptr, StructCVPtr::u32ptr, Union64::u64, UnionVPtr::u64ptr, UnionCVPtr::u64ptr, StructCVPtr::u64ptr, Union64::u8, UnionVPtr::u8ptr, UnionCVPtr::u8ptr, and StructCVPtr::u8ptr.

Referenced by flashcalw_memset32().

volatile void* flashcalw_memset8 ( volatile void *  dst,
uint8_t  src,
size_t  nbytes,
bool  erase 
)

Copies nbytes bytes to the flash destination pointed to by dst from the repeated src source byte.

All pointer and size alignments are supported.

Parameters
dstPointer to flash destination.
srcSource byte.
nbytesNumber of bytes to set.
eraseWhether to erase before writing: true or false.
Returns
The value of dst.
Warning
This function may be called with erase set to false only if the destination consists only of erased words, i.e. this function cannot be used to write only one bit of a previously written word. E.g., if 0x00000001 then 0xFFFFFFFE are written to a word, the resulting value in flash may be different from 0x00000000.
A Lock Error is issued if the command is applied to pages belonging to a locked region or to the bootloader protected area.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_memset16().

void flashcalw_no_operation ( void  )

Issues a No Operation command to the FLASHCALW.

Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_issue_command().

void flashcalw_picocache_disable ( void  )
void flashcalw_picocache_disable_monitor ( void  )

Disable PicoCache monitor.

void flashcalw_picocache_enable ( void  )
void flashcalw_picocache_enable_monitor ( void  )

Enable PicoCache monitor.

uint32_t flashcalw_picocache_get_monitor_cnt ( void  )

Get PicoCache monitor count number.

Returns
Monitor counter number.
uint32_t flashcalw_picocache_get_status ( void  )

Get PicoCache status.

Returns
1 If PicoCahe is enabled, else disabled.

Referenced by flashcalw_picocache_disable(), flashcalw_picocache_enable(), and flashcalw_picocache_invalid_line().

uint32_t flashcalw_picocache_get_version ( void  )

Get PicoCache version.

Returns
PicoCache version.
void flashcalw_picocache_invalid_all ( void  )

Invalid all PicoCache lines.

void flashcalw_picocache_invalid_line ( uint32_t  index)

Invalid specific cache line.

Parameters
indexLines to be invalid.

References flashcalw_picocache_get_status().

void flashcalw_picocache_reset_monitor ( void  )

Reset PicoCache monitor.

void flashcalw_picocache_set_monitor_mode ( uint32_t  mode)

Set PicoCache monitor mode.

Parameters
modePicoCache mode, 0 for cycle, 1 for instruction hit and 2 for data hit.
bool flashcalw_quick_page_read ( int  page_number)

Applies the Quick Page Read command to a page.

Parameters
page_numberThe page number:
Returns
Whether the specified page is erased.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_is_page_erased(), and flashcalw_issue_command().

Referenced by flashcalw_erase_page().

bool flashcalw_quick_user_page_read ( void  )

Issues a Quick Page Read User Page command to the FLASHCALW.

Returns
Whether the User page is erased.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_is_page_erased(), and flashcalw_issue_command().

Referenced by flashcalw_erase_user_page().

uint64_t flashcalw_read_all_gp_fuses ( void  )

Reads all general-purpose fuses.

Returns
The value of all general-purpose fuses as a word.
Note
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

Referenced by flashcalw_erase_all_gp_fuses(), flashcalw_erase_gp_fuse_byte(), flashcalw_read_gp_fuse_bit(), flashcalw_read_gp_fuse_bitfield(), and flashcalw_read_gp_fuse_byte().

bool flashcalw_read_gp_fuse_bit ( uint32_t  gp_fuse_bit)

Reads a general-purpose fuse bit.

Parameters
gp_fuse_bitThe general-purpose fuse bit: 0 to 63.
Returns
The value of the specified general-purpose fuse bit.
Note
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_read_all_gp_fuses().

Referenced by bootloader_mode_check(), flashcalw_erase_gp_fuse_bit(), and main().

uint64_t flashcalw_read_gp_fuse_bitfield ( uint32_t  pos,
uint32_t  width 
)

Reads a general-purpose fuse bit-field.

Parameters
posThe bit-position of the general-purpose fuse bit-field: 0 to 63.
widthThe bit-width of the general-purpose fuse bit-field: 0 to 64.
Returns
The value of the specified general-purpose fuse bit-field.
Note
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_read_all_gp_fuses(), and Min.

Referenced by flashcalw_erase_gp_fuse_bitfield().

uint8_t flashcalw_read_gp_fuse_byte ( uint32_t  gp_fuse_byte)

Reads a general-purpose fuse byte.

Parameters
gp_fuse_byteThe general-purpose fuse byte: 0 to 7.
Returns
The value of the specified general-purpose fuse byte.
Note
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_read_all_gp_fuses().

Referenced by flashcalw_erase_gp_fuse_byte().

void flashcalw_set_all_gp_fuses ( uint64_t  value)

Sets all general-purpose fuses with the appropriate erase and write operations.

Parameters
valueThe value of all general-purpose fuses as a word.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

use (uint64_t)-1 instead of 0xFFFFFFFFFFFFFFFFULL to avoid compilation warning

References flashcalw_erase_all_gp_fuses(), flashcalw_error_status, and flashcalw_write_all_gp_fuses().

void flashcalw_set_flash_waitstate_and_readmode ( uint32_t  cpu_f_hz,
uint32_t  ps_value,
bool  is_fwu_enabled 
)

Depending on the CPU frequency, on the Power Scaling mode and on the Fast Wakeup mode, set the wait states of flash read accesses and enable or disable the High speed read mode.

Parameters
cpu_f_hzThe CPU frequency
ps_valuePower Scaling mode value (0, 1)
is_fwu_enabled(boolean), Is fast wakeup mode enabled or not

References FLASH_FREQ_PS0_FWS_0_MAX_FREQ, FLASH_FREQ_PS0_FWS_1_MAX_FREQ, FLASH_FREQ_PS1_FWS_0_MAX_FREQ, FLASH_FREQ_PS1_FWS_1_FWU_MAX_FREQ, FLASH_FREQ_PS2_FWS_0_MAX_FREQ, flashcalw_issue_command(), flashcalw_set_wait_state(), and UNUSED.

void flashcalw_set_gp_fuse_bit ( uint32_t  gp_fuse_bit,
bool  value 
)

Sets a general-purpose fuse bit with the appropriate erase and write operations.

Parameters
gp_fuse_bitThe general-purpose fuse bit: 0 to 63.
valueThe value of the specified general-purpose fuse bit.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_erase_gp_fuse_bit(), and flashcalw_write_gp_fuse_bit().

Referenced by flashcalw_set_gp_fuse_bitfield().

void flashcalw_set_gp_fuse_bitfield ( uint32_t  pos,
uint32_t  width,
uint64_t  value 
)

Sets a general-purpose fuse bit-field with the appropriate erase and write operations.

Parameters
posThe bit-position of the general-purpose fuse bit-field: 0 to 63.
widthThe bit-width of the general-purpose fuse bit-field: 0 to 64.
valueThe value of the specified general-purpose fuse bit-field.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_error_status, flashcalw_set_gp_fuse_bit(), and Min.

void flashcalw_set_gp_fuse_byte ( uint32_t  gp_fuse_byte,
uint8_t  value 
)

Sets a general-purpose fuse byte with the appropriate erase and write operations.

Parameters
gp_fuse_byteThe general-purpose fuse byte: 0 to 7.
valueThe value of the specified general-purpose fuse byte.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_erase_gp_fuse_byte(), flashcalw_error_status, and flashcalw_write_gp_fuse_byte().

void flashcalw_set_security_bit ( void  )

Activates the Security bit.

Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.

References flashcalw_issue_command().

Referenced by main().

void flashcalw_set_wait_state ( uint32_t  wait_state)

Sets the number of wait states of flash read accesses.

Parameters
wait_stateThe number of wait states of flash read accesses: 0 to 1.

Referenced by flashcalw_set_flash_waitstate_and_readmode().

void flashcalw_write_all_gp_fuses ( uint64_t  value)

Writes all general-purpose fuses.

Parameters
valueThe value of all general-purpose fuses as a word.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_error_status, and flashcalw_write_gp_fuse_byte().

Referenced by flashcalw_set_all_gp_fuses().

void flashcalw_write_gp_fuse_bit ( uint32_t  gp_fuse_bit,
bool  value 
)

Writes a general-purpose fuse bit.

Parameters
gp_fuse_bitThe general-purpose fuse bit: 0 to 63.
valueThe value of the specified general-purpose fuse bit.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_issue_command().

Referenced by flashcalw_set_gp_fuse_bit(), and flashcalw_write_gp_fuse_bitfield().

void flashcalw_write_gp_fuse_bitfield ( uint32_t  pos,
uint32_t  width,
uint64_t  value 
)

Writes a general-purpose fuse bit-field.

Parameters
posThe bit-position of the general-purpose fuse bit-field: 0 to 63.
widthThe bit-width of the general-purpose fuse bit-field: 0 to 64.
valueThe value of the specified general-purpose fuse bit-field.
Warning
A Lock Error is issued if the Security bit is active and the command is applied to BOOTPROT.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_error_status, flashcalw_write_gp_fuse_bit(), and Min.

void flashcalw_write_gp_fuse_byte ( uint32_t  gp_fuse_byte,
uint8_t  value 
)

Writes a general-purpose fuse byte.

Parameters
gp_fuse_byteThe general-purpose fuse byte: 0 to 7.
valueThe value of the specified general-purpose fuse byte.
Warning
A Lock Error is issued if the Security bit is active.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.
The actual number of general-purpose fuse bits implemented by hardware is given by FLASH_GPF_NUM. The other bits among the 64 are fixed at 1 by hardware.

References flashcalw_issue_command().

Referenced by flashcalw_erase_gp_fuse_byte(), flashcalw_set_gp_fuse_byte(), and flashcalw_write_all_gp_fuses().

void flashcalw_write_page ( int  page_number)

Writes a page from the page buffer.

Parameters
page_numberThe page number:
Warning
A Lock Error is issued if the command is applied to a page belonging to a locked region or to the bootloader protected area.
The page buffer is not automatically reset after a page write.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.

References flashcalw_issue_command().

Referenced by flashcalw_memcpy(), and flashcalw_memset64().

void flashcalw_write_user_page ( void  )

Writes the User page from the page buffer.

Warning
The page buffer is not automatically reset after a page write.
Note
The FLASHCALW error status returned by flashcalw_is_lock_error and flashcalw_is_programming_error is updated.
A write operation can only clear bits; in other words, an erase operation must first be done if some bits need to be set to 1.

References flashcalw_issue_command().

Referenced by flashcalw_memcpy(), and flashcalw_memset64().

uint32_t flashcalw_error_status = 0
static

Sticky error status of the FLASHCALW.

This variable is updated by functions that issue FLASHCALW commands. It contains the cumulated FLASHCALW error status of all the FLASHCALW commands issued by a function.

Referenced by flashcalw_erase_all_pages(), flashcalw_erase_gp_fuse_bitfield(), flashcalw_erase_gp_fuse_byte(), flashcalw_erase_page(), flashcalw_lock_all_regions(), flashcalw_memcpy(), flashcalw_memset64(), flashcalw_set_all_gp_fuses(), flashcalw_set_gp_fuse_bitfield(), flashcalw_set_gp_fuse_byte(), flashcalw_write_all_gp_fuses(), and flashcalw_write_gp_fuse_bitfield().

void(*volatile flashcalw_wait_until_ready)(void) = flashcalw_default_wait_until_ready

Pointer to the function used by the driver when it needs to wait until the FLASHCALW is ready to run a new command.

The default function is flashcalw_default_wait_until_ready. The user may change this pointer to use another implementation.

Referenced by flashcalw_issue_command().