app.c | Application layer for low power and full features demo initialization |
 app.h | Application layer for low power and full features demo initialization |
 ast.c | SAM Asynchronous Timer (AST) driver |
 ast.h | SAM Asynchronous Timer (AST) driver |
 ast_example1.h | SAM Asynchronous Timer (AST) Example 1 Calendar Mode |
 ast_example2.h | SAM Asynchronous Timer (AST) example 2 alarm wakeup |
 BitBangSPI_Master.c | This file contains the BitBangSPI public API that can be used to transfer data from a Touch Device to QTouch Studio using the QT600 USB Bridge |
 BitBangSPI_Master.h | |
 board.h | Standard board header file |
 board_monitor.c | SAM4L-EK Board Monitor Control |
 board_monitor.h | SAM4L-EK Board Monitor Control |
 bpm.c | BPM driver |
 bpm.h | BPM driver |
 c42364a.h | Management of C42364A LCD Glass component |
 c42364a_lcdca.c | Management of C42364A LCD Glass component |
 c42364a_segmap.h | Default configuration of C42364A LCD Segment Map |
 compiler.h | Commonly used includes, types and macros |
 conf_ast.h | AST configuration |
 conf_board.h | Configuration File for SAM4L-EK Board |
 conf_c42364a_lcdca.h | C42364A configuration |
 conf_clock.h | Chip-specific system clock manager configuration |
 conf_lcdca.h | SAM Liquid Crystal Display driver (LCDCA) |
 conf_sleepmgr.h | Chip-specific sleep manager configuration |
 cycle_counter.c | ARM functions for busy-wait delay loops |
 cycle_counter.h | ARM functions for busy-wait delay loops |
 delay.h | Common Delay Service |
 dfll.c | Chip-specific DFLL implementation |
 dfll.h | DFLL management |
 sam4l/dfll.h | Chip-specific DFLL definitions |
 eic.c | EIC driver for SAM |
 eic.h | EIC driver for SAM |
 event.c | Event Manager |
 event.h | Event Manager |
 flashcalw.c | FlashCALW driver for SAM4L |
 flashcalw.h | FlashCALW driver for SAM4L |
 genclk.h | Generic clock management |
 sam4l/genclk.h | Chip-specific generic clock management |
 init.c | SAM4L-EK Board init |
 interrupt.h | Global interrupt management for 8- and 32-bit AVR |
 interrupt_sam_nvic.c | Global interrupt management for SAM D20, SAM3 and SAM4 (NVIC based) |
 interrupt_sam_nvic.h | Global interrupt management for SAM D20, SAM3 and SAM4 (NVIC based) |
 io.h | Arch file for SAM |
 ioport.h | Common IOPORT service main header file for AVR, UC3 and ARM architectures |
 ioport_gpio.h | SAM architecture specific IOPORT service implementation header file |
 lcdca.c | SAM4L Liquid Crystal Display driver (LCDCA) |
 lcdca.h | SAM4L Liquid Crystal Display driver (LCDCA) |
 lcdca_example.h | SAM4L LCDCA example |
 led.h | SAM4L-EK Board LEDs support package |
 main.c | Low Power and QTouch Demo for SAM4L |
 mrepeat.h | Preprocessor macro repeating utils |
 osc.c | Chip-specific oscillator management functions |
 osc.h | Oscillator management |
 sam4l/osc.h | Chip-specific oscillator management functions |
 parts.h | Atmel part identification macros |
 pdca.c | PDCA driver for SAM4L |
 pdca.h | PDCA driver for SAM4L |
 pll.c | Chip-specific PLL implementation |
 pll.h | PLL management |
 sam4l/pll.h | Chip-specific PLL definitions |
 preprocessor.h | Preprocessor utils |
 QDebug_sam4l.c | This file contains the QDebug public API that can be used to transfer data from a Touch Device to QTouch Studio using the QT600 USB Bridge |
 QDebug_sam4l.h | This file contains the QDebug public API that can be used to transfer data from a Touch Device to QTouch Studio using the QT600 USB Bridge |
 QDebugSettings.h | QTouch debug settings |
 QDebugTransport.c | |
 QDebugTransport.h | |
 read.c | System-specific implementation of the _read function used by the standard library |
 sam4l_ek.h | SAM4L-EK Board header file |
 sleepmgr.c | Chip-specific sleep manager configuration |
 sam4l/sleepmgr.h | Chip-specific sleep manager configuration |
 sleepmgr.h | Sleep manager |
 status_codes.h | Status code definitions |
 stringz.h | Preprocessor stringizing utils |
 sysclk.c | Chip-specific system clock management functions |
 sam4l/sysclk.h | Chip-specific system clock management functions |
 sysclk.h | System clock management |
 touch.c | QTouch example for SAM4L |
 touch_api_sam4l.h | This file contains the SAM4L QTouch Libary API interface for QMatrix, QTouch and Autonomous Touch method using the Capacitive Touch (CATB) module |
 touch_config_sam4l.h | This file contains the SAM4L QTouch Library pin, register and sensors configuration options for Capacitive Touch acquisition using the CATB module |
 tpaste.h | Preprocessor token pasting utils |
 ui.c | User Interface |
 ui.h | User Interface |
 usart.c | Universal Synchronous Asynchronous Receiver Transmitter (USART) driver for SAM |
 usart.h | Universal Synchronous Asynchronous Receiver Transmitter (USART) driver for SAM |
 wdt_sam4l.c | Watchdog Timer (WDT) driver for SAM4L |
 wdt_sam4l.h | Watchdog Timer (WDT) driver for SAM4L |
 write.c | System-specific implementation of the _write function used by the standard library |