This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Asynchronous Timer functionality.
The Asynchronous Timer can generate periodic interrupts and peripheral events from output from the prescaler, as well as alarm interrupts and peripheral events, which can trigger at any counter value.
Devices from the following series can use this module:
The outline of this documentation is as follows:
There are no prerequisites for this module.
The AST module in the SAM4L devices is a 32-bit counter, with a 32-bit programmable prescaler. Typically, the AST clock is run continuously, including in the device's low-power sleep modes, to track the current time and date information. The AST can also wake-up the system from backup mode using either the alarm wakeup, periodic wakeup, or overflow wake-up mechanisms.
The AST has been designed to meet the system tick and Real-Time Clock requirements of most embedded operating systems.
In this driver, the AST is operated in Calendar Mode. This allows for an easy integration of a Real-Time Clock and calendar into a user application to track the passing of time and/or perform scheduled tasks.
Whilst operating in Calendar Mode, the AST features:
The AST has a device dependent number of independent hardware alarms that can be configured by the user application. These alarms will be triggered on a match with the current clock value, and can be set up to trigger an interrupt, event, or both. The AST can also be configured to clear the clock value on alarm match which will generate an overflow interrupt.
Whilst in Calendar Mode and using a nominal 1Hz input clock frequency, a register overflow will occur after 64 years.
The AST can generate events at periodic intervals, allowing for direct peripheral actions without CPU intervention. The periodic events can be generated on an AST prescaler match, and will be generated on the rising edge transition of the specified bit. The resulting periodic frequency can be calculated by the following formula:
\[ f_{PERIODIC}=\frac{f_{ASY}}{2^{n+1}} \]
Where \(f_{ASY}\) refers to the asynchronous clock set up in the AST module configuration.
The AST module contains Digital Tuner logic to compensate for inaccurate source clock frequencies, which would otherwise result in skewed time measurements.
The external crystal selection used by the AST module in the final system design must take into account:
The AST module has a year range of 63 years from the starting year configured when the module is initialized. Dates outside the start to end year range described below will need software adjustment:
\[ [YEAR_{START}, YEAR_{START}+64] \]
For extra information, see Extra Information for Asynchronous Timer Driver. This includes:
For a list of examples related to this driver, see Examples for Asynchronous Timer Driver.
Data Structures | |
struct | ast_calendar |
struct | ast_calv |
Description for Calendar Field. More... | |
struct | ast_config |
AST configuration. More... | |
Macros | |
#define | AST_POLL_TIMEOUT 10000 |
Timeout to prevent code hang in clock initialization. More... | |
Typedefs | |
typedef void(* | ast_callback_t )(void) |
AST interrupt callback. More... | |
typedef enum ast_event_source | ast_event_source_t |
AST event source. More... | |
typedef enum ast_interrupt_source | ast_interrupt_source_t |
AST interrupt source. More... | |
typedef enum ast_mode | ast_mode_t |
AST Calendar Mode. More... | |
typedef enum ast_oscillator_type | ast_oscillator_type_t |
AST Oscillator type. More... | |
typedef enum ast_wakeup_source | ast_wakeup_source_t |
AST wake-up source. More... | |
Enumerations | |
enum | ast_event_source { AST_EVENT_ALARM = 0, AST_EVENT_PER, AST_EVENT_OVF } |
AST event source. More... | |
enum | ast_interrupt_source { AST_INTERRUPT_ALARM = 0, AST_INTERRUPT_PER, AST_INTERRUPT_OVF, AST_INTERRUPT_READY, AST_INTERRUPT_CLKREADY } |
AST interrupt source. More... | |
enum | ast_mode { AST_COUNTER_MODE = 0, AST_CALENDAR_MODE = 1 } |
AST Calendar Mode. More... | |
enum | ast_oscillator_type { AST_OSC_RC = 0, AST_OSC_32KHZ = 1, AST_OSC_PB = 2, AST_OSC_GCLK = 3, AST_OSC_1KHZ = 4 } |
AST Oscillator type. More... | |
enum | ast_wakeup_source { AST_WAKEUP_ALARM = 0, AST_WAKEUP_PER, AST_WAKEUP_OVF } |
AST wake-up source. More... | |
Functions | |
void | ast_clear_interrupt_flag (Ast *ast, ast_interrupt_source_t source) |
Clear an AST interrupt status flag. More... | |
void | ast_clear_prescalar (Ast *ast) |
Clear the AST periodic prescaler counter to zero. More... | |
uint32_t | ast_configure_digital_tuner (Ast *ast, uint32_t input_freq, uint32_t tuned_freq) |
Tune the AST prescaler frequency to the desired frequency. More... | |
void | ast_disable (Ast *ast) |
Disable the AST counter and module. More... | |
void | ast_disable_digital_tuner (Ast *ast) |
Disable the AST digital tuner. More... | |
void | ast_disable_event (Ast *ast, ast_event_source_t source) |
Disable an AST event. More... | |
void | ast_disable_interrupt (Ast *ast, ast_interrupt_source_t source) |
Disable an AST interrupt. More... | |
void | ast_disable_wakeup (Ast *ast, ast_wakeup_source_t source) |
Disable an AST asynchronous wake-up source. More... | |
void | ast_enable (Ast *ast) |
Enable the AST module. More... | |
void | ast_enable_counter_clear_on_alarm (Ast *ast, uint8_t alarm_channel) |
Enable the option to clear the counter on an AST alarm. More... | |
void | ast_enable_event (Ast *ast, ast_event_source_t source) |
Enable an AST event. More... | |
void | ast_enable_interrupt (Ast *ast, ast_interrupt_source_t source) |
Enable an AST interrupt. More... | |
void | ast_enable_wakeup (Ast *ast, ast_wakeup_source_t source) |
Enable an AST asynchronous wake-up source. More... | |
void | ast_init_digital_tuner (Ast *ast, bool add, uint8_t value, uint8_t exp) |
Initialize the AST digital tuner. More... | |
static bool | ast_is_busy (Ast *ast) |
Check the busy status of AST. More... | |
static bool | ast_is_clkbusy (Ast *ast) |
Check the busy status of the AST clock. More... | |
bool | ast_is_enabled (Ast *ast) |
Check the status of the AST module. More... | |
struct ast_calendar | ast_read_calendar_value (Ast *ast) |
Get the AST current calendar value. More... | |
static uint32_t | ast_read_counter_value (Ast *ast) |
Get the AST current counter value. More... | |
static uint32_t | ast_read_interrupt_mask (Ast *ast) |
Get the AST interrupt mask value. More... | |
static uint32_t | ast_read_status (Ast *ast) |
Get the status of AST. More... | |
void | ast_set_callback (Ast *ast, ast_interrupt_source_t source, ast_callback_t callback, uint8_t irq_line, uint8_t irq_level) |
Set callback for AST interrupts. More... | |
uint32_t | ast_set_config (Ast *ast, struct ast_config *ast_conf) |
Initialize and enable the AST module in Calendar Mode or Counter Mode. More... | |
static void | ast_start (Ast *ast) |
Start the AST counter. More... | |
static void | ast_stop (Ast *ast) |
Stop the AST counter. More... | |
void | ast_write_alarm0_value (Ast *ast, uint32_t alarm_value) |
Set the AST alarm0 value. More... | |
void | ast_write_calendar_value (Ast *ast, struct ast_calendar calendar) |
Set the AST current calendar value. More... | |
void | ast_write_counter_value (Ast *ast, uint32_t ast_counter) |
Set the AST current counter value. More... | |
void | ast_write_periodic0_value (Ast *ast, uint32_t pir) |
Set the AST periodic0 value. More... | |
Predefined PSEL Values | |
#define | AST_PSEL_32KHZ_1HZ 14 |
The PSEL value to set the AST source clock (after the prescaler) to 1Hz, when using an external 32-kHz crystal. More... | |
#define | AST_PSEL_RC_1_76HZ 15 |
The PSEL value to set the AST source clock (after the prescaler) to 1.76Hz when using the internal RC oscillator (~ 115kHz) More... | |
#define AST_POLL_TIMEOUT 10000 |
Timeout to prevent code hang in clock initialization.
Referenced by ast_set_config().
#define AST_PSEL_32KHZ_1HZ 14 |
The PSEL value to set the AST source clock (after the prescaler) to 1Hz, when using an external 32-kHz crystal.
Referenced by event_qtouch_init().
#define AST_PSEL_RC_1_76HZ 15 |
The PSEL value to set the AST source clock (after the prescaler) to 1.76Hz when using the internal RC oscillator (~ 115kHz)
typedef void(* ast_callback_t)(void) |
AST interrupt callback.
typedef enum ast_event_source ast_event_source_t |
typedef enum ast_interrupt_source ast_interrupt_source_t |
typedef enum ast_mode ast_mode_t |
typedef enum ast_oscillator_type ast_oscillator_type_t |
typedef enum ast_wakeup_source ast_wakeup_source_t |
enum ast_event_source |
enum ast_interrupt_source |
enum ast_mode |
enum ast_oscillator_type |
enum ast_wakeup_source |
void ast_clear_interrupt_flag | ( | Ast * | ast, |
ast_interrupt_source_t | source | ||
) |
Clear an AST interrupt status flag.
[in,out] | ast | Module hardware register base address pointer |
[in] | source | AST interrupt source for which the status is to be cleared |
References AST_INTERRUPT_ALARM, AST_INTERRUPT_CLKREADY, AST_INTERRUPT_OVF, AST_INTERRUPT_PER, AST_INTERRUPT_READY, and ast_is_busy().
Referenced by ast_per_callback(), and event_qtouch_init().
void ast_clear_prescalar | ( | Ast * | ast | ) |
Clear the AST periodic prescaler counter to zero.
[in,out] | ast | Module hardware register base address pointer |
References ast_is_busy().
uint32_t ast_configure_digital_tuner | ( | Ast * | ast, |
uint32_t | input_freq, | ||
uint32_t | tuned_freq | ||
) |
Tune the AST prescaler frequency to the desired frequency.
[in,out] | ast | Module hardware register base address pointer |
[in] | input_freq | Prescaled AST Clock Frequency |
[in] | tuned_freq | Desired AST frequency |
References ast_init_digital_tuner(), and div_ceil.
void ast_disable | ( | Ast * | ast | ) |
Disable the AST counter and module.
[in,out] | ast | Module hardware register base address pointer |
References ast_is_busy(), SLEEPMGR_BACKUP, sleepmgr_unlock_mode(), and sysclk_disable_peripheral_clock().
void ast_disable_digital_tuner | ( | Ast * | ast | ) |
Disable the AST digital tuner.
[in,out] | ast | Module hardware register base address pointer |
References ast_is_busy().
void ast_disable_event | ( | Ast * | ast, |
ast_event_source_t | source | ||
) |
Disable an AST event.
[in,out] | ast | Module hardware register base address pointer |
[in] | source | AST event source to be disabled |
References AST_EVENT_ALARM, AST_EVENT_OVF, AST_EVENT_PER, and ast_is_busy().
void ast_disable_interrupt | ( | Ast * | ast, |
ast_interrupt_source_t | source | ||
) |
Disable an AST interrupt.
[in,out] | ast | Module hardware register base address pointer |
[in] | source | AST interrupt source to be disabled |
References AST_INTERRUPT_ALARM, AST_INTERRUPT_CLKREADY, AST_INTERRUPT_OVF, AST_INTERRUPT_PER, AST_INTERRUPT_READY, and ast_is_busy().
void ast_disable_wakeup | ( | Ast * | ast, |
ast_wakeup_source_t | source | ||
) |
Disable an AST asynchronous wake-up source.
[in,out] | ast | Module hardware register base address pointer |
[in] | source | AST wake-up source to be disabled |
References ast_is_busy(), AST_WAKEUP_ALARM, AST_WAKEUP_OVF, and AST_WAKEUP_PER.
void ast_enable | ( | Ast * | ast | ) |
Enable the AST module.
[in] | ast | Module hardware register base address pointer |
References SLEEPMGR_BACKUP, sleepmgr_lock_mode(), and sysclk_enable_peripheral_clock().
Referenced by event_qtouch_init().
void ast_enable_counter_clear_on_alarm | ( | Ast * | ast, |
uint8_t | alarm_channel | ||
) |
Enable the option to clear the counter on an AST alarm.
[in,out] | ast | Module hardware register base address pointer |
[in] | alarm_channel | AST Alarm Channel |
References ast_is_busy().
void ast_enable_event | ( | Ast * | ast, |
ast_event_source_t | source | ||
) |
Enable an AST event.
[in,out] | ast | Module hardware register base address pointer |
[in] | source | AST event source to be enabled |
References AST_EVENT_ALARM, AST_EVENT_OVF, AST_EVENT_PER, and ast_is_busy().
void ast_enable_interrupt | ( | Ast * | ast, |
ast_interrupt_source_t | source | ||
) |
Enable an AST interrupt.
[in,out] | ast | Module hardware register base address pointer |
[in] | source | AST interrupt source to be enabled |
References AST_INTERRUPT_ALARM, AST_INTERRUPT_CLKREADY, AST_INTERRUPT_OVF, AST_INTERRUPT_PER, AST_INTERRUPT_READY, and ast_is_busy().
Referenced by ast_set_callback().
void ast_enable_wakeup | ( | Ast * | ast, |
ast_wakeup_source_t | source | ||
) |
Enable an AST asynchronous wake-up source.
[in,out] | ast | Module hardware register base address pointer |
[in] | source | AST wake-up source to be enabled |
References ast_is_busy(), AST_WAKEUP_ALARM, AST_WAKEUP_OVF, and AST_WAKEUP_PER.
void ast_init_digital_tuner | ( | Ast * | ast, |
bool | add, | ||
uint8_t | value, | ||
uint8_t | exp | ||
) |
Initialize the AST digital tuner.
[in,out] | ast | Module hardware register base address pointer |
[in] | add | Set to true if the frequency needs to be increased, false if it has to be decreased. |
[in] | value | Parameter used in the formula |
[in] | exp | Parameter used in the formula |
References ast_is_busy().
Referenced by ast_configure_digital_tuner().
|
inlinestatic |
Check the busy status of AST.
[in] | ast | Module hardware register base address pointer |
false | AST is not busy |
true | AST is busy |
Referenced by ast_clear_interrupt_flag(), ast_clear_prescalar(), ast_disable(), ast_disable_digital_tuner(), ast_disable_event(), ast_disable_interrupt(), ast_disable_wakeup(), ast_enable_counter_clear_on_alarm(), ast_enable_event(), ast_enable_interrupt(), ast_enable_wakeup(), ast_init_digital_tuner(), ast_is_enabled(), ast_set_config(), ast_start(), ast_stop(), ast_write_alarm0_value(), ast_write_calendar_value(), ast_write_counter_value(), and ast_write_periodic0_value().
|
inlinestatic |
Check the busy status of the AST clock.
[in] | ast | Module hardware register base address pointer |
false | AST clock is not busy |
true | AST clock is busy |
Referenced by ast_set_config().
bool ast_is_enabled | ( | Ast * | ast | ) |
Check the status of the AST module.
[in,out] | ast | Module hardware register base address pointer |
false | AST is not enabled |
true | AST is enabled |
References ast_is_busy().
struct ast_calendar ast_read_calendar_value | ( | Ast * | ast | ) |
Get the AST current calendar value.
[in] | ast | Module hardware register base address pointer |
References ast_calendar::field.
|
inlinestatic |
Get the AST current counter value.
[in] | ast | Module hardware register base address pointer |
|
inlinestatic |
Get the AST interrupt mask value.
[in] | ast | Module hardware register base address pointer |
|
inlinestatic |
Get the status of AST.
[in] | ast | Module hardware register base address pointer |
void ast_set_callback | ( | Ast * | ast, |
ast_interrupt_source_t | source, | ||
ast_callback_t | callback, | ||
uint8_t | irq_line, | ||
uint8_t | irq_level | ||
) |
Set callback for AST interrupts.
[in,out] | ast | Module hardware register base address pointer |
[in] | source | AST interrupt source |
[in] | callback | Callback function pointer |
[in] | irq_line | Interrupt line |
[in] | irq_level | Interrupt level |
References ast_callback_pointer, and ast_enable_interrupt().
Referenced by event_qtouch_init().
uint32_t ast_set_config | ( | Ast * | ast, |
struct ast_config * | ast_conf | ||
) |
Initialize and enable the AST module in Calendar Mode or Counter Mode.
[in,out] | ast | Module hardware register base address pointer |
[in] | ast_conf | AST configuration structure pointer |
0 | Initialization failed due to a software timeout |
1 | Initialization succeeded |
References AST_CALENDAR_MODE, AST_COUNTER_MODE, ast_is_busy(), ast_is_clkbusy(), AST_POLL_TIMEOUT, ast_write_calendar_value(), ast_write_counter_value(), ast_config::calendar, ast_config::counter, ast_config::mode, ast_config::osc_type, and ast_config::psel.
Referenced by event_qtouch_init().
|
inlinestatic |
Start the AST counter.
[in,out] | ast | Module hardware register base address pointer |
References ast_is_busy().
|
inlinestatic |
Stop the AST counter.
[in,out] | ast | Module hardware register base address pointer |
References ast_is_busy().
void ast_write_alarm0_value | ( | Ast * | ast, |
uint32_t | alarm_value | ||
) |
Set the AST alarm0 value.
[in,out] | ast | Module hardware register base address pointer |
[in] | alarm_value | AST alarm0 value |
References ast_is_busy().
void ast_write_calendar_value | ( | Ast * | ast, |
struct ast_calendar | calendar | ||
) |
Set the AST current calendar value.
[in,out] | ast | Module hardware register base address pointer |
[in] | calendar | Startup date structure |
References ast_is_busy(), and ast_calendar::field.
Referenced by ast_set_config().
void ast_write_counter_value | ( | Ast * | ast, |
uint32_t | ast_counter | ||
) |
Set the AST current counter value.
[in,out] | ast | Module hardware register base address pointer |
[in] | ast_counter | Startup counter value |
References ast_is_busy().
Referenced by ast_set_config().
void ast_write_periodic0_value | ( | Ast * | ast, |
uint32_t | pir | ||
) |
Set the AST periodic0 value.
[in,out] | ast | Module hardware register base address pointer |
[in] | pir | AST periodic0 |
References ast_is_busy().
Referenced by event_qtouch_init().