AP Configuration Extension.
This structure holds additional configuration parameters for the M2M AP mode. If modification of the extended parameters in AP mode is desired then tstrM2MAPModeConfig should be set by the application, which contains the main AP configuration structure as well as this extended parameters structure. When configuring provisioning mode then tstrM2MProvisionModeConfig should be used, which also contains the main AP configuration structure, this extended parameters structure and additional provisioning parameters.
#include <m2m_types.h>
Data Fields | |
uint8 | au8DefRouterIP [4] |
uint8 | au8DNSServerIP [4] |
uint8 | au8SubnetMask [4] |
uint8 tstrM2MAPConfigExt::au8DefRouterIP[4] |
Ap Default Router address
Referenced by m2m_wifi_enable_ap(), and m2m_wifi_start_provision_mode().
uint8 tstrM2MAPConfigExt::au8DNSServerIP[4] |
Ap DNS server address
Referenced by m2m_wifi_enable_ap(), and m2m_wifi_start_provision_mode().
uint8 tstrM2MAPConfigExt::au8SubnetMask[4] |
Network Subnet Mask
Referenced by m2m_wifi_enable_ap(), and m2m_wifi_start_provision_mode().