Low-level driver for the AT30TSE75X Series EEPROM controller.
This driver provides access to the main features of the AT30TSE75X Series EEPROM.
Macros | |
#define | AT30TSE75X_DEVICE_TYPE_ID_EEPROM 0x50 |
#define | AT30TSE75X_DEVICE_TYPE_ID_TEMP 0x48 |
#define | AT30TSE_EEPROM_TWI_ADDR |
#define | AT30TSE_TEMPERATURE_TWI_ADDR |
#define | BOARD_AT30TSE_DEVICE_ADDR 0x07 /* 0b111 */ |
#define | BOARD_AT30TSE_TWI TWI0 |
#define | BOARD_AT30TSE_TWI_ID ID_TWI0 |
#define | BOARD_TWI_SPEED 10000 |
#define | BOARD_USING_AT30TSE AT30TSE758 |
Functions | |
uint8_t | at30tse_eeprom_read (uint8_t *data, uint8_t length, uint8_t word_addr, uint8_t page) |
Read EEPROM in AT30TSE75x. More... | |
uint8_t | at30tse_eeprom_write (uint8_t *data, uint8_t length, uint8_t word_addr, uint8_t page) |
Write EEPROM in AT30TSE75x. More... | |
void | at30tse_init (void) |
Initialize the TWI instance used for AT30TSE75x. More... | |
uint8_t | at30tse_read_register (uint8_t reg, uint8_t reg_type, uint8_t reg_size, uint8_t *buffer) |
Read register in AT30TSE75x. More... | |
uint8_t | at30tse_read_temperature (double *temperature) |
Read temperature. More... | |
uint8_t | at30tse_write_config_register (uint16_t value) |
Write nonvolatile configuration register in AT30TSE75x. More... | |
uint8_t | at30tse_write_register (uint8_t reg, uint8_t reg_type, uint8_t reg_size, uint16_t reg_value) |
Write register in AT30TSE75x. More... | |
Variables | |
volatile uint8_t | resolution = AT30TSE_CONFIG_RES_9_bit |
#define AT30TSE75X_DEVICE_TYPE_ID_EEPROM 0x50 |
#define AT30TSE75X_DEVICE_TYPE_ID_TEMP 0x48 |
#define AT30TSE_EEPROM_TWI_ADDR |
Referenced by at30tse_eeprom_read(), and at30tse_eeprom_write().
#define AT30TSE_TEMPERATURE_TWI_ADDR |
Referenced by at30tse_read_register(), and at30tse_write_register().
#define BOARD_AT30TSE_DEVICE_ADDR 0x07 /* 0b111 */ |
#define BOARD_AT30TSE_TWI TWI0 |
Referenced by at30tse_eeprom_read(), at30tse_eeprom_write(), at30tse_init(), at30tse_read_register(), and at30tse_write_register().
#define BOARD_AT30TSE_TWI_ID ID_TWI0 |
Referenced by at30tse_init().
#define BOARD_TWI_SPEED 10000 |
Referenced by at30tse_init().
#define BOARD_USING_AT30TSE AT30TSE758 |
uint8_t at30tse_eeprom_read | ( | uint8_t * | data, |
uint8_t | length, | ||
uint8_t | word_addr, | ||
uint8_t | page | ||
) |
Read EEPROM in AT30TSE75x.
data | Pointer to the data to be read |
length | Length of the data to be read |
word_addr | Start EEPROM address to be read |
page | Specify the page to be read |
References twi_packet::addr, AT30TSE_EEPROM_TWI_ADDR, BOARD_AT30TSE_TWI, and twi_master_read().
uint8_t at30tse_eeprom_write | ( | uint8_t * | data, |
uint8_t | length, | ||
uint8_t | word_addr, | ||
uint8_t | page | ||
) |
Write EEPROM in AT30TSE75x.
data | Pointer to the data to be written |
length | Length of the data to be written |
word_addr | Start EEPROM address to be written |
page | Specify the page to be written |
References twi_packet::addr, AT30TSE_EEPROM_TWI_ADDR, BOARD_AT30TSE_TWI, and twi_master_write().
void at30tse_init | ( | void | ) |
Initialize the TWI instance used for AT30TSE75x.
References BOARD_AT30TSE_TWI, BOARD_AT30TSE_TWI_ID, BOARD_TWI_SPEED, twi_options::master_clk, sysclk_enable_peripheral_clock(), sysclk_get_cpu_hz(), and twi_master_init().
Referenced by main().
uint8_t at30tse_read_register | ( | uint8_t | reg, |
uint8_t | reg_type, | ||
uint8_t | reg_size, | ||
uint8_t * | buffer | ||
) |
Read register in AT30TSE75x.
reg | Register in AT30TSE75x to be read |
reg_type | Specify the type of the register, nonvolatile or not |
reg_size | Read lenght |
buffer | Pointer to the buffer where the read data will be stored |
References twi_packet::addr, AT30TSE_TEMPERATURE_TWI_ADDR, BOARD_AT30TSE_TWI, and twi_master_read().
Referenced by at30tse_read_temperature().
uint8_t at30tse_read_temperature | ( | double * | temperature | ) |
Read temperature.
temperature | Pointer to the buffer where the temperature will be stored |
References AT30TSE_CONFIG_RES_10_bit, AT30TSE_CONFIG_RES_11_bit, AT30TSE_CONFIG_RES_12_bit, AT30TSE_CONFIG_RES_9_bit, AT30TSE_NON_VOLATILE_REG, at30tse_read_register(), AT30TSE_TEMPERATURE_REG, AT30TSE_TEMPERATURE_REG_SIZE, resolution, and TWI_SUCCESS.
Referenced by main().
uint8_t at30tse_write_config_register | ( | uint16_t | value | ) |
Write nonvolatile configuration register in AT30TSE75x.
value | Value to be written |
References AT30TSE_CONFIG_REG, AT30TSE_CONFIG_REG_SIZE, AT30TSE_CONFIG_RES_Msk, AT30TSE_CONFIG_RES_Pos, AT30TSE_NON_VOLATILE_REG, at30tse_write_register(), resolution, and TWI_SUCCESS.
uint8_t at30tse_write_register | ( | uint8_t | reg, |
uint8_t | reg_type, | ||
uint8_t | reg_size, | ||
uint16_t | reg_value | ||
) |
Write register in AT30TSE75x.
reg | Register in AT30TSE75x to be read |
reg_type | Specify the type of the register, nonvolatile or not |
reg_size | Write lenght |
reg_value | Value to be written |
References twi_packet::addr, AT30TSE_TEMPERATURE_TWI_ADDR, BOARD_AT30TSE_TWI, and twi_master_write().
Referenced by at30tse_write_config_register().
volatile uint8_t resolution = AT30TSE_CONFIG_RES_9_bit |
Referenced by adc_set_resolution(), at30tse_read_temperature(), and at30tse_write_config_register().