Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
SAM3A/3U/3X/4E DMA Controller (DMAC) Driver

This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Direct Memory Access DMA Controller (DMAC) functionality.

The DMAC is an AHB-central DMA controller core that transfers data from a source peripheral to a destination peripheral over one or more AMBA buses. This is a driver for the configuration, enabling, disabling, and use of the DMAC peripheral.

Devices from the following series can use this module:

The outline of this documentation is as follows:

Prerequisites

There are no prerequisites for this module.

Module Overview

The DMA Controller (DMAC) is an AHB-central DMA controller core that transfers data from a source peripheral to a destination peripheral over one or more AMBA buses. One channel is required for each source/destination pair. In the most basic configuration, the DMAC has one master interface and one channel. The master interface reads the data from a source and writes it to a destination. Two AMBA transfers are required for each DMAC data transfer. This is also known as a dual-access transfer.

Special Considerations

There are no special considerations for this module.

Extra Information

For extra information, see Extra Information for Direct Memory Access Controller Driver. This includes:

Examples

For a list of examples related to this driver, see Examples for Direct Memory Access Controller Driver.

API Overview

Data Structures

struct  dma_transfer_descriptor_t
 DMA transfer descriptor structure, otherwise known as a Linked List Item (LLI). More...
 

Enumerations

enum  dmac_priority_mode_t {
  DMAC_PRIORITY_FIXED = 0,
  DMAC_PRIORITY_ROUND_ROBIN = DMAC_GCFG_ARB_CFG
}
 DMAC priority mode. More...
 

Functions

void dmac_channel_disable (Dmac *p_dmac, uint32_t ul_num)
 Disable the specified DMA Channel. More...
 
void dmac_channel_enable (Dmac *p_dmac, uint32_t ul_num)
 Enable the specified DMA Channel. More...
 
uint32_t dmac_channel_get_status (Dmac *p_dmac)
 Get the DMAC Channel handler status. More...
 
uint32_t dmac_channel_is_enable (Dmac *p_dmac, uint32_t ul_num)
 Check if the specified DMA Channel is enabled. More...
 
uint32_t dmac_channel_is_transfer_done (Dmac *p_dmac, uint32_t ul_num)
 Check if the data transfer occurring on the specified DMA Channel is complete. More...
 
void dmac_channel_keep (Dmac *p_dmac, uint32_t ul_num)
 Resume the specified DMA Channel from an automatic stall state. More...
 
void dmac_channel_multi_buf_transfer_init (Dmac *p_dmac, uint32_t ul_num, dma_transfer_descriptor_t *p_desc)
 Initialize the DMA Channel for a multiple buffer transfer. More...
 
void dmac_channel_resume (Dmac *p_dmac, uint32_t ul_num)
 Resume the specified DMA Channel transfer (restoring its context). More...
 
void dmac_channel_set_configuration (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_cfg)
 Set the DMAC configuration register of the specified DMA Channel. More...
 
void dmac_channel_set_ctrlA (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_ctrlA)
 Set the DMA control A of the specified DMA Channel. More...
 
void dmac_channel_set_ctrlB (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_ctrlB)
 Set the DMA control B of the specified DMA Channel. More...
 
void dmac_channel_set_descriptor_addr (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_desc)
 Set the DMA descriptor address of the specified DMA Channel. More...
 
void dmac_channel_set_destination_addr (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_addr)
 Set the DMA destination address of the specified DMA Channel. More...
 
void dmac_channel_set_source_addr (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_addr)
 Set the DMA source address of the specified DMA Channel. More...
 
void dmac_channel_single_buf_transfer_init (Dmac *p_dmac, uint32_t ul_num, dma_transfer_descriptor_t *p_desc)
 Initialize the DMA Channel for a single buffer transfer. More...
 
void dmac_channel_stop_transfer (Dmac *p_dmac, uint32_t ul_num)
 Stop a DMA transfer occurring on the specified DMA Channel. More...
 
void dmac_channel_suspend (Dmac *p_dmac, uint32_t ul_num)
 Suspend the specified DMA Channel and its current context. More...
 
void dmac_disable (Dmac *p_dmac)
 Disable the DMA Controller. More...
 
void dmac_disable_interrupt (Dmac *p_dmac, uint32_t ul_mask)
 Disable DMAC interrupts. More...
 
void dmac_enable (Dmac *p_dmac)
 Enable the DMA Controller. More...
 
void dmac_enable_interrupt (Dmac *p_dmac, uint32_t ul_mask)
 Enable DMAC interrupts. More...
 
uint32_t dmac_get_interrupt_mask (Dmac *p_dmac)
 Get the DMAC Interrupt Mask. More...
 
uint32_t dmac_get_status (Dmac *p_dmac)
 Get the DMAC transfer status. More...
 
void dmac_init (Dmac *p_dmac)
 Initialize the DMA controller and disable it. More...
 
void dmac_set_priority_mode (Dmac *p_dmac, dmac_priority_mode_t mode)
 Set the DMA priority mode. More...
 
void dmac_soft_chunk_transfer_request (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_src_req, uint32_t ul_dst_req)
 DMA Channel software chunk request. More...
 
void dmac_soft_set_last_transfer_flag (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_src_flag, uint32_t ul_dst_flag)
 Set the DMA Channel's last transfer flag. More...
 
void dmac_soft_single_transfer_request (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_src_req, uint32_t ul_dst_req)
 DMA Channel software single request. More...
 

DMAC priority mode.

Enumerator
DMAC_PRIORITY_FIXED 

Fixed priority arbiter.

DMAC_PRIORITY_ROUND_ROBIN 

Modified round robin arbiter.

void dmac_channel_disable ( Dmac *  p_dmac,
uint32_t  ul_num 
)

Disable the specified DMA Channel.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)

References Assert.

Referenced by dmac_channel_stop_transfer(), and init_dma().

void dmac_channel_enable ( Dmac *  p_dmac,
uint32_t  ul_num 
)

Enable the specified DMA Channel.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)

References Assert.

Referenced by ssc_dma().

uint32_t dmac_channel_get_status ( Dmac *  p_dmac)

Get the DMAC Channel handler status.

Parameters
[in]p_dmacModule hardware register base address pointer
Returns
DMAC Channel handler status register. Refer to the section called "DMAC Channel Handler Status Register" in the device-specific datasheet for more information.

References Assert.

Referenced by dmac_channel_is_transfer_done(), and dmac_channel_stop_transfer().

uint32_t dmac_channel_is_enable ( Dmac *  p_dmac,
uint32_t  ul_num 
)

Check if the specified DMA Channel is enabled.

Parameters
[in]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
Returns
The DMA Channel's enable/disable status.
Return values
0DMA Channel is disabled
1DMA Channel is enabled

References Assert.

uint32_t dmac_channel_is_transfer_done ( Dmac *  p_dmac,
uint32_t  ul_num 
)

Check if the data transfer occurring on the specified DMA Channel is complete.

Note
This function is used in polling mode.
Parameters
[in]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
Returns
The data transfer status.
Return values
0Data is transferring
1Data transfer complete

References Assert, and dmac_channel_get_status().

void dmac_channel_keep ( Dmac *  p_dmac,
uint32_t  ul_num 
)

Resume the specified DMA Channel from an automatic stall state.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)

References Assert.

void dmac_channel_multi_buf_transfer_init ( Dmac *  p_dmac,
uint32_t  ul_num,
dma_transfer_descriptor_t p_desc 
)

Initialize the DMA Channel for a multiple buffer transfer.

Parameters
[in,out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]p_descPointer to a transfer descriptor

References Assert, dmac_channel_set_ctrlB(), and dmac_channel_set_descriptor_addr().

void dmac_channel_resume ( Dmac *  p_dmac,
uint32_t  ul_num 
)

Resume the specified DMA Channel transfer (restoring its context).

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)

References Assert.

Referenced by dmac_channel_stop_transfer().

void dmac_channel_set_configuration ( Dmac *  p_dmac,
uint32_t  ul_num,
uint32_t  ul_cfg 
)

Set the DMAC configuration register of the specified DMA Channel.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]ul_cfgConfiguration of CFG register

References Assert.

Referenced by init_dma().

void dmac_channel_set_ctrlA ( Dmac *  p_dmac,
uint32_t  ul_num,
uint32_t  ul_ctrlA 
)

Set the DMA control A of the specified DMA Channel.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]ul_ctrlAConfiguration of control A register

References Assert.

Referenced by dmac_channel_single_buf_transfer_init().

void dmac_channel_set_ctrlB ( Dmac *  p_dmac,
uint32_t  ul_num,
uint32_t  ul_ctrlB 
)

Set the DMA control B of the specified DMA Channel.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]ul_ctrlBConfiguration of control B register

References Assert.

Referenced by dmac_channel_multi_buf_transfer_init(), and dmac_channel_single_buf_transfer_init().

void dmac_channel_set_descriptor_addr ( Dmac *  p_dmac,
uint32_t  ul_num,
uint32_t  ul_desc 
)

Set the DMA descriptor address of the specified DMA Channel.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]ul_descDescriptor address

References Assert.

Referenced by dmac_channel_multi_buf_transfer_init(), and dmac_channel_single_buf_transfer_init().

void dmac_channel_set_destination_addr ( Dmac *  p_dmac,
uint32_t  ul_num,
uint32_t  ul_addr 
)

Set the DMA destination address of the specified DMA Channel.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]ul_addrDestination address
Note
This register must be aligned with the source transfer width.

References Assert.

Referenced by dmac_channel_single_buf_transfer_init().

void dmac_channel_set_source_addr ( Dmac *  p_dmac,
uint32_t  ul_num,
uint32_t  ul_addr 
)

Set the DMA source address of the specified DMA Channel.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]ul_addrSource address
Note
This register must be aligned with the source transfer width.

References Assert.

Referenced by dmac_channel_single_buf_transfer_init().

void dmac_channel_single_buf_transfer_init ( Dmac *  p_dmac,
uint32_t  ul_num,
dma_transfer_descriptor_t p_desc 
)

Initialize the DMA Channel for a single buffer transfer.

Parameters
[in,out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]p_descPointer to a transfer descriptor

References Assert, dmac_channel_set_ctrlA(), dmac_channel_set_ctrlB(), dmac_channel_set_descriptor_addr(), dmac_channel_set_destination_addr(), dmac_channel_set_source_addr(), dma_transfer_descriptor_t::ul_ctrlA, dma_transfer_descriptor_t::ul_ctrlB, dma_transfer_descriptor_t::ul_destination_addr, and dma_transfer_descriptor_t::ul_source_addr.

Referenced by ssc_dma().

void dmac_channel_stop_transfer ( Dmac *  p_dmac,
uint32_t  ul_num 
)

Stop a DMA transfer occurring on the specified DMA Channel.

Note
Under normal operation, the hardware disables a channel on transfer completion by clearing the DMAC_CHSR.ENAx register bit. The recommended way for software to disable a channel without losing data is to use the SUSPx bit in conjunction with the EMPTx bit in the Channel Handler Status Register.
Parameters
[in,out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)

References Assert, dmac_channel_disable(), dmac_channel_get_status(), dmac_channel_resume(), and dmac_channel_suspend().

Referenced by stop_play_wav().

void dmac_channel_suspend ( Dmac *  p_dmac,
uint32_t  ul_num 
)

Suspend the specified DMA Channel and its current context.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)

References Assert.

Referenced by dmac_channel_stop_transfer().

void dmac_disable ( Dmac *  p_dmac)

Disable the DMA Controller.

Parameters
[in,out]p_dmacModule hardware register base address pointer

References Assert.

Referenced by dmac_init().

void dmac_disable_interrupt ( Dmac *  p_dmac,
uint32_t  ul_mask 
)

Disable DMAC interrupts.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_maskA bitmask of interrupts to be disabled

Where input parameter ul_mask is a bitmask containing one or more of the following:

Parameter Value Description
DMAC_EBCIDR_BTC0Channel 0 Buffer Transfer Completed
DMAC_EBCIDR_BTC1Channel 1 Buffer Transfer Completed
DMAC_EBCIDR_BTC2Channel 2 Buffer Transfer Completed
DMAC_EBCIDR_BTC3Channel 3 Buffer Transfer Completed
DMAC_EBCIDR_CBTC0Channel 0 Chained Buffer Transfer Completed
DMAC_EBCIDR_CBTC1Channel 1 Chained Buffer Transfer Completed
DMAC_EBCIDR_CBTC2Channel 2 Chained Buffer Transfer Completed
DMAC_EBCIDR_CBTC3Channel 3 Chained Buffer Transfer Completed
DMAC_EBCIDR_ERR0Channel 0 Access Error
DMAC_EBCIDR_ERR1Channel 1 Access Error
DMAC_EBCIDR_ERR2Channel 2 Access Error
DMAC_EBCIDR_ERR3Channel 3 Access Error

References Assert.

void dmac_enable ( Dmac *  p_dmac)

Enable the DMA Controller.

Parameters
[out]p_dmacModule hardware register base address pointer

References Assert.

Referenced by init_dma().

void dmac_enable_interrupt ( Dmac *  p_dmac,
uint32_t  ul_mask 
)

Enable DMAC interrupts.

Parameters
[out]p_dmacModule hardware register base address pointer
[in]ul_maskA bitmask of interrupts to be enabled

Where input parameter ul_mask is a bitmask containing one or more of the following:

Parameter Value Description
DMAC_EBCIER_BTC0Channel 0 Buffer Transfer Completed
DMAC_EBCIER_BTC1Channel 1 Buffer Transfer Completed
DMAC_EBCIER_BTC2Channel 2 Buffer Transfer Completed
DMAC_EBCIER_BTC3Channel 3 Buffer Transfer Completed
DMAC_EBCIER_CBTC0Channel 0 Chained Buffer Transfer Completed
DMAC_EBCIER_CBTC1Channel 1 Chained Buffer Transfer Completed
DMAC_EBCIER_CBTC2Channel 2 Chained Buffer Transfer Completed
DMAC_EBCIER_CBTC3Channel 3 Chained Buffer Transfer Completed
DMAC_EBCIER_ERR0Channel 0 Access Error
DMAC_EBCIER_ERR1Channel 1 Access Error
DMAC_EBCIER_ERR2Channel 2 Access Error
DMAC_EBCIER_ERR3Channel 3 Access Error

References Assert.

Referenced by init_dma().

uint32_t dmac_get_interrupt_mask ( Dmac *  p_dmac)

Get the DMAC Interrupt Mask.

Parameters
[in]p_dmacModule hardware register base address pointer
Returns
DMAC Interrupt mask.

References Assert.

uint32_t dmac_get_status ( Dmac *  p_dmac)

Get the DMAC transfer status.

Parameters
[in]p_dmacModule hardware register base address pointer
Returns
DMAC transfer status. Refer to section called "DMAC Error, Buffer Transfer and Chained Buffer Transfer Status Register" in the device-specific datasheet for more information.

References Assert.

Referenced by DMAC_Handler().

void dmac_init ( Dmac *  p_dmac)

Initialize the DMA controller and disable it.

Parameters
[in,out]p_dmacModule hardware register base address pointer

References dmac_disable().

Referenced by init_dma().

void dmac_set_priority_mode ( Dmac *  p_dmac,
dmac_priority_mode_t  mode 
)

Set the DMA priority mode.

Parameters
[in,out]p_dmacModule hardware register base address pointer
[in]modePriority mode

References Assert.

Referenced by init_dma().

void dmac_soft_chunk_transfer_request ( Dmac *  p_dmac,
uint32_t  ul_num,
uint32_t  ul_src_req,
uint32_t  ul_dst_req 
)

DMA Channel software chunk request.

Parameters
[in,out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]ul_src_reqRequest a source transfer
[in]ul_dst_reqRequest a destination transfer

References Assert.

void dmac_soft_set_last_transfer_flag ( Dmac *  p_dmac,
uint32_t  ul_num,
uint32_t  ul_src_flag,
uint32_t  ul_dst_flag 
)

Set the DMA Channel's last transfer flag.

Parameters
[in,out]p_dmacModule hardware register base address pointer
[in]ul_numChannel number
[in]ul_src_flagLast source transfer flag
[in]ul_dst_flagLast destination transfer flag

References Assert.

void dmac_soft_single_transfer_request ( Dmac *  p_dmac,
uint32_t  ul_num,
uint32_t  ul_src_req,
uint32_t  ul_dst_req 
)

DMA Channel software single request.

Parameters
[in,out]p_dmacModule hardware register base address pointer
[in]ul_numDMA Channel number (range 0 to 3)
[in]ul_src_reqRequest a source transfer
[in]ul_dst_reqRequest a destination transfer

References Assert.