Microchip® Advanced Software Framework

Quick Start Guide for the DMAC driver

This is the quick start guide for the SAM3A/3U/3X/4E DMA Controller (DMAC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case.

The code examples can be copied into the main application loop or any other function that will need to control the DMAC module.

Use Cases

DMAC Basic Usage

This use case will demonstrate how to initialize the DMAC module to perform a single memory to memory transfer.

Setup Steps

Prerequisites

This module requires the following service

Setup Code

Add these macros and global variable to the top of your application's C-file:

#define DMA_CH 0
#define DMA_BUF_SIZE 32
uint32_t g_dma_buf[6][DMA_BUF_SIZE];

Add this to the main loop or a setup function:

Workflow

  1. Define the variables needed, in order to perform a data transfer:
    uint32_t i;
    uint32_t cfg;
  2. Prepare the data buffer to be transferred:
    for (i = 0; i < DMA_BUF_SIZE; i++) {
    g_dma_buf[0][i] = i;
    g_dma_buf[1][i] = 0;
    }
  3. Initialize the DMAC module:
    dmac_init(DMAC);
  4. Set the priority to round-robin:
  5. Enable the DMAC module:
    dmac_enable(DMAC);
  6. Configure the channel for:
    • Enable stop on done
    • Enable AHB protection
    • Set the FIFO so that largest defined length AHB burst is performed
      cfg = DMAC_CFG_SOD_ENABLE |
      DMAC_CFG_AHB_PROT(1) |
      DMAC_CFG_FIFOCFG_ALAP_CFG;

Usage Steps

Usage Code

Configure the DMA source and destination buffer addresses:

desc.ul_source_addr = (uint32_t) g_dma_buf[0];
desc.ul_destination_addr = (uint32_t) g_dma_buf[1];

Configure DMA CTRLA:

  • Set the buffer transfer size to DMA_BUF_SIZE
  • Set the source transfer width to 32-bit
  • Set the destination transfer width to 32-bit
    desc.ul_ctrlA = DMAC_CTRLA_BTSIZE(DMA_BUF_SIZE) |
    DMAC_CTRLA_SRC_WIDTH_WORD |
    DMAC_CTRLA_DST_WIDTH_WORD;
    Configure DMA CTRLB:
  • Disable source buffer descriptor fetch
  • Disable destination buffer descriptor Fetch
  • Enable memory-to-memory transfer
  • Increment the source address
  • Increment the destination address
    desc.ul_ctrlB = DMAC_CTRLB_SRC_DSCR_FETCH_DISABLE |
    DMAC_CTRLB_DST_DSCR_FETCH_DISABLE |
    DMAC_CTRLB_FC_MEM2MEM_DMA_FC |
    DMAC_CTRLB_SRC_INCR_INCREMENTING |
    DMAC_CTRLB_DST_INCR_INCREMENTING;
    Initialize the DMA transfer: Start the DMA transfer: Finally, poll for the DMA transfer to complete: