Driver for the TWI (Two-Wire Interface).
This driver provides access to the main features of the TWI controller. The TWI interconnects components on a unique two-wire bus. The TWI is programmable as a master or a slave with sequential or single-byte access. Multiple master capability is supported.
Macros | |
#define | I2C_FAST_MODE_SPEED 400000 |
#define | LOW_LEVEL_TIME_LIMIT 384000 |
#define | TWI_CLK_CALC_ARGU 3 |
#define | TWI_CLK_DIV_MAX 0xFF |
#define | TWI_CLK_DIV_MIN 7 |
#define | TWI_CLK_DIVIDER 2 |
#define | TWI_WP_KEY_VALUE TWI_WPMR_WPKEY_PASSWD |
Functions | |
void | twi_disable_interrupt (Twi *p_twi, uint32_t ul_sources) |
Disable TWI interrupts. More... | |
void | twi_disable_master_mode (Twi *p_twi) |
Disable TWI master mode. More... | |
void | twi_disable_slave_mode (Twi *p_twi) |
Disable TWI slave mode. More... | |
void | twi_enable_interrupt (Twi *p_twi, uint32_t ul_sources) |
Enable TWI interrupts. More... | |
void | twi_enable_master_mode (Twi *p_twi) |
Enable TWI master mode. More... | |
void | twi_enable_slave_mode (Twi *p_twi) |
Enable TWI slave mode. More... | |
uint32_t | twi_get_interrupt_mask (Twi *p_twi) |
Read TWI interrupt mask. More... | |
uint32_t | twi_get_interrupt_status (Twi *p_twi) |
Get TWI interrupt status. More... | |
Pdc * | twi_get_pdc_base (Twi *p_twi) |
Get TWI PDC base address. More... | |
uint32_t | twi_master_init (Twi *p_twi, const twi_options_t *p_opt) |
Initialize TWI master mode. More... | |
uint32_t | twi_master_read (Twi *p_twi, twi_packet_t *p_packet) |
Read multiple bytes from a TWI compatible slave device. More... | |
uint32_t | twi_master_write (Twi *p_twi, twi_packet_t *p_packet) |
Write multiple bytes to a TWI compatible slave device. More... | |
uint32_t | twi_mk_addr (const uint8_t *addr, int len) |
Construct the TWI module address register field. More... | |
uint32_t | twi_probe (Twi *p_twi, uint8_t uc_slave_addr) |
Test if a chip answers a given I2C address. More... | |
uint8_t | twi_read_byte (Twi *p_twi) |
Reads a byte from the TWI bus. More... | |
void | twi_reset (Twi *p_twi) |
Reset TWI. More... | |
void | twi_set_slave_addr (Twi *p_twi, uint32_t ul_device_addr) |
Set TWI slave address. More... | |
uint32_t | twi_set_speed (Twi *p_twi, uint32_t ul_speed, uint32_t ul_mck) |
Set the I2C bus speed in conjunction with the clock frequency. More... | |
void | twi_slave_init (Twi *p_twi, uint32_t ul_device_addr) |
Initialize TWI slave mode. More... | |
uint32_t | twi_slave_read (Twi *p_twi, uint8_t *p_data) |
Read data from master. More... | |
uint32_t | twi_slave_write (Twi *p_twi, uint8_t *p_data) |
Write data to TWI bus. More... | |
void | twi_write_byte (Twi *p_twi, uint8_t uc_byte) |
Sends a byte of data to one of the TWI slaves on the bus. More... | |
#define I2C_FAST_MODE_SPEED 400000 |
Referenced by twi_set_speed().
#define LOW_LEVEL_TIME_LIMIT 384000 |
Referenced by twi_set_speed().
#define TWI_CLK_CALC_ARGU 3 |
Referenced by twi_set_speed().
#define TWI_CLK_DIV_MAX 0xFF |
Referenced by twi_set_speed().
#define TWI_CLK_DIV_MIN 7 |
Referenced by twi_set_speed().
#define TWI_CLK_DIVIDER 2 |
Referenced by twi_set_speed().
#define TWI_WP_KEY_VALUE TWI_WPMR_WPKEY_PASSWD |
void twi_disable_interrupt | ( | Twi * | p_twi, |
uint32_t | ul_sources | ||
) |
Disable TWI interrupts.
p_twi | Pointer to a TWI instance. |
ul_sources | Interrupts to be disabled. |
void twi_disable_master_mode | ( | Twi * | p_twi | ) |
Disable TWI master mode.
p_twi | Pointer to a TWI instance. |
void twi_disable_slave_mode | ( | Twi * | p_twi | ) |
Disable TWI slave mode.
p_twi | Pointer to a TWI instance. |
void twi_enable_interrupt | ( | Twi * | p_twi, |
uint32_t | ul_sources | ||
) |
Enable TWI interrupts.
p_twi | Pointer to a TWI instance. |
ul_sources | Interrupts to be enabled. |
void twi_enable_master_mode | ( | Twi * | p_twi | ) |
void twi_enable_slave_mode | ( | Twi * | p_twi | ) |
uint32_t twi_get_interrupt_mask | ( | Twi * | p_twi | ) |
Read TWI interrupt mask.
p_twi | Pointer to a TWI instance. |
uint32_t twi_get_interrupt_status | ( | Twi * | p_twi | ) |
Get TWI interrupt status.
p_twi | Pointer to a TWI instance. |
TWI | interrupt status. |
Pdc* twi_get_pdc_base | ( | Twi * | p_twi | ) |
Get TWI PDC base address.
p_twi | Pointer to a TWI instance. |
References Assert.
uint32_t twi_master_init | ( | Twi * | p_twi, |
const twi_options_t * | p_opt | ||
) |
Initialize TWI master mode.
p_twi | Pointer to a TWI instance. |
p_opt | Options for initializing the TWI module (see twi_options_t). |
References FAIL, twi_options::master_clk, twi_options::smbus, twi_options::speed, twi_enable_master_mode(), TWI_INVALID_ARGUMENT, twi_reset(), twi_set_speed(), and TWI_SUCCESS.
Referenced by twi_master_setup().
uint32_t twi_master_read | ( | Twi * | p_twi, |
twi_packet_t * | p_packet | ||
) |
Read multiple bytes from a TWI compatible slave device.
p_twi | Pointer to a TWI instance. |
p_packet | Packet information and data (see twi_packet_t). |
References twi_packet::addr, twi_packet::addr_length, twi_packet::buffer, twi_packet::chip, twi_packet::length, TWI_ERROR_TIMEOUT, TWI_INVALID_ARGUMENT, twi_mk_addr(), TWI_RECEIVE_NACK, TWI_SUCCESS, and TWI_TIMEOUT.
Referenced by at24cxx_read_byte(), at24cxx_read_continuous(), and at24cxx_read_page().
uint32_t twi_master_write | ( | Twi * | p_twi, |
twi_packet_t * | p_packet | ||
) |
Write multiple bytes to a TWI compatible slave device.
p_twi | Pointer to a TWI instance. |
p_packet | Packet information and data (see twi_packet_t). |
References twi_packet::addr, twi_packet::addr_length, twi_packet::buffer, twi_packet::chip, twi_packet::length, TWI_INVALID_ARGUMENT, twi_mk_addr(), TWI_RECEIVE_NACK, and TWI_SUCCESS.
Referenced by at24cxx_acknowledge_polling(), at24cxx_write_byte(), at24cxx_write_continuous(), at24cxx_write_page(), twi_probe(), and wm8731_write_register().
uint32_t twi_mk_addr | ( | const uint8_t * | addr, |
int | len | ||
) |
Construct the TWI module address register field.
The TWI module address register is sent out MSB first. And the size controls which byte is the MSB to start with.
Please see the device datasheet for details on this.
Referenced by twi_master_read(), and twi_master_write().
uint32_t twi_probe | ( | Twi * | p_twi, |
uint8_t | uc_slave_addr | ||
) |
Test if a chip answers a given I2C address.
p_twi | Pointer to a TWI instance. |
uc_slave_addr | Address of the remote chip to search for. |
References twi_packet::addr, twi_packet::addr_length, twi_packet::buffer, twi_packet::chip, twi_packet::length, and twi_master_write().
uint8_t twi_read_byte | ( | Twi * | p_twi | ) |
Reads a byte from the TWI bus.
p_twi | Pointer to a TWI instance. |
void twi_reset | ( | Twi * | p_twi | ) |
Reset TWI.
p_twi | Pointer to a TWI instance. |
Referenced by twi_master_init(), and twi_slave_init().
void twi_set_slave_addr | ( | Twi * | p_twi, |
uint32_t | ul_device_addr | ||
) |
Set TWI slave address.
p_twi | Pointer to a TWI instance. |
ul_device_addr | Device address of the SAM slave device on the I2C bus. |
uint32_t twi_set_speed | ( | Twi * | p_twi, |
uint32_t | ul_speed, | ||
uint32_t | ul_mck | ||
) |
Set the I2C bus speed in conjunction with the clock frequency.
p_twi | Pointer to a TWI instance. |
ul_speed | The desired I2C bus speed (in Hz). |
ul_mck | Main clock of the device (in Hz). |
PASS | New speed setting is accepted. |
FAIL | New speed setting is rejected. |
References FAIL, I2C_FAST_MODE_SPEED, LOW_LEVEL_TIME_LIMIT, PASS, TWI_CLK_CALC_ARGU, TWI_CLK_DIV_MAX, TWI_CLK_DIV_MIN, and TWI_CLK_DIVIDER.
Referenced by twi_master_init().
void twi_slave_init | ( | Twi * | p_twi, |
uint32_t | ul_device_addr | ||
) |
Initialize TWI slave mode.
p_twi | Pointer to a TWI instance. |
ul_device_addr | Device address of the SAM slave device on the I2C bus. |
References twi_enable_slave_mode(), and twi_reset().
Referenced by twi_slave_setup().
uint32_t twi_slave_read | ( | Twi * | p_twi, |
uint8_t * | p_data | ||
) |
Read data from master.
p_twi | Pointer to a TWI instance. |
p_data | Pointer to the data buffer where data received will be stored. |
uint32_t twi_slave_write | ( | Twi * | p_twi, |
uint8_t * | p_data | ||
) |
Write data to TWI bus.
p_twi | Pointer to a TWI instance. |
p_data | Pointer to the data buffer to be sent. |
void twi_write_byte | ( | Twi * | p_twi, |
uint8_t | uc_byte | ||
) |
Sends a byte of data to one of the TWI slaves on the bus.
p_twi | Pointer to a TWI instance. |
byte | The byte to send. |