Low-level driver for the ILI93XX LCD controller.
This is a driver for LCD with ili93xx.
This driver provides access to the main features of the ILI93XX controller. Now ILI9325 and ILI9341 are supported.
Now this driver supports ili9325 and ili9341.This component is custom LCD used for SAM4E-EK. The driver provides functions for initializtion and control of the LCD.
See Quick Start Guide for the ILI93XX.
Data Structures | |
struct | ili93xx_font |
Font structure. More... | |
struct | ili93xx_opt_t |
Input parameters when initializing ili9325 driver. More... | |
Macros | |
#define | COLOR_AZUR (0xF0FFFFu) |
#define | COLOR_BEIGE (0xF5F5DCu) |
#define | COLOR_BLACK (0x000000u) |
RGB 24-bits color table definition (RGB888). More... | |
#define | COLOR_BLUE (0x0000FFu) |
#define | COLOR_BLUEVIOLET (0x8A2BE2u) |
#define | COLOR_BROWN (0xA52A2Au) |
#define | COLOR_CYAN (0x00FFFFu) |
#define | COLOR_DARKBLUE (0x00008Bu) |
#define | COLOR_DARKCYAN (0x008B8Bu) |
#define | COLOR_DARKGRAY (0xA9A9A9u) |
#define | COLOR_DARKGREEN (0x006400u) |
#define | COLOR_DARKRED (0x800000u) |
#define | COLOR_DARKVIOLET (0x9400D3u) |
#define | COLOR_GOLD (0xFFD700u) |
#define | COLOR_GRAY (0x808080u) |
#define | COLOR_GREEN (0x00FF00u) |
#define | COLOR_GREENYELLOW (0xADFF2Fu) |
#define | COLOR_INDIGO (0x4B0082u) |
#define | COLOR_LIGHTBLUE (0xADD8E6u) |
#define | COLOR_LIGHTCYAN (0xE0FFFFu) |
#define | COLOR_LIGHTGREEN (0x90EE90u) |
#define | COLOR_LIGHTGREY (0xD3D3D3u) |
#define | COLOR_MAGENTA (0xFF00FFu) |
#define | COLOR_NAVY (0x000080u) |
#define | COLOR_OLIVE (0x808000u) |
#define | COLOR_ORANGE (0xFFA500u) |
#define | COLOR_RED (0xFF0000u) |
#define | COLOR_SIENNA (0xA0522Du) |
#define | COLOR_SILVER (0xC0C0C0u) |
#define | COLOR_SKYBLUE (0x87CEEBu) |
#define | COLOR_SNOW (0xFFFAFAu) |
#define | COLOR_TOMATO (0xFF6347u) |
#define | COLOR_TURQUOISE (0x40E0D0u) |
#define | COLOR_VIOLET (0xEE82EEu) |
#define | COLOR_WHITE (0xFFFFFFu) |
#define | COLOR_YELLOW (0xFFFF00u) |
#define | COLOR_YELLOWGREEN (0x9ACD32u) |
#define | DEVICE_TYPE_ILI9325 1 |
#define | DEVICE_TYPE_ILI9341 2 |
#define | ILI9325_DEVICE_CODE (0x9325u) |
ili93xx ID code More... | |
#define | ILI9341_DEVICE_CODE (0x9341u) |
#define | ILI93XX_COLOR(r, g, b) ((r << 16) | (g << 8) | b) |
This macro generates a 16-bit native color for the display from a 24-bit RGB value. More... | |
#define | ILI93XX_FLIP_X 1 |
Bit mask for flipping X for ili93xx_set_orientation() More... | |
#define | ILI93XX_FLIP_Y 2 |
Bit mask for flipping Y for ili93xx_set_orientation() More... | |
#define | ILI93XX_LCD_HEIGHT 320 |
#define | ILI93XX_LCD_WIDTH 240 |
ili93xx screen size More... | |
#define | ILI93XX_SWITCH_XY 4 |
Bit mask for swapping X and Y for ili93xx_set_orientation() More... | |
#define | ILI93XX_SWITCH_XY_HEIGHT 320 |
#define | ILI93XX_SWITCH_XY_WIDTH 240 |
#define | LCD_DATA_CACHE_SIZE ILI93XX_LCD_WIDTH |
Pixel cache used to speed up communication. More... | |
Typedefs | |
typedef ili93xx_color_t | gfx_color_t |
typedef int16_t | gfx_coord_t |
typedef uint32_t | ili93xx_color_t |
Type define for an integer type large enough to store a pixel color. More... | |
typedef int16_t | ili93xx_coord_t |
Type define for an integer type large enough to store a pixel coordinate. More... | |
Enumerations | |
enum | ili93xx_display_direction { LANDSCAPE = 0, PORTRAIT = 1 } |
Display direction option. More... | |
enum | ili93xx_scan_direction { V_INCREASE = 0, V_DEREASE = 1 } |
Scan direction option. More... | |
enum | ili93xx_shift_direction { H_INCREASE = 0, H_DECREASE = 1 } |
Shift direction option. More... | |
Functions | |
static void | ili93xx_check_box_coordinates (uint32_t *p_ul_x1, uint32_t *p_ul_y1, uint32_t *p_ul_x2, uint32_t *p_ul_y2) |
Check box coordinates. More... | |
void | ili93xx_copy_pixels_from_screen (ili93xx_color_t *pixels, uint32_t count) |
Copy pixels from the screen to a pixel buffer. More... | |
void | ili93xx_copy_pixels_to_screen (const ili93xx_color_t *pixels, uint32_t count) |
Copy pixels from SRAM to the screen. More... | |
void | ili93xx_copy_raw_pixel_24bits_to_screen (const uint8_t *raw_pixels, uint32_t count) |
Copy pixels from SRAM to the screen. More... | |
static void | ili93xx_delay (uint32_t ul_ms) |
Delay function. More... | |
uint8_t | ili93xx_device_type (void) |
get the device type. More... | |
uint8_t | ili93xx_device_type_identify (void) |
Read device ID to idenfity the device ILI9325 device ID locates in Device Code Read (R00h) register. More... | |
void | ili93xx_disable_scroll (void) |
Disable the scrolling feature. More... | |
void | ili93xx_display_off (void) |
Turn off the LCD. More... | |
void | ili93xx_display_on (void) |
Turn on the LCD. More... | |
static void | ili93xx_draw_char (uint32_t ul_x, uint32_t ul_y, uint8_t uc_c) |
Draw an ASCII character on LCD. More... | |
uint32_t | ili93xx_draw_circle (uint32_t ul_x, uint32_t ul_y, uint32_t ul_r) |
Draw a circle on LCD. More... | |
uint32_t | ili93xx_draw_filled_circle (uint32_t ul_x, uint32_t ul_y, uint32_t ul_r) |
Draw a filled circle on LCD. More... | |
void | ili93xx_draw_filled_rectangle (uint32_t ul_x1, uint32_t ul_y1, uint32_t ul_x2, uint32_t ul_y2) |
Draw a filled rectangle on LCD. More... | |
void | ili93xx_draw_line (uint32_t ul_x1, uint32_t ul_y1, uint32_t ul_x2, uint32_t ul_y2) |
Draw a line on LCD. More... | |
static void | ili93xx_draw_line_bresenham (uint32_t ul_x1, uint32_t ul_y1, uint32_t ul_x2, uint32_t ul_y2) |
Draw a line on LCD, which is not horizontal or vertical. More... | |
uint32_t | ili93xx_draw_pixel (uint32_t ul_x, uint32_t ul_y) |
Draw a pixel on LCD. More... | |
void | ili93xx_draw_pixmap (uint32_t ul_x, uint32_t ul_y, uint32_t ul_width, uint32_t ul_height, const ili93xx_color_t *p_ul_pixmap) |
Draw a pixmap on LCD. More... | |
void | ili93xx_draw_rectangle (uint32_t ul_x1, uint32_t ul_y1, uint32_t ul_x2, uint32_t ul_y2) |
Draw a rectangle on LCD. More... | |
void | ili93xx_draw_string (uint32_t ul_x, uint32_t ul_y, const uint8_t *p_str) |
Draw a string on LCD. More... | |
void | ili93xx_duplicate_pixel (const ili93xx_color_t color, uint32_t count) |
Set a given number of pixels to the same color. More... | |
void | ili93xx_enable_scroll (void) |
Enable the scrolling feature. More... | |
void | ili93xx_fill (ili93xx_color_t ul_color) |
Fill the LCD buffer with the specified color. More... | |
uint32_t | ili93xx_get_lcd_type (void) |
ili93xx_color_t | ili93xx_get_pixel (uint32_t ul_x, uint32_t ul_y) |
Get a pixel from LCD. More... | |
uint32_t | ili93xx_init (struct ili93xx_opt_t *p_opt) |
Initialize the ILI93XX lcd driver. More... | |
ili93xx_color_t | ili93xx_read_gram (void) |
Read a single color from the graphical memory. More... | |
static uint32_t | ili93xx_read_ram (void) |
Read data to LCD GRAM for ili93xx. More... | |
static void | ili93xx_read_ram_prepare (void) |
Prepare to read GRAM data for ili93xx. More... | |
static void | ili93xx_read_register (uint8_t uc_reg, uint8_t *p_data, uint8_t uc_datacnt) |
Read data from LCD Register. More... | |
void | ili93xx_scroll (int32_t ul_lines) |
Scroll up/down for the number of specified lines. More... | |
static void | ili93xx_send_draw_limits (const bool send_end_limits) |
Helper function to send the drawing limits (boundaries) to the display. More... | |
void | ili93xx_set_bottom_right_limit (ili93xx_coord_t x, ili93xx_coord_t y) |
Set the display bottom right drawing limit. More... | |
void | ili93xx_set_cursor_position (uint16_t us_x, uint16_t us_y) |
Set cursor of LCD screen. More... | |
void | ili93xx_set_display_direction (enum ili93xx_display_direction e_dd, enum ili93xx_shift_direction e_shd, enum ili93xx_scan_direction e_scd) |
Set display direction. More... | |
void | ili93xx_set_foreground_color (ili93xx_color_t ul_color) |
Set foreground color. More... | |
void | ili93xx_set_limits (ili93xx_coord_t start_x, ili93xx_coord_t start_y, ili93xx_coord_t end_x, ili93xx_coord_t end_y) |
Set the full display drawing limits. More... | |
void | ili93xx_set_orientation (uint8_t flags) |
Sets the orientation of the display data. More... | |
void | ili93xx_set_top_left_limit (ili93xx_coord_t x, ili93xx_coord_t y) |
Set the display top left drawing limit. More... | |
void | ili93xx_set_window (uint32_t ul_x, uint32_t ul_y, uint32_t ul_width, uint32_t ul_height) |
Set display window. More... | |
void | ili93xx_vscroll_area_define (uint16_t us_tfa, uint16_t us_vsa, uint16_t us_bfa) |
Vertical Scroll area definition for ili9341. More... | |
void | ili93xx_write_gram (ili93xx_color_t color) |
Write the graphical memory with a single color pixel. More... | |
static void | ili93xx_write_ram (ili93xx_color_t ul_color) |
Write data to LCD GRAM. More... | |
static void | ili93xx_write_ram_buffer (const ili93xx_color_t *p_ul_buf, uint32_t ul_size) |
Write multiple data in buffer to LCD controller for ili93xx. More... | |
static void | ili93xx_write_ram_prepare (void) |
Prepare to write GRAM data for ili93xx. More... | |
static void | ili93xx_write_register (uint8_t uc_reg, uint8_t *p_data, uint8_t uc_datacnt) |
Write data to LCD Register for ili93xx. More... | |
static void | ili93xx_write_register_word (uint8_t uc_reg, uint16_t us_data) |
Write a word (16bits)to LCD Register. More... | |
static void | LCD_IR (uint8_t lcd_index) |
Define EBI access for ILI93xx 8-bit System Interface. More... | |
static uint8_t | LCD_RD (void) |
static void | LCD_WD (uint8_t lcd_data) |
Variables | |
static uint8_t | g_uc_device_type = 0 |
Device type. More... | |
static uint32_t | g_ul_lcd_x_length = ILI93XX_LCD_WIDTH |
LCD X-axis and Y-axis length. More... | |
static uint32_t | g_ul_lcd_y_length = ILI93XX_LCD_HEIGHT |
static ili93xx_color_t | g_ul_pixel_cache [LCD_DATA_CACHE_SIZE] |
struct ili93xx_font | gfont = {10, 14} |
Global variable describing the font size used by the driver. More... | |
static volatile ili93xx_coord_t | limit_end_x |
static volatile ili93xx_coord_t | limit_end_y |
static volatile ili93xx_coord_t | limit_start_x |
static volatile ili93xx_coord_t | limit_start_y |
const uint8_t | p_uc_charset10x14 [] |
Character set table for font 10x14 Coding format: Char height is 14 bits, which is coded using 2 bytes per column (2 unused bits). More... | |
#define COLOR_AZUR (0xF0FFFFu) |
#define COLOR_BEIGE (0xF5F5DCu) |
#define COLOR_BLACK (0x000000u) |
RGB 24-bits color table definition (RGB888).
Referenced by run_test_init().
#define COLOR_BLUE (0x0000FFu) |
Referenced by run_test_init().
#define COLOR_BLUEVIOLET (0x8A2BE2u) |
#define COLOR_BROWN (0xA52A2Au) |
#define COLOR_CYAN (0x00FFFFu) |
#define COLOR_DARKBLUE (0x00008Bu) |
#define COLOR_DARKCYAN (0x008B8Bu) |
#define COLOR_DARKGRAY (0xA9A9A9u) |
#define COLOR_DARKGREEN (0x006400u) |
#define COLOR_DARKRED (0x800000u) |
#define COLOR_DARKVIOLET (0x9400D3u) |
#define COLOR_GOLD (0xFFD700u) |
#define COLOR_GRAY (0x808080u) |
#define COLOR_GREEN (0x00FF00u) |
#define COLOR_GREENYELLOW (0xADFF2Fu) |
#define COLOR_INDIGO (0x4B0082u) |
#define COLOR_LIGHTBLUE (0xADD8E6u) |
#define COLOR_LIGHTCYAN (0xE0FFFFu) |
#define COLOR_LIGHTGREEN (0x90EE90u) |
#define COLOR_LIGHTGREY (0xD3D3D3u) |
#define COLOR_MAGENTA (0xFF00FFu) |
#define COLOR_NAVY (0x000080u) |
#define COLOR_OLIVE (0x808000u) |
#define COLOR_ORANGE (0xFFA500u) |
#define COLOR_RED (0xFF0000u) |
#define COLOR_SIENNA (0xA0522Du) |
#define COLOR_SILVER (0xC0C0C0u) |
#define COLOR_SKYBLUE (0x87CEEBu) |
Referenced by run_test_data_read_write().
#define COLOR_SNOW (0xFFFAFAu) |
#define COLOR_TOMATO (0xFF6347u) |
#define COLOR_TURQUOISE (0x40E0D0u) |
#define COLOR_VIOLET (0xEE82EEu) |
#define COLOR_WHITE (0xFFFFFFu) |
Referenced by run_test_init().
#define COLOR_YELLOW (0xFFFF00u) |
#define COLOR_YELLOWGREEN (0x9ACD32u) |
#define DEVICE_TYPE_ILI9325 1 |
Referenced by ili93xx_copy_pixels_to_screen(), ili93xx_copy_raw_pixel_24bits_to_screen(), ili93xx_device_type_identify(), ili93xx_disable_scroll(), ili93xx_display_off(), ili93xx_display_on(), ili93xx_draw_pixel(), ili93xx_draw_pixmap(), ili93xx_duplicate_pixel(), ili93xx_enable_scroll(), ili93xx_fill(), ili93xx_get_pixel(), ili93xx_init(), ili93xx_read_gram(), ili93xx_read_ram(), ili93xx_read_ram_prepare(), ili93xx_scroll(), ili93xx_send_draw_limits(), ili93xx_set_cursor_position(), ili93xx_set_display_direction(), ili93xx_set_orientation(), ili93xx_set_window(), ili93xx_write_gram(), ili93xx_write_ram_prepare(), run_test_control_setting(), and run_test_init().
#define DEVICE_TYPE_ILI9341 2 |
Referenced by ili93xx_copy_pixels_to_screen(), ili93xx_copy_raw_pixel_24bits_to_screen(), ili93xx_device_type_identify(), ili93xx_disable_scroll(), ili93xx_display_off(), ili93xx_display_on(), ili93xx_draw_pixel(), ili93xx_draw_pixmap(), ili93xx_duplicate_pixel(), ili93xx_enable_scroll(), ili93xx_fill(), ili93xx_get_pixel(), ili93xx_init(), ili93xx_read_gram(), ili93xx_read_ram(), ili93xx_read_ram_prepare(), ili93xx_scroll(), ili93xx_send_draw_limits(), ili93xx_set_cursor_position(), ili93xx_set_display_direction(), ili93xx_set_window(), ili93xx_vscroll_area_define(), ili93xx_write_gram(), ili93xx_write_ram_prepare(), run_test_control_setting(), and run_test_init().
#define ILI9325_DEVICE_CODE (0x9325u) |
ili93xx ID code
Referenced by ili93xx_device_type_identify().
#define ILI9341_DEVICE_CODE (0x9341u) |
Referenced by ili93xx_device_type_identify().
#define ILI93XX_COLOR | ( | r, | |
g, | |||
b | |||
) | ((r << 16) | (g << 8) | b) |
This macro generates a 16-bit native color for the display from a 24-bit RGB value.
#define ILI93XX_FLIP_X 1 |
Bit mask for flipping X for ili93xx_set_orientation()
Referenced by ili93xx_set_orientation().
#define ILI93XX_FLIP_Y 2 |
Bit mask for flipping Y for ili93xx_set_orientation()
Referenced by ili93xx_set_orientation().
#define ILI93XX_LCD_HEIGHT 320 |
Referenced by ili93xx_fill(), ili93xx_init(), ili93xx_set_display_direction(), and run_test_init().
#define ILI93XX_LCD_WIDTH 240 |
ili93xx screen size
Referenced by ili93xx_fill(), ili93xx_init(), ili93xx_set_display_direction(), and run_test_init().
#define ILI93XX_SWITCH_XY 4 |
Bit mask for swapping X and Y for ili93xx_set_orientation()
Referenced by ili93xx_set_orientation().
#define ILI93XX_SWITCH_XY_HEIGHT 320 |
#define ILI93XX_SWITCH_XY_WIDTH 240 |
#define LCD_DATA_CACHE_SIZE ILI93XX_LCD_WIDTH |
Pixel cache used to speed up communication.
Referenced by ili93xx_draw_filled_rectangle(), and ili93xx_set_foreground_color().
typedef ili93xx_color_t gfx_color_t |
typedef int16_t gfx_coord_t |
typedef uint32_t ili93xx_color_t |
Type define for an integer type large enough to store a pixel color.
typedef int16_t ili93xx_coord_t |
Type define for an integer type large enough to store a pixel coordinate.
|
static |
Check box coordinates.
p_ul_x1 | X coordinate of upper-left corner on LCD. |
p_ul_y1 | Y coordinate of upper-left corner on LCD. |
p_ul_x2 | X coordinate of lower-right corner on LCD. |
p_ul_y2 | Y coordinate of lower-right corner on LCD. |
References g_ul_lcd_x_length, and g_ul_lcd_y_length.
Referenced by ili93xx_draw_filled_rectangle(), ili93xx_draw_pixmap(), and ili93xx_draw_rectangle().
void ili93xx_copy_pixels_from_screen | ( | ili93xx_color_t * | pixels, |
uint32_t | count | ||
) |
Copy pixels from the screen to a pixel buffer.
Use this function to copy pixels from the display to an internal SRAM buffer.
pixels | Pointer to the pixel buffer to read to |
count | Number of pixels to read |
Remove warnings
References UNUSED.
void ili93xx_copy_pixels_to_screen | ( | const ili93xx_color_t * | pixels, |
uint32_t | count | ||
) |
Copy pixels from SRAM to the screen.
Used to copy a large quantitative of data to the screen in one go.
pixels | Pointer to the pixel data |
count | Number of pixels to copy to the screen |
Sanity check to make sure that the pixel count is not zero
References Assert, DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_GRAM_DATA_REG, ILI9341_CMD_MEMORY_WRITE, ILI9341_CMD_WRITE_MEMORY_CONTINUE, LCD_IR(), and LCD_WD().
void ili93xx_copy_raw_pixel_24bits_to_screen | ( | const uint8_t * | raw_pixels, |
uint32_t | count | ||
) |
Copy pixels from SRAM to the screen.
Used to copy a large quantitative of data to the screen in one go.
pixels | Pointer to the pixel data |
count | Number of pixels to copy to the screen |
Sanity check to make sure that the pixel count is not zero
References Assert, DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_GRAM_DATA_REG, ILI9341_CMD_MEMORY_WRITE, ILI9341_CMD_WRITE_MEMORY_CONTINUE, LCD_IR(), and LCD_WD().
|
static |
Delay function.
Referenced by ili93xx_init().
uint8_t ili93xx_device_type | ( | void | ) |
get the device type.
References g_uc_device_type.
Referenced by run_test_control_setting(), and run_test_init().
uint8_t ili93xx_device_type_identify | ( | void | ) |
Read device ID to idenfity the device ILI9325 device ID locates in Device Code Read (R00h) register.
ILI9341 device ID locates in Read ID4 (RD3h) register.
Read ID4 (RD4h) register to get device code for ILI9341
Driver Code Read (R00h) for ILI9325
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_DEVICE_CODE, ILI9325_DEVICE_CODE_REG, ILI9341_CMD_READ_ID4, ILI9341_DEVICE_CODE, and ili93xx_read_register().
Referenced by ili93xx_init().
void ili93xx_disable_scroll | ( | void | ) |
Disable the scrolling feature.
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_BASE_IMG_DISP_CTRL, ILI9325_BASE_IMG_DISP_CTRL_REV, ILI9341_CMD_NORMAL_DISP_MODE_ON, ili93xx_display_off(), ili93xx_display_on(), ili93xx_write_register(), and ili93xx_write_register_word().
void ili93xx_display_off | ( | void | ) |
Turn off the LCD.
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_DISP_CTRL1, ILI9341_CMD_DISPLAY_OFF, ili93xx_write_register(), and ili93xx_write_register_word().
Referenced by ili93xx_disable_scroll().
void ili93xx_display_on | ( | void | ) |
Turn on the LCD.
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_DISP_CTRL1, ILI9325_DISP_CTRL1_BASEE, ILI9325_DISP_CTRL1_D, ILI9325_DISP_CTRL1_DTE, ILI9325_DISP_CTRL1_GON, ILI9341_CMD_DISPLAY_ON, ili93xx_write_register(), and ili93xx_write_register_word().
Referenced by ili93xx_disable_scroll(), and run_test_control_setting().
|
static |
Draw an ASCII character on LCD.
ul_x | X coordinate of character upper-left corner. |
ul_y | Y coordinate of character upper-left corner. |
uc_c | character to print. |
Compute offset according of the specified ASCII character Note: the first 32 characters of the ASCII table are not handled
Compute the first and second byte offset of a column
Draw pixel on screen depending on the corresponding bit value from the charset
References ili93xx_draw_pixel(), and p_uc_charset10x14.
Referenced by ili93xx_draw_string().
uint32_t ili93xx_draw_circle | ( | uint32_t | ul_x, |
uint32_t | ul_y, | ||
uint32_t | ul_r | ||
) |
Draw a circle on LCD.
ul_x | X coordinate of circle center. |
ul_y | Y coordinate of circle center. |
ul_r | circle radius. |
References ili93xx_draw_pixel().
uint32_t ili93xx_draw_filled_circle | ( | uint32_t | ul_x, |
uint32_t | ul_y, | ||
uint32_t | ul_r | ||
) |
Draw a filled circle on LCD.
ul_x | X coordinate of circle center. |
ul_y | Y coordinate of circle center. |
ul_r | circle radius. |
References ili93xx_draw_filled_rectangle().
void ili93xx_draw_filled_rectangle | ( | uint32_t | ul_x1, |
uint32_t | ul_y1, | ||
uint32_t | ul_x2, | ||
uint32_t | ul_y2 | ||
) |
Draw a filled rectangle on LCD.
ul_x1 | X coordinate of upper-left corner on LCD. |
ul_y1 | Y coordinate of upper-left corner on LCD. |
ul_x2 | X coordinate of lower-right corner on LCD. |
ul_y2 | Y coordinate of lower-right corner on LCD. |
Swap coordinates if necessary
Determine the refresh window area
Set cursor
Prepare to write in Graphic RAM
Send pixels blocks => one SPI IT / block
Send remaining pixels
Reset the refresh window area
References g_ul_lcd_x_length, g_ul_lcd_y_length, g_ul_pixel_cache, ili93xx_check_box_coordinates(), ili93xx_set_cursor_position(), ili93xx_set_window(), ili93xx_write_ram_buffer(), ili93xx_write_ram_prepare(), and LCD_DATA_CACHE_SIZE.
Referenced by ili93xx_draw_filled_circle(), ili93xx_draw_line(), ili93xx_draw_rectangle(), and run_test_init().
void ili93xx_draw_line | ( | uint32_t | ul_x1, |
uint32_t | ul_y1, | ||
uint32_t | ul_x2, | ||
uint32_t | ul_y2 | ||
) |
Draw a line on LCD.
ul_x1 | X coordinate of line start. |
ul_y1 | Y coordinate of line start. |
ul_x2 | X coordinate of line end. |
ul_y2 | Y coordinate of line end. |
References ili93xx_draw_filled_rectangle(), and ili93xx_draw_line_bresenham().
|
static |
Draw a line on LCD, which is not horizontal or vertical.
ul_x1 | X coordinate of line start. |
ul_y1 | Y coordinate of line start. |
ul_x2 | X coordinate of line end. |
ul_y2 | Y coordinate of line endl. |
References ili93xx_draw_pixel().
Referenced by ili93xx_draw_line().
uint32_t ili93xx_draw_pixel | ( | uint32_t | ul_x, |
uint32_t | ul_y | ||
) |
Draw a pixel on LCD.
ul_x | X coordinate of pixel. |
ul_y | Y coordinate of pixel. |
Set cursor
Prepare to write in GRAM
Prepare to write in GRAM
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, g_ul_lcd_x_length, g_ul_lcd_y_length, g_ul_pixel_cache, ili93xx_set_cursor_position(), ili93xx_set_window(), ili93xx_write_ram(), and ili93xx_write_ram_prepare().
Referenced by ili93xx_draw_char(), ili93xx_draw_circle(), ili93xx_draw_line_bresenham(), and run_test_data_read_write().
void ili93xx_draw_pixmap | ( | uint32_t | ul_x, |
uint32_t | ul_y, | ||
uint32_t | ul_width, | ||
uint32_t | ul_height, | ||
const ili93xx_color_t * | p_ul_pixmap | ||
) |
Draw a pixmap on LCD.
ul_x | X coordinate of upper-left corner on LCD. |
ul_y | Y coordinate of upper-left corner on LCD. |
ul_width | width of the picture. |
ul_height | height of the picture. |
p_ul_pixmap | pixmap of the image. |
Swap coordinates if necessary
Determine the refresh window area
Set cursor
Prepare to write in GRAM
Reset the refresh window area
Prepare to write in GRAM
Reset the refresh window area
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, g_ul_lcd_x_length, g_ul_lcd_y_length, ili93xx_check_box_coordinates(), ili93xx_set_cursor_position(), ili93xx_set_window(), ili93xx_write_ram_buffer(), and ili93xx_write_ram_prepare().
void ili93xx_draw_rectangle | ( | uint32_t | ul_x1, |
uint32_t | ul_y1, | ||
uint32_t | ul_x2, | ||
uint32_t | ul_y2 | ||
) |
Draw a rectangle on LCD.
ul_x1 | X coordinate of upper-left corner on LCD. |
ul_y1 | Y coordinate of upper-left corner on LCD. |
ul_x2 | X coordinate of lower-right corner on LCD. |
ul_y2 | Y coordinate of lower-right corner on LCD. |
References ili93xx_check_box_coordinates(), and ili93xx_draw_filled_rectangle().
void ili93xx_draw_string | ( | uint32_t | ul_x, |
uint32_t | ul_y, | ||
const uint8_t * | p_str | ||
) |
Draw a string on LCD.
ul_x | X coordinate of string top-left corner. |
ul_y | Y coordinate of string top-left corner. |
p_str | String to display. |
If newline, jump to the next line (font height + 2)
Draw the character and place cursor right after (font width + 2)
References ili93xx_font::height, ili93xx_draw_char(), and ili93xx_font::width.
void ili93xx_duplicate_pixel | ( | const ili93xx_color_t | color, |
uint32_t | count | ||
) |
Set a given number of pixels to the same color.
Use this function to write a certain number of pixels to the same color within a set limit.
color | The color to write to the display |
count | The number of pixels to write with this color |
Sanity check to make sure that the pixel count is not zero
Write Data to GRAM (R22h)
References Assert, DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_GRAM_DATA_REG, ILI9341_CMD_MEMORY_WRITE, ILI9341_CMD_WRITE_MEMORY_CONTINUE, LCD_IR(), and LCD_WD().
void ili93xx_enable_scroll | ( | void | ) |
Enable the scrolling feature.
no operation needed for ILI9341
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_BASE_IMG_DISP_CTRL, ILI9325_BASE_IMG_DISP_CTRL_REV, ILI9325_BASE_IMG_DISP_CTRL_VLE, and ili93xx_write_register_word().
void ili93xx_fill | ( | ili93xx_color_t | ul_color | ) |
Fill the LCD buffer with the specified color.
ul_color | fill color. |
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, g_ul_lcd_x_length, g_ul_lcd_y_length, ILI93XX_LCD_HEIGHT, ILI93XX_LCD_WIDTH, ili93xx_set_cursor_position(), ili93xx_set_window(), ili93xx_write_ram(), and ili93xx_write_ram_prepare().
uint32_t ili93xx_get_lcd_type | ( | void | ) |
References g_uc_device_type.
ili93xx_color_t ili93xx_get_pixel | ( | uint32_t | ul_x, |
uint32_t | ul_y | ||
) |
Get a pixel from LCD.
ul_x | X coordinate of pixel. |
ul_y | Y coordinate of pixel. |
Set cursor
Prepare to write in GRAM
Prepare to write in GRAM
References Assert, DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, g_ul_lcd_x_length, g_ul_lcd_y_length, ili93xx_read_ram(), ili93xx_read_ram_prepare(), ili93xx_set_cursor_position(), and ili93xx_set_window().
Referenced by run_test_data_read_write().
uint32_t ili93xx_init | ( | struct ili93xx_opt_t * | p_opt | ) |
Initialize the ILI93XX lcd driver.
p_opt | pointer to ILI93xx option structure. |
Identify the LCD driver device
Turn off LCD
Start initial sequence
Disable sleep and standby mode
Start internal OSC
Set SS bit and direction output from S720 to S1
Set 1 line inversion
Disable resizing feature
Set the back porch and front porch
Set non-display area refresh cycle ISC[3:0]
Disable FMARK function
18-bit RGB interface and writing display data by system interface
Set the output position of frame cycle
RGB interface polarity
Power on sequence
Disable sleep and standby mode
Selects the operating frequency of the step-up circuit 1,2 and Sets the ratio factor of Vci.
Set VREG1OUT voltage
Set VCOM amplitude
Enable power supply and source driver
Adjusts the constant current and Sets the factor used in the step-up circuits.
Select the operating frequency of the step-up circuit 1,2 and Sets the ratio factor of Vci
Internal reference voltage= Vci
Set VDV[4:0] for VCOM amplitude
Set VCM[5:0] for VCOMH
Set Frame Rate
Adjust the Gamma Curve
Use the high speed write mode (HWM=1) When TRI = 1, data are transferred to the internal RAM in 8-bit x 3 transfers mode via the 8-bit interface. DFM Set the mode of transferring data to the internal RAM when TRI = 1. I/D[1:0] = 11 Horizontal : increment Vertical : increment, AM=0:Horizontal
Sets the number of lines to drive the LCD at an interval of 8 lines. The scan direction is from G320 to G1
Vertical Scrolling
Disable scrolling and enable the grayscale inversion
Disable Partial Display
Panel Control
init for ILI9341
power control A configuration
power control B configuration
Pump Ratio Control configuration
Power Control 1 configuration
Power Control 2 configuration
VOM Control 1 configuration
VOM control 2 configuration
Driver Timing Control A configuration
Driver Timing Control B configuration
Memory Access Control configuration
Colmod Pixel Format Set configuation
Display Function Control
set window area
Leave sleep mode
Display on
exit with return value 1 if device type is not supported.
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, ili93xx_opt_t::foreground_color, g_uc_device_type, g_ul_lcd_x_length, g_ul_lcd_y_length, ILI9325_BASE_IMG_DISP_CTRL, ILI9325_BASE_IMG_DISP_CTRL_REV, ILI9325_DISP_CTRL1, ILI9325_DISP_CTRL1_D, ILI9325_DISP_CTRL1_DTE, ILI9325_DISP_CTRL1_GON, ILI9325_DISP_CTRL2, ILI9325_DISP_CTRL2_BP, ILI9325_DISP_CTRL2_FP, ILI9325_DISP_CTRL3, ILI9325_DISP_CTRL4, ILI9325_DRIVER_OUTPUT_CTRL1, ILI9325_DRIVER_OUTPUT_CTRL1_SS, ILI9325_DRIVER_OUTPUT_CTRL2, ILI9325_DRIVER_OUTPUT_CTRL2_GS, ILI9325_DRIVER_OUTPUT_CTRL2_NL, ILI9325_ENTRY_MODE, ILI9325_ENTRY_MODE_BGR, ILI9325_ENTRY_MODE_DFM, ILI9325_ENTRY_MODE_ID, ILI9325_ENTRY_MODE_TRI, ILI9325_FRAME_MAKER_POS, ILI9325_FRAME_RATE_AND_COLOR_CTRL, ILI9325_FRAME_RATE_AND_COLOR_CTRL_FRS, ILI9325_GAMMA_CTL1, ILI9325_GAMMA_CTL10, ILI9325_GAMMA_CTL10_VRN0, ILI9325_GAMMA_CTL10_VRN1, ILI9325_GAMMA_CTL2, ILI9325_GAMMA_CTL2_KP2, ILI9325_GAMMA_CTL2_KP3, ILI9325_GAMMA_CTL3, ILI9325_GAMMA_CTL3_KP4, ILI9325_GAMMA_CTL3_KP5, ILI9325_GAMMA_CTL4, ILI9325_GAMMA_CTL4_RP0, ILI9325_GAMMA_CTL4_RP1, ILI9325_GAMMA_CTL5, ILI9325_GAMMA_CTL5_VRP0, ILI9325_GAMMA_CTL5_VRP1, ILI9325_GAMMA_CTL6, ILI9325_GAMMA_CTL6_KN0, ILI9325_GAMMA_CTL6_KN1, ILI9325_GAMMA_CTL7, ILI9325_GAMMA_CTL7_KN2, ILI9325_GAMMA_CTL7_KN3, ILI9325_GAMMA_CTL8, ILI9325_GAMMA_CTL8_KN4, ILI9325_GAMMA_CTL8_KN5, ILI9325_GAMMA_CTL9, ILI9325_GAMMA_CTL9_RN0, ILI9325_GAMMA_CTL9_RN1, ILI9325_LCD_DRIVING_CTRL, ILI9325_LCD_DRIVING_CTRL_BC0, ILI9325_LCD_DRIVING_CTRL_BIT10, ILI9325_LCD_DRIVING_CTRL_EOR, ILI9325_PANEL_INTERFACE_CTRL1, ILI9325_PANEL_INTERFACE_CTRL1_RTNI, ILI9325_PANEL_INTERFACE_CTRL2, ILI9325_PANEL_INTERFACE_CTRL2_NOWI, ILI9325_PANEL_INTERFACE_CTRL4, ILI9325_PANEL_INTERFACE_CTRL4_DIVE, ILI9325_PANEL_INTERFACE_CTRL4_RTNE, ILI9325_PARTIAL_IMG1_AREA_END_LINE, ILI9325_PARTIAL_IMG1_AREA_START_LINE, ILI9325_PARTIAL_IMG1_DISP_POS, ILI9325_PARTIAL_IMG2_AREA_END_LINE, ILI9325_PARTIAL_IMG2_AREA_START_LINE, ILI9325_PARTIAL_IMG2_DISP_POS, ILI9325_POWER_CTRL1, ILI9325_POWER_CTRL1_AP, ILI9325_POWER_CTRL1_APE, ILI9325_POWER_CTRL1_BT, ILI9325_POWER_CTRL1_SAP, ILI9325_POWER_CTRL2, ILI9325_POWER_CTRL2_DC0, ILI9325_POWER_CTRL2_DC1, ILI9325_POWER_CTRL2_VC, ILI9325_POWER_CTRL3, ILI9325_POWER_CTRL3_PON, ILI9325_POWER_CTRL3_VRH, ILI9325_POWER_CTRL4, ILI9325_POWER_CTRL4_VDV, ILI9325_POWER_CTRL7, ILI9325_POWER_CTRL7_VCM, ILI9325_RESIZE_CTRL, ILI9325_RGB_DISP_INTERFACE_CTRL1, ILI9325_RGB_DISP_INTERFACE_CTRL2, ILI9325_START_OSC_CTRL, ILI9325_START_OSC_CTRL_EN, ILI9325_VERTICAL_SCROLL_CTRL, ILI9341_CMD_DISPLAY_FUNCTION_CTL, ILI9341_CMD_DISPLAY_ON, ILI9341_CMD_DRIVER_TIMING_CTL_A, ILI9341_CMD_DRIVER_TIMING_CTL_B, ILI9341_CMD_MEMORY_ACCESS_CONTROL, ILI9341_CMD_MEMORY_ACCESS_CONTROL_BGR, ILI9341_CMD_MEMORY_ACCESS_CONTROL_MX, ILI9341_CMD_PIXEL_FORMAT_SET, ILI9341_CMD_POWER_CONTROL_1, ILI9341_CMD_POWER_CONTROL_2, ILI9341_CMD_POWER_CONTROL_A, ILI9341_CMD_POWER_CONTROL_B, ILI9341_CMD_PUMP_RATIO_CONTROL, ILI9341_CMD_SLEEP_OUT, ILI9341_CMD_VCOM_CONTROL_1, ILI9341_CMD_VCOM_CONTROL_2, ili93xx_delay(), ili93xx_device_type_identify(), ILI93XX_LCD_HEIGHT, ILI93XX_LCD_WIDTH, ili93xx_set_cursor_position(), ili93xx_set_foreground_color(), ili93xx_set_window(), ili93xx_write_register(), ili93xx_write_register_word(), ili93xx_opt_t::ul_height, and ili93xx_opt_t::ul_width.
Referenced by run_test_init().
ili93xx_color_t ili93xx_read_gram | ( | void | ) |
Read a single color from the graphical memory.
Use this function to read a color from the graphical memory of the controller.
ili93xx_color_t | The read color pixel |
Write Data to GRAM (R22h)
two dummy read
data upper byte
data lower byte
Convert RGB565 to RGB888
For BGR format
Write Data to GRAM (R2Eh)
dummy read
the highest byte - R byte
the middle byte - G byte
the lowest byte - B byte
combine R, G, B byte to a color value
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_GRAM_DATA_REG, ILI9341_CMD_MEMORY_READ, LCD_IR(), and LCD_RD().
|
static |
Read data to LCD GRAM for ili93xx.
dummy read
data upper byte
data lower byte
Convert RGB565 to RGB888
For BGR format
dummy read
the highest byte - R byte
the middle byte - G byte
the lowest byte - B byte
combine R, G, B byte to a color value
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, and LCD_RD().
Referenced by ili93xx_get_pixel().
|
static |
Prepare to read GRAM data for ili93xx.
Write Data to GRAM (R22h)
Write Data to GRAM (R2Eh)
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_GRAM_DATA_REG, ILI9341_CMD_MEMORY_READ, and LCD_IR().
Referenced by ili93xx_get_pixel().
|
static |
Read data from LCD Register.
uc_reg | register address. |
p_data | the pointer to the read data. |
uc_datacnt | the number of the read data |
References LCD_IR(), and LCD_RD().
Referenced by ili93xx_device_type_identify().
void ili93xx_scroll | ( | int32_t | ul_lines | ) |
Scroll up/down for the number of specified lines.
ul_lines | number of lines to scroll. |
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_VERTICAL_SCROLL_CTRL, ILI9341_CMD_VERT_SCROLL_START_ADDRESS, ili93xx_write_register(), and ili93xx_write_register_word().
|
inlinestatic |
Helper function to send the drawing limits (boundaries) to the display.
This function is used to send the currently set upper-left and lower-right drawing limits to the display, as set through the various limit functions.
send_end_limits | True to also send the lower-right drawing limits |
Set Horizontal Address Start Position
Set Horizontal Address End Position
Set Vertical Address Start Position
Set Vertical Address End Position
GRAM Horizontal/Vertical Address Set (R20h, R21h)
Set Column Address Position
Set Page Address Position
Set Horizontal Address Start Position
Set Vertical Address Start Position
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_HORIZONTAL_ADDR_END, ILI9325_HORIZONTAL_ADDR_START, ILI9325_HORIZONTAL_GRAM_ADDR_SET, ILI9325_VERTICAL_ADDR_END, ILI9325_VERTICAL_ADDR_START, ILI9325_VERTICAL_GRAM_ADDR_SET, ILI9341_CMD_COLUMN_ADDRESS_SET, ILI9341_CMD_PAGE_ADDRESS_SET, ili93xx_write_register(), ili93xx_write_register_word(), limit_end_x, limit_end_y, limit_start_x, and limit_start_y.
Referenced by ili93xx_set_bottom_right_limit(), ili93xx_set_limits(), and ili93xx_set_top_left_limit().
void ili93xx_set_bottom_right_limit | ( | ili93xx_coord_t | x, |
ili93xx_coord_t | y | ||
) |
Set the display bottom right drawing limit.
Use this function to set the bottom right corner of the drawing limit box.
x | The x coordinate of the bottom right corner |
y | The y coordinate of the bottom right corner |
References ili93xx_send_draw_limits(), limit_end_x, and limit_end_y.
void ili93xx_set_cursor_position | ( | uint16_t | us_x, |
uint16_t | us_y | ||
) |
Set cursor of LCD screen.
us_x | X coordinate of upper-left corner on LCD. |
us_y | Y coordinate of upper-left corner on LCD. |
GRAM Horizontal/Vertical Address Set (R20h, R21h)
There is no corresponding operation for ILI9341.
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_HORIZONTAL_GRAM_ADDR_SET, ILI9325_VERTICAL_GRAM_ADDR_SET, and ili93xx_write_register_word().
Referenced by ili93xx_draw_filled_rectangle(), ili93xx_draw_pixel(), ili93xx_draw_pixmap(), ili93xx_fill(), ili93xx_get_pixel(), and ili93xx_init().
void ili93xx_set_display_direction | ( | enum ili93xx_display_direction | e_dd, |
enum ili93xx_shift_direction | e_shd, | ||
enum ili93xx_scan_direction | e_scd | ||
) |
Set display direction.
e_dd | 0: horizontal direction, 1: vertical direction |
e_shd,: | horizontal increase(0) or decrease(1) |
e_scd,: | vertical increase(1) or decrease(0) |
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, g_ul_lcd_x_length, g_ul_lcd_y_length, H_INCREASE, ILI9325_DRIVER_OUTPUT_CTRL1, ILI9325_DRIVER_OUTPUT_CTRL1_SS, ILI9325_DRIVER_OUTPUT_CTRL2, ILI9325_DRIVER_OUTPUT_CTRL2_GS, ILI9325_DRIVER_OUTPUT_CTRL2_NL, ILI9325_ENTRY_MODE, ILI9325_ENTRY_MODE_AM, ILI9325_ENTRY_MODE_BGR, ILI9325_ENTRY_MODE_DFM, ILI9325_ENTRY_MODE_ID, ILI9325_ENTRY_MODE_TRI, ILI9341_CMD_MEMORY_ACCESS_CONTROL, ILI9341_CMD_MEMORY_ACCESS_CONTROL_BGR, ILI9341_CMD_MEMORY_ACCESS_CONTROL_MV, ILI9341_CMD_MEMORY_ACCESS_CONTROL_MX, ILI93XX_LCD_HEIGHT, ILI93XX_LCD_WIDTH, ili93xx_write_register(), ili93xx_write_register_word(), LANDSCAPE, and V_INCREASE.
void ili93xx_set_foreground_color | ( | ili93xx_color_t | ul_color | ) |
Set foreground color.
ul_color | foreground color. |
Fill the cache with selected color
References g_ul_pixel_cache, and LCD_DATA_CACHE_SIZE.
Referenced by ili93xx_init(), run_test_data_read_write(), and run_test_init().
void ili93xx_set_limits | ( | ili93xx_coord_t | start_x, |
ili93xx_coord_t | start_y, | ||
ili93xx_coord_t | end_x, | ||
ili93xx_coord_t | end_y | ||
) |
Set the full display drawing limits.
Use this function to set the full drawing limit box.
start_x | The x coordinate of the top left corner |
start_y | The y coordinate of the top left corner |
end_x | The x coordinate of the bottom right corner |
end_y | The y coordinate of the bottom right corner |
References ili93xx_send_draw_limits(), limit_end_x, limit_end_y, limit_start_x, and limit_start_y.
void ili93xx_set_orientation | ( | uint8_t | flags | ) |
Sets the orientation of the display data.
Configures the display for a given orientation, including mirroring and/or screen rotation.
flags | Orientation flags to use, see ILI93XX_FLIP_X, ILI93XX_FLIP_Y and ILI93XX_SWITCH_XY. |
References DEVICE_TYPE_ILI9325, g_uc_device_type, ILI9325_ENTRY_MODE, ILI9325_ENTRY_MODE_AM, ILI9325_ENTRY_MODE_BGR, ILI9325_ENTRY_MODE_DFM, ILI9325_ENTRY_MODE_ID, ILI9325_ENTRY_MODE_TRI, ILI9341_CMD_MEMORY_ACCESS_CONTROL, ILI93XX_FLIP_X, ILI93XX_FLIP_Y, ILI93XX_SWITCH_XY, ili93xx_write_register(), and ili93xx_write_register_word().
void ili93xx_set_top_left_limit | ( | ili93xx_coord_t | x, |
ili93xx_coord_t | y | ||
) |
Set the display top left drawing limit.
Use this function to set the top left limit of the drawing limit box.
x | The x coordinate of the top left corner |
y | The y coordinate of the top left corner |
References ili93xx_send_draw_limits(), limit_start_x, and limit_start_y.
void ili93xx_set_window | ( | uint32_t | ul_x, |
uint32_t | ul_y, | ||
uint32_t | ul_width, | ||
uint32_t | ul_height | ||
) |
Set display window.
ul_x | Horizontal address start position |
ul_y | Vertical address start position |
ul_width | The width of the window. |
ul_height | The height of the window. |
Set Horizontal Address Start Position
Set Horizontal Address End Position
Set Vertical Address Start Position
Set Vertical Address End Position
Set Column Address Position
Set Page Address Position
References Assert, DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, g_ul_lcd_x_length, g_ul_lcd_y_length, ILI9325_HORIZONTAL_ADDR_END, ILI9325_HORIZONTAL_ADDR_START, ILI9325_VERTICAL_ADDR_END, ILI9325_VERTICAL_ADDR_START, ILI9341_CMD_COLUMN_ADDRESS_SET, ILI9341_CMD_PAGE_ADDRESS_SET, ili93xx_write_register(), and ili93xx_write_register_word().
Referenced by ili93xx_draw_filled_rectangle(), ili93xx_draw_pixel(), ili93xx_draw_pixmap(), ili93xx_fill(), ili93xx_get_pixel(), and ili93xx_init().
void ili93xx_vscroll_area_define | ( | uint16_t | us_tfa, |
uint16_t | us_vsa, | ||
uint16_t | us_bfa | ||
) |
Vertical Scroll area definition for ili9341.
us_tfa | the top fixed area (the No. of lines) |
us_vsa | the height of the vetical scrolling area |
us_bfa | the bottom fixed area (the No. of lines) |
References DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9341_CMD_VERT_SCROLL_DEFINITION, and ili93xx_write_register().
void ili93xx_write_gram | ( | ili93xx_color_t | color | ) |
Write the graphical memory with a single color pixel.
Use this function to write a single color pixel to the controller memory.
color | The color pixel to write to the screen |
Write Data to GRAM (R22h)
memory write command (R2Ch)
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_GRAM_DATA_REG, ILI9341_CMD_MEMORY_WRITE, ILI9341_CMD_WRITE_MEMORY_CONTINUE, LCD_IR(), and LCD_WD().
|
static |
Write data to LCD GRAM.
ul_color | 24-bits RGB color. |
References LCD_WD().
Referenced by ili93xx_draw_pixel(), ili93xx_fill(), and ili93xx_write_ram_buffer().
|
static |
Write multiple data in buffer to LCD controller for ili93xx.
p_ul_buf | data buffer. |
ul_size | size in pixels. |
References ili93xx_write_ram().
Referenced by ili93xx_draw_filled_rectangle(), and ili93xx_draw_pixmap().
|
static |
Prepare to write GRAM data for ili93xx.
Write Data to GRAM (R22h)
memory write command (R2Ch)
References DEVICE_TYPE_ILI9325, DEVICE_TYPE_ILI9341, g_uc_device_type, ILI9325_GRAM_DATA_REG, ILI9341_CMD_MEMORY_WRITE, ILI9341_CMD_WRITE_MEMORY_CONTINUE, and LCD_IR().
Referenced by ili93xx_draw_filled_rectangle(), ili93xx_draw_pixel(), ili93xx_draw_pixmap(), and ili93xx_fill().
|
static |
Write data to LCD Register for ili93xx.
uc_reg | register address. |
us_data | data to be written. |
References LCD_IR(), and LCD_WD().
Referenced by ili93xx_disable_scroll(), ili93xx_display_off(), ili93xx_display_on(), ili93xx_init(), ili93xx_scroll(), ili93xx_send_draw_limits(), ili93xx_set_display_direction(), ili93xx_set_orientation(), ili93xx_set_window(), and ili93xx_vscroll_area_define().
|
static |
Write a word (16bits)to LCD Register.
uc_reg | register address. |
us_data | data to be written. |
References LCD_IR(), and LCD_WD().
Referenced by ili93xx_disable_scroll(), ili93xx_display_off(), ili93xx_display_on(), ili93xx_enable_scroll(), ili93xx_init(), ili93xx_scroll(), ili93xx_send_draw_limits(), ili93xx_set_cursor_position(), ili93xx_set_display_direction(), ili93xx_set_orientation(), and ili93xx_set_window().
|
inlinestatic |
Define EBI access for ILI93xx 8-bit System Interface.
ILI93XX index register address
References BOARD_ILI93XX_ADDR.
Referenced by ili93xx_copy_pixels_to_screen(), ili93xx_copy_raw_pixel_24bits_to_screen(), ili93xx_duplicate_pixel(), ili93xx_read_gram(), ili93xx_read_ram_prepare(), ili93xx_read_register(), ili93xx_read_register_byte(), ili93xx_write_gram(), ili93xx_write_ram_prepare(), ili93xx_write_register(), ili93xx_write_register_word(), and run_test_control_setting().
|
inlinestatic |
References BOARD_ILI93XX_ADDR, and BOARD_ILI93XX_RS.
Referenced by ili93xx_read_gram(), ili93xx_read_ram(), ili93xx_read_register(), ili93xx_read_register_byte(), and run_test_control_setting().
|
inlinestatic |
|
static |
Device type.
Referenced by ili93xx_copy_pixels_to_screen(), ili93xx_copy_raw_pixel_24bits_to_screen(), ili93xx_device_type(), ili93xx_device_type_identify(), ili93xx_disable_scroll(), ili93xx_display_off(), ili93xx_display_on(), ili93xx_draw_pixel(), ili93xx_draw_pixmap(), ili93xx_duplicate_pixel(), ili93xx_enable_scroll(), ili93xx_fill(), ili93xx_get_lcd_type(), ili93xx_get_pixel(), ili93xx_init(), ili93xx_read_gram(), ili93xx_read_ram(), ili93xx_read_ram_prepare(), ili93xx_scroll(), ili93xx_send_draw_limits(), ili93xx_set_cursor_position(), ili93xx_set_display_direction(), ili93xx_set_orientation(), ili93xx_set_window(), ili93xx_vscroll_area_define(), ili93xx_write_gram(), and ili93xx_write_ram_prepare().
|
static |
LCD X-axis and Y-axis length.
Referenced by ili93xx_check_box_coordinates(), ili93xx_draw_filled_rectangle(), ili93xx_draw_pixel(), ili93xx_draw_pixmap(), ili93xx_fill(), ili93xx_get_pixel(), ili93xx_init(), ili93xx_set_display_direction(), and ili93xx_set_window().
|
static |
|
static |
Referenced by ili93xx_draw_filled_rectangle(), ili93xx_draw_pixel(), and ili93xx_set_foreground_color().
struct ili93xx_font gfont = {10, 14} |
Global variable describing the font size used by the driver.
|
static |
Referenced by ili93xx_send_draw_limits(), ili93xx_set_bottom_right_limit(), and ili93xx_set_limits().
|
static |
Referenced by ili93xx_send_draw_limits(), ili93xx_set_bottom_right_limit(), and ili93xx_set_limits().
|
static |
Referenced by ili93xx_send_draw_limits(), ili93xx_set_limits(), and ili93xx_set_top_left_limit().
|
static |
Referenced by ili93xx_send_draw_limits(), ili93xx_set_limits(), and ili93xx_set_top_left_limit().
const uint8_t p_uc_charset10x14[] |
Character set table for font 10x14 Coding format: Char height is 14 bits, which is coded using 2 bytes per column (2 unused bits).
Char width is 10 bits.
Referenced by ili93xx_draw_char().