Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Static Memory Controller (SMC)

Driver for the Static Memory Controller.

It provides functions for configuring and using the on-chip SMC.

API Overview

Note
Some APIs are only available for specific SAM devices.

Macros

#define ECC_STATUS_MASK   0x07
 
#define NFC_BUSY_FLAG   0x8000000
 
#define NFCADDR_CMD_ACYCLE   (0x7u << 19) /* Number of Address required for the current command */
 
#define NFCADDR_CMD_ACYCLE_FIVE   (0x5u << 19) /* Five address cycles */
 
#define NFCADDR_CMD_ACYCLE_FOUR   (0x4u << 19) /* Four address cycles */
 
#define NFCADDR_CMD_ACYCLE_NONE   (0x0u << 19) /* No address cycle */
 
#define NFCADDR_CMD_ACYCLE_ONE   (0x1u << 19) /* One address cycle */
 
#define NFCADDR_CMD_ACYCLE_THREE   (0x3u << 19) /* Three address cycles */
 
#define NFCADDR_CMD_ACYCLE_TWO   (0x2u << 19) /* Two address cycles */
 
#define NFCADDR_CMD_CMD1   (0xFFu << 2) /* Command Register Value for Cycle 1 */
 
#define NFCADDR_CMD_CMD2   (0xFFu << 10) /* Command Register Value for Cycle 2 */
 
#define NFCADDR_CMD_CSID(value)   ((NFCADDR_CMD_CSID_Msk & ((value) << NFCADDR_CMD_CSID_Pos)))
 
#define NFCADDR_CMD_CSID_Msk   (0x7u << NFCADDR_CMD_CSID_Pos) /* Chip Select Identifier */
 
#define NFCADDR_CMD_CSID_Pos   22
 
#define NFCADDR_CMD_NFC_READ   (0x0u << 26) /* NFC Write Enable */
 
#define NFCADDR_CMD_NFC_WIRTE   (0x1u << 26) /* NFC Write Enable */
 
#define NFCADDR_CMD_NFCCMD   (0x1u << 27) /* NFC Command Enable */
 
#define NFCADDR_CMD_NFCEN   (0x1u << 25) /* NFC Enable */
 
#define NFCADDR_CMD_VCMD2   (0x1u << 18) /* Valid Cycle 2 Command */
 

Functions

uint32_t smc_ecc_get_status (Smc *p_smc, uint32_t ul_parity_number)
 
void smc_ecc_get_value (Smc *p_smc, uint32_t *p_ecc)
 
void smc_ecc_init (Smc *p_smc, uint32_t ul_type, uint32_t ul_pagesize)
 
void smc_enable_writeprotect (Smc *p_smc, uint32_t ul_enable)
 
uint32_t smc_get_mode (Smc *p_smc, uint32_t ul_cs)
 
uint32_t smc_get_writeprotect_status (Smc *p_smc)
 
void smc_nfc_disable (Smc *p_smc)
 
void smc_nfc_disable_interrupt (Smc *p_smc, uint32_t ul_sources)
 
void smc_nfc_disable_spare_read (Smc *p_smc)
 
void smc_nfc_disable_spare_write (Smc *p_smc)
 
void smc_nfc_enable (Smc *p_smc)
 
void smc_nfc_enable_interrupt (Smc *p_smc, uint32_t ul_sources)
 
void smc_nfc_enable_spare_read (Smc *p_smc)
 
void smc_nfc_enable_spare_write (Smc *p_smc)
 
uint32_t smc_nfc_get_interrupt_mask (Smc *p_smc)
 
uint32_t smc_nfc_get_status (Smc *p_smc)
 
void smc_nfc_init (Smc *p_smc, uint32_t ul_config)
 
void smc_nfc_send_command (Smc *p_smc, uint32_t ul_cmd, uint32_t ul_address_cycle, uint32_t ul_cycle0)
 
void smc_nfc_set_address0 (Smc *p_smc, uint8_t uc_address0)
 
void smc_nfc_set_bank (Smc *p_smc, uint32_t ul_bank)
 
void smc_nfc_set_page_size (Smc *p_smc, uint32_t ul_page_size)
 
void smc_set_cycle_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_cycle_timing)
 
void smc_set_mode (Smc *p_smc, uint32_t ul_cs, uint32_t ul_mode)
 
void smc_set_nand_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_nand_timing)
 
void smc_set_pulse_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_pulse_timing)
 
void smc_set_setup_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_setup_timing)
 

#define ECC_STATUS_MASK   0x07
#define NFC_BUSY_FLAG   0x8000000
#define NFCADDR_CMD_ACYCLE   (0x7u << 19) /* Number of Address required for the current command */
#define NFCADDR_CMD_ACYCLE_FIVE   (0x5u << 19) /* Five address cycles */
#define NFCADDR_CMD_ACYCLE_FOUR   (0x4u << 19) /* Four address cycles */
#define NFCADDR_CMD_ACYCLE_NONE   (0x0u << 19) /* No address cycle */
#define NFCADDR_CMD_ACYCLE_ONE   (0x1u << 19) /* One address cycle */
#define NFCADDR_CMD_ACYCLE_THREE   (0x3u << 19) /* Three address cycles */
#define NFCADDR_CMD_ACYCLE_TWO   (0x2u << 19) /* Two address cycles */
#define NFCADDR_CMD_CMD1   (0xFFu << 2) /* Command Register Value for Cycle 1 */
#define NFCADDR_CMD_CMD2   (0xFFu << 10) /* Command Register Value for Cycle 2 */
#define NFCADDR_CMD_CSID (   value)    ((NFCADDR_CMD_CSID_Msk & ((value) << NFCADDR_CMD_CSID_Pos)))
#define NFCADDR_CMD_CSID_Msk   (0x7u << NFCADDR_CMD_CSID_Pos) /* Chip Select Identifier */
#define NFCADDR_CMD_CSID_Pos   22
#define NFCADDR_CMD_NFC_READ   (0x0u << 26) /* NFC Write Enable */
#define NFCADDR_CMD_NFC_WIRTE   (0x1u << 26) /* NFC Write Enable */
#define NFCADDR_CMD_NFCCMD   (0x1u << 27) /* NFC Command Enable */
#define NFCADDR_CMD_NFCEN   (0x1u << 25) /* NFC Enable */
#define NFCADDR_CMD_VCMD2   (0x1u << 18) /* Valid Cycle 2 Command */

uint32_t smc_ecc_get_status ( Smc *  p_smc,
uint32_t  ul_parity_number 
)
void smc_ecc_get_value ( Smc *  p_smc,
uint32_t *  p_ecc 
)
void smc_ecc_init ( Smc *  p_smc,
uint32_t  ul_type,
uint32_t  ul_pagesize 
)
void smc_enable_writeprotect ( Smc *  p_smc,
uint32_t  ul_enable 
)
uint32_t smc_get_mode ( Smc *  p_smc,
uint32_t  ul_cs 
)
uint32_t smc_get_writeprotect_status ( Smc *  p_smc)
void smc_nfc_disable ( Smc *  p_smc)
void smc_nfc_disable_interrupt ( Smc *  p_smc,
uint32_t  ul_sources 
)
void smc_nfc_disable_spare_read ( Smc *  p_smc)
void smc_nfc_disable_spare_write ( Smc *  p_smc)
void smc_nfc_enable ( Smc *  p_smc)
void smc_nfc_enable_interrupt ( Smc *  p_smc,
uint32_t  ul_sources 
)
void smc_nfc_enable_spare_read ( Smc *  p_smc)
void smc_nfc_enable_spare_write ( Smc *  p_smc)
uint32_t smc_nfc_get_interrupt_mask ( Smc *  p_smc)
uint32_t smc_nfc_get_status ( Smc *  p_smc)
void smc_nfc_init ( Smc *  p_smc,
uint32_t  ul_config 
)
void smc_nfc_send_command ( Smc *  p_smc,
uint32_t  ul_cmd,
uint32_t  ul_address_cycle,
uint32_t  ul_cycle0 
)
void smc_nfc_set_address0 ( Smc *  p_smc,
uint8_t  uc_address0 
)
void smc_nfc_set_bank ( Smc *  p_smc,
uint32_t  ul_bank 
)
void smc_nfc_set_page_size ( Smc *  p_smc,
uint32_t  ul_page_size 
)
void smc_set_cycle_timing ( Smc *  p_smc,
uint32_t  ul_cs,
uint32_t  ul_cycle_timing 
)

Referenced by main().

void smc_set_mode ( Smc *  p_smc,
uint32_t  ul_cs,
uint32_t  ul_mode 
)

Referenced by main().

void smc_set_nand_timing ( Smc *  p_smc,
uint32_t  ul_cs,
uint32_t  ul_nand_timing 
)
void smc_set_pulse_timing ( Smc *  p_smc,
uint32_t  ul_cs,
uint32_t  ul_pulse_timing 
)

Referenced by main().

void smc_set_setup_timing ( Smc *  p_smc,
uint32_t  ul_cs,
uint32_t  ul_setup_timing 
)

Referenced by main().