Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
BPM - Backup Power Manager

Driver for the BPM (Backup Power Manager).

This driver provides access to the main features of the BPM controller. It provides functions for different power mode management.

Macros

#define BPM_UNLOCK(reg)
 BPM unlock macro. More...
 

Sleep mode definitions

#define BPM_SM_ACTIVE   0
 Active mode. More...
 
#define BPM_SM_SLEEP_0   1
 Sleep mode 0. More...
 
#define BPM_SM_SLEEP_1   2
 Sleep mode 1. More...
 
#define BPM_SM_SLEEP_2   3
 Sleep mode 2. More...
 
#define BPM_SM_SLEEP_3   4
 Sleep mode 3. More...
 
#define BPM_SM_WAIT   5
 Wait mode. More...
 
#define BPM_SM_RET   6
 Retention mode. More...
 
#define BPM_SM_BACKUP   7
 Backup mode. More...
 

Power scaling change mode

#define BPM_PSCM_CPU_HALT   0
 Power scaling change mode: halting the CPU execution. More...
 
#define BPM_PSCM_CPU_NOT_HALT   1
 Power scaling change mode: CPU execution not halted. More...
 

Power scaling mode value

#define BPM_PS_0   0
 Power scaling mode 0. More...
 
#define BPM_PS_1   1
 Power scaling mode 1. More...
 
#define BPM_PS_2   2
 Power scaling mode 2. More...
 

CLK32 32Khz-1Khz clock source selection

#define BPM_CLK32_SOURCE_OSC32K   0
 OSC32K : Low frequency crystal oscillator. More...
 
#define BPM_CLK32_SOURCE_RC32K   1
 RC32K : Internal Low frequency RC oscillator. More...
 

Backup wake up sources

#define BPM_BKUP_WAKEUP_SRC_EIC   (1UL << BPM_BKUPWEN_EIC)
 EIC wake up. More...
 
#define BPM_BKUP_WAKEUP_SRC_AST   (1UL << BPM_BKUPWEN_AST)
 AST wake up. More...
 
#define BPM_BKUP_WAKEUP_SRC_WDT   (1UL << BPM_BKUPWEN_WDT)
 WDT wake up. More...
 
#define BPM_BKUP_WAKEUP_SRC_BOD33   (1UL << BPM_BKUPWEN_BOD33)
 BOD33 wake up. More...
 
#define BPM_BKUP_WAKEUP_SRC_BOD18   (1UL << BPM_BKUPWEN_BOD18)
 BOD18 wake up. More...
 
#define BPM_BKUP_WAKEUP_SRC_PICOUART   (1UL << BPM_BKUPWEN_PICOUART)
 PICOUART wake up. More...
 

Backup pin muxing

#define BPM_BKUP_PIN_PB01_EIC0   BPM_BKUPPMUX_BKUPPMUX(0)
 
#define BPM_BKUP_PIN_PA06_EIC1   BPM_BKUPPMUX_BKUPPMUX(1)
 
#define BPM_BKUP_PIN_PA04_EIC2   BPM_BKUPPMUX_BKUPPMUX(2)
 
#define BPM_BKUP_PIN_PA05_EIC3   BPM_BKUPPMUX_BKUPPMUX(3)
 
#define BPM_BKUP_PIN_PA07_EIC4   BPM_BKUPPMUX_BKUPPMUX(4)
 
#define BPM_BKUP_PIN_PC03_EIC5   BPM_BKUPPMUX_BKUPPMUX(5)
 
#define BPM_BKUP_PIN_PC04_EIC6   BPM_BKUPPMUX_BKUPPMUX(6)
 
#define BPM_BKUP_PIN_PC05_EIC7   BPM_BKUPPMUX_BKUPPMUX(7)
 
#define BPM_BKUP_PIN_PC06_EIC8   BPM_BKUPPMUX_BKUPPMUX(8)
 

Power management

void bpm_sleep (Bpm *bpm, uint32_t sleep_mode)
 Enter sleep mode. More...
 
void bpm_power_scaling_cpu (Bpm *bpm, uint32_t ps_value)
 Change Power Scaling mode. More...
 
bool bpm_power_scaling_cpu_failsafe (Bpm *bpm, uint32_t ps_value, uint32_t timeout)
 Change Power Scaling mode and check results. More...
 
static __always_inline bool bpm_configure_power_scaling (Bpm *bpm, uint32_t ps_value, uint32_t no_halt)
 Configure power scaling mode. More...
 
void bpm_enable_fast_wakeup (Bpm *bpm)
 Enable fast wakeup for analog modules. More...
 
void bpm_disable_fast_wakeup (Bpm *bpm)
 Disable fast wakeup for analog modules. More...
 
void bpm_set_clk32_source (Bpm *bpm, uint32_t source)
 Set clock source for 32KHz clock. More...
 
uint32_t bpm_get_backup_wakeup_cause (Bpm *bpm)
 Get wakeup cause from backup mode. More...
 
void bpm_enable_wakeup_source (Bpm *bpm, uint32_t sources)
 Enable wakeup source. More...
 
void bpm_disable_wakeup_source (Bpm *bpm, uint32_t sources)
 Disable wakeup source. More...
 
void bpm_enable_backup_pin (Bpm *bpm, uint32_t backup_pins)
 Enable backup pin for wakeup. More...
 
void bpm_disable_backup_pin (Bpm *bpm, uint32_t backup_pins)
 Disable backup pin for wakeup. More...
 
void bpm_enable_io_retention (Bpm *bpm)
 Enable IO retention for backup mode. More...
 
void bpm_disable_io_retention (Bpm *bpm)
 Disable IO retention for backup mode. More...
 

Interrupt and status management

void bpm_enable_interrupt (Bpm *bpm, uint32_t sources)
 Enable interrupt with given sources mask. More...
 
void bpm_disable_interrupt (Bpm *bpm, uint32_t sources)
 Disable interrupt with given sources mask. More...
 
uint32_t bpm_get_interrupt_mask (Bpm *bpm)
 Get BPM interrupt mask. More...
 
uint32_t bpm_get_interrupt_status (Bpm *bpm)
 Get BPM interrupt status. More...
 
void bpm_clear_interrupt (Bpm *bpm, uint32_t sources)
 Clear BPM interrupt. More...
 
uint32_t bpm_get_status (Bpm *bpm)
 Get BPM status. More...
 
uint32_t bpm_get_version (Bpm *bpm)
 Get version of BPM module. More...
 

#define BPM_BKUP_PIN_PA04_EIC2   BPM_BKUPPMUX_BKUPPMUX(2)
#define BPM_BKUP_PIN_PA05_EIC3   BPM_BKUPPMUX_BKUPPMUX(3)
#define BPM_BKUP_PIN_PA06_EIC1   BPM_BKUPPMUX_BKUPPMUX(1)
#define BPM_BKUP_PIN_PA07_EIC4   BPM_BKUPPMUX_BKUPPMUX(4)
#define BPM_BKUP_PIN_PB01_EIC0   BPM_BKUPPMUX_BKUPPMUX(0)
#define BPM_BKUP_PIN_PC03_EIC5   BPM_BKUPPMUX_BKUPPMUX(5)
#define BPM_BKUP_PIN_PC04_EIC6   BPM_BKUPPMUX_BKUPPMUX(6)
#define BPM_BKUP_PIN_PC05_EIC7   BPM_BKUPPMUX_BKUPPMUX(7)
#define BPM_BKUP_PIN_PC06_EIC8   BPM_BKUPPMUX_BKUPPMUX(8)
#define BPM_BKUP_WAKEUP_SRC_AST   (1UL << BPM_BKUPWEN_AST)

AST wake up.

#define BPM_BKUP_WAKEUP_SRC_BOD18   (1UL << BPM_BKUPWEN_BOD18)

BOD18 wake up.

#define BPM_BKUP_WAKEUP_SRC_BOD33   (1UL << BPM_BKUPWEN_BOD33)

BOD33 wake up.

#define BPM_BKUP_WAKEUP_SRC_EIC   (1UL << BPM_BKUPWEN_EIC)

EIC wake up.

#define BPM_BKUP_WAKEUP_SRC_PICOUART   (1UL << BPM_BKUPWEN_PICOUART)

PICOUART wake up.

#define BPM_BKUP_WAKEUP_SRC_WDT   (1UL << BPM_BKUPWEN_WDT)

WDT wake up.

#define BPM_CLK32_SOURCE_OSC32K   0

OSC32K : Low frequency crystal oscillator.

Referenced by bpm_set_clk32_source().

#define BPM_CLK32_SOURCE_RC32K   1

RC32K : Internal Low frequency RC oscillator.

#define BPM_PS_0   0

Power scaling mode 0.

Referenced by sysclk_init().

#define BPM_PS_1   1

Power scaling mode 1.

Referenced by sysclk_init().

#define BPM_PS_2   2

Power scaling mode 2.

Referenced by sysclk_init().

#define BPM_PSCM_CPU_HALT   0

Power scaling change mode: halting the CPU execution.

#define BPM_PSCM_CPU_NOT_HALT   1

Power scaling change mode: CPU execution not halted.

Referenced by sysclk_init().

#define BPM_SM_ACTIVE   0

Active mode.

#define BPM_SM_BACKUP   7

Backup mode.

Referenced by bpm_sleep(), and main().

#define BPM_SM_RET   6

Retention mode.

Referenced by bpm_sleep(), and main().

#define BPM_SM_SLEEP_0   1

Sleep mode 0.

Referenced by bpm_sleep().

#define BPM_SM_SLEEP_1   2

Sleep mode 1.

Referenced by bpm_sleep().

#define BPM_SM_SLEEP_2   3

Sleep mode 2.

Referenced by bpm_sleep(), and main().

#define BPM_SM_SLEEP_3   4

Sleep mode 3.

Referenced by bpm_sleep().

#define BPM_SM_WAIT   5

Wait mode.

Referenced by bpm_sleep().

#define BPM_UNLOCK (   reg)
Value:
do { \
BPM->BPM_UNLOCK = BPM_UNLOCK_KEY(0xAAu) \
| BPM_UNLOCK_ADDR((uint32_t)&BPM->BPM_##reg - (uint32_t)BPM);\
} while (0)

BPM unlock macro.

Referenced by bpm_disable_fast_wakeup(), bpm_enable_fast_wakeup(), bpm_power_scaling_cpu(), bpm_ps_no_halt_exec(), bpm_set_clk32_source(), and bpm_sleep().

void bpm_clear_interrupt ( Bpm *  bpm,
uint32_t  sources 
)

Clear BPM interrupt.

Parameters
bpmBase address of the BPM instance.
sourcesBPM interrupt source mask.
static __always_inline bool bpm_configure_power_scaling ( Bpm *  bpm,
uint32_t  ps_value,
uint32_t  no_halt 
)
static

Configure power scaling mode.

While checking PSOK in power safe (no halt) mode, timeout is set to 240000 by default, which takes 20ms when 12MHz clock is used.

Parameters
bpmBase address of the BPM instance.
ps_valuePower scaling value, see power_scaling_mode_value.
no_haltNo halt or Fail safe, see bpm_power_scaling_cpu() and bpm_power_scaling_cpu_failsafe()
Returns
true if no error.

References bpm_power_scaling_cpu(), and bpm_power_scaling_cpu_failsafe().

Referenced by sysclk_init().

void bpm_disable_backup_pin ( Bpm *  bpm,
uint32_t  backup_pins 
)

Disable backup pin for wakeup.

Parameters
bpmBase address of the BPM instance.
backup_pinsBackup pin mask, see backup_pin_muxing.
void bpm_disable_fast_wakeup ( Bpm *  bpm)

Disable fast wakeup for analog modules.

Parameters
bpmBase address of the BPM instance.

References BPM_UNLOCK.

void bpm_disable_interrupt ( Bpm *  bpm,
uint32_t  sources 
)

Disable interrupt with given sources mask.

Parameters
bpmBase address of the BPM instance.
sourcesBPM interrupt source mask.
void bpm_disable_io_retention ( Bpm *  bpm)

Disable IO retention for backup mode.

Parameters
bpmBase address of the BPM instance.
void bpm_disable_wakeup_source ( Bpm *  bpm,
uint32_t  sources 
)

Disable wakeup source.

Parameters
bpmBase address of the BPM instance.
sourcesWakeup source mask, see backup_wake_up_sources.
void bpm_enable_backup_pin ( Bpm *  bpm,
uint32_t  backup_pins 
)

Enable backup pin for wakeup.

Parameters
bpmBase address of the BPM instance.
backup_pinsBackup pin mask, see backup_pin_muxing.

Referenced by config_wakeup().

void bpm_enable_fast_wakeup ( Bpm *  bpm)

Enable fast wakeup for analog modules.

Parameters
bpmBase address of the BPM instance.

References BPM_UNLOCK.

Referenced by sysclk_init().

void bpm_enable_interrupt ( Bpm *  bpm,
uint32_t  sources 
)

Enable interrupt with given sources mask.

Parameters
bpmBase address of the BPM instance.
sourcesBPM interrupt source mask.
void bpm_enable_io_retention ( Bpm *  bpm)

Enable IO retention for backup mode.

Parameters
bpmBase address of the BPM instance.
void bpm_enable_wakeup_source ( Bpm *  bpm,
uint32_t  sources 
)

Enable wakeup source.

Parameters
bpmBase address of the BPM instance.
sourcesWakeup source mask, see backup_wake_up_sources.

Referenced by config_wakeup().

uint32_t bpm_get_backup_wakeup_cause ( Bpm *  bpm)

Get wakeup cause from backup mode.

Parameters
bpmBase address of the BPM instance.
uint32_t bpm_get_interrupt_mask ( Bpm *  bpm)

Get BPM interrupt mask.

Parameters
bpmBase address of the BPM instance.
Returns
BPM interrupt mask.
uint32_t bpm_get_interrupt_status ( Bpm *  bpm)

Get BPM interrupt status.

Parameters
bpmBase address of the BPM instance.
Returns
BPM interrupt status.
uint32_t bpm_get_status ( Bpm *  bpm)

Get BPM status.

Parameters
bpmBase address of the BPM instance.
Returns
BPM status.

Referenced by sysclk_init().

uint32_t bpm_get_version ( Bpm *  bpm)

Get version of BPM module.

Parameters
bpmBase address of the BPM instance.
Returns
Version of BPM module.
void bpm_power_scaling_cpu ( Bpm *  bpm,
uint32_t  ps_value 
)

Change Power Scaling mode.

PSOK is not checked while switching PS mode.

Parameters
bpmBase address of the BPM instance.
ps_valuePower scaling value, see power_scaling_mode_value.

References BPM_UNLOCK.

Referenced by bpm_configure_power_scaling().

bool bpm_power_scaling_cpu_failsafe ( Bpm *  bpm,
uint32_t  ps_value,
uint32_t  timeout 
)

Change Power Scaling mode and check results.

Wait for a while to check if PSOK is ready.

Parameters
bpmBase address of the BPM instance.
ps_valuePower scaling value, see power_scaling_mode_value.
timeoutTimeout, in number of processor clocks, max 0xFFFFFF.
Returns
true if PSOK is ready.

References bpm_ps_no_halt_exec(), cpu_irq_restore(), and cpu_irq_save().

Referenced by bpm_configure_power_scaling().

void bpm_set_clk32_source ( Bpm *  bpm,
uint32_t  source 
)

Set clock source for 32KHz clock.

Parameters
bpmBase address of the BPM instance.
sourceClock source, see CLK32_32Khz_1Khz.

References BPM_CLK32_SOURCE_OSC32K, and BPM_UNLOCK.

void bpm_sleep ( Bpm *  bpm,
uint32_t  sleep_mode 
)

Enter sleep mode.

Parameters
bpmBase address of the BPM instance.
sleep_modeExpected sleep mode (active case not included).

References BPM_SM_BACKUP, BPM_SM_RET, BPM_SM_SLEEP_0, BPM_SM_SLEEP_1, BPM_SM_SLEEP_2, BPM_SM_SLEEP_3, BPM_SM_WAIT, BPM_UNLOCK, and cpu_irq_enable.

Referenced by main(), and sleepmgr_sleep().