Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Pulse Width Modulation (PWM)

See Quickstart guide for SAM PWM module.

Driver for the PWM (Pulse Width Modulation). This driver provides access to the main features of the PWM controller.

Macros

#define PWM_CLOCK_DIV_MAX   256
 
#define PWM_CLOCK_PRE_MAX   11
 
#define PWM_WPCR_WPCMD_DISABLE_SW_PROT   (PWM_WPCR_WPCMD(0))
 
#define PWM_WPCR_WPCMD_ENABLE_HW_PROT   (PWM_WPCR_WPCMD(2))
 
#define PWM_WPCR_WPCMD_ENABLE_SW_PROT   (PWM_WPCR_WPCMD(1))
 
#define PWM_WPCR_WPKEY_PASSWD   0x50574D00
 

Functions

void pwm_channel_disable (Pwm *p_pwm, uint32_t ul_channel)
 Disable the PWM channel. More...
 
void pwm_channel_disable_interrupt (Pwm *p_pwm, uint32_t ul_event, uint32_t ul_fault)
 Disable the interrupt of a channel counter event and fault protection. More...
 
void pwm_channel_enable (Pwm *p_pwm, uint32_t ul_channel)
 Enable the PWM channel. More...
 
void pwm_channel_enable_interrupt (Pwm *p_pwm, uint32_t ul_event, uint32_t ul_fault)
 Enable the interrupt of a channel counter event and fault protection. More...
 
uint32_t pwm_channel_get_counter (Pwm *p_pwm, pwm_channel_t *p_channel)
 Return channel counter value. More...
 
uint32_t pwm_channel_get_interrupt_mask (Pwm *p_pwm)
 Get channel counter event and fault protection trigger interrupt mask. More...
 
uint32_t pwm_channel_get_interrupt_status (Pwm *p_pwm)
 Get channel counter event and fault protection trigger interrupt status. More...
 
uint32_t pwm_channel_get_status (Pwm *p_pwm)
 Check which PWM channel is enabled. More...
 
uint32_t pwm_channel_init (Pwm *p_pwm, pwm_channel_t *p_channel)
 Initialize one PWM channel. More...
 
void pwm_channel_update_dead_time (Pwm *p_pwm, pwm_channel_t *p_channel, uint16_t us_deadtime_pwmh, uint16_t us_deadtime_pwml)
 Change dead-time value for PWM outputs. More...
 
uint32_t pwm_channel_update_duty (Pwm *p_pwm, pwm_channel_t *p_channel, uint32_t ul_duty)
 Change the duty cycle of the PWM channel. More...
 
void pwm_channel_update_output (Pwm *p_pwm, pwm_channel_t *p_channel, pwm_output_t *p_output, bool b_sync)
 Change output selection of the PWM channel. More...
 
uint32_t pwm_channel_update_period (Pwm *p_pwm, pwm_channel_t *p_channel, uint32_t ul_period)
 Change the period of the PWM channel. More...
 
void pwm_channel_update_polarity_mode (Pwm *p_pwm, pwm_channel_t *p_channel, bool polarity_inversion_flag, pwm_level_t polarity_value)
 Change polarity mode. More...
 
void pwm_channel_update_spread (Pwm *p_pwm, pwm_channel_t *p_channel, uint32_t ul_spread)
 Change spread spectrum value. More...
 
static uint32_t pwm_clocks_generate (uint32_t ul_frequency, uint32_t ul_mck)
 Find a prescaler/divisor couple to generate the desired ul_frequency from ul_mck. More...
 
uint32_t pwm_cmp_change_setting (Pwm *p_pwm, pwm_cmp_t *p_cmp)
 Change the setting of PWM comparison. More...
 
void pwm_cmp_disable_interrupt (Pwm *p_pwm, uint32_t ul_sources, pwm_cmp_interrupt_t type)
 Disable the interrupt of comparison. More...
 
void pwm_cmp_enable_interrupt (Pwm *p_pwm, uint32_t ul_sources, pwm_cmp_interrupt_t type)
 Enable the interrupt of comparison. More...
 
uint32_t pwm_cmp_get_period_counter (Pwm *p_pwm, uint32_t ul_cmp_unit)
 Report the value of the comparison period counter. More...
 
uint32_t pwm_cmp_get_update_counter (Pwm *p_pwm, uint32_t ul_cmp_unit)
 Report the value of the comparison update period counter. More...
 
uint32_t pwm_cmp_init (Pwm *p_pwm, pwm_cmp_t *p_cmp)
 Initialize PWM comparison unit. More...
 
void pwm_disable_protect (Pwm *p_pwm, uint32_t ul_group)
 Disable PWM write protect. More...
 
void pwm_enable_protect (Pwm *p_pwm, uint32_t ul_group, bool b_sw)
 Enable PWM write protect. More...
 
void pwm_fault_clear_status (Pwm *p_pwm, pwm_fault_id_t id)
 Clear a fault input. More...
 
pwm_level_t pwm_fault_get_input_level (Pwm *p_pwm, pwm_fault_id_t id)
 Get the level of a fault input. More...
 
uint32_t pwm_fault_get_status (Pwm *p_pwm)
 Get fault status. More...
 
uint32_t pwm_fault_init (Pwm *p_pwm, pwm_fault_t *p_fault)
 Initialize the behavior of a fault input. More...
 
uint32_t pwm_get_interrupt_mask (Pwm *p_pwm)
 Get interrupt mask of PDC transfer, synchronous channels and comparison. More...
 
uint32_t pwm_get_interrupt_status (Pwm *p_pwm)
 Get interrupt status of PDC transfer, synchronous channels and comparison. More...
 
bool pwm_get_protect_status (Pwm *p_pwm, pwm_protect_t *p_protect)
 Get PWM write protect status. More...
 
uint32_t pwm_init (Pwm *p_pwm, pwm_clock_t *clock_config)
 Initialize the PWM source clock (clock A and clock B). More...
 
void pwm_pdc_disable_interrupt (Pwm *p_pwm, uint32_t ul_sources)
 Disable the interrupt of PDC transfer. More...
 
void pwm_pdc_enable_interrupt (Pwm *p_pwm, uint32_t ul_sources)
 Enable the interrupt of PDC transfer. More...
 
void pwm_pdc_set_request_mode (Pwm *p_pwm, pwm_pdc_request_mode_t request_mode, uint32_t ul_cmp_unit)
 Set PDC transfer request mode. More...
 
void pwm_set_dma_duty (Pwm *p_pwm, uint32_t ul_dma_duty_value)
 Set dma duty. More...
 
void pwm_set_ext_trigger_mode (Pwm *p_pwm, pwm_channel_t *p_channel, uint32_t ul_mode)
 set external trigger mode. More...
 
void pwm_stepper_motor_init (Pwm *p_pwm, pwm_stepper_motor_pair_t pair, bool b_enable_gray, bool b_down)
 Initialize PWM stepper motor mode. More...
 
void pwm_sync_change_period (Pwm *p_pwm, uint32_t ul_update_period)
 Change the wanted time between each update of the synchronous channels. More...
 
void pwm_sync_disable_interrupt (Pwm *p_pwm, uint32_t ul_sources)
 Disable the interrupt of synchronous channels. More...
 
void pwm_sync_enable_interrupt (Pwm *p_pwm, uint32_t ul_sources)
 Enable the interrupt of synchronous channel. More...
 
uint32_t pwm_sync_get_period_counter (Pwm *p_pwm)
 Get the value of the synchronization update period counter. More...
 
uint32_t pwm_sync_init (Pwm *p_pwm, pwm_sync_update_mode_t mode, uint32_t ul_update_period)
 Initialize synchronous channels update mode and period. More...
 
void pwm_sync_unlock_update (Pwm *p_pwm)
 Unlock the update of synchronous channels. More...
 

#define PWM_CLOCK_DIV_MAX   256

Referenced by pwm_clocks_generate().

#define PWM_CLOCK_PRE_MAX   11

Referenced by pwm_clocks_generate().

#define PWM_WPCR_WPCMD_DISABLE_SW_PROT   (PWM_WPCR_WPCMD(0))

Referenced by pwm_disable_protect().

#define PWM_WPCR_WPCMD_ENABLE_HW_PROT   (PWM_WPCR_WPCMD(2))

Referenced by pwm_enable_protect().

#define PWM_WPCR_WPCMD_ENABLE_SW_PROT   (PWM_WPCR_WPCMD(1))

Referenced by pwm_enable_protect().

#define PWM_WPCR_WPKEY_PASSWD   0x50574D00

void pwm_channel_disable ( Pwm *  p_pwm,
uint32_t  ul_channel 
)

Disable the PWM channel.

Note
A disabled PWM channel can be re-initialized using pwm_channel_init().
Parameters
p_pwmPointer to a PWM instance.
ul_channelPWM channel number to disable.

Referenced by run_pwm_test().

void pwm_channel_disable_interrupt ( Pwm *  p_pwm,
uint32_t  ul_event,
uint32_t  ul_fault 
)

Disable the interrupt of a channel counter event and fault protection.

Parameters
p_pwmPointer to a PWM instance.
ul_eventBitmask of channel number to disable counter event interrupt.
ul_faultBitmask of channel number to disable fault protection interrupt(ignored by SAM3N/SAM4N/SAM4C/SAM4CP/SAM4CM).

References UNUSED.

Referenced by run_pwm_test().

void pwm_channel_enable ( Pwm *  p_pwm,
uint32_t  ul_channel 
)

Enable the PWM channel.

Note
The PWM channel should be initialized by pwm_channel_init() before it is enabled.
Parameters
p_pwmPointer to a PWM instance.
ul_channelPWM channel number to enable.

Referenced by run_pwm_test().

void pwm_channel_enable_interrupt ( Pwm *  p_pwm,
uint32_t  ul_event,
uint32_t  ul_fault 
)

Enable the interrupt of a channel counter event and fault protection.

Parameters
p_pwmPointer to a PWM instance.
ul_eventChannel number to enable counter event interrupt.
ul_faultChannel number to enable fault protection interrupt(ignored by SAM3N/SAM4N/SAM4C/SAM4CP/SAM4CM).

References UNUSED.

Referenced by run_pwm_test().

uint32_t pwm_channel_get_counter ( Pwm *  p_pwm,
pwm_channel_t p_channel 
)

Return channel counter value.

Parameters
p_pwmPointer to a PWM instance.
p_channelConfigurations of the specified PWM channel.
Returns
channel Counter value.

References pwm_channel_t::channel.

uint32_t pwm_channel_get_interrupt_mask ( Pwm *  p_pwm)

Get channel counter event and fault protection trigger interrupt mask.

Parameters
p_pwmPointer to a PWM instance.
Returns
Channel counter event and fault protection trigger interrupt mask.
uint32_t pwm_channel_get_interrupt_status ( Pwm *  p_pwm)

Get channel counter event and fault protection trigger interrupt status.

Parameters
p_pwmPointer to a PWM instance.
Returns
Channel counter event and fault protection trigger interrupt status.

Referenced by PWM_Handler().

uint32_t pwm_channel_get_status ( Pwm *  p_pwm)

Check which PWM channel is enabled.

Parameters
p_pwmPointer to a PWM instance.
p_channelConfigurations of the specified PWM channel.
Returns
Bitmask of enabled PWM channel(s).
void pwm_channel_update_dead_time ( Pwm *  p_pwm,
pwm_channel_t p_channel,
uint16_t  us_deadtime_pwmh,
uint16_t  us_deadtime_pwml 
)

Change dead-time value for PWM outputs.

Parameters
p_pwmPointer to a PWM instance.
p_channelConfigurations of the specified PWM channel.
us_deadtime_pwmhNew dead-time value for PWMH output.
us_deadtime_pwmlNew dead-time value for PWML output.

References pwm_channel_t::channel, pwm_channel_t::us_deadtime_pwmh, and pwm_channel_t::us_deadtime_pwml.

uint32_t pwm_channel_update_duty ( Pwm *  p_pwm,
pwm_channel_t p_channel,
uint32_t  ul_duty 
)

Change the duty cycle of the PWM channel.

Parameters
p_pwmPointer to a PWM instance.
p_channelConfigurations of the specified PWM channel.
ul_dutyNew duty cycle value.
Return values
0if changing succeeds, otherwise fails.

Check parameter

References pwm_channel_t::channel, PWM_INVALID_ARGUMENT, pwm_channel_t::ul_duty, and pwm_channel_t::ul_period.

void pwm_channel_update_output ( Pwm *  p_pwm,
pwm_channel_t p_channel,
pwm_output_t p_output,
bool  b_sync 
)

Change output selection of the PWM channel.

Parameters
p_pwmPointer to a PWM instance.
p_channelConfigurations of the specified PWM channel.
p_outputNew PWM channel output selection.
b_syncBoolean of changing of output selection. Set true to change the output synchronously (at the beginning of the next PWM period). Set false to change the output asynchronously (at the end of the execution of the function).

References pwm_output_t::b_override_pwmh, pwm_output_t::b_override_pwml, pwm_channel_t::channel, pwm_channel_t::output_selection, pwm_output_t::override_level_pwmh, and pwm_output_t::override_level_pwml.

uint32_t pwm_channel_update_period ( Pwm *  p_pwm,
pwm_channel_t p_channel,
uint32_t  ul_period 
)

Change the period of the PWM channel.

Parameters
p_pwmPointer to a PWM instance.
p_channelConfigurations of the specified PWM channel.
ul_periodNew period value.
Return values
0if changing succeeds, otherwise fails.

Check parameter

References pwm_channel_t::channel, PWM_INVALID_ARGUMENT, pwm_channel_t::ul_duty, and pwm_channel_t::ul_period.

void pwm_channel_update_polarity_mode ( Pwm *  p_pwm,
pwm_channel_t p_channel,
bool  polarity_inversion_flag,
pwm_level_t  polarity_value 
)

Change polarity mode.

Parameters
p_pwmPointer to a PWM instance.
p_channelConfigurations of the specified PWM channel.
polarity_inversion_flagPolarity invertion.
polarity_flagPolarity value.

References pwm_channel_t::channel, pwm_channel_t::polarity, and PWM_HIGH.

void pwm_channel_update_spread ( Pwm *  p_pwm,
pwm_channel_t p_channel,
uint32_t  ul_spread 
)

Change spread spectrum value.

Parameters
p_pwmPointer to a PWM instance.
p_channelConfigurations of the specified PWM channel.
ul_spreadNew spread spectrum value.

References pwm_channel_t::ul_spread.

static uint32_t pwm_clocks_generate ( uint32_t  ul_frequency,
uint32_t  ul_mck 
)
static

Find a prescaler/divisor couple to generate the desired ul_frequency from ul_mck.

Parameters
ul_frequencyDesired frequency in Hz.
ul_mckMaster clock frequency in Hz.
Return values
Returnthe value to be set in the PWM Clock Register (PWM Mode Register for SAM3N/SAM4N/SAM4C/SAM4CP/SAM4CM) or PWM_INVALID_ARGUMENT if the configuration cannot be met.

References PWM_CLOCK_DIV_MAX, PWM_CLOCK_PRE_MAX, and PWM_INVALID_ARGUMENT.

Referenced by pwm_init().

uint32_t pwm_cmp_change_setting ( Pwm *  p_pwm,
pwm_cmp_t p_cmp 
)

Change the setting of PWM comparison.

Parameters
p_pwmPointer to a PWM instance.
p_cmpConfigurations of PWM comparison tagged by unit.
Return values
0if changing succeeds, otherwise fails.

Boolean of generating a match pulse

Boolean of generating a match pulse

Boolean of comparison enable

References pwm_cmp_t::b_enable, pwm_cmp_t::b_is_decrementing, pwm_cmp_t::b_pulse_on_line_0, pwm_cmp_t::b_pulse_on_line_1, pwm_cmp_t::ul_period, pwm_cmp_t::ul_trigger, pwm_cmp_t::ul_update_period, pwm_cmp_t::ul_value, and pwm_cmp_t::unit.

void pwm_cmp_disable_interrupt ( Pwm *  p_pwm,
uint32_t  ul_sources,
pwm_cmp_interrupt_t  type 
)

Disable the interrupt of comparison.

Parameters
p_pwmPointer to a PWM instance.
ul_sourcesBitmask of comparison unit.
typePWM_CMP_MATCH disables the match interrupt of the unit. PWM_CMP_UPDATE disables the update interrupt of the comparison unit.

References PWM_CMP_MATCH, and PWM_CMP_UPDATE.

Referenced by run_pwm_test().

void pwm_cmp_enable_interrupt ( Pwm *  p_pwm,
uint32_t  ul_sources,
pwm_cmp_interrupt_t  type 
)

Enable the interrupt of comparison.

Parameters
p_pwmPointer to a PWM instance.
ul_sourcesBitmask of comparison unit.
typePWM_CMP_MATCH enables the match interrupt of the unit. PWM_CMP_UPDATE enables the update interrupt of the comparison unit.

References PWM_CMP_MATCH, and PWM_CMP_UPDATE.

Referenced by run_pwm_test().

uint32_t pwm_cmp_get_period_counter ( Pwm *  p_pwm,
uint32_t  ul_cmp_unit 
)

Report the value of the comparison period counter.

Parameters
p_pwmPointer to a PWM instance.
ul_cmp_unitPWM comparison unit number.
Returns
Value of the comparison period counter.
uint32_t pwm_cmp_get_update_counter ( Pwm *  p_pwm,
uint32_t  ul_cmp_unit 
)

Report the value of the comparison update period counter.

Parameters
p_pwmPointer to a PWM instance.
ul_cmp_unitPWM comparison unit number.
Returns
Value of the comparison update period counter.
uint32_t pwm_cmp_init ( Pwm *  p_pwm,
pwm_cmp_t p_cmp 
)

Initialize PWM comparison unit.

Parameters
p_pwmPointer to a PWM instance.
p_cmpConfigurations of PWM comparison tagged by unit.
Return values
0if initialization succeeds, otherwise fails.

Boolean of generating a match pulse

Boolean of generating a match pulse

Boolean of comparison enable

References pwm_cmp_t::b_enable, pwm_cmp_t::b_is_decrementing, pwm_cmp_t::b_pulse_on_line_0, pwm_cmp_t::b_pulse_on_line_1, pwm_cmp_t::ul_period, pwm_cmp_t::ul_trigger, pwm_cmp_t::ul_update_period, pwm_cmp_t::ul_value, and pwm_cmp_t::unit.

Referenced by run_pwm_test().

void pwm_disable_protect ( Pwm *  p_pwm,
uint32_t  ul_group 
)

Disable PWM write protect.

Note
Only a hardware reset of PWM controller (handled by PMC) can disable hardware write protect.
Parameters
p_pwmPointer to a PWM instance.
ul_groupBitmask of PWM register group.

References PWM_WPCR_WPCMD_DISABLE_SW_PROT, and PWM_WPCR_WPKEY_PASSWD.

void pwm_enable_protect ( Pwm *  p_pwm,
uint32_t  ul_group,
bool  b_sw 
)

Enable PWM write protect.

Parameters
p_pwmPointer to a PWM instance.
ul_groupBitmask of PWM register group.
b_swBoolean of software protect. True for software protect and false for hardware protect.

References PWM_WPCR_WPCMD_ENABLE_HW_PROT, PWM_WPCR_WPCMD_ENABLE_SW_PROT, and PWM_WPCR_WPKEY_PASSWD.

void pwm_fault_clear_status ( Pwm *  p_pwm,
pwm_fault_id_t  id 
)

Clear a fault input.

Parameters
p_pwmPointer to a PWM instance.
idFaulty ID.
pwm_level_t pwm_fault_get_input_level ( Pwm *  p_pwm,
pwm_fault_id_t  id 
)

Get the level of a fault input.

Parameters
p_pwmPointer to a PWM instance.
idFaulty ID.
Returns
Level of the fault input.

References PWM_HIGH, and PWM_LOW.

uint32_t pwm_fault_get_status ( Pwm *  p_pwm)

Get fault status.

Parameters
p_pwmPointer to a PWM instance.
Returns
Bitmask of IDs of all active faulty.
uint32_t pwm_fault_init ( Pwm *  p_pwm,
pwm_fault_t p_fault 
)

Initialize the behavior of a fault input.

Parameters
p_pwmPointer to a PWM instance.
p_faultConfigurations of a fault input.
Return values
0if configuration succeeds, otherwise fails.

Polarity of fault input

Boolean of clearing fault flag

Boolean of fault filtering

References pwm_fault_t::b_clear, pwm_fault_t::b_filtered, pwm_fault_t::fault_id, pwm_fault_t::polarity, and PWM_HIGH.

uint32_t pwm_get_interrupt_mask ( Pwm *  p_pwm)

Get interrupt mask of PDC transfer, synchronous channels and comparison.

Parameters
p_pwmPointer to a PWM instance.
Returns
Interrupt mask of PDC transfer, synchronous channels and comparison.
uint32_t pwm_get_interrupt_status ( Pwm *  p_pwm)

Get interrupt status of PDC transfer, synchronous channels and comparison.

Parameters
p_pwmPointer to a PWM instance.
Returns
Interrupt status of PDC transfer, synchronous channels and comparison.

Referenced by PWM_Handler().

bool pwm_get_protect_status ( Pwm *  p_pwm,
pwm_protect_t p_protect 
)

Get PWM write protect status.

Parameters
p_pwmPointer to a PWM instance.
p_protectPointer to a structure stored PWM protect status.
Return values
0Protection disabled.
1Protection enabled.

Bitmask of PWM register group for write protect software status

References pwm_protect_t::ul_hw_status, pwm_protect_t::ul_offset, and pwm_protect_t::ul_sw_status.

uint32_t pwm_init ( Pwm *  p_pwm,
pwm_clock_t clock_config 
)

Initialize the PWM source clock (clock A and clock B).

Parameters
p_pwmPointer to a PWM instance.
clock_configPWM clock configuration.
Return values
0if initialization succeeds, otherwise fails.

References pwm_clocks_generate(), PWM_INVALID_ARGUMENT, pwm_clock_t::ul_clka, pwm_clock_t::ul_clkb, and pwm_clock_t::ul_mck.

Referenced by run_pwm_test().

void pwm_pdc_disable_interrupt ( Pwm *  p_pwm,
uint32_t  ul_sources 
)

Disable the interrupt of PDC transfer.

Parameters
p_pwmPointer to a PWM instance.
ul_sourcesBitmask of PWM PDC transfer interrupt sources.
void pwm_pdc_enable_interrupt ( Pwm *  p_pwm,
uint32_t  ul_sources 
)

Enable the interrupt of PDC transfer.

Parameters
p_pwmPointer to a PWM instance.
ul_sourcesBitmask of PWM PDC transfer interrupt sources.

Referenced by run_pwm_test().

void pwm_pdc_set_request_mode ( Pwm *  p_pwm,
pwm_pdc_request_mode_t  request_mode,
uint32_t  ul_cmp_unit 
)

Set PDC transfer request mode.

Note
If configure Synchronous channels update mode as 'PWM_SYNC_UPDATE_MODE_0' or 'PWM_SYNC_UPDATE_MODE_1' via pwm_sync_init(), ul_pdc_request will be ignored and PDC transfer request will never occur.
Parameters
p_pwmPointer to a PWM instance.
request_modePDC transfer request mode.
ul_cmp_unitPWM comparison unit number for PDC transfer request.

Referenced by run_pwm_test().

void pwm_set_dma_duty ( Pwm *  p_pwm,
uint32_t  ul_dma_duty_value 
)

Set dma duty.

Parameters
p_pwmPointer to a PWM instance.
ul_dma_duty_valueThe dma duty to be set.
void pwm_set_ext_trigger_mode ( Pwm *  p_pwm,
pwm_channel_t p_channel,
uint32_t  ul_mode 
)

set external trigger mode.

Parameters
p_pwmPointer to a PWM instance.
p_channelConfigurations of the specified PWM channel.
ul_modeThe external trigger mode to be set.

References pwm_channel_t::channel.

void pwm_stepper_motor_init ( Pwm *  p_pwm,
pwm_stepper_motor_pair_t  pair,
bool  b_enable_gray,
bool  b_down 
)

Initialize PWM stepper motor mode.

Parameters
p_pwmPointer to a PWM instance.
pairPWM channels used by stepper motor.
b_enable_graySet true to enable gray count generation. Set false to disable it.
b_downSet true to use down counter. Set false to use up counter.
void pwm_sync_change_period ( Pwm *  p_pwm,
uint32_t  ul_update_period 
)

Change the wanted time between each update of the synchronous channels.

Parameters
p_pwmPointer to a PWM instance.
ul_update_periodTime between each update of the synchronous channels.
void pwm_sync_disable_interrupt ( Pwm *  p_pwm,
uint32_t  ul_sources 
)

Disable the interrupt of synchronous channels.

Parameters
p_pwmPointer to a PWM instance.
ul_sourcesBitmask of PWM synchronous channels interrupt sources.
void pwm_sync_enable_interrupt ( Pwm *  p_pwm,
uint32_t  ul_sources 
)

Enable the interrupt of synchronous channel.

Parameters
p_pwmPointer to a PWM instance.
ul_sourcesBitmask of PWM synchronous channels interrupt sources.
uint32_t pwm_sync_get_period_counter ( Pwm *  p_pwm)

Get the value of the synchronization update period counter.

Parameters
p_pwmPointer to a PWM instance.
Returns
Value of the synchronization update Period Counter.
uint32_t pwm_sync_init ( Pwm *  p_pwm,
pwm_sync_update_mode_t  mode,
uint32_t  ul_update_period 
)

Initialize synchronous channels update mode and period.

Parameters
p_pwmPointer to a PWM instance.
modeSynchronous channels update mode.
ul_update_periodTime between each update of the synchronous channels.
Return values
0if initialization succeeds, otherwise fails.

Referenced by run_pwm_test().

void pwm_sync_unlock_update ( Pwm *  p_pwm)

Unlock the update of synchronous channels.

Note
After unlock, synchronous channels will be updated at the next PWM period.
Parameters
p_pwmPointer to a PWM instance.