License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Quickstart guide for SAM SPI driver | This is the quickstart guide for the SAM SPI driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the System Clock Management | Service (SAMV71) |
Advanced use case - Peripheral Bus Clock | Management (SAMV71) |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Extra Information for Extensible Direct Memory Access Controller Driver | |
Examples for Direct Memory Access Controller Driver | This is a list of the available Quick Start Guides (QSGs) and example applications for SAMV71/V70/E70/S70 XDMA Controller (XDMAC) Driver |
 Quick Start Guide for the XDMAC driver | This is the quick start guide for the SAMV71/V70/E70/S70 XDMA Controller (XDMAC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the XDMAC module |
Document Revision History | |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
 Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Quick start guide for the SAM USART module | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 USART receive character and echo back | In this use case, the USART module is configured for: |
 USART receive character and echo back via interrupts | In this use case, the USART module is configured for: |
"SAME70-XPLD - Operating frequencies" | This page lists several definition related to the board operating frequency |
"SAME70-XPLD - Board informations" | This page lists several definition related to the board description |
"SAME70-XPLD - CAN" | This page lists definitions related to CAN0 and CAN1 |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
Todo List | |