Configuration of the USI example application.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | COUNT_MS_SWAP_LED 500 |
LED blinking rate in msec. More... | |
#define | MAX_COMMAND_LENGTH 20 |
Maximum length of the input command. More... | |
#define | PROGRAM_MAIN_MENU "Introduce command:\n"STRING_EOL |
#define | STRING_EOL "\r" |
#define | STRING_HEADER |
TC configuration for msec timer | |
#define | ID_TC_1MS ID_TC3 |
#define | TC_1MS TC1 |
#define | TC_1MS_CHN 0 |
#define | TC_1MS_IRQn TC3_IRQn |
#define | TC_1MS_Handler TC3_Handler |
#define COUNT_MS_SWAP_LED 500 |
LED blinking rate in msec.
#define ID_TC_1MS ID_TC3 |
#define MAX_COMMAND_LENGTH 20 |
Maximum length of the input command.
#define PROGRAM_MAIN_MENU "Introduce command:\n"STRING_EOL |
#define STRING_EOL "\r" |
#define STRING_HEADER |
#define TC_1MS TC1 |
#define TC_1MS_CHN 0 |
#define TC_1MS_Handler TC3_Handler |
#define TC_1MS_IRQn TC3_IRQn |