This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Timer Counter functionality.
The Timer Counter (TC) includes several identical 16-bit or 32-bit Timer Counter channels. Each channel can be independently programmed to perform a wide range of functions that includes frequency measurement, event counting, interval measurement, pulse generation, delay timing, and pulse width modulation.
Devices from the following series can use this module:
The outline of this documentation is as follows:
There are no prerequisites for this module.
The Timer Counter (TC) includes several identical 16-bit or 32-bit Timer Counter channels. The number of TC channels is device specific, refer to the device-specific datasheet for more information.
Each channel can be independently programmed to perform a wide range of functions that includes frequency measurement, event counting, interval measurement, pulse generation, delay timing, and pulse width modulation.
Each channel has three external clock inputs, five internal clock inputs, and two multi-purpose input/output signals which can be configured by the user. Each channel drives an internal interrupt signal which can be programmed to generate processor interrupts.
The Timer Counter (TC) embeds a quadrature decoder logic connected in front of the timers. When enabled, the quadrature decoder performs the input line filtering, decoding of quadrature signals and connects to the timers/counters in order to read the position and speed of the motor.
In all cases, if an external clock is used, the duration of each of its levels must be longer than the master clock (MCLK) period. The external clock frequency must be at least 2.5 times lower than the master clock.
If an external trigger is used, the duration of its pulses must be longer than the master clock (MCLK) period in order to be detected.
For extra information, see Extra Information for Timer Counter Driver. This includes:
For a list of examples related to this driver, see Examples for Timer Counter.
Functions | |
void | tc_disable_interrupt (Tc *p_tc, uint32_t ul_channel, uint32_t ul_sources) |
Disable TC interrupts on the specified channel. More... | |
void | tc_disable_qdec_interrupt (Tc *p_tc, uint32_t ul_sources) |
Disable TC QDEC interrupts. More... | |
void | tc_enable_interrupt (Tc *p_tc, uint32_t ul_channel, uint32_t ul_sources) |
Enable the TC interrupts on the specified channel. More... | |
void | tc_enable_qdec_interrupt (Tc *p_tc, uint32_t ul_sources) |
Enable TC QDEC interrupts. More... | |
uint32_t | tc_find_mck_divisor (uint32_t ul_freq, uint32_t ul_mck, uint32_t *p_uldiv, uint32_t *ul_tcclks, uint32_t ul_boardmck) |
Find the best MCK divisor. More... | |
uint32_t | tc_get_feature (Tc *p_tc) |
Indicate TC features. More... | |
uint32_t | tc_get_interrupt_mask (Tc *p_tc, uint32_t ul_channel) |
Read the TC interrupt mask for the specified channel. More... | |
uint32_t | tc_get_qdec_interrupt_mask (Tc *p_tc) |
Read TC QDEC interrupt mask. More... | |
uint32_t | tc_get_qdec_interrupt_status (Tc *p_tc) |
Get current TC QDEC interrupt status. More... | |
uint32_t | tc_get_status (Tc *p_tc, uint32_t ul_channel) |
Get the current status for the specified TC channel. More... | |
uint32_t | tc_get_version (Tc *p_tc) |
Indicate TC version. More... | |
void | tc_init (Tc *p_tc, uint32_t ul_Channel, uint32_t ul_Mode) |
Configure TC for timer, waveform generation, or capture. More... | |
uint32_t | tc_init_2bit_gray (Tc *p_tc, uint32_t ul_channel, uint32_t ul_steppermode) |
Configure TC for 2-bit Gray Counter for Stepper Motor. More... | |
uint32_t | tc_read_cv (Tc *p_tc, uint32_t ul_channel) |
Read the counter value on the specified channel. More... | |
uint32_t | tc_read_ra (Tc *p_tc, uint32_t ul_channel) |
Read TC Register A (RA) on the specified channel. More... | |
uint32_t | tc_read_rb (Tc *p_tc, uint32_t ul_channel) |
Read TC Register B (RB) on the specified channel. More... | |
uint32_t | tc_read_rc (Tc *p_tc, uint32_t ul_channel) |
Read TC Register C (RC) on the specified channel. More... | |
void | tc_set_block_mode (Tc *p_tc, uint32_t ul_blockmode) |
Configure the TC Block mode. More... | |
void | tc_set_writeprotect (Tc *p_tc, uint32_t ul_enable) |
Enable or disable write protection of TC registers. More... | |
void | tc_start (Tc *p_tc, uint32_t ul_channel) |
Start the TC clock on the specified channel. More... | |
void | tc_stop (Tc *p_tc, uint32_t ul_channel) |
Stop the TC clock on the specified channel. More... | |
void | tc_sync_trigger (Tc *p_tc) |
Asserts a SYNC signal to generate a software trigger on all channels. More... | |
void | tc_write_ra (Tc *p_tc, uint32_t ul_channel, uint32_t ul_value) |
Write to TC Register A (RA) on the specified channel. More... | |
void | tc_write_rb (Tc *p_tc, uint32_t ul_channel, uint32_t ul_value) |
Write to TC Register B (RB) on the specified channel. More... | |
void | tc_write_rc (Tc *p_tc, uint32_t ul_channel, uint32_t ul_value) |
Write to TC Register C (RC) on the selected channel. More... | |
void tc_disable_interrupt | ( | Tc * | p_tc, |
uint32_t | ul_channel, | ||
uint32_t | ul_sources | ||
) |
Disable TC interrupts on the specified channel.
[in,out] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to configure |
[in] | ul_sources | A bitmask of Interrupt sources |
Where the input parameter ul_sources can be one or more of the following:
Parameter Value | Description |
---|---|
TC_IDR_COVFS | Disables the Counter Overflow Interrupt |
TC_IDR_LOVRS | Disables the Load Overrun Interrupt |
TC_IDR_CPAS | Disables the RA Compare Interrupt |
TC_IDR_CPBS | Disables the RB Compare Interrupt |
TC_IDR_CPCS | Disables the RC Compare Interrupt |
TC_IDR_LDRAS | Disables the RA Load Interrupt |
TC_IDR_LDRBS | Disables the RB Load Interrupt |
TC_IDR_ETRGS | Disables the External Trigger Interrupt |
References Assert.
void tc_disable_qdec_interrupt | ( | Tc * | p_tc, |
uint32_t | ul_sources | ||
) |
Disable TC QDEC interrupts.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_sources | A bitmask of QDEC interrupts to be disabled |
Where the input parameter ul_sources can be one or more of the following:
Parameter Value | Description |
---|---|
TC_QIDR_IDX | Disable the rising edge detected on IDX input interrupt |
TC_QIDR_DIRCHG | Disable the change in rotation direction detected interrupt |
TC_QIDR_QERR | Disable the quadrature error detected on PHA/PHB interrupt |
References Assert.
void tc_enable_interrupt | ( | Tc * | p_tc, |
uint32_t | ul_channel, | ||
uint32_t | ul_sources | ||
) |
Enable the TC interrupts on the specified channel.
[in,out] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to configure |
[in] | ul_sources | Bitmask of interrupt sources |
Where the input parameter ul_sources can be one or more of the following:
Parameter Value | Description |
---|---|
TC_IER_COVFS | Enables the Counter Overflow Interrupt |
TC_IER_LOVRS | Enables the Load Overrun Interrupt |
TC_IER_CPAS | Enables the RA Compare Interrupt |
TC_IER_CPBS | Enables the RB Compare Interrupt |
TC_IER_CPCS | Enables the RC Compare Interrupt |
TC_IER_LDRAS | Enables the RA Load Interrupt |
TC_IER_LDRBS | Enables the RB Load Interrupt |
TC_IER_ETRGS | Enables the External Trigger Interrupt |
References Assert.
Referenced by _configure_TC_uart().
void tc_enable_qdec_interrupt | ( | Tc * | p_tc, |
uint32_t | ul_sources | ||
) |
Enable TC QDEC interrupts.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_sources | A bitmask of QDEC interrupts to be enabled |
Where the input parameter ul_sources can be one or more of the following:
Parameter Value | Description |
---|---|
TC_QIER_IDX | Enable the rising edge detected on IDX input interrupt |
TC_QIER_DIRCHG | Enable the change in rotation direction detected interrupt |
TC_QIER_QERR | Enable the quadrature error detected on PHA/PHB interrupt |
References Assert.
uint32_t tc_find_mck_divisor | ( | uint32_t | ul_freq, |
uint32_t | ul_mck, | ||
uint32_t * | p_uldiv, | ||
uint32_t * | p_ultcclks, | ||
uint32_t | ul_boardmck | ||
) |
Find the best MCK divisor.
Find the best PBA/MCK divisor.
Finds the best MCK divisor given the timer frequency and MCK. The result is guaranteed to satisfy the following equation:
With DIV being the lowest possible value, to maximize timing adjust resolution.
[in] | ul_freq | Desired timer frequency |
[in] | ul_mck | Master clock frequency |
[out] | p_uldiv | Divisor value |
[out] | p_ultcclks | TCCLKS field value for divisor |
[in] | ul_boardmck | Board clock frequency |
0 | No suitable divisor was found |
1 | A divisor was found |
For SAM4L devices: Finds the best PBA divisor given the timer frequency and PBA clock. The result is guaranteed to satisfy the following equation:
with DIV being the lowest possible value, to maximize timing adjust resolution.
For non SAM4L devices: Finds the best MCK divisor given the timer frequency and MCK. The result is guaranteed to satisfy the following equation:
with DIV being the lowest possible value, to maximize timing adjust resolution.
[in] | ul_freq | Desired timer frequency |
[in] | ul_mck | PBA clock frequency |
[out] | p_uldiv | Divisor value |
[out] | p_ultcclks | TCCLKS field value for divisor |
[in] | ul_boardmck | Board clock frequency (set to 0 for SAM4L devices) |
0 | No suitable divisor was found |
1 | A divisor was found |
References FREQ_SLOW_CLOCK_EXT, and TC_DIV_FACTOR.
Referenced by _configure_TC_uart().
uint32_t tc_get_feature | ( | Tc * | p_tc | ) |
Indicate TC features.
[in] | p_tc | Module hardware register base address pointer |
References Assert.
uint32_t tc_get_interrupt_mask | ( | Tc * | p_tc, |
uint32_t | ul_channel | ||
) |
Read the TC interrupt mask for the specified channel.
[in] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to read |
References Assert.
uint32_t tc_get_qdec_interrupt_mask | ( | Tc * | p_tc | ) |
Read TC QDEC interrupt mask.
[in] | p_tc | Module hardware register base address pointer |
References Assert.
uint32_t tc_get_qdec_interrupt_status | ( | Tc * | p_tc | ) |
Get current TC QDEC interrupt status.
[in] | p_tc | Module hardware register base address pointer |
References Assert.
uint32_t tc_get_status | ( | Tc * | p_tc, |
uint32_t | ul_channel | ||
) |
Get the current status for the specified TC channel.
[in] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel number |
References Assert.
Referenced by TC_UART_Handler().
uint32_t tc_get_version | ( | Tc * | p_tc | ) |
Indicate TC version.
[in] | p_tc | Module hardware register base address pointer |
References Assert.
void tc_init | ( | Tc * | p_tc, |
uint32_t | ul_channel, | ||
uint32_t | ul_mode | ||
) |
Configure TC for timer, waveform generation, or capture.
[in,out] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to configure |
[in] | ul_mode | Control mode register bitmask value to set |
References Assert.
Referenced by _configure_TC_uart().
uint32_t tc_init_2bit_gray | ( | Tc * | p_tc, |
uint32_t | ul_channel, | ||
uint32_t | ul_steppermode | ||
) |
Configure TC for 2-bit Gray Counter for Stepper Motor.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to configure |
[in] | ul_steppermode | Stepper motor mode register value to set |
References Assert.
uint32_t tc_read_cv | ( | Tc * | p_tc, |
uint32_t | ul_channel | ||
) |
Read the counter value on the specified channel.
[in] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to read |
References Assert.
uint32_t tc_read_ra | ( | Tc * | p_tc, |
uint32_t | ul_channel | ||
) |
Read TC Register A (RA) on the specified channel.
[in] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to read |
References Assert.
uint32_t tc_read_rb | ( | Tc * | p_tc, |
uint32_t | ul_channel | ||
) |
Read TC Register B (RB) on the specified channel.
[in] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to read |
References Assert.
uint32_t tc_read_rc | ( | Tc * | p_tc, |
uint32_t | ul_channel | ||
) |
Read TC Register C (RC) on the specified channel.
[in] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to read |
References Assert.
void tc_set_block_mode | ( | Tc * | p_tc, |
uint32_t | ul_blockmode | ||
) |
Configure the TC Block mode.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_blockmode | Block mode register value to set |
References Assert.
void tc_set_writeprotect | ( | Tc * | p_tc, |
uint32_t | ul_enable | ||
) |
Enable or disable write protection of TC registers.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_enable | 1 to enable, 0 to disable |
References Assert, and TC_WPMR_WPKEY_PASSWD.
void tc_start | ( | Tc * | p_tc, |
uint32_t | ul_channel | ||
) |
Start the TC clock on the specified channel.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to configure |
References Assert.
Referenced by buart_if_open(), busart_if_open(), and UART0_Handler().
void tc_stop | ( | Tc * | p_tc, |
uint32_t | ul_channel | ||
) |
Stop the TC clock on the specified channel.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to configure |
References Assert.
Referenced by buart_if_close(), busart_if_close(), and TC_UART_Handler().
void tc_sync_trigger | ( | Tc * | p_tc | ) |
Asserts a SYNC signal to generate a software trigger on all channels.
[out] | p_tc | Module hardware register base address pointer |
References Assert.
void tc_write_ra | ( | Tc * | p_tc, |
uint32_t | ul_channel, | ||
uint32_t | ul_value | ||
) |
Write to TC Register A (RA) on the specified channel.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to write |
[in] | ul_value | Value to write |
References Assert.
void tc_write_rb | ( | Tc * | p_tc, |
uint32_t | ul_channel, | ||
uint32_t | ul_value | ||
) |
Write to TC Register B (RB) on the specified channel.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to write |
[in] | ul_value | Value to write |
References Assert.
void tc_write_rc | ( | Tc * | p_tc, |
uint32_t | ul_channel, | ||
uint32_t | ul_value | ||
) |
Write to TC Register C (RC) on the selected channel.
[out] | p_tc | Module hardware register base address pointer |
[in] | ul_channel | Channel to write |
[in] | ul_value | Value to write |
References Assert.
Referenced by _configure_TC_uart().