Data Structures | |
struct | i2c_slave_config |
Configuration structure for the I2C slave device. More... | |
struct | i2c_slave_module |
SERCOM I2C slave driver software device instance structure. More... | |
struct | i2c_slave_packet |
I2C slave packet for read/write. More... | |
Enumerations | |
enum | i2c_slave_address_mode { I2C_SLAVE_ADDRESS_MODE_MASK = SERCOM_I2CS_CTRLB_AMODE(0), I2C_SLAVE_ADDRESS_MODE_TWO_ADDRESSES = SERCOM_I2CS_CTRLB_AMODE(1), I2C_SLAVE_ADDRESS_MODE_RANGE = SERCOM_I2CS_CTRLB_AMODE(2) } |
Enum for the possible address modes. More... | |
enum | i2c_slave_direction { I2C_SLAVE_DIRECTION_READ, I2C_SLAVE_DIRECTION_WRITE, I2C_SLAVE_DIRECTION_NONE } |
Enum for the direction of a request. More... | |
enum | i2c_slave_sda_hold_time { I2C_SLAVE_SDA_HOLD_TIME_DISABLED, I2C_SLAVE_SDA_HOLD_TIME_50NS_100NS, I2C_SLAVE_SDA_HOLD_TIME_300NS_600NS, I2C_SLAVE_SDA_HOLD_TIME_400NS_800NS } |
Enum for the possible SDA hold times with respect to the negative edge of SCL. More... | |
I2C Slave Status Flags | |
I2C slave status flags, returned by i2c_slave_get_status() and cleared by i2c_slave_clear_status(). | |
#define | I2C_SLAVE_STATUS_ADDRESS_MATCH (1UL << 0) |
Address Match. More... | |
#define | I2C_SLAVE_STATUS_DATA_READY (1UL << 1) |
Data Ready. More... | |
#define | I2C_SLAVE_STATUS_STOP_RECEIVED (1UL << 2) |
Stop Received. More... | |
#define | I2C_SLAVE_STATUS_CLOCK_HOLD (1UL << 3) |
Clock Hold. More... | |
#define | I2C_SLAVE_STATUS_SCL_LOW_TIMEOUT (1UL << 4) |
SCL Low Timeout. More... | |
#define | I2C_SLAVE_STATUS_REPEATED_START (1UL << 5) |
Repeated Start. More... | |
#define | I2C_SLAVE_STATUS_RECEIVED_NACK (1UL << 6) |
Received not acknowledge. More... | |
#define | I2C_SLAVE_STATUS_COLLISION (1UL << 7) |
Transmit Collision. More... | |
#define | I2C_SLAVE_STATUS_BUS_ERROR (1UL << 8) |
Bus error. More... | |
Lock/Unlock | |
static enum status_code | i2c_slave_lock (struct i2c_slave_module *const module) |
Attempt to get lock on driver instance. More... | |
static void | i2c_slave_unlock (struct i2c_slave_module *const module) |
Unlock driver instance. More... | |
Configuration and Initialization | |
static bool | i2c_slave_is_syncing (const struct i2c_slave_module *const module) |
Returns the synchronization status of the module. More... | |
static void | i2c_slave_get_config_defaults (struct i2c_slave_config *const config) |
Gets the I2C slave default configurations. More... | |
enum status_code | i2c_slave_init (struct i2c_slave_module *const module, Sercom *const hw, const struct i2c_slave_config *const config) |
Initializes the requested I2C hardware module. More... | |
static void | i2c_slave_enable (const struct i2c_slave_module *const module) |
Enables the I2C module. More... | |
static void | i2c_slave_disable (const struct i2c_slave_module *const module) |
Disables the I2C module. More... | |
void | i2c_slave_reset (struct i2c_slave_module *const module) |
Resets the hardware module. More... | |
Read and Write | |
enum status_code | i2c_slave_write_packet_wait (struct i2c_slave_module *const module, struct i2c_slave_packet *const packet) |
Writes a packet to the master. More... | |
enum status_code | i2c_slave_read_packet_wait (struct i2c_slave_module *const module, struct i2c_slave_packet *const packet) |
Reads a packet from the master. More... | |
enum i2c_slave_direction | i2c_slave_get_direction_wait (struct i2c_slave_module *const module) |
Waits for a start condition on the bus. More... | |
Status Management | |
uint32_t | i2c_slave_get_status (struct i2c_slave_module *const module) |
Retrieves the current module status. More... | |
void | i2c_slave_clear_status (struct i2c_slave_module *const module, uint32_t status_flags) |
Clears a module status flag. More... | |
#define I2C_SLAVE_STATUS_ADDRESS_MATCH (1UL << 0) |
Address Match.
Referenced by i2c_slave_clear_status(), and i2c_slave_get_status().
#define I2C_SLAVE_STATUS_BUS_ERROR (1UL << 8) |
Bus error.
Referenced by i2c_slave_clear_status(), and i2c_slave_get_status().
#define I2C_SLAVE_STATUS_CLOCK_HOLD (1UL << 3) |
Clock Hold.
Referenced by i2c_slave_get_status().
#define I2C_SLAVE_STATUS_COLLISION (1UL << 7) |
Transmit Collision.
Referenced by i2c_slave_clear_status(), and i2c_slave_get_status().
#define I2C_SLAVE_STATUS_DATA_READY (1UL << 1) |
Data Ready.
Referenced by i2c_slave_clear_status(), and i2c_slave_get_status().
#define I2C_SLAVE_STATUS_RECEIVED_NACK (1UL << 6) |
#define I2C_SLAVE_STATUS_REPEATED_START (1UL << 5) |
Repeated Start.
Referenced by i2c_slave_get_status().
#define I2C_SLAVE_STATUS_SCL_LOW_TIMEOUT (1UL << 4) |
SCL Low Timeout.
Referenced by i2c_slave_clear_status(), and i2c_slave_get_status().
#define I2C_SLAVE_STATUS_STOP_RECEIVED (1UL << 2) |
Stop Received.
Referenced by i2c_slave_clear_status(), and i2c_slave_get_status().
Enum for the possible address modes.
Enum for the possible address modes.
enum i2c_slave_direction |
Enum for the possible SDA hold times with respect to the negative edge of SCL.
Enum for the possible SDA hold times with respect to the negative edge of SCL.
void i2c_slave_clear_status | ( | struct i2c_slave_module *const | module, |
uint32_t | status_flags | ||
) |
Clears a module status flag.
Clears the given status flag of the module.
[in] | module | Pointer to the I2C software device struct |
[in] | status_flags | Bit mask of status flags to clear |
References Assert, I2C_SLAVE_STATUS_ADDRESS_MATCH, I2C_SLAVE_STATUS_BUS_ERROR, I2C_SLAVE_STATUS_COLLISION, I2C_SLAVE_STATUS_DATA_READY, I2C_SLAVE_STATUS_SCL_LOW_TIMEOUT, and I2C_SLAVE_STATUS_STOP_RECEIVED.
|
inlinestatic |
Disables the I2C module.
This will disable the I2C module specified in the provided software module structure.
[in] | module | Pointer to the software module struct |
References Assert, and system_interrupt_disable().
Referenced by i2c_slave_reset().
|
inlinestatic |
Enables the I2C module.
This will enable the requested I2C module.
[in] | module | Pointer to the software module struct |
References Assert, and system_interrupt_enable().
Referenced by configure_i2c().
|
inlinestatic |
Gets the I2C slave default configurations.
This will initialize the configuration structure to known default values.
The default configuration is as follows:
Those default configuration only available if the device supports it:
[out] | config | Pointer to configuration structure to be initialized |
References i2c_slave_config::address, i2c_slave_config::address_mask, i2c_slave_config::address_mode, Assert, i2c_slave_config::buffer_timeout, i2c_slave_config::enable_general_call_address, i2c_slave_config::enable_scl_low_timeout, GCLK_GENERATOR_0, i2c_slave_config::generator_source, I2C_SLAVE_ADDRESS_MODE_MASK, I2C_SLAVE_SDA_HOLD_TIME_300NS_600NS, PINMUX_DEFAULT, i2c_slave_config::pinmux_pad0, i2c_slave_config::pinmux_pad1, i2c_slave_config::run_in_standby, i2c_slave_config::scl_low_timeout, and i2c_slave_config::sda_hold_time.
Referenced by configure_i2c().
enum i2c_slave_direction i2c_slave_get_direction_wait | ( | struct i2c_slave_module *const | module | ) |
Waits for a start condition on the bus.
Waits for the master to issue a start condition on the bus.
[in] | module | Pointer to software module structure |
I2C_SLAVE_DIRECTION_NONE | No request from master within timeout period |
I2C_SLAVE_DIRECTION_READ | Write request from master |
I2C_SLAVE_DIRECTION_WRITE | Read request from master |
References _i2c_slave_wait_for_bus(), Assert, I2C_SLAVE_DIRECTION_NONE, I2C_SLAVE_DIRECTION_READ, I2C_SLAVE_DIRECTION_WRITE, and STATUS_OK.
uint32_t i2c_slave_get_status | ( | struct i2c_slave_module *const | module | ) |
Retrieves the current module status.
Checks the status of the module and returns it as a bitmask of status flags.
[in] | module | Pointer to the I2C slave software device struct |
I2C_SLAVE_STATUS_ADDRESS_MATCH | A valid address has been received |
I2C_SLAVE_STATUS_DATA_READY | A I2C slave byte transmission is successfully completed |
I2C_SLAVE_STATUS_STOP_RECEIVED | A stop condition is detected for a transaction being processed |
I2C_SLAVE_STATUS_CLOCK_HOLD | The slave is holding the SCL line low |
I2C_SLAVE_STATUS_SCL_LOW_TIMEOUT | An SCL low time-out has occurred |
I2C_SLAVE_STATUS_REPEATED_START | Indicates a repeated start, only valid if I2C_SLAVE_STATUS_ADDRESS_MATCH is set |
I2C_SLAVE_STATUS_RECEIVED_NACK | The last data packet sent was not acknowledged |
I2C_SLAVE_STATUS_COLLISION | The I2C slave was not able to transmit a high data or NACK bit |
I2C_SLAVE_STATUS_BUS_ERROR | An illegal bus condition has occurred on the bus |
References Assert, I2C_SLAVE_STATUS_ADDRESS_MATCH, I2C_SLAVE_STATUS_BUS_ERROR, I2C_SLAVE_STATUS_CLOCK_HOLD, I2C_SLAVE_STATUS_COLLISION, I2C_SLAVE_STATUS_DATA_READY, I2C_SLAVE_STATUS_RECEIVED_NACK, I2C_SLAVE_STATUS_REPEATED_START, I2C_SLAVE_STATUS_SCL_LOW_TIMEOUT, and I2C_SLAVE_STATUS_STOP_RECEIVED.
enum status_code i2c_slave_init | ( | struct i2c_slave_module *const | module, |
Sercom *const | hw, | ||
const struct i2c_slave_config *const | config | ||
) |
Initializes the requested I2C hardware module.
Initializes the SERCOM I2C slave device requested and sets the provided software module struct. Run this function before any further use of the driver.
[out] | module | Pointer to software module struct |
[in] | hw | Pointer to the hardware instance |
[in] | config | Pointer to the configuration struct |
STATUS_OK | Module initiated correctly |
STATUS_ERR_DENIED | If module is enabled |
STATUS_BUSY | If module is busy resetting |
STATUS_ERR_ALREADY_INITIALIZED | If setting other GCLK generator than previously set |
References _i2c_slave_set_config(), _sercom_get_sercom_inst_index(), Assert, i2c_slave_config::generator_source, sercom_set_gclk_generator(), system_gclk_chan_config::source_generator, STATUS_BUSY, STATUS_ERR_DENIED, system_apb_clock_set_mask(), SYSTEM_CLOCK_APB_APBC, system_gclk_chan_enable(), system_gclk_chan_get_config_defaults(), and system_gclk_chan_set_config().
Referenced by configure_i2c().
|
inlinestatic |
Returns the synchronization status of the module.
Returns the synchronization status of the module.
[out] | module | Pointer to software module structure |
true | Module is busy synchronizing |
false | Module is not synchronizing |
References Assert.
|
inlinestatic |
Attempt to get lock on driver instance.
This function checks the instance's lock, which indicates whether or not it is currently in use, and sets the lock if it was not already set.
The purpose of this is to enable exclusive access to driver instances, so that, e.g., transactions by different services will not interfere with each other.
[in,out] | module | Pointer to the driver instance to lock |
STATUS_OK | If the module was locked |
STATUS_BUSY | If the module was already locked |
References STATUS_BUSY, STATUS_OK, system_interrupt_enter_critical_section(), and system_interrupt_leave_critical_section().
enum status_code i2c_slave_read_packet_wait | ( | struct i2c_slave_module *const | module, |
struct i2c_slave_packet *const | packet | ||
) |
Reads a packet from the master.
Reads a packet from the master. This will wait for the master to issue a request.
[in] | module | Pointer to software module structure |
[out] | packet | Packet to read from master |
STATUS_OK | Packet was read successfully |
STATUS_ABORTED | Master sent stop condition or repeated start before specified length of bytes was received |
STATUS_ERR_IO | There was an error in the previous transfer |
STATUS_ERR_DENIED | Start condition not received, another interrupt flag is set |
STATUS_ERR_INVALID_ARG | Invalid argument(s) was provided |
STATUS_ERR_BUSY | The I2C module is busy with a job |
STATUS_ERR_BAD_FORMAT | Master wants to read data |
STATUS_ERR_ERR_OVERFLOW | Last byte received overflows buffer |
References _i2c_slave_wait_for_bus(), Assert, i2c_slave_packet::data, i2c_slave_packet::data_length, STATUS_ABORTED, STATUS_BUSY, STATUS_ERR_BAD_FORMAT, STATUS_ERR_DENIED, STATUS_ERR_INVALID_ARG, STATUS_ERR_IO, and STATUS_OK.
Referenced by fetch_data(), and get_length().
void i2c_slave_reset | ( | struct i2c_slave_module *const | module | ) |
Resets the hardware module.
This will reset the module to hardware defaults.
[in,out] | module | Pointer to software module structure |
References Assert, i2c_slave_disable(), system_interrupt_clear_pending(), system_interrupt_enter_critical_section(), and system_interrupt_leave_critical_section().
|
inlinestatic |
Unlock driver instance.
This function clears the instance lock, indicating that it is available for use.
[in,out] | module | Pointer to the driver instance to lock |
STATUS_OK | If the module was locked |
STATUS_BUSY | If the module was already locked |
enum status_code i2c_slave_write_packet_wait | ( | struct i2c_slave_module *const | module, |
struct i2c_slave_packet *const | packet | ||
) |
Writes a packet to the master.
Writes a packet to the master. This will wait for the master to issue a request.
[in] | module | Pointer to software module structure |
[in] | packet | Packet to write to master |
STATUS_OK | Packet was written successfully |
STATUS_ERR_DENIED | Start condition not received, another interrupt flag is set |
STATUS_ERR_IO | There was an error in the previous transfer |
STATUS_ERR_BAD_FORMAT | Master wants to write data |
STATUS_ERR_INVALID_ARG | Invalid argument(s) was provided |
STATUS_ERR_BUSY | The I2C module is busy with a job |
STATUS_ERR_ERR_OVERFLOW | Master NACKed before entire packet was transferred |
STATUS_ERR_TIMEOUT | No response was given within the timeout period |
References _i2c_slave_wait_for_bus(), Assert, i2c_slave_packet::data, i2c_slave_packet::data_length, STATUS_BUSY, STATUS_ERR_BAD_FORMAT, STATUS_ERR_DENIED, STATUS_ERR_INVALID_ARG, STATUS_ERR_IO, STATUS_ERR_OVERFLOW, STATUS_ERR_TIMEOUT, and STATUS_OK.
Referenced by send_ack().