SAM RTC Driver (Count Mode)
Copyright (c) 2012-2020 Microchip Technology Inc. and its subsidiaries.
Functions | |
static enum status_code | _rtc_count_set_config (struct rtc_module *const module, const struct rtc_count_config *const config) |
enum status_code | rtc_count_clear_compare_match (struct rtc_module *const module, const enum rtc_count_compare comp_index) |
Clears RTC compare match flag. More... | |
void | rtc_count_disable (struct rtc_module *const module) |
Disables the RTC module. More... | |
void | rtc_count_enable (struct rtc_module *const module) |
Enables the RTC module. More... | |
enum status_code | rtc_count_frequency_correction (struct rtc_module *const module, const int8_t value) |
Calibrate for too-slow or too-fast oscillator. More... | |
enum status_code | rtc_count_get_compare (struct rtc_module *const module, uint32_t *const comp_value, const enum rtc_count_compare comp_index) |
Get the current compare value of specified compare. More... | |
uint32_t | rtc_count_get_count (struct rtc_module *const module) |
Get the current count value. More... | |
enum status_code | rtc_count_get_period (struct rtc_module *const module, uint16_t *const period_value) |
Retrieves the value of period. More... | |
enum status_code | rtc_count_init (struct rtc_module *const module, Rtc *const hw, const struct rtc_count_config *const config) |
Initializes the RTC module with given configurations. More... | |
bool | rtc_count_is_compare_match (struct rtc_module *const module, const enum rtc_count_compare comp_index) |
Check if RTC compare match has occurred. More... | |
static bool | rtc_count_is_syncing (struct rtc_module *const module) |
Determines if the hardware module(s) are currently synchronizing to the bus. More... | |
void | rtc_count_reset (struct rtc_module *const module) |
Resets the RTC module. More... | |
enum status_code | rtc_count_set_compare (struct rtc_module *const module, const uint32_t comp_value, const enum rtc_count_compare comp_index) |
Set the compare value for the specified compare. More... | |
enum status_code | rtc_count_set_count (struct rtc_module *const module, const uint32_t count_value) |
Set the current count value to desired value. More... | |
enum status_code | rtc_count_set_period (struct rtc_module *const module, const uint16_t period_value) |
Set the given value to the period. More... | |
|
static |
Applies the given configuration.
Sets the configurations given from the configuration structure to the hardware module
[in,out] | module | Pointer to the software instance struct |
[in] | config | Pointer to the configuration structure |
STATUS_OK | RTC configurations was set successfully |
STATUS_ERR_INVALID_ARG | If invalid argument(s) were given |
References Assert, rtc_count_config::clear_on_match, rtc_count_config::compare_values, rtc_count_config::enable_read_sync, rtc_count_config::mode, rtc_count_config::prescaler, RTC_COUNT_MODE_16BIT, RTC_COUNT_MODE_32BIT, rtc_count_set_compare(), SAMC20, SAMC21, SAML22, STATUS_ERR_INVALID_ARG, and STATUS_OK.
Referenced by rtc_count_init().
|
static |
Determines if the hardware module(s) are currently synchronizing to the bus.
Checks to see if the underlying hardware peripheral module(s) are currently synchronizing across multiple clock domains to the hardware bus, This function can be used to delay further operations on a module until such time that it is ready, to prevent blocking delays for synchronization in the user application.
[in] | module | RTC hardware module |
true | if the module synchronization is ongoing |
false | if the module has completed synchronization |
References Assert.
Referenced by rtc_count_disable(), rtc_count_enable(), rtc_count_frequency_correction(), rtc_count_get_compare(), rtc_count_get_count(), rtc_count_get_period(), rtc_count_reset(), rtc_count_set_compare(), rtc_count_set_count(), and rtc_count_set_period().