ADC configuration structure.
Configuration structure for an ADC instance. This structure should be initialized by the adc_get_config_defaults() function before being modified by the user application.
#include <adc_feature.h>
Data Fields | |
enum adc_accumulate_samples | accumulate_samples |
Number of ADC samples to accumulate when using the ADC_RESOLUTION_CUSTOM mode. More... | |
enum adc_clock_prescaler | clock_prescaler |
Clock prescaler. More... | |
enum gclk_generator | clock_source |
GCLK generator used to clock the peripheral. More... | |
struct adc_correction_config | correction |
Gain and offset correction configuration structure. More... | |
bool | differential_mode |
Enables differential mode if true. More... | |
enum adc_divide_result | divide_result |
Division ration when using the ADC_RESOLUTION_CUSTOM mode. More... | |
enum adc_event_action | event_action |
Event action to take on incoming event. More... | |
bool | freerunning |
Enables free running mode if true. More... | |
bool | left_adjust |
Left adjusted result. More... | |
enum adc_negative_input | negative_input |
Negative MUX input. More... | |
bool | on_demand |
ADC On demand control. More... | |
enum adc_positive_input | positive_input |
Positive MUX input. More... | |
uint32_t | positive_input_sequence_mask_enable |
Positive input enabled mask for conversion sequence. More... | |
enum adc_reference | reference |
Voltage reference. More... | |
bool | reference_compensation_enable |
Enables reference buffer offset compensation if true. More... | |
enum adc_resolution | resolution |
Result resolution. More... | |
bool | run_in_standby |
ADC run in standby control. More... | |
uint8_t | sample_length |
This value (0-63) control the ADC sampling time in number of half ADC prescaled clock cycles (depends of ADC_PRESCALER value), thus controlling the ADC input impedance. More... | |
bool | sampling_time_compensation_enable |
Enables sampling period offset compensation if true. More... | |
struct adc_window_config | window |
Window monitor configuration structure. More... | |
enum adc_accumulate_samples adc_config::accumulate_samples |
Number of ADC samples to accumulate when using the ADC_RESOLUTION_CUSTOM
mode.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_setup().
enum adc_clock_prescaler adc_config::clock_prescaler |
Clock prescaler.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_setup().
enum gclk_generator adc_config::clock_source |
GCLK generator used to clock the peripheral.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_setup().
struct adc_correction_config adc_config::correction |
Gain and offset correction configuration structure.
Referenced by _adc_set_config(), and adc_get_config_defaults().
bool adc_config::differential_mode |
Enables differential mode if true.
Referenced by _adc_set_config(), and adc_get_config_defaults().
enum adc_divide_result adc_config::divide_result |
Division ration when using the ADC_RESOLUTION_CUSTOM mode.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_setup().
enum adc_event_action adc_config::event_action |
Event action to take on incoming event.
Referenced by _adc_set_config(), adc_get_config_defaults(), adc_init(), and adc_setup().
bool adc_config::freerunning |
Enables free running mode if true.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_init().
bool adc_config::left_adjust |
Left adjusted result.
Referenced by _adc_set_config(), and adc_get_config_defaults().
enum adc_negative_input adc_config::negative_input |
Negative MUX input.
Referenced by _adc_set_config(), and adc_get_config_defaults().
bool adc_config::on_demand |
ADC On demand control.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_setup().
enum adc_positive_input adc_config::positive_input |
Positive MUX input.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_setup().
uint32_t adc_config::positive_input_sequence_mask_enable |
Positive input enabled mask for conversion sequence.
The sequence start from the lowest input, and go to the next enabled input automatically when the conversion is done. If no bits are set the sequence is disabled.
Referenced by _adc_set_config(), and adc_get_config_defaults().
enum adc_reference adc_config::reference |
Voltage reference.
Referenced by _adc_set_config(), adc_get_config_defaults(), adc_init(), and adc_setup().
bool adc_config::reference_compensation_enable |
Enables reference buffer offset compensation if true.
This will increase the accuracy of the gain stage, but decreases the input impedance; therefore the startup time of the reference must be increased.
Referenced by _adc_set_config(), and adc_get_config_defaults().
enum adc_resolution adc_config::resolution |
Result resolution.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_setup().
bool adc_config::run_in_standby |
ADC run in standby control.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_setup().
uint8_t adc_config::sample_length |
This value (0-63) control the ADC sampling time in number of half ADC prescaled clock cycles (depends of ADC_PRESCALER
value), thus controlling the ADC input impedance.
Sampling time is set according to the formula: Sample time = (sample_length+1) * (ADCclk / 2).
Referenced by _adc_set_config(), and adc_get_config_defaults().
bool adc_config::sampling_time_compensation_enable |
Enables sampling period offset compensation if true.
Referenced by _adc_set_config(), and adc_get_config_defaults().
struct adc_window_config adc_config::window |
Window monitor configuration structure.
Referenced by _adc_set_config(), adc_get_config_defaults(), and adc_setup().