SAM RTC Driver (Calendar Mode)
Copyright (c) 2012-2020 Microchip Technology Inc. and its subsidiaries.
Functions | |
static void | _rtc_calendar_set_config (struct rtc_module *const module, const struct rtc_calendar_config *const config) |
void | rtc_calendar_disable (struct rtc_module *const module) |
Disables the RTC module. More... | |
void | rtc_calendar_enable (struct rtc_module *const module) |
Enables the RTC module. More... | |
enum status_code | rtc_calendar_frequency_correction (struct rtc_module *const module, const int8_t value) |
Calibrate for too-slow or too-fast oscillator. More... | |
enum status_code | rtc_calendar_get_alarm (struct rtc_module *const module, struct rtc_calendar_alarm_time *const alarm, const enum rtc_calendar_alarm alarm_index) |
Get the current alarm time of specified alarm. More... | |
void | rtc_calendar_get_time (struct rtc_module *const module, struct rtc_calendar_time *const time) |
Get the current calendar value. More... | |
void | rtc_calendar_init (struct rtc_module *const module, Rtc *const hw, const struct rtc_calendar_config *const config) |
Initializes the RTC module with given configurations. More... | |
static bool | rtc_calendar_is_syncing (struct rtc_module *const module) |
Determines if the hardware module(s) are currently synchronizing to the bus. More... | |
void | rtc_calendar_register_value_to_time (struct rtc_module *const module, const uint32_t register_value, struct rtc_calendar_time *const time) |
Convert register_value to time structure. More... | |
void | rtc_calendar_reset (struct rtc_module *const module) |
Resets the RTC module. More... | |
enum status_code | rtc_calendar_set_alarm (struct rtc_module *const module, const struct rtc_calendar_alarm_time *const alarm, const enum rtc_calendar_alarm alarm_index) |
Set the alarm time for the specified alarm. More... | |
void | rtc_calendar_set_time (struct rtc_module *const module, const struct rtc_calendar_time *const time) |
Set the current calendar time to desired time. More... | |
void | rtc_calendar_swap_time_mode (struct rtc_module *const module) |
Swaps between 12h and 24h clock mode. More... | |
uint32_t | rtc_calendar_time_to_register_value (struct rtc_module *const module, const struct rtc_calendar_time *const time) |
Convert time structure to register_value. More... | |
|
static |
Applies the given configuration.
Set the configurations given from the configuration structure to the hardware module.
[in,out] | module | Pointer to the software instance struct |
[in] | config | Pointer to the configuration structure |
References rtc_calendar_config::alarm, Assert, rtc_calendar_config::clear_on_match, rtc_calendar_config::clock_24h, rtc_calendar_config::enable_read_sync, rtc_calendar_config::prescaler, and rtc_calendar_set_alarm().
Referenced by rtc_calendar_init().
|
inlinestatic |
Determines if the hardware module(s) are currently synchronizing to the bus.
Checks to see if the underlying hardware peripheral module(s) are currently synchronizing across multiple clock domains to the hardware bus, This function can be used to delay further operations on a module until such time that it is ready, to prevent blocking delays for synchronization in the user application.
[in] | module | RTC hardware module |
true | if the module synchronization is ongoing |
false | if the module has completed synchronization |
References Assert.
Referenced by rtc_calendar_disable(), rtc_calendar_enable(), rtc_calendar_frequency_correction(), rtc_calendar_get_time(), rtc_calendar_reset(), rtc_calendar_set_alarm(), and rtc_calendar_set_time().