Macros | |
#define | PIN_ACK_OK_END() |
#define | PIN_ACK_OK_START() |
#define | PIN_ACK_WAITING_END() |
#define | PIN_ACK_WAITING_START() |
#define | PIN_BACKOFF_END() |
#define | PIN_BACKOFF_START() |
#define | PIN_BEACON_END() |
#define | PIN_BEACON_LOSS_TIMER_END() |
#define | PIN_BEACON_LOSS_TIMER_START() |
#define | PIN_BEACON_START() |
#define | PIN_CCA_END() |
#define | PIN_CCA_START() |
#define | PIN_CSMA_END() |
#define | PIN_CSMA_START() |
#define | PIN_NO_ACK_END() |
#define | PIN_NO_ACK_START() |
#define | PIN_TX_END() |
#define | PIN_TX_START() |
#define | PIN_WAITING_FOR_BEACON_END() |
#define | PIN_WAITING_FOR_BEACON_START() |
#define | TAL_PSDU_US_PER_OCTET(octets) |
Conversion of number of PSDU octets to duration in microseconds. More... | |
#define | TRX_IRQ_DEFAULT TRX_IRQ_3_TRX_END | TRX_IRQ_2_RX_START |
Typedefs | |
typedef enum tal_state_tag | tal_state_t |
TAL states. More... | |
Enumerations | |
enum | tal_state_tag { TAL_IDLE = 0, TAL_TX_AUTO = 1, TAL_TX_DONE = 2, TAL_SLOTTED_CSMA = 3, TAL_IDLE = 0, TAL_TX_AUTO = 1, TAL_TX_DONE = 2, TAL_SLOTTED_CSMA = 3, TAL_IDLE = 0, TAL_TX_AUTO = 1, TAL_TX_DONE = 2, TAL_SLOTTED_CSMA = 3, TAL_IDLE, TAL_SLEEP, TAL_RESET, TAL_WAKING_UP, TAL_TX, TAL_ED_SCAN, TAL_TFA_CW_RX, TAL_TFA_CW, TAL_TFA_CCA, TAL_IDLE = 0, TAL_TX_AUTO = 1, TAL_TX_DONE = 2, TAL_SLOTTED_CSMA = 3, TAL_IDLE = 0, TAL_TX_AUTO = 1, TAL_TX_DONE = 2, TAL_SLOTTED_CSMA = 3 } |
TAL states. More... | |
Functions | |
tal_trx_status_t | set_trx_state (trx_cmd_t trx_cmd) |
Sets transceiver state. More... | |
Variables | |
uint8_t | last_frame_length |
frame_info_t * | mac_frame_ptr |
Frame pointer for the frame structure provided by the MCL. More... | |
volatile bool | tal_awake_end_flag |
csma_state_t | tal_csma_state |
CSMA state machine variable. More... | |
uint8_t * | tal_frame_to_tx |
Pointer to the 15.4 frame created by the TAL to be handed over to the transceiver. More... | |
queue_t | tal_incoming_frame_queue |
Queue that contains all frames that are uploaded from the trx, but have not be processed by the MCL yet. More... | |
buffer_t * | tal_rx_buffer |
Pointer to receive buffer that can be used to upload a frame from the trx. More... | |
bool | tal_rx_on_required |
Indicates if the transceiver needs to switch on its receiver by tal_task(), because it could not be switched on due to buffer shortage. More... | |
uint32_t | tal_rx_timestamp |
Timestamp The timestamping is only required for beaconing networks or if timestamping is explicitly enabled. More... | |
tal_state_t | tal_state |
Current state of the TAL state machine. More... | |
tal_trx_status_t | tal_trx_status |
Current state of the transceiver. More... | |
#define PIN_ACK_OK_END | ( | ) |
#define PIN_ACK_OK_START | ( | ) |
#define PIN_ACK_WAITING_END | ( | ) |
#define PIN_ACK_WAITING_START | ( | ) |
#define PIN_BACKOFF_END | ( | ) |
#define PIN_BACKOFF_START | ( | ) |
#define PIN_BEACON_END | ( | ) |
#define PIN_BEACON_LOSS_TIMER_END | ( | ) |
#define PIN_BEACON_LOSS_TIMER_START | ( | ) |
#define PIN_BEACON_START | ( | ) |
#define PIN_CCA_END | ( | ) |
#define PIN_CCA_START | ( | ) |
#define PIN_CSMA_END | ( | ) |
#define PIN_CSMA_START | ( | ) |
#define PIN_NO_ACK_END | ( | ) |
#define PIN_NO_ACK_START | ( | ) |
#define PIN_TX_END | ( | ) |
#define PIN_TX_START | ( | ) |
#define PIN_WAITING_FOR_BEACON_END | ( | ) |
#define PIN_WAITING_FOR_BEACON_START | ( | ) |
#define TAL_PSDU_US_PER_OCTET | ( | octets | ) |
Conversion of number of PSDU octets to duration in microseconds.
#define TRX_IRQ_DEFAULT TRX_IRQ_3_TRX_END | TRX_IRQ_2_RX_START |
typedef enum tal_state_tag tal_state_t |
TAL states.
enum tal_state_tag |
TAL states.
uint8_t last_frame_length |
frame_info_t* mac_frame_ptr |
Frame pointer for the frame structure provided by the MCL.
volatile bool tal_awake_end_flag |
csma_state_t tal_csma_state |
CSMA state machine variable.
uint8_t* tal_frame_to_tx |
Pointer to the 15.4 frame created by the TAL to be handed over to the transceiver.
queue_t tal_incoming_frame_queue |
Queue that contains all frames that are uploaded from the trx, but have not be processed by the MCL yet.
buffer_t* tal_rx_buffer |
Pointer to receive buffer that can be used to upload a frame from the trx.
uint32_t tal_rx_timestamp |
Timestamp The timestamping is only required for beaconing networks or if timestamping is explicitly enabled.