FreeRTOS configuration.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
int | main (void) |
Main function. Execution starts here. More... | |
static void | main_memories_trans_task (void *pvParameters) |
void | main_msc_disable (void) |
Called by MSC interface Callback running when USB Host disable MSC interface. More... | |
bool | main_msc_enable (void) |
Called by MSC interface Callback running when USB Host enable MSC interface. More... | |
void | main_msc_notify_trans (void) |
Called when a data transfer on MSC must be executed Thus, the udi_msc_process_trans() function must be called. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | vApplicationIdleHook (void) |
Variables | |
static volatile bool | main_b_msc_enable = false |
static xSemaphoreHandle | main_trans_semphr = NULL |
Handle to the semaphore protecting memories transfer. More... | |
int main | ( | void | ) |
Main function. Execution starts here.
References Assert, board_init(), cpu_irq_enable, irq_initialize_vectors, main_memories_trans_task(), memories_initialization(), NULL, sleepmgr_init(), sysclk_init(), tskIDLE_PRIORITY, udc_start(), ui_init(), ui_powerdown(), vSemaphoreCreateBinary, vTaskStartScheduler(), and xTaskCreate.
|
static |
References pdTRUE, udi_msc_process_trans(), UNUSED, and xSemaphoreTake.
Referenced by main().
void main_msc_disable | ( | void | ) |
Called by MSC interface Callback running when USB Host disable MSC interface.
References main_b_msc_enable.
bool main_msc_enable | ( | void | ) |
Called by MSC interface Callback running when USB Host enable MSC interface.
true | if MSC startup is ok |
References main_b_msc_enable.
void main_msc_notify_trans | ( | void | ) |
Called when a data transfer on MSC must be executed Thus, the udi_msc_process_trans() function must be called.
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
References ui_wakeup().
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
References main_b_msc_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
Turn off all leds Callback running when USB Host set USB line in suspend state.
References ui_powerdown().
void vApplicationIdleHook | ( | void | ) |
Referenced by main_msc_disable(), main_msc_enable(), and main_sof_action().
|
static |
Handle to the semaphore protecting memories transfer.