User interface for mXT143E Xplained trackpad demo.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <asf.h>
Functions | |
static void | ui_flag_new_touch_event (void) |
Flag to UI that touch event is pending. More... | |
void | ui_init (void) |
Initialize the user interface. More... | |
void | ui_powerdown (void) |
Put the user interface in power down. More... | |
void | ui_process (uint16_t framenumber) |
Process the user interface. More... | |
void | ui_wakeup (void) |
Wake the user interface up. More... | |
void | ui_wakeup_disable (void) |
Disable asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enable asynchronous interrupts of the user interface. More... | |
Variables | |
bool | ui_new_touch_event |
Flag that a new touch event is pending. More... | |
struct mxt_touch_event | ui_touch_event |
Struct to hold touch events to process. More... | |
|
inlinestatic |
void ui_init | ( | void | ) |
Initialize the user interface.
Called at firmware startup.
Initializes the user interface.
void ui_powerdown | ( | void | ) |
Put the user interface in power down.
Called before enter in powerdown mode.
Enters the user interface in power down mode.
Sets the user interface in power down mode.
void ui_process | ( | uint16_t | framenumber | ) |
Process the user interface.
This process is called called each 1ms It is called only if MSC interface is enable.
This process is called each 1ms It is called only if the USB interface is enabled.
This function processes user touch events and updates the display.
The first registered touch is used to control the cursor. Its presence is indicated with a red frame around the display. When the cursor touch moves, its movement is visualized with a trace on the display.
The second registered touch is used to control mouse buttons, and is indicated with an inner frame of which the color depends on which side the touch is for: blue for left and green for right button click. The frame is shown until the touch is released. To detect which side click it is, the position relative to the cursor touch is used, i.e., a touch to the left of the first touch will cause a left mouse click.
framenumber | Current USB frame number |
void ui_wakeup | ( | void | ) |
Wake the user interface up.
Called when CPU exit of powerdown mode.
Exits the user interface of power down mode.
void ui_wakeup_disable | ( | void | ) |
Disable asynchronous interrupts of the user interface.
Disables the asynchronous interrupts of the user interface.
void ui_wakeup_enable | ( | void | ) |
Enable asynchronous interrupts of the user interface.
Enables the asynchronous interrupts of the user interface.
bool ui_new_touch_event |
Flag that a new touch event is pending.
Referenced by ui_flag_new_touch_event(), ui_init(), and ui_process().
struct mxt_touch_event ui_touch_event |
Struct to hold touch events to process.
Referenced by main(), and ui_process().