|
at_ble_status_t | at_ble_addr_get (at_ble_addr_t *address) |
| Get device BT Address. More...
|
|
at_ble_status_t | at_ble_addr_set (at_ble_addr_t *address) |
| Set device BT Address. More...
|
|
at_ble_status_t | at_ble_adv_data_set (uint8_t const *const adv_data, uint8_t adv_data_len, uint8_t const *const scan_resp_data, uint8_t scan_response_data_len) |
| Set, clear or update advertisement and scan response data. More...
|
|
at_ble_status_t | at_ble_adv_set_tx_power (int8_t power) |
| Set the Advertising transmission power. More...
|
|
at_ble_status_t | at_ble_adv_start (at_ble_adv_type_t type, at_ble_adv_mode_t mode, at_ble_addr_t *peer_addr, at_ble_filter_type_t filtered, uint16_t interval, uint16_t timeout, bool disable_randomness) |
| Start advertising (GAP Discoverable, Connectable modes, Broadcast Procedure). More...
|
|
at_ble_status_t | at_ble_adv_stop (void) |
| Stop advertising (GAP Discoverable, Connectable modes, Broadcast Procedure). More...
|
|
void | at_ble_conn_update_reply (at_ble_handle_t conn_handle, at_ble_connection_params_t *connection_params) |
| Reply to connection parameters update request AT_BLE_CONN_PARAM_UPDATE_REQUEST. More...
|
|
at_ble_status_t | at_ble_connect (at_ble_addr_t peers[], uint8_t peer_count, uint16_t scan_interval, uint16_t scan_window, at_ble_connection_params_t *connection_params) |
| Connect to a peer device. More...
|
|
at_ble_status_t | at_ble_connect_cancel (void) |
| Cancels an ongoing connection attempt. More...
|
|
at_ble_status_t | at_ble_connection_param_update (at_ble_handle_t handle, at_ble_connection_params_t *connection_params) |
| Update the connection parameters of an ongoing connection. More...
|
|
at_ble_status_t | at_ble_device_name_set (uint8_t *dev_name, uint8_t len) |
| Set device name. More...
|
|
at_ble_status_t | at_ble_disconnect (at_ble_handle_t handle, at_ble_disconnect_reason_t reason) |
| Disconnect a connected peer device and receive response through AT_BLE_DISCONNECTED event. More...
|
|
at_ble_status_t | at_ble_init (void *args) |
| Reset the link layer and the host. More...
|
|
int8_t | at_ble_max_PA_gain_get (at_ble_handle_t conn_handle) |
| Gets maximum allowed TX gain of a given connection. More...
|
|
at_ble_status_t | at_ble_random_address_resolve (uint8_t nb_key, at_ble_addr_t *rand_addr, uint8_t *irk_key) |
| Handles request of resolving a resolvable random address ,AT_BLE_RESOLV_RAND_ADDR_STATUS event is used to inform which key has been used to perform resolution for the returned address. More...
|
|
int8_t | at_ble_rx_power_get (at_ble_handle_t conn_handle) |
| Gets RX power of a given connection. More...
|
|
at_ble_status_t | at_ble_scan_start (uint16_t interval, uint16_t window, uint16_t timeout, at_ble_scan_type_t type, at_ble_scan_mode_t mode, bool filter_whitelist, bool filter_duplicates) |
| Start scan operation. More...
|
|
at_ble_status_t | at_ble_scan_stop (void) |
| Stops an ongoing scan operation. More...
|
|
at_ble_status_t | at_ble_sec_info_set (at_ble_handle_t handle, at_ble_signature_info_t signature_info, at_ble_auth_t auth, at_ble_author_t author) |
| Set specific link security configuration and bonding data. More...
|
|
at_ble_status_t | at_ble_set_dev_config (at_ble_gap_role role) |
| Set GAP attribute data base into BLE chip. More...
|
|
at_ble_status_t | at_ble_set_gap_deviceinfo (at_ble_gap_deviceinfo_t *gap_deviceinfo) |
| Set GAP attribute data base (Appearance , slave preferred connection parameters , device name write permissions) More...
|
|
at_ble_status_t | at_ble_set_privacy_key (at_ble_gap_irk_t *irk, uint16_t interval) |
| Set device Identity Resolving Key. More...
|
|
int8_t | at_ble_tx_power_get (at_ble_handle_t conn_handle) |
| Gets TX power of a given connection. More...
|
|
at_ble_status_t | at_ble_tx_power_set (at_ble_handle_t conn_handle, int8_t powerdBm) |
| Sets TX gain, relative to maximum gain, for a given connection. More...
|
|
at_ble_status_t | at_ble_whitelist_add (at_ble_addr_t *address) |
| Adds a peer device address to the white-list. More...
|
|
at_ble_status_t | at_ble_whitelist_clear (void) |
| Clear the white-list. More...
|
|
at_ble_status_t | at_ble_whitelist_remove (at_ble_addr_t *address) |
| Removes a peer device address from the white-list. More...
|
|
static uint8_t | gapm_get_adv_type (uint8_t type) |
|
static uint8_t | gapm_get_device_address_type (uint8_t local_addr_type, bool device_addr_auto_gen) |
|