Synchronous function which returns a BSD socket compliant Internet Protocol (IPv4) socket address.
This IPv4 address in the input string parameter could either be specified as a host name, or as a numeric string representation like n.n.n.n known as the IPv4 dotted-decimal format (i.e. "192.168.10.1"). This function is used whenever an ip address needs to be set in the proper format (i.e. for the tstrM2MIPConfig structure).
- Parameters
-
[in] | pcIpAddr | A null terminated string containing the IP address in IPv4 dotted-decimal address. |
- Returns
- Unsigned 32-bit integer representing the IP address in Network byte order (eg. "192.168.10.1" will be expressed as 0x010AA8C0).
Synchronous function which returns a BSD socket compliant Internet Protocol (IPv4) socket address.
This IPv4 address in the input string parameter could either be specified as a hostname, or as a numeric string
representation like n.n.n.n known as the IPv4 dotted-decimal format (i.e. "192.168.10.1").
This function is used whenever an ip address needs to be set in the proper format
(i.e. for the @ref tstrM2MIPConfig structure).
- Parameters
-
[in] | pcIpAddr | A null terminated string containing the IP address in IPv4 dotted-decimal address. |
- Returns
- Unsigned 32-bit integer representing the IP address in Network byte order (eg. "192.168.10.1" will be expressed as 0x010AA8C0).